Acquisition Start, Stop, and Abort#
Info
- These commands aren't available via the pylon Viewer feature tree. Instead,
AcquisitionStart
andAcquisitionStop
commands are generated automatically when you use the Single Shot, Continuous Shot, and Stop buttons in the toolbar of the pylon Viewer. - The pylon C++ API and the pylon .NET API provide camera classes that handle these commands automatically. Basler recommends using these classes.
For more information, see the Grab (C++) and Grab (.NET) code samples in the pylon API Documentation.
Using the Feature#
Starting Image Acquisition#
To switch on image acquisition, execute the AcquisitionStart
command.
After the command has been executed, the camera waits for trigger signals. Trigger signals can either be generated internally by the camera (free run) or applied externally (triggered image acquisition).
Info
To check whether the camera is currently waiting for a trigger signal, monitor the camera's Trigger Wait signals or use the Acquisition Status feature, if available.
Stopping Image Acquisition#
To switch off image acquisition, execute the AcquisitionStop
command.
After the command has been executed, the following occurs:
- If the camera is not currently acquiring a frame, image acquisition is switched off immediately.
- If the camera is currently reading out image data, the readout process will be allowed to finish. Afterwards, image acquisition is switched off.
- If the camera is currently exposing a frame:
- On some camera models, executing an
AcquisitionStop
command aborts exposure. In this case, the camera stops exposing immediately and starts reading out image data. The readout process will be allowed to finish. Afterwards, image acquisition is switched off. - On some camera models, you can configure whether executing an
AcquisitionStop
command aborts exposure or not. To do so, set theBslAcquisitionStopMode
parameter toAbortExposure
orCompleteExposure
.
- On some camera models, executing an
Aborting Image Acquisition#
To abort image acquisition, execute the AcquisitionAbort
command (if available).
After the command has been executed, the following occurs:
- If the camera is not currently acquiring a frame, image acquisition is switched off immediately.
- If the camera is currently exposing a frame, the camera stops exposing immediately. The readout process, if already started, is aborted. The current frame will be incomplete. Afterwards, image acquisition is switched off.
- If the camera is currently reading out image data, the camera stops the readout process immediately. The current frame will be incomplete. Afterwards, image acquisition is switched off.
Specifics#
Camera Model | AcquisitionAbort Command Available | AcquisitionStop Command Aborts Exposure |
---|---|---|
a2A640-240gmSWIR | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A640-240umSWIR | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1280-80gmSWIR | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1280-125umSWIR | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-51gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-51gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-51gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-51gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-160ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-160ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-160umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-160umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-165g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A1920-165g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2440-98g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2440-98g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-23gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-23gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-23gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-23gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-75ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-75ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-75umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-75umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-105g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-105g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-120cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-120cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-210cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2448-210cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-22gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-22gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-22gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-22gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-60ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-60ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-60umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2590-60umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-20gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-20gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-20gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-20gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-64ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-64ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-64umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2600-64umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-14gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-14gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-14gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-14gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-14gmUV | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-48ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-48ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-48umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-48umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-48umUV | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-67g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-67g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-67g5mUV | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-86cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A2840-86cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-13gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-13gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-13gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-13gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-45ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-45ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-45umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A3840-45umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-9gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-9gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-9gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-9gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-30ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-30ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-30umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-30umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-44g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-44g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-67cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4096-67cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-12gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-12gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-12gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-12gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-40ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-40ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-40umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4200-40umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-5gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-5gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-5gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-5gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-18ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-18ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-18umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-18umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-27g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-27g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-42cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4504-42cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-6gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-6gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-6gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-6gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-20ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-20ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-20umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A4508-20umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-7gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-7gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-7gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-7gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-23ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-23ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-23umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-23umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-34g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-34g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-52cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5320-52cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-4gcBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-4gcPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-4gmBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-4gmPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-15ucBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-15ucPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-15umBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-15umPRO | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-22g5cBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-22g5mBAS | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-35cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
a2A5328-35cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
acA640-121gm | No | Yes |
acA640-300gc | No | Yes |
acA640-300gm | No | Yes |
acA640-750uc | No | Yes |
acA640-750um | No | Yes |
acA720-290gc | No | Yes |
acA720-290gm | No | Yes |
acA720-520uc | No | Yes |
acA720-520um | No | Yes |
acA800-200gc | No | Yes |
acA800-200gm | No | Yes |
acA800-510uc | No | Yes |
acA800-510um | No | Yes |
acA1280-60gc | No | Yes |
acA1280-60gm | No | Yes |
acA1300-60gc | No | Yes |
acA1300-60gm | No | Yes |
acA1300-60gmNIR | No | Yes |
acA1300-75gc | No | Yes |
acA1300-75gm | No | Yes |
acA1300-200uc | No | Yes |
acA1300-200um | No | Yes |
acA1440-73gc | No | Yes |
acA1440-73gm | No | Yes |
acA1440-220uc | No | Yes |
acA1440-220um | No | Yes |
acA1600-20gc | No | Yes |
acA1600-20uc | No | Yes |
acA1600-60gc | No | Yes |
acA1600-60gm | No | Yes |
acA1920-25gc | No | Yes |
acA1920-25gm | No | Yes |
acA1920-25uc | No | Yes |
acA1920-25um | No | Yes |
acA1920-40gc | No | Yes |
acA1920-40gm | No | Yes |
acA1920-40uc | No | Yes |
acA1920-40ucMED | No | Yes |
acA1920-40um | No | Yes |
acA1920-40umMED | No | Yes |
acA1920-48gc | No | Yes |
acA1920-48gm | No | Yes |
acA1920-50gc | No | Yes |
acA1920-50gm | No | Yes |
acA1920-150uc | No | Yes |
acA1920-150um | No | Yes |
acA1920-155uc | No | Yes |
acA1920-155ucMED | No | Yes |
acA1920-155um | No | Yes |
acA1920-155umMED | No | Yes |
acA2000-50gc | No | Yes |
acA2000-50gm | No | Yes |
acA2000-165uc | No | Yes |
acA2000-165um | No | Yes |
acA2040-25gc | No | Yes |
acA2040-25gm | No | Yes |
acA2040-25gmNIR | No | Yes |
acA2040-35gc | No | Yes |
acA2040-35gm | No | Yes |
acA2040-55uc | No | Yes |
acA2040-55um | No | Yes |
acA2040-90uc | No | Yes |
acA2040-90um | No | Yes |
acA2040-90umNIR | No | Yes |
acA2040-120uc | No | Yes |
acA2040-120um | No | Yes |
acA2440-20gc | No | Yes |
acA2440-20gm | No | Yes |
acA2440-35uc | No | Yes |
acA2440-35ucMED | No | Yes |
acA2440-35um | No | Yes |
acA2440-35umMED | No | Yes |
acA2440-75uc | No | Yes |
acA2440-75ucMED | No | Yes |
acA2440-75um | No | Yes |
acA2440-75umMED | No | Yes |
acA2500-14gc | No | Yes |
acA2500-14gm | No | Yes |
acA2500-14uc | No | Yes |
acA2500-14um | No | Yes |
acA2500-20gc | No | Yes |
acA2500-20gcMED | No | Yes |
acA2500-20gm | No | Yes |
acA2500-20gmMED | No | Yes |
acA2500-60uc | No | Yes |
acA2500-60um | No | Yes |
acA3088-16gc | No | Yes |
acA3088-16gm | No | Yes |
acA3088-57uc | No | Yes |
acA3088-57ucMED | No | Yes |
acA3088-57um | No | Yes |
acA3088-57umMED | No | Yes |
acA3800-10gc | No | Yes |
acA3800-10gm | No | Yes |
acA3800-14uc | No | Yes |
acA3800-14um | No | Yes |
acA4024-8gc | No | Yes |
acA4024-8gm | No | Yes |
acA4024-29uc | No | Yes |
acA4024-29um | No | Yes |
acA4096-11gc | No | Yes |
acA4096-11gm | No | Yes |
acA4096-30uc | No | Yes |
acA4096-30ucMED | No | Yes |
acA4096-30um | No | Yes |
acA4096-30umMED | No | Yes |
acA4096-40uc | No | Yes |
acA4096-40ucMED | No | Yes |
acA4096-40um | No | Yes |
acA4096-40umMED | No | Yes |
acA4112-8gc | No | Yes |
acA4112-8gm | No | Yes |
acA4112-20uc | No | Yes |
acA4112-20ucMED | No | Yes |
acA4112-20um | No | Yes |
acA4112-20umMED | No | Yes |
acA4112-30uc | No | Yes |
acA4112-30ucMED | No | Yes |
acA4112-30um | No | Yes |
acA4112-30umMED | No | Yes |
acA5472-5gc | No | Yes |
acA5472-5gm | No | Yes |
acA5472-17uc | No | Yes |
acA5472-17ucMED | No | Yes |
acA5472-17um | No | Yes |
acA5472-17umMED | No | Yes |
boA1936-400cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA1936-400cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA2448-250cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA2448-250cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA2832-190cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA2832-190cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4096-93cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4096-93cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4096-180cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4096-180cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4112-68cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4112-68cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4500-45cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4500-45cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4504-100cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA4504-100cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA5120-150cc | No | Yes |
boA5120-150cm | No | Yes |
boA5120-230cc | No | Yes |
boA5120-230cm | No | Yes |
boA5320-150cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA5320-150cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA5328-100cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA5328-100cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA6500-36cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA6500-36cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA8100-16cc | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA8100-16cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
boA9344-30cc | No | Yes |
boA9344-30cm | No | Yes |
boA9344-70cc | No | Yes |
boA9344-70cm | No | Yes |
boA13440-17cm | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA720-520uc | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA720-520um | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA1280-54uc | No | Yes |
daA1280-54um | No | Yes |
daA1440-220uc | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA1440-220um | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA1600-60uc | No | Yes |
daA1600-60um | No | Yes |
daA1920-15um | No | Yes |
daA1920-30uc | No | Yes |
daA1920-30um | No | Yes |
daA1920-160uc | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA1920-160um | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA2448-70uc | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA2448-70um | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA2500-14uc | No | Yes |
daA2500-14um | No | Yes |
daA3840-45uc | Yes | Configurable via the BslAcquisitionStopMode parameter |
daA3840-45um | Yes | Configurable via the BslAcquisitionStopMode parameter |
puA1280-54uc | No | Yes |
puA1280-54um | No | Yes |
puA1600-60uc | No | Yes |
puA1600-60um | No | Yes |
puA1920-30uc | No | Yes |
puA1920-30um | No | Yes |
puA2500-14uc | No | Yes |
puA2500-14um | No | Yes |
Sample Code#
// Configure continuous image acquisition on the cameras
camera.AcquisitionMode.SetValue(AcquisitionMode_Continuous);
// Switch on image acquisition
camera.AcquisitionStart.Execute();
// The camera waits for trigger signals
// (...)
// Switch off image acquisition
camera.AcquisitionStop.Execute();
// Switch image acquisition back on
camera.AcquisitionStart.Execute();
// The camera waits for trigger signals
// (...)
// Abort image acquisition
camera.AcquisitionAbort.Execute();
INodeMap& nodemap = camera.GetNodeMap();
// Configure continuous image acquisition on the cameras
CEnumParameter(nodemap, "AcquisitionMode").SetValue("Continuous");
// Switch on image acquisition
CCommandParameter(nodemap, "AcquisitionStart").Execute();
// The camera waits for trigger signals
// (...)
// Switch off image acquisition
CCommandParameter(nodemap, "AcquisitionStop").Execute();
// Switch image acquisition back on
CCommandParameter(nodemap, "AcquisitionStart").Execute();
// The camera waits for trigger signals
// (...)
// Abort image acquisition
CCommandParameter(nodemap, "AcquisitionAbort").Execute();
// Configure continuous image acquisition on the cameras
camera.Parameters[PLCamera.AcquisitionMode].SetValue(PLCamera.AcquisitionMode.Continuous);
// Switch on image acquisition
camera.Parameters[PLCamera.AcquisitionStart].Execute();
// The camera waits for trigger signals
// (...)
// Switch off image acquisition
camera.Parameters[PLCamera.AcquisitionStop].Execute();
// Switch image acquisition back on
camera.Parameters[PLCamera.AcquisitionStart].Execute();
// The camera waits for trigger signals
// (...)
// Abort image acquisition
camera.Parameters[PLCamera.AcquisitionAbort].Execute();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Configure continuous image acquisition on the cameras */
errRes = PylonDeviceFeatureFromString(hdev, "AcquisitionMode", "Continuous");
CHECK(errRes);
/* Switch on image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStart");
CHECK(errRes);
/* The camera waits for trigger signals */
/* (...) */
/* Switch off image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStop");
CHECK(errRes);
/* Switch image acquisition back on */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStart");
CHECK(errRes);
/* The camera waits for trigger signals */
/* (...) */
/* Abort image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionAbort");
CHECK(errRes);
# Configure continuous image acquisition on the cameras
camera.AcquisitionMode.Value = "Continuous"
# Switch on image acquisition
camera.AcquisitionStart.Execute()
# The camera waits for trigger signals
# (...)
# Switch off image acquisition
camera.AcquisitionStop.Execute()
# Switch image acquisition back on
camera.AcquisitionStart.Execute()
# The camera waits for trigger signals
# (...)
# Abort image acquisition
camera.AcquisitionAbort.Execute()
You can also use the pylon Viewer to easily set the parameters.