Skip to content

Basler dart BCON for MIPI#

Basler's proprietary BCON for MIPI interface is based on the MIPI CSI-2 video interface standard. This makes it really easy to integrate Basler dart BCON for MIPI camera modules into embedded vision systems with MIPI CSI-2 connections.

Basler dart BCON for MIPI Camera Modules

Basler dart BCON for MIPI camera modules are available in the following variants:

  • Bare board: Consists of a circuit board only.
  • S-mount: Consists of a circuit board with a camera front attached. S-mount lenses can be attached to the lens mount on the camera front.

Models#

Embedded Vision Kits#