Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Basler Vision Connector Messaging: Camera Operation#

Camera operations are handled by sending JSON strings via MQTT or ZMQ according to the Topic Structure.

If a requested command or argument isn't supported by the Basler Vision Connector (e.g., the command in the given action field of the command is unknown), the Basler Vision Connector replies the return code 0x03000003. See also Error message codes.

Getting List of Supported Commands#

To get the full list of commands that are currently supported by the Basler Vision Connector, the client can send the following command:

JSON Payload#

Field Optional Type Description
TransactionID Yes String Transaction identification
Action No String Method called. Fixed value: GetSupportedCommands
{
    "TransactionID": "123456",
    "Action": "GetSupportedCommands"
}

Response Object#

Field Optional Type Description
TransactionID Yes String Transaction identification
ReturnCode No Integer Message code following Message Codes
Message Yes String Response message
SupportedCommandList No Array of strings Array of commands: the possible values for the Action field
{
    "TransactionID": "123456",
    "ReturnCode": 0,
    "Message": "Supported commands retrieved.",
    "SupportedCommandList":
    [
      "EnumerateDevices",
      "GetStatus",
      "OpenDevice",
      "CloseDevice",
      "StartStreaming",
      "StopStreaming",
      "GetParameterNames",
      "GetParameters",
      "SetParameters",
      "SetQuickParameters",
      "SoftwareTrigger",
      "GetUserSets",
      "LoadUserSet",
      "SaveUserSet",
      "SetDefaultUserSet",
      "SetDeviceConfig",
      "GetDeviceConfig",
      "GetSupportedCommands"
    ]
}