Compression Beyond#
Compressing image data may lower the camera's bandwidth usage, increase the frame rate, or both.
For more information, see the feature description on the Basler website.
Using the Feature#
How It Works#
Compression is performed automatically whenever the ImageCompressionMode
parameter is set to BaslerCompressionBeyond
.
When enabled, the feature always compresses images as much as possible. This lowers the amount of data ("payload") output by the camera, i.e., its bandwidth usage. This is especially useful for Basler GigE cameras in a multi-camera setup.
If you want the camera to also optimize the frame rate, further configuration is required. This is because the camera doesn't "know" how much it will be able to compress an image before exposure starts.
To get around this, you must tell the camera how much it will at least be able to compress images. Do this by specifying a compression ratio (BslImageCompressionRatio
parameter).
For example, setting the BslImageCompressionRatio
parameter to 90, tells the camera that it will be able to compress any image to at least 90 % of its original size. With this information, the camera can increase its frame rate by up to 10 %.
However, if you set the value too low, i.e., if the camera can't achieve the estimated compression ratio, frames will be skipped. In this case, you can change the ImageCompressionRateOption
parameter from Lossless
to FixRatio
. This allows even lower compression rates, but reduces image quality.
Info
- During image acquisition, you can determine the payload size and compression ratio of the last acquired image by reading the
BslImageCompressionLastRatio
andBslImageCompressionLastSize
parameter values. -
When Compression Beyond is enabled, the pylon Viewer displays information about the feature in the status bar of the image display area:
-
When implementing your own image grabbing routine, you must decompress the grabbed images using the CImageDecompressor class. For more information, see the "Advanced Topics" topic, section "Image Decompression", in the C++ Programmer's Guide and Reference Documentation delivered with the Basler pylon Camera Software Suite.
Configuring Compression Beyond#
How to configure Compression Beyond depends on your requirements.
Optimize Bandwidth#
Assume you want the camera to do the following:
- Lower the bandwidth usage
- Increase the frame rate
- Preserve optimum image quality
To achieve this:
- Make sure that the camera is idle, i.e., not capturing images.
- Set the
ImageCompressionMode
parameter toBaslerCompressionBeyond
. - Set the
ImageCompressionRateOption
parameter toLossless
. - Set the
BslImageCompressionRatio
parameter to 100.
With these settings, the camera compresses images as much as possible without sacrificing image quality.
Optimize Bandwidth and Frame Rate With Lossless Compression#
Assume you want the camera to do the following:
- Lower the bandwidth usage
- Increase the frame rate
- Preserve optimum image quality
To achieve this:
- Make sure that the camera is idle, i.e., not capturing images.
- Set the
ImageCompressionMode
parameter toBaslerCompressionBeyond
. - Set the
ImageCompressionRateOption
parameter toLossless
. - Set the
BslImageCompressionRatio
parameter to a value lower than 100, e.g., 90. - Get the value of the
ResultingFrameRate
parameter to determine the estimated frame rate. - If the frame rate is not high enough for your application, repeat steps 4 and 5 with a lower
BslImageCompressionRatio
parameter value. - Start image acquisition. If the camera can't acquire images without skipping frames, the desired frame rate can't be achieved. Try the following:
- If a lower frame rate is acceptable, increase the value of the
BslImageCompressionRatio
parameter until the camera is able to acquire images continuously. - If a lower image quality is acceptable, carry out the procedure detailed below.
- If a lower frame rate is acceptable, increase the value of the
Optimize Bandwidth and Frame Rate With Lossy Compression#
Info
Always try lossless compression first. Only use lossy compression if you can't achieve the required results with lossless compression.
Assume you want the camera to do the following:
- Lower the bandwidth usage
- Increase the frame rate
- Preserve optimum image quality
To achieve this:
- Make sure that the camera is idle, i.e., not capturing images.
- Set the
ImageCompressionMode
parameter toBaslerCompressionBeyond
. - Set the
ImageCompressionRateOption
parameter toFixRatio
. - Set the
BslImageCompressionRatio
parameter to100
. - Acquire at least one image.
- Get the value of the
BslImageCompressionLastRatio
parameter.
The value indicates the threshold between lossless and lossy image acquisition. - Set the
BslImageCompressionRatio
parameter to a value lower than the value of theBslImageCompressionLastRatio
parameter.
The lower the parameter value, the lower the image quality. - Start image acquisition. If the camera can't acquire images without skipping frames, increase the value of the
BslImageCompressionRatio
parameter until the camera is able to acquire images.
With these settings, you may be able to achieve lower bandwidth usage and higher frame rates compared to lossless compression. However, this will reduce image quality.
Sample Code#
// Enable Compression Beyond with lossless compression
camera.ImageCompressionMode.SetValue(ImageCompressionMode_BaslerCompressionBeyond);
camera.ImageCompressionRateOption.SetValue(ImageCompressionRateOption_Lossless);
// To increase the frame rate, tell the camera that it will be able
// to compress any image to at least 70 % of its original size
camera.BslImageCompressionRatio.SetValue(70);
// Get the resulting frame rate
double resultingFrameRate = camera.ResultingFrameRate.GetValue();
if (resultingFrameRate < desiredFrameRate) {
// Frame rate isn't high enough for the application.
// Therefore, enable lossy compression. This allows even
// lower compression rates, but reduces image quality.
camera.ImageCompressionRateOption.SetValue(ImageCompressionRateOption_FixRatio);
camera.BslImageCompressionRatio.SetValue(50);
}
// Start image acquisition
// ...
// (Implement your own image grabbing routine here.
// For example, the InstantCamera class provides the StartGrabbing() method.
// Note that you must decompress grabbed images using the CImageDecompressor class.)
// ...
// Determine the compression ratio of the last acquired image
double lastRatio = camera.BslImageCompressionLastRatio.GetValue();
// Determine the payload size of the last acquired image in bytes
int64_t lastSize = camera.BslImageCompressionLastSize.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Enable Compression Beyond with lossless compression
CEnumParameter(nodemap, "ImageCompressionMode").SetValue("BaslerCompressionBeyond");
CEnumParameter(nodemap, "ImageCompressionRateOption").SetValue("Lossless");
// To increase the frame rate, tell the camera that it will be able
// to compress any image to at least 70 % of its original size
CIntegerParameter(nodemap, "BslImageCompressionRatio").SetValue(70);
// Get the resulting frame rate
double resultingFrameRate = CFloatParameter(nodemap, "ResultingFrameRate").GetValue();
if(resultingFrameRate < desiredFrameRate){
// Frame rate isn't high enough for the application.
// Therefore, enable lossy compression. This allows even
// lower compression rates, but reduces image quality.
CEnumParameter(nodemap, "ImageCompressionRateOption").SetValue("FixRatio");
CIntegerParameter(nodemap, "BslImageCompressionRatio").SetValue(50);
}
// Start image acquisition
// ...
// (Implement your own image grabbing routine here.
// For example, the InstantCamera class provides the StartGrabbing() method.
// Note that you must decompress grabbed images using the CImageDecompressor class.)
// ...
// Determine the compression ratio of the last acquired image
double lastRatio = CFloatParameter(nodemap, "BslImageCompressionLastRatio").GetValue();
// Determine the payload size of the last acquired image in bytes
int64_t lastSize = CIntegerParameter(nodemap, "BslImageCompressionLastSize").GetValue();
// Enable Compression Beyond with lossless compression
camera.Parameters[PLCamera.ImageCompressionMode].SetValue(PLCamera.ImageCompressionMode.BaslerCompressionBeyond);
camera.Parameters[PLCamera.ImageCompressionRateOption].SetValue(PLCamera.ImageCompressionRateOption.Lossless);
// To increase the frame rate, tell the camera that it will be able
// to compress any image to at least 70 % of its original size
camera.Parameters[PLCamera.BslImageCompressionRatio].SetValue(70);
// Get the resulting frame rate
double resultingFrameRate = camera.Parameters[PLCamera.ResultingFrameRate].GetValue();
if(resultingFrameRate < desiredFrameRate){
// Frame rate isn't high enough for the application.
// Therefore, enable lossy compression. This allows even
// lower compression rates, but reduces image quality.
camera.Parameters[PLCamera.ImageCompressionRateOption].SetValue(PLCamera.ImageCompressionRateOption.FixRatio);
camera.Parameters[PLCamera.BslImageCompressionRatio].SetValue(50);
}
// Start image acquisition
// ...
// (Implement your own image grabbing routine here.
// For example, the InstantCamera class provides the StartGrabbing() method.
// Note that you must decompress grabbed images using the CImageDecompressor class.)
// ...
// Determine the compression ratio of the last acquired image
double lastRatio = camera.Parameters[PLCamera.BslImageCompressionLastRatio].GetValue();
// Determine the payload size of the last acquired image in bytes
Int64 lastSize = camera.Parameters[PLCamera.BslImageCompressionLastSize].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double resultingFrameRate = 0;
double lastRatio = 0;
int64_t lastSize = 0;
/* Enable Compression Beyond with lossless compression */
errRes = PylonDeviceFeatureFromString(hdev, "ImageCompressionMode", "BaslerCompressionBeyond");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "ImageCompressionRateOption", "Lossless");
CHECK(errRes);
/* To increase the frame rate, tell the camera that it will be able */
/* to compress any image to at least 70 % of its original size */
errRes = PylonDeviceSetIntegerFeature(hdev, "BslImageCompressionRatio", 70);
CHECK(errRes);
/* Get the resulting frame rate */
errRes = PylonDeviceGetFloatFeature(hdev, "ResultingFrameRate", &resultingFrameRate);
CHECK(errRes);
if(resultingFrameRate < desiredFrameRate){
/* Frame rate isn't high enough for the application. */
/* Therefore, enable lossy compression. This allows even */
/* lower compression rates, but reduces image quality. */
errRes = PylonDeviceFeatureFromString(hdev, "ImageCompressionRateOption", "FixRatio");
CHECK(errRes);
errRes = PylonDeviceSetIntegerFeature(hdev, "BslImageCompressionRatio", 50);
CHECK(errRes);
}
/* Start image acquisition */
/* ... */
/* (Implement your own image grabbing routine here. */
/* For example, the InstantCamera class provides the StartGrabbing() method. */
/* Note that you must decompress grabbed images using the CImageDecompressor class.) */
/* ... */
/* Determine the compression ratio of the last acquired image */
errRes = PylonDeviceGetFloatFeature(hdev, "BslImageCompressionLastRatio", &lastRatio);
CHECK(errRes);
/* Determine the payload size of the last acquired image in bytes */
errRes = PylonDeviceGetIntegerFeature(hdev, "BslImageCompressionLastSize", &lastSize);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.