Counter#
Using the Feature#
The implementation of this feature varies by camera series:
ace 2, boost R, dart M/R, and racer 2 Cameras#
How It Works#
Depending on your camera model, up to three counters are available: Counter 1, Counter 2, and Counter 3.
Every counter has the following characteristics:
- It starts at 0.
- It must be started before it can count.
- Once started, it can count a specific type of event (the "event source"). For example, it can count the number of images exposed.
- It can be reset to 0 at any time.
- Its current value can be determined by getting the value of the
CounterValue
parameter. - Its maximum value is defined by the
CounterDuration
parameter value (default: 4 294 967 295). After reaching the maximum value, the counter stops counting and must be reset. - Its current status can be determined by getting the value of the
CounterStatus
parameter. - It is reset to 0 whenever the camera is powered off and on again.
Info
For racer 2 S GigE cameras, you can use the Counter and Data Chunks features, in combination with the trigger settings, to specify which lines belong to a frame and which frames belong to the correct test object.
Getting the Value of a Counter#
To determine the current value of a counter, get the value of the CounterValue
parameter. This parameter is read-only.
Starting a Counter#
To start a counter:
- Set the
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - Set the
CounterTriggerSource
parameter to the source that you want to use to start the counter, e.g.,Line2
. - If applicable, set the
CounterTriggerActivation
parameter to one of the following values:RisingEdge
(default): The counter starts when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter starts when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter starts when the signal falls or rises.LevelHigh
: The counter starts when the signal is high. When the signal changes to low, the counter status is set toCounterTriggerWait
and must be started again.LevelLow
: The counter starts when the signal is low. When the signal changes to high, the counter status is set toCounterTriggerWait
and must be started again.
- Start the counter by sending a signal on the selected counter trigger source.
When started, the counter's status changes from CounterTriggerWait
to CounterActive
.
Info
- If you start a counter, it will not necessarily start counting. If and when the counter counts depends on the event source set.
- The
CounterTriggerActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal likeExposureActive
.
Increasing a Counter#
Once a counter is started, it can be increased, i.e., it can count.
To increase a counter:
- Set the
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - Set the
CounterEventSource
parameter to the source that you want to use to increase the counter, e.g.,Line2
. - If applicable, set the
CounterEventActivation
parameter to one of the following values:RisingEdge
(default): The counter counts when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter counts when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter counts when the signal falls or rises.
- Set the
CounterDuration
parameter to the desired maximum value. - Increase the counter by sending a signal on the selected counter event source.
Whenever the camera detects a signal on the selected source, the timer increases, up to the defined maximum value.
Info
The CounterEventActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive
.
Resetting a Counter#
You can reset the counter to 0 at any time.
You must reset the counter if it has reached its maximum value (defined by the CounterDuration
parameter value) and you want to reuse it.
Reset by Software#
To reset a counter by software, execute the CounterReset
command.
Alternatively, you can set a software signal as the reset source (see below).
Reset Using a Reset Source#
The CounterResetSource
parameter allows you to specify which source resets the counter.
To reset the counter using a reset source:
- Set the
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - Set the
CounterResetSource
parameter to the source that you want to use to reset the counter, e.g.,Line2
. - If applicable, set the
CounterResetActivation
parameter to one of the following values:RisingEdge
(default): The counter resets when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter resets when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter resets when the signal falls or rises.
- Reset the counter by sending a signal on the selected counter reset source.
When reset, the counter's status changes to CounterTriggerWait
and must be started again.
Info
The CounterResetActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive
.
Stopping a Counter#
To stop a counter, do any of the following:
- Stop sending signals on the selected event source.
- Set the
CounterEventSource
parameter toOff
. - Reset the counter.
Getting the Status of a Counter#
To get the current status of a counter, get the value of the CounterStatus
parameter. This parameter is read-only.
Possible values are:
CounterTriggerWait
: The counter is waiting to be started.CounterActive
: The counter is waiting to be increased by the selected event source or is currently counting.CounterCompleted
: The counter has reached its maximum value defined by theCounterDuration
parameter.CounterIdle
: The counter is idle. A counter is in this state whenever theCounterTriggerSource
parameter is set toOff
, i.e., the counter can't be started.
ace Classic/U/L Cameras#
How It Works#
Two counters are available: Counter 1 and Counter 2.
With one exception (see below), every counter has the following characteristics:
- It starts at 0.
- It counts a specific type of event (the "event source"). For example, it counts the number of images acquired. The event source is preset and can't be changed.
- Its current value can be determined by retrieving the related data chunk, e.g., the Frame Counter chunk.
- Its maximum value is 4 294 967 295. After reaching the maximum value, the counter is reset to 0 and then continues counting.
- It can be reset manually.
- It is reset to 0 whenever the camera is powered off and on again.
Exception: On some camera models, Counter 2 can be used to control the sequencer. This counter has different characteristics due to its specific purpose.
Getting the Value of a Counter#
To determine the current value of a counter, retrieve the related data chunk using the Data Chunks feature.
Resetting a Counter#
To reset a counter:
Set the CounterSelector
parameter to the desired counter, e.g., Counter2
.
Set the CounterResetSource
parameter to a software source (Software
) or to a hardware source (e.g., Line1
).
Depending on the source selected in step 2, do one of the following:
- If you set a software source, execute the
CounterReset
command. - If you set a hardware source, apply an electrical signal to one of the camera's input lines.
Additional Parameters#
- The
CounterEventSource
parameter allows you to get the event source of the currently selected counter, i.e., determine in which case the counter increases. - The
CounterResetActivation
parameter currently serves no function. It is preset toRisingEdge
. This means that if the counter is configured for hardware reset, the counter resets when the hardware trigger signal rises.
Specifics#
Camera Model | Available Counters | Function | Event Source | Related Data Chunk | Can Be Reset |
---|---|---|---|---|---|
a2A640-240gmSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A640-240umSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1280-80gmSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1280-125umSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-51gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-51gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-51gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-51gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-160ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-160ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-160umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-160umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-165g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A1920-165g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2048-35gmSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2048-110umSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2440-98g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2440-98g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-23gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-23gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-23gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-23gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-75ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-75ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-75umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-75umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-105g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-105g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-120cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-120cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-210cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2448-210cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2560-20gmSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2560-70umSWIR | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-22gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-22gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-22gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-22gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-60ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-60ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-60umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2590-60umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-20gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-20gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-20gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-20gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-64ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-64ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-64umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2600-64umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-14gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-14gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-14gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-14gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-14gmUV | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-48ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-48ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-48umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-48umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-48umUV | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-67g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-67g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-67g5mUV | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-86cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A2840-86cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-13gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-13gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-13gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-13gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-45ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-45ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-45umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A3840-45umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-9gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-9gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-9gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-9gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-30ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-30ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-30umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-30umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-44g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-44g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-67cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4096-67cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-12gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-12gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-12gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-12gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-40ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-40ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-40umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4200-40umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-5gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-5gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-5gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-5gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-18ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-18ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-18umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-18umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-27g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-27g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-42cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4504-42cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-6gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-6gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-6gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-6gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-20ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-20ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-20umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A4508-20umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-7gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-7gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-7gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-7gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-23ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-23ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-23umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-23umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-34g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-34g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-52cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5320-52cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-4gcBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-4gcPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-4gmBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-4gmPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-15ucBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-15ucPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-15umBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-15umPRO | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-22g5cBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-22g5mBAS | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-35cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
a2A5328-35cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
acA640-121gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA640-300gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA640-300gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA640-750uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA640-750um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA720-290gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA720-290gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA720-520uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA720-520um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA800-200gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA800-200gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA800-510uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA800-510um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1280-60gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1280-60gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1300-60gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1300-60gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1300-60gmNIR | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1300-75gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1300-75gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1300-200uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1300-200um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1440-73gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1440-73gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1440-220uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1440-220um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1600-20gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1600-20uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1600-60gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1600-60gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-25gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-25gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-25uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-25um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-40gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-40gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-40uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-40ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-40um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-40umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-48gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-48gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-50gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-50gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA1920-150uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-150um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-155uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-155ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-155um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA1920-155umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2000-50gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2000-50gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2000-165uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2000-165um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2040-25gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2040-25gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2040-25gmNIR | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2040-35gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2040-35gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2040-55uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2040-55um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2040-90uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2040-90um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2040-90umNIR | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2040-120uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2040-120um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-20gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2440-20gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2440-35uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-35ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-35um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-35umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-75uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-75ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-75um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2440-75umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2500-14gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2500-14gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2500-14uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2500-14um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2500-20gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2500-20gcMED | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2500-20gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2500-20gmMED | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA2500-60uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA2500-60um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA3088-16gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA3088-16gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA3088-57uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA3088-57ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA3088-57um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA3088-57umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA3800-10gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA3800-10gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA3800-14uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA3800-14um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4024-8gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA4024-8gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA4024-29uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4024-29um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-11gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA4096-11gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA4096-30uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-30ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-30um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-30umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-40uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-40ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-40um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4096-40umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-8gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA4112-8gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA4112-20uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-20ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-20um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-20umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-30uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-30ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-30um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA4112-30umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA5472-5gc | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA5472-5gm | Counter 1 Counter 2 | Counter 1: Counts number of hardware frame start trigger signals received, regardless of whether they cause image acquisitions or not Counter 2: Counts number of acquired images | Counter 1: Frame Trigger Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: Yes |
acA5472-17uc | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA5472-17ucMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA5472-17um | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
acA5472-17umMED | Counter 1 Counter 2 | Counter 1: Counts number of acquired images Counter 2: Can be used to control the sequencer | Counter 1: Frame Start Counter 2: Frame Start | Counter 1: Trigger Input Counter Chunk Counter 2: Frame Counter Chunk | Counter 1: Yes Counter 2: No |
boA1936-400cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA1936-400cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA2448-250cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA2448-250cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA2832-190cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA2832-190cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4096-93cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4096-93cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4096-180cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4096-180cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4112-68cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4112-68cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4500-45cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4500-45cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4504-100cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA4504-100cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA5120-150cc | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA5120-150cm | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA5120-230cc | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA5120-230cm | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA5320-150cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA5320-150cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA5328-100cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA5328-100cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA6500-36cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA6500-36cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA8100-16cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA8100-16cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
boA9344-30cc | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA9344-30cm | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA9344-70cc | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA9344-70cm | None | Counter feature not supported | Counter feature not supported | Counter feature not supported | Counter feature not supported |
boA13440-17cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA720-520uc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA720-520um | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA1280-54uc | Counter feature not supported | – | – | – | – |
daA1280-54um | Counter feature not supported | – | – | – | – |
daA1440-220uc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA1440-220um | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA1600-60uc | Counter feature not supported | – | – | – | – |
daA1600-60um | Counter feature not supported | – | – | – | – |
daA1920-15um | Counter feature not supported | – | – | – | – |
daA1920-30uc | Counter feature not supported | – | – | – | – |
daA1920-30um | Counter feature not supported | – | – | – | – |
daA1920-160uc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA1920-160um | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA2448-70uc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA2448-70um | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA2500-14uc | Counter feature not supported | – | – | – | – |
daA2500-14um | Counter feature not supported | – | – | – | – |
daA3840-45uc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
daA3840-45um | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
dmA720-290gc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
dmA720-290gm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
dmA1440-73gc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
dmA1440-73gm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
dmA1920-51gc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
dmA1920-51gm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
puA1280-54uc | Counter feature not supported | – | – | – | – |
puA1280-54um | Counter feature not supported | – | – | – | – |
puA1600-60uc | Counter feature not supported | – | – | – | – |
puA1600-60um | Counter feature not supported | – | – | – | – |
puA1920-30uc | Counter feature not supported | – | – | – | – |
puA1920-30um | Counter feature not supported | – | – | – | – |
puA2500-14uc | Counter feature not supported | – | – | – | – |
puA2500-14um | Counter feature not supported | – | – | – | – |
r2L2048-29gc | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-58gm | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-62cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
r2L2048-62g5c | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-172cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
r2L2048-172g5m | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-14gc | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-29gm | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-42cc | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
r2L4096-42g5c | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-84cm | Counter 1 Counter 2 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes |
r2L4096-84g5m | Counter 1 Counter 2 Counter 3 Counter 4 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L8192-200cm | Counter 1 Counter 2 Counter 3 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes |
r2L16384-120cm | Counter 1 Counter 2 Counter 3 | Configurable | Configurable | N/A | Counter 1: Yes Counter 2: Yes Counter 3: Yes |
Sample Code#
ace 2, boost R, dart M/R, and racer 2 Cameras#
// Select Counter 1
camera.CounterSelector.SetValue(CounterSelector_Counter1);
// Specify that the counter starts when a software signal is sent via channel 1
camera.CounterTriggerSource.SetValue(CounterTriggerSource_SoftwareSignal1);
// Specify that the counter increases whenever a rising signal is detected on Line 1
camera.CounterEventSource.SetValue(CounterEventSource_Line1);
camera.CounterEventActivation.SetValue(CounterEventActivation_RisingEdge);
// Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.CounterResetSource.SetValue(CounterResetSource_Line2);
camera.CounterResetActivation.SetValue(CounterEventActivation_FallingEdge);
// Set the maximum value of the counter to 1000
camera.CounterDuration.SetValue(1000);
// Manually reset the counter
camera.CounterReset.Execute();
// Get the current status of the counter
CounterStatusEnums counterStatus = camera.CounterStatus.GetValue();
// Get the current value of the counter
int64_t i = camera.CounterValue.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Select Counter 1
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
// Specify that the counter starts when a software signal is sent via channel 1
CEnumParameter(nodemap, "CounterTriggerSource").SetValue("SoftwareSignal1");
// Specify that the counter increases whenever a rising signal is detected on Line 1
CEnumParameter(nodemap, "CounterEventSource").SetValue("Line1");
CEnumParameter(nodemap, "CounterEventActivation").SetValue("RisingEdge");
// Specify that the counter is reset whenever a falling signal is detected on Line 2
CEnumParameter(nodemap, "CounterResetSource").SetValue("Line2");
CEnumParameter(nodemap, "CounterResetActivation").SetValue("FallingEdge");
// Set the maximum value of the counter to 1000
CIntegerParameter(nodemap, "CounterDuration").SetValue(1000);
// Manually reset the counter
CCommandParameter(nodemap, "CounterReset").Execute();
// Get the current status of the counter
String_t counterStatus = CEnumParameter(nodemap, "CounterStatus").GetValue();
// Get the current value of the counter
int64_t i = CIntegerParameter(nodemap, "CounterValue").GetValue();
// Select Counter 1
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
// Specify that the counter starts when a software signal is sent via channel 1
camera.Parameters[PLCamera.CounterTriggerSource].SetValue(PLCamera.CounterTriggerSource.SoftwareSignal1);
// Specify that the counter increases whenever a rising signal is detected on Line 1
camera.Parameters[PLCamera.CounterEventSource].SetValue(PLCamera.CounterEventSource.Line1);
camera.Parameters[PLCamera.CounterEventActivation].SetValue(PLCamera.CounterEventActivation.RisingEdge);
// Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.Parameters[PLCamera.CounterResetSource].SetValue(PLCamera.CounterResetSource.Line2);
camera.Parameters[PLCamera.CounterResetActivation].SetValue(PLCamera.CounterEventActivation.FallingEdge);
// Set the maximum value of the counter to 1000
camera.Parameters[PLCamera.CounterDuration].SetValue(1000);
// Manually reset the counter
camera.Parameters[PLCamera.CounterReset].Execute();
// Get the current status of the counter
string counterStatus = camera.Parameters[PLCamera.CounterStatus].GetValue();
// Get the current value of the counter
Int64 i = camera.Parameters[PLCamera.CounterValue].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char counterStatus_str[64] = {0};
int64_t i = 0;
/* Select Counter 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
/* Specify that the counter starts when a software signal is sent via channel 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterTriggerSource", "SoftwareSignal1");
CHECK(errRes);
/* Specify that the counter increases whenever a rising signal is detected on Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterEventSource", "Line1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterEventActivation", "RisingEdge");
CHECK(errRes);
/* Specify that the counter is reset whenever a falling signal is detected on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetSource", "Line2");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetActivation", "FallingEdge");
CHECK(errRes);
/* Set the maximum value of the counter to 1000 */
errRes = PylonDeviceSetIntegerFeature(hdev, "CounterDuration", 1000);
CHECK(errRes);
/* Manually reset the counter */
errRes = PylonDeviceExecuteCommandFeature(hdev, "CounterReset");
CHECK(errRes);
/* Get the current status of the counter */
len = sizeof(counterStatus_str);
errRes = PylonDeviceFeatureToString(hdev, "CounterStatus", counterStatus_str, &len);
CHECK(errRes);
/* Get the current value of the counter */
errRes = PylonDeviceGetIntegerFeature(hdev, "CounterValue", &i);
CHECK(errRes);
# Select Counter 1
camera.CounterSelector.Value = "Counter1"
# Specify that the counter starts when a software signal is sent via channel 1
camera.CounterTriggerSource.Value = "SoftwareSignal1"
# Specify that the counter increases whenever a rising signal is detected on Line 1
camera.CounterEventSource.Value = "Line1"
camera.CounterEventActivation.Value = "RisingEdge"
# Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.CounterResetSource.Value = "Line2"
camera.CounterResetActivation.Value = "FallingEdge"
# Set the maximum value of the counter to 1000
camera.CounterDuration.Value = 1000
# Manually reset the counter
camera.CounterReset.Execute()
# Get the current status of the counter
counterStatus = camera.CounterStatus.Value
# Get the current value of the counter
i = camera.CounterValue.Value
ace Classic/U/L Cameras#
// Reset Counter 1 via software command
camera.CounterSelector.SetValue(CounterSelector_Counter1);
camera.CounterResetSource.SetValue(CounterResetSource_Software);
camera.CounterReset.Execute();
// Get the event source of Counter 1
camera.CounterSelector.SetValue(CounterSelector_Counter1);
CounterEventSourceEnums e = camera.CounterEventSource.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Reset Counter 1 via software command
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
CEnumParameter(nodemap, "CounterResetSource").SetValue("Software");
CCommandParameter(nodemap, "CounterReset").Execute();
// Get the event source of Counter 1
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
String_t e = CEnumParameter(nodemap, "CounterEventSource").GetValue();
// Reset Counter 1 via software command
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
camera.Parameters[PLCamera.CounterResetSource].SetValue(PLCamera.CounterResetSource.Software);
camera.Parameters[PLCamera.CounterReset].Execute();
// Get the event source of Counter 1
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
string e = camera.Parameters[PLCamera.CounterEventSource].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Reset Counter 1 via software command */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetSource", "Software");
CHECK(errRes);
errRes = PylonDeviceExecuteCommandFeature(hdev, "CounterReset");
CHECK(errRes);
/* Get the event source of Counter 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "CounterEventSource", e_str, &len);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.