Data Chunks#
Using the Feature#
How It Works#
Data chunks allow you to add supplementary information to individual image acquisitions. The desired supplementary information is generated and appended as data chunks to the image data.
Image data is also considered a "chunk". This "image data chunk" can't be disabled and is always the first chunk transmitted by the camera. If one or more data chunks are enabled, these chunks are transmitted as chunk 2, 3, and so on.
The figure below shows a set of chunks with the leading image data chunk and appended data chunks. The example assumes that the CRC checksum chunk feature is enabled.
After data chunks have been transmitted to the computer, they must be retrieved to obtain their information. The exact procedure depends on your camera model and the programming language used for your application. For more information about retrieving data chunks, see the pylon API Documentation.
Additional Metadata#
Besides the data chunks, the camera adds additional metadata to individual images, e.g., the image height, image width, the image ROI offset, and the pixel format used. This information can be retrieved by accessing the grab result data via the pylon API.
Info
If all of the following conditions are met, the grab result data doesn't contain any useful information (image height, image width, etc. will be set to -1):
- You are using a Basler ace Classic GigE camera.
- You are using the pylon C API, the pylon C. NET API, or the pylon C++ low level API.
- The
ChunkModeActive
parameter is set totrue
.
In this case, you must retrieve the additional metadata using the pylon chunk parser. For more information, see the code samples in the pylon API Documentation.
Enabling and Retrieving Data Chunks#
- Set the
ChunkModeActive
parameter totrue
. - Set the
ChunkSelector
parameter to the kind of chunk that you want to enable (if available): - Enable the selected chunk by setting the
ChunkEnable
parameter totrue
. - Repeat steps 2 and 3 for every desired chunk.
- Implement chunk retrieval in your application.
For information about implementing chunk retrieval, see the pylon API Documentation.
Info
Data chunks can also be viewed in the pylon Viewer.
Available Data Chunks#
Auto Brightness Status Chunk#
If this chunk is available and enabled, the camera appends the status of the target brightness adjustments to every image.
Target brightness adjustments are performed whenever the Exposure Auto or the Gain Auto auto function or both are enabled.
-
On ace 2, boost, and dart R cameras, the
BslChunkAutoBrightnessStatus
parameter is available. It indicates the auto brightness status using the following enumeration:Disabled
: Target brightness adjustments are disabled, i.e., Gain Auto and Exposure Auto are set toOff
.TargetNotReached
: Target brightness adjustments are enabled, but the target brightness value has not been reached.TargetReached
: Target brightness adjustments are enabled, and the target brightness value has been reached.
-
On other cameras, the status is indicated using the following values:
- 0: Equals the
Disabled
status, see above. - 1: Equals the
TargetNotReached
status, see above. - 2: Equals the
TargetReached
status, see above.
- 0: Equals the
Counter Value Chunk#
If this chunk is available and enabled, the camera appends the current value of the camera's counter to every image.
- On ace 2, boost, and dart R cameras, the
ChunkCounterSelector
parameter is available. It allows you to choose which counter to retrieve data from. To do so, set the parameter toCounter1
orCounter2
. - On other cameras, the camera always retrieves the current value of Counter 1, which counts the number of acquired images.
Exposure Time Chunk#
If this chunk is enabled, the camera appends the exposure time used for image acquisition to every image.
The data chunk includes the ExposureTime
parameter value.
Info
When using the Trigger Width exposure mode on ace Classic/U/L cameras, the Exposure Time chunk feature is not available.
Focus Indicator Chunk#
If this chunk is available and enabled, the camera appends a value indicating the level of focus in every acquired image.
The value can range from 0.0 to 4095.0. A higher value indicates a higher level of focus. Calculations are based on a 5x5 sharpness detection algorithm.
A typical use case of the focus indicator chunk would be to monitor changes in the chunk value while the lens is being focused. For example, if the value after continuously increasing starts to decrease, this may indicate that a good level of focus has been reached.
Changes in the scene, e.g., increased brightness, will affect the chunk value. Therefore, while monitoring the chunk value, make sure that the target scene doesn't change.
Focus Indicator ROIs#
By default, the camera uses almost the full image ROI to calculate the level of focus.
You can change this and specify up to two parts of the sensor array that should be used to calculate the level of focus. Doing so is similar to setting up an auto function ROI. Two focus indicator ROIs are available.
To configure the focus indicator ROIs:
- Set the
BslFocusIndicatorROISelector
parameter to the desired focus indicator ROI, e.g.,ROI1
. - Set the
BslFocusIndicatorROIEnable
parameter totrue
to enable the focus indicator ROI selected.
By default, ROI 1 is enabled and ROI 2 is disabled. - Enter values for the following parameters to specify the position of the focus indicator ROI selected:
AutoFunctionROIOffsetX
(see note below)AutoFunctionROIOffsetY
- Enter values for the following parameters to specify the size of the focus indicator ROI selected:
AutoFunctionROIWidth
AutoFunctionROIHeight
Info
- The names of the above parameters start with
AutoFunctionROI
. This is because the focus indicator implementation is based on the Auto Function ROI feature. Nevertheless, you can use them to configure the focus indicator ROIs. - The minimum size of a focus indicator ROI is 9 x 5 pixels on mono cameras and 12 x 6 pixels on color cameras. If the ROI has less width or height or both, the focus indicator chunk will always be 0.0.
-
There must be at least 8 pixel space between the left and right side of the focus indicator ROI and the image ROI. Otherwise, the focus indicator ROI won't be fully effective.
Example: Assume you set theOffsetX
parameter of the image ROI to 4, and theAutoFunctionROIOffsetX
parameter of the focus indicator ROI to 5. There's not enough space for the focus indicator ROI to be fully effective:To solve this, set the
AutoFunctionROIOffsetX
parameter to at least 12:
Frame Counter Chunk#
If this chunk is available and enabled, the camera appends the number of acquired images to every image.
To do so, the camera retrieves the current value of the Counter 2 counter. On cameras with the Frame Counter chunk, Counter 2 counts the number of acquired images.
To manually reset the counter, reset Counter 2.
Info
Numbers in the counting sequence may be skipped when the acquisition mode is changed from Continuous to Single Frame. Numbers may also be skipped when overtriggering occurs.
Frame ID Chunk#
If this chunk is available and enabled, the camera appends the frame ID indicating the number of the image that has been exposed.
The frame ID starts at 0 and keeps incrementing by 1 for each exposed image until the camera is powered off. The maximum value is 2^48.
Gain Chunk (= GainAll Chunk)#
If this chunk is available and enabled, the camera appends the gain used for image acquisition to every image.
The data chunk includes the Gain
parameter value.
Line Status All Chunk#
If this chunk is enabled, the camera appends the status of all I/O lines at the moment when image acquisition was triggered to every image.
The data chunk includes the LineStatusAll
parameter value.
Payload CRC 16 Chunk#
If this chunk is enabled, the camera appends a CRC (Cyclic Redundancy Check) checksum to every image.
The checksum is calculated using the X-modem method and includes the image data and all appended chunks, if any, except the CRC chunk itself.
The CRC checksum chunk is always the last chunk appended to image data.
Sequencer Set Active Chunk (= Sequence Set Index Chunk)#
If this chunk is available and enabled, the camera appends the sequencer set used for image acquisition to every image.
The data chunk includes the SequencerSetActive
or SequenceSetIndex
parameter value (depending on your camera model).
Info
Enabling this chunk is only useful if the camera's Sequencer feature is used for image acquisition.
Timestamp Chunk#
If this chunk is enabled, the camera appends an internal timestamp (in ticks) of a certain event to every image.
-
On ace 2, boost, and dart R cameras, the parameter including the timestamp is named
BslChunkTimestampValue
.
Also, theBslChunkTimestampSelector
parameter is available, which allows you to choose the type of event that the timestamp should refer to:FrameStart
: TheBslChunkTimestampValue
parameter indicates when acquisition of the current image started.ExposureStart
: TheBslChunkTimestampValue
parameter indicates when exposure of the current image started. On rolling shutter cameras, the parameter indicates when exposure of the first row started.ExposureEnd
: TheBslChunkTimestampValue
parameter indicates when exposure of the current image ended. On rolling shutter cameras, this parameter serves no function and is preset to 0.
-
On other cameras, the parameter including the timestamp is named
ChunkTimestamp
. It always indicates when acquisition of the current image started.
Info
On ace 2, boost, and dart R cameras, the legacy ChunkTimestamp
parameter is also available. However, Basler recommends using the BslChunkTimestampValue
parameter instead.
Trigger Input Counter Chunk#
If this chunk is available and enabled, the camera appends the number of hardware frame start trigger signals received to every image.
To do so, the camera retrieves the current value of the Counter 1 counter. On cameras with the Trigger Input Counter chunk, Counter 1 counts the number of hardware trigger signals received.
Info
The trigger input counter only counts hardware trigger signals. If the camera is configured for software triggering or free run, the counter value will not increase.
Specifics#
Camera Model | Available Data Chunks |
---|---|
a2A640-240gmSWIR | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A640-240umSWIR | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1280-80gmSWIR | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1280-125umSWIR | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-51gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-51gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-51gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-51gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-160ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-160ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-160umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-160umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-165g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A1920-165g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2440-98g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2440-98g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-23gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-23gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-23gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-23gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-75ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-75ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-75umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-75umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-105g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2448-105g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-22gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-22gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-22gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-22gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-60ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-60ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-60umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2590-60umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-20gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-20gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-20gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-20gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-64ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-64ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-64umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2600-64umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-14gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-14gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-14gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-14gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-48ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-48ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-48umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-48umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-67g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A2840-67g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-13gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-13gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-13gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-13gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-45ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-45ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-45umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A3840-45umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-9gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-9gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-9gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-9gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-30ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-30ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-30umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-30umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-44g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4096-44g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-12gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-12gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-12gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-12gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-40ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-40ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-40umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4200-40umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-5gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-5gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-5gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-5gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-18ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-18ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-18umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-18umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-27g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4504-27g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-6gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-6gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-6gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-6gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-20ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-20ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-20umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A4508-20umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-7gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-7gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-7gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-7gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-23ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-23ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-23umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-23umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-34g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5320-34g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-4gcBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-4gcPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-4gmBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-4gmPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-15ucBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-15ucPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-15umBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-15umPRO | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-22g5cBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
a2A5328-22g5mBAS | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
acA640-121gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA640-300gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA640-300gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA640-750uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA640-750um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA720-290gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA720-290gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA720-520uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA720-520um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA800-200gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA800-200gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA800-510uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA800-510um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1280-60gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1280-60gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1300-60gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1300-60gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1300-60gmNIR | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1300-75gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1300-75gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1300-200uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1300-200um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1440-73gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1440-73gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1440-220uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1440-220um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1600-20gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1600-20uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1600-60gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1600-60gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-25gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-25gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-25uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA1920-25um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA1920-40gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-40gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-40uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1920-40ucMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1920-40um | Gain Chunk Exposure Time Chunk Timestamp Chunk Line Status All Chunk Counter Value Chunk CRC Checksum Chunk |
acA1920-40umMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1920-48gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-48gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-50gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-50gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA1920-150uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1920-150um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA1920-155uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA1920-155ucMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA1920-155um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA1920-155umMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2000-50gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2000-50gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2000-165uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2000-165um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2040-25gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2040-25gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2040-25gmNIR | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2040-35gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2040-35gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2040-55uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2040-55um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2040-90uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2040-90um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2040-90umNIR | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2040-120uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2040-120um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-20gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2440-20gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2440-35uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-35ucMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-35um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-35umMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-75uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-75ucMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-75um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2440-75umMED | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA2500-14gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2500-14gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2500-14uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2500-14um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2500-20gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2500-20gcMED | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2500-20gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2500-20gmMED | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA2500-60uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA2500-60um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Timestamp Chunk |
acA3088-16gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA3088-16gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA3088-57uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA3088-57ucMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Focus Indicator Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA3088-57um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA3088-57umMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Focus Indicator Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA3800-10gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA3800-10gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA3800-14uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA3800-14um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4024-8gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA4024-8gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA4024-29uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4024-29um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-11gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA4096-11gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA4096-30uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-30ucMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-30um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-30umMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-40uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-40ucMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-40um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4096-40umMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-8gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA4112-8gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA4112-20uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-20ucMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-20um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-20umMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-30uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-30ucMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-30um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA4112-30umMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA5472-5gc | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA5472-5gm | CRC Checksum Chunk Exposure Time Chunk Frame Counter Chunk Gain All Chunk Line Status All Chunk Sequence Set Index Chunk Timestamp Chunk Trigger Input Counter |
acA5472-17uc | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA5472-17ucMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Focus Indicator Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA5472-17um | Counter Value Chunk CRC Checksum Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
acA5472-17umMED | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Focus Indicator Chunk Gain Chunk Exposure Time Chunk Line Status All Chunk Sequencer Set Active Chunk Timestamp Chunk |
boA1936-400cc | Data Chunks feature not supported |
boA1936-400cm | Data Chunks feature not supported |
boA2448-250cc | Data Chunks feature not supported |
boA2448-250cm | Data Chunks feature not supported |
boA2832-190cc | Data Chunks feature not supported |
boA2832-190cm | Data Chunks feature not supported |
boA4096-93cc | Data Chunks feature not supported |
boA4096-93cm | Data Chunks feature not supported |
boA4096-180cc | Data Chunks feature not supported |
boA4096-180cm | Data Chunks feature not supported |
boA4112-68cc | Data Chunks feature not supported |
boA4112-68cm | Data Chunks feature not supported |
boA4500-45cc | Data Chunks feature not supported |
boA4500-45cm | Data Chunks feature not supported |
boA4504-100cc | Data Chunks feature not supported |
boA4504-100cm | Data Chunks feature not supported |
boA5120-150cc | Data Chunks feature not supported |
boA5120-150cm | Data Chunks feature not supported |
boA5120-230cc | Data Chunks feature not supported |
boA5120-230cm | Data Chunks feature not supported |
boA5320-150cc | Data Chunks feature not supported |
boA5320-150cm | Data Chunks feature not supported |
boA5328-100cc | Data Chunks feature not supported |
boA5328-100cm | Data Chunks feature not supported |
boA6500-36cc | Data Chunks feature not supported |
boA6500-36cm | Data Chunks feature not supported |
boA8100-16cc | Data Chunks feature not supported |
boA8100-16cm | Data Chunks feature not supported |
boA9344-30cc | Data Chunks feature not supported |
boA9344-30cm | Data Chunks feature not supported |
boA9344-70cc | Data Chunks feature not supported |
boA9344-70cm | Data Chunks feature not supported |
boA13440-17cm | Data Chunks feature not supported |
daA720-520uc | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA720-520um | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA1280-54uc | Data Chunks feature not supported |
daA1280-54um | Data Chunks feature not supported |
daA1440-220uc | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA1440-220um | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA1600-60uc | Data Chunks feature not supported |
daA1600-60um | Data Chunks feature not supported |
daA1920-15um | Data Chunks feature not supported |
daA1920-30uc | Data Chunks feature not supported |
daA1920-30um | Data Chunks feature not supported |
daA1920-160uc | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA1920-160um | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA2448-70uc | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA2448-70um | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA2500-14uc | Data Chunks feature not supported |
daA2500-14um | Data Chunks feature not supported |
daA3840-45uc | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
daA3840-45um | Auto Brightness Status Chunk Counter Value Chunk CRC Checksum Chunk Exposure Time Chunk Frame ID Chunk Gain Chunk Line Status All Chunk Timestamp Value Chunk |
puA1280-54uc | Data Chunks feature not supported |
puA1280-54um | Data Chunks feature not supported |
puA1600-60uc | Data Chunks feature not supported |
puA1600-60um | Data Chunks feature not supported |
puA1920-30uc | Data Chunks feature not supported |
puA1920-30um | Data Chunks feature not supported |
puA2500-14uc | Data Chunks feature not supported |
puA2500-14um | Data Chunks feature not supported |
Sample Code#
// Enable data chunks
camera.ChunkModeActive.SetValue(true);
// Select a chunk, e.g., the Exposure Time chunk
camera.ChunkSelector.SetValue(ChunkSelector_ExposureTime);
// Enable the selected chunk
camera.ChunkEnable.SetValue(true);
// Now, you must implement chunk retrieval in your application.
// For C++, C, and .NET sample implementations, see the "Grab_ChunkImage" and
// "Chunks" code samples in the pylon API Documentation
INodeMap& nodemap = camera.GetNodeMap();
// Enable data chunks
CBooleanParameter(nodemap, "ChunkModeActive").SetValue(true);
// Select a chunk, e.g., the Exposure Time chunk
CEnumParameter(nodemap, "ChunkSelector").SetValue("ExposureTime");
// Enable the selected chunk
CBooleanParameter(nodemap, "ChunkEnable").SetValue(true);
// Now, you must implement chunk retrieval in your application.
// For C++, C, and .NET sample implementations, see the "Grab_ChunkImage" and
// "Chunks" code samples in the pylon API Documentation
// Enable data chunks
camera.Parameters[PLCamera.ChunkModeActive].SetValue(true);
// Select a chunk, e.g., the Exposure Time chunk
camera.Parameters[PLCamera.ChunkSelector].SetValue(PLCamera.ChunkSelector.ExposureTime);
// Enable the selected chunk
camera.Parameters[PLCamera.ChunkEnable].SetValue(true);
// Now, you must implement chunk retrieval in your application.
// For C++, C, and .NET sample implementations, see the "Grab_ChunkImage" and
// "Chunks" code samples in the pylon API Documentation
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Enable data chunks */
errRes = PylonDeviceSetBooleanFeature(hdev, "ChunkModeActive", 1);
CHECK(errRes);
/* Select a chunk, e.g., the Exposure Time chunk */
errRes = PylonDeviceFeatureFromString(hdev, "ChunkSelector", "ExposureTime");
CHECK(errRes);
/* Enable the selected chunk */
errRes = PylonDeviceSetBooleanFeature(hdev, "ChunkEnable", 1);
CHECK(errRes);
/* Now, you must implement chunk retrieval in your application. */
/* For C++, C, and .NET sample implementations, see the "Grab_ChunkImage" and */
/* "Chunks" code samples in the pylon API Documentation */
# Enable data chunks
camera.ChunkModeActive.Value = True
# Select a chunk, e.g., the Exposure Time chunk
camera.ChunkSelector.Value = "ExposureTime"
# Enable the selected chunk
camera.ChunkEnable.Value = True
# Now, you must implement chunk retrieval in your application.
# For C++, C, and .NET sample implementations, see the "Grab_ChunkImage" and
# "Chunks" code samples in the pylon API Documentation
You can also use the pylon Viewer to easily set the parameters.