Skip to content

History#

Version 10#

  • Revised the Scaling feature and added information about the feature implementation on camera models with an integrated ISP.

Version 09#

  • Changed the brand name ON Semiconductor to onsemi.

Version 08 (March 2022)#

  • Corrected serial port configuration and pylon path in the daA4200-30mci-MX8MM-VAR topic.

Version 07 (January 2022)#

  • Revised the Installation topic to include generic software installation information.

Version 06 (December 2021)#

  • Added the prB-IMX8MP development kit.
  • Corrected pin names in the Output Voltages table of the BCON for MIPI Interface Description topic.
  • Removed the number of I/O lines from the specification tables of all BCON for MIPI camera models.
  • Removed the discontinued daA2500-14lc-MZ7010 Embedded Vision Kit from the documentation.

Version 05 (August 2021)#

  • Removed the discontinued daA2500-60mc-SD820-DB8 Embedded Vision Kit from the documentation.

Version 04 (July 2021)#

  • Added the Adaptive Tone Mapping camera feature topic.

Version 03 (May 2021)#

  • Added information about the daA3840-30mc camera model.

Version 02 (March 2021)#

  • Added the following camera feature topics:
    • Periodic Signal
    • Trigger Activation
    • Trigger Mode
    • Trigger Source
  • Moved the "Physical Interface" and "Electrical Requirements" sections from the BCON for MIPI camera topics to the BCON for MIPI Interface Description topic.

Version 01 (February 2021)#

Initial version of this documentation.

Content is based on the "Embedded Vision Kits" section of the Basler Product Documentation (AW001406), version 45, with the following changes:

  • Moved the Basler dart BCON for MIPI camera module documentation to this documentation.
  • Revised and restructured the BCON for MIPI camera module documentation.
  • Updated pin names and functions in all dart BCON for MIPI camera module topics.
  • Added information about external triggering and the NVIDIA Jetson Xavier NX developer board in the following Add-On Camera Kits topics:
    • daA2500-60mci-NVJET-NVDK-AddOn
    • daA4200-30mci-NVJET-NVDK-AddOn
    • daA4200-30mci-JNANO-NVDK