Skip to content

Event Notification#

The Event Notification camera feature allows you to enable camera events and event messages.

Using the Feature#

Enabling Event Notification#

  1. Set the EventSelector parameter to one of the following values (if available):
  2. Set the EventNotification parameter to On.
  3. Repeat steps 1 and 2 for all types of event notifications that you want to enable.
  4. Implement event handling in your application:
    • For a C++ sample implementation, see the "Grab_CameraEvents" and "Grab_CameraEvents_Usb" code samples in the C++ Programmer's Guide and Reference Documentation delivered with the Basler pylon Camera Software Suite.
    • For a C and C .NET sample implementation, see the "Events Sample" code sample in the C Programmer's Guide and Reference Documentation and the pylon C .NET Programmer's Guide and Reference Documentation delivered with the Basler pylon Camera Software Suite.

Info

  • Event messages are sent to the computer if there is sufficient bandwidth available. When the camera operates at high frame rates, event messages may be lost. There is no mechanism to monitor the number of event messages lost.
  • After the camera has sent an event message, it waits for an acknowledgement. If no acknowledgement is received within a specified time frame, the camera resends the event message. If an acknowledgement is still not received, the resend mechanism repeats until the maximum number of retries is reached. If this maximum number of retries is reached, the message is dropped. While the camera is waiting for an acknowledgement, no new event messages can be transmitted.
  • An event message is only useful when its cause still exists at the time when the event is received by the computer.

Available Events#

Action Late Event#

If available, the Action Late event occurs if the camera receives a scheduled action command with a timestamp in the past.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Critical Temperature Event#

If available, the Critical Temperature event occurs if the camera's temperature state has reached a critical level.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Event Overrun Event#

If available, the Event Overrun event (also called Overrun event) occurs if the camera's internal event queue has overrun. This happens if events are generated at a very high frequency and there isn't enough bandwidth available to send the events.

The event overrun event is a warning that events are being dropped. The notification contains no specific information about how many or which events have been dropped.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Exposure End Event#

The Exposure End event occurs whenever an image has been exposed.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated. Also, it contains a frame ID indicating the number of the image that has been exposed.

Frame Buffer Overrun Event#

If available, the Frame Buffer Overrun event occurs whenever frames were skipped because the camera's internal frame buffer was already full.

If the host controller doesn't retrieve the acquired images in time, the camera buffers images in its internal frame buffer. When the internal frame buffer is full, the camera will start skipping newly acquired sensor data.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Frame Burst Start (= Acquisition Start) Event#

Info

The Frame Burst Start event and the Acquisition Start event are identical, only their names differ. The naming depends on your camera model. See the list of available events.
In the following, the term "Frame Burst Start event" refers to both.

If available, the Frame Burst Start event occurs whenever a Frame Burst Start trigger has been generated by the camera (free run) or applied externally (triggered image acquisition).

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Frame Burst Start Overtrigger (= Acquisition Start Overtrigger) Event#

Info

The Frame Burst Start Overtrigger event and the Acquisition Start Overtrigger event are identical, only their names differ. The naming depends on your camera model. See the list of available events.
In the following, the term "Frame Burst Start Overtrigger event" refers to both.

If available, the Frame Burst Start Overtrigger event occurs whenever the Frame Burst Start trigger has been overtriggered. This happens if you apply a Frame Burst Start trigger signal when the camera is not ready to receive the signal.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Frame Burst Start Wait (= Acquisition Start Wait) Event#

Info

The Frame Burst Start Wait event and the Acquisition Start Wait event are identical, only their names differ. The naming depends on your camera model. See the list of available events.
In the following, the term "Frame Burst Start Wait event" refers to both.

If available, the Frame Burst Start Wait event occurs whenever the camera is ready to receive a Frame Burst Start trigger signal.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Frame Start Event#

The Frame Start event occurs whenever a Frame Start trigger has been generated by the camera (free run) or applied externally (triggered image acquisition).

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Frame Start Overtrigger Event#

If available, the Frame Start Overtrigger event occurs whenever the Frame Start trigger has been overtriggered. This happens if you apply a Frame Start trigger signal when the camera is not ready to receive the signal.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Frame Start Wait Event#

If available, the Frame Start Wait event occurs whenever the camera is ready to receive a Frame Start trigger signal.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Frame Trigger Missed Event#

This event is identical to the Frame Start Overtrigger event, only the name differs.

Over Temperature Event#

If available, the Over Temperature event occurs if the camera's temperature state has reached the over temperature level.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

Temperature Status Changed Event#

If available, the Temperature Status Changed event occurs whenever the camera's temperature state has changed.

When this event occurs, the corresponding message contains the EventTemperatureStatusChangedStatus parameter. This parameter indicates the new temperature status that applies after the event was raised:

  • Ok: The temperature status changed to Ok.
  • Critical: The temperature status changed to Critical.
  • Error: The temperature status changed to Error.

Also, the corresponding message contains a timestamp indicating the time when the event was generated.

Test Event#

If available, the Test event allows you to test the Event Notification feature.

When this event occurs, the corresponding message contains a timestamp indicating the time when the event was generated.

To test event notification:

  1. Execute the TestEventGenerate command.
  2. Handle the Test event in your application.

Info

The Test event is always enabled. You don't need to enable it via the EventSelector parameter.

Specifics#

Show all camera models

Camera Model Available Events
a2A1920-51gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A1920-51gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A1920-51gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A1920-51gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A1920-160ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A1920-160ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A1920-160umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A1920-160umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-23gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-23gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-23gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-23gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-75ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-75ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-75umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2448-75umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-22gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-22gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-22gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-22gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-60ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-60ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-60umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2590-60umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-14gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-14gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-14gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-14gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-48ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-48ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-48umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A2840-48umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-13gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-13gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-13gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-13gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-45ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-45ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-45umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A3840-45umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-9gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-9gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-9gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-9gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-30ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-30ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-30umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4096-30umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-5gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-5gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-5gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-5gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-18ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-18ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-18umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A4504-18umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-7gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-7gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-7gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-7gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-23ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-23ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-23umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5320-23umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-4gcBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-4gcPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-4gmBAS Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-4gmPRO Action Late
Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-15ucBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-15ucPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-15umBAS Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
a2A5328-15umPRO Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
acA640-90gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA640-90gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA640-90uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA640-90um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA640-120gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA640-120gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA640-120uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA640-120um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA640-121gm Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA640-300gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA640-300gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA640-750uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA640-750um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA720-290gc Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA720-290gm Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA720-520uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA720-520um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA780-75gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA780-75gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA800-200gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA800-200gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA800-510uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA800-510um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1280-60gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1280-60gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-22gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-22gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-30gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-30gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-30uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA1300-30um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA1300-60gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-60gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-60gmNIR Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1300-75gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1300-75gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1300-200uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1300-200um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1440-73gc Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1440-73gm Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1440-220uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1440-220um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1600-20gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1600-20gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1600-20uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA1600-20um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA1600-60gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1600-60gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1920-25gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1920-25gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA1920-25uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA1920-25um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA1920-40gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1920-40gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1920-40uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-40ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-40um Frame Start
Frame Start Overtrigger
Frame Start Wait
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Exposure End
Critical Temperature
Over Temperature
acA1920-40umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-48gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1920-48gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1920-50gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1920-50gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA1920-150uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-150um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-155uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-155ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-155um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA1920-155umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2000-50gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2000-50gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2000-50gmNIR Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2000-165uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2000-165um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2000-165umNIR Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2040-25gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2040-25gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2040-25gmNIR Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2040-35gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2040-35gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2040-55uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2040-55um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2040-90uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2040-90um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2040-90umNIR Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2040-120uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2040-120um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-20gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2440-20gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2440-35uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-35ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-35um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-35umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-75uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-75ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-75um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2440-75umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2500-14gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2500-14gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA2500-14uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2500-14um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA2500-20gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2500-20gcMED Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2500-20gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2500-20gmMED Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature
Exposure End
Frame Start
Frame Start Overtrigger
Over Temperature
acA2500-60uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA2500-60um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA3088-16gc Acquisition Start
Acquisition Start Overtrigger
Critical Temperature (not used)
Event Overrun
Exposure End
Frame Start Overtrigger
Over Temperature (not used)
acA3088-16gm Acquisition Start
Acquisition Start Overtrigger
Critical Temperature (not used)
Event Overrun
Exposure End
Frame Start Overtrigger
Over Temperature (not used)
acA3088-57uc Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA3088-57ucMED Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA3088-57um Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA3088-57umMED Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA3800-10gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA3800-10gm Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA3800-14uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA3800-14um Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA4024-8gc Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature (not used)
Event Overrun
Exposure End
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA4024-8gm Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature (not used)
Event Overrun
Exposure End
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA4024-29uc Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA4024-29um Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA4096-11gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature (not used)
Frame Start
Frame Start Overtrigger
Exposure End
Over Temperature (not used)
acA4096-11gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature (not used)
Frame Start
Frame Start Overtrigger
Exposure End
Over Temperature (not used)
acA4096-30uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4096-30ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4096-30um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4096-30umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4096-40uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4096-40ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4096-40um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4096-40umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-8gc Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature (not used)
Frame Start
Frame Start Overtrigger
Exposure End
Over Temperature (not used)
acA4112-8gm Acquisition Start
Acquisition Start Overtrigger
Action Late
Critical Temperature (not used)
Frame Start
Frame Start Overtrigger
Exposure End
Over Temperature (not used)
acA4112-20uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-20ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-20um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-20umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-30uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-30ucMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-30um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4112-30umMED Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA4600-7gc Acquisition Start
Acquisition Start Overtrigger
Event Overrun
Exposure End
Frame Start
Frame Start Overtrigger
acA4600-10uc Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start
Frame Start Overtrigger
Frame Start Wait
acA5472-5gc Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature
Event Overrun
Exposure End
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA5472-5gm Acquisition Start
Acquisition Start Overtrigger
Acquisition Start Wait
Action Late
Critical Temperature
Event Overrun
Exposure End
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA5472-17uc Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA5472-17ucMED Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
acA5472-17um Critical Temperature
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature
acA5472-17umMED Critical Temperature (not used)
Exposure End
Frame Burst Start
Frame Burst Start Overtrigger
Frame Burst Start Wait
Frame Start Overtrigger
Frame Start Wait
Over Temperature (not used)
boA4096-93cc Event Notification feature not supported
boA4096-93cm Event Notification feature not supported
boA4112-68cc Event Notification feature not supported
boA4112-68cm Event Notification feature not supported
boA4500-45cc Event Notification feature not supported
boA4500-45cm Event Notification feature not supported
boA6500-36cc Event Notification feature not supported
boA6500-36cm Event Notification feature not supported
boA8100-16cc Event Notification feature not supported
boA8100-16cm Event Notification feature not supported
daA1280-54lc Event Notification feature not supported
daA1280-54lm Event Notification feature not supported
daA1280-54uc Event Notification feature not supported
daA1280-54um Event Notification feature not supported
daA1600-60lc Event Notification feature not supported
daA1600-60lm Event Notification feature not supported
daA1600-60uc Event Notification feature not supported
daA1600-60um Event Notification feature not supported
daA1920-15um Event Notification feature not supported
daA1920-30uc Event Notification feature not supported
daA1920-30um Event Notification feature not supported
daA1920-160uc Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
daA1920-160um Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
daA2500-14lc Event Notification feature not supported
daA2500-14lm Event Notification feature not supported
daA2500-14uc Event Notification feature not supported
daA2500-14um Event Notification feature not supported
daA3840-45uc Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
daA3840-45um Exposure End
Frame Buffer Overrun
Frame Start
Frame Trigger Missed
Overrun
Temperature Status Changed
Test
puA1280-54uc Event Notification feature not supported
puA1280-54um Event Notification feature not supported
puA1600-60uc Event Notification feature not supported
puA1600-60um Event Notification feature not supported
puA1920-30uc Event Notification feature not supported
puA1920-30um Event Notification feature not supported
puA2500-14uc Event Notification feature not supported
puA2500-14um Event Notification feature not supported

Sample Code#

// Enable the Exposure End event notification
camera.EventSelector.SetValue(EventSelector_ExposureEnd);
camera.EventNotification.SetValue(EventNotification_On);
// Enable the Critical Temperature event notification
camera.EventSelector.SetValue(EventSelector_CriticalTemperature);
camera.EventNotification.SetValue(EventNotification_On);
// Now, you must implement event handling in your application.
// For C++, C, and .NET sample implementations, see the "Grab_CameraEvents" and
// "Events" code samples in the Programmer's Guide and Reference Documentation
// delivered with the Basler pylon Camera Software Suite.
INodeMap& nodemap = camera.GetNodeMap();
// Enable the Exposure End event notification
CEnumParameter(nodemap, "EventSelector").SetValue("ExposureEnd");
CEnumParameter(nodemap, "EventNotification").SetValue("On");
// Enable the Critical Temperature event notification
CEnumParameter(nodemap, "EventSelector").SetValue("CriticalTemperature");
CEnumParameter(nodemap, "EventNotification").SetValue("On");
// Now, you must implement event handling in your application.
// For C++, C, and .NET sample implementations, see the "Grab_CameraEvents" and
// "Events" code samples in the Programmer's Guide and Reference Documentation
// delivered with the Basler pylon Camera Software Suite.
// Enable the Exposure End event notification
camera.Parameters[PLCamera.EventSelector].SetValue(PLCamera.EventSelector.ExposureEnd);
camera.Parameters[PLCamera.EventNotification].SetValue(PLCamera.EventNotification.On);
// Enable the Critical Temperature event notification
camera.Parameters[PLCamera.EventSelector].SetValue(PLCamera.EventSelector.CriticalTemperature);
camera.Parameters[PLCamera.EventNotification].SetValue(PLCamera.EventNotification.On);
// Now, you must implement event handling in your application.
// For C++, C, and .NET sample implementations, see the "Grab_CameraEvents" and
// "Events" code samples in the Programmer's Guide and Reference Documentation
// delivered with the Basler pylon Camera Software Suite.
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Enable the Exposure End event notification */
errRes = PylonDeviceFeatureFromString(hdev, "EventSelector", "ExposureEnd");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "EventNotification", "On");
CHECK(errRes);
/* Enable the Critical Temperature event notification */
errRes = PylonDeviceFeatureFromString(hdev, "EventSelector", "CriticalTemperature");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "EventNotification", "On");
CHECK(errRes);
/* Now, you must implement event handling in your application. */
/* For C++, C, and .NET sample implementations, see the "Grab_CameraEvents" and */
/* "Events" code samples in the Programmer's Guide and Reference Documentation */
/* delivered with the Basler pylon Camera Software Suite. */

You can also use the pylon Viewer to easily set the parameters.

Back to top