TTL Trigger Board
The TTL Trigger Board
- is a trigger extension board that can be used together with all frame grabbers of the microEnable 5 marathon and microEnable 5 ironman series.1
- provides an adaption to the TTL signal level.
- offers 8 input and 8 output signals for controlling cameras and peripheral devices.
- allows to synchronize multiple frame grabbers.
The I/O TTL Trigger Board is connected to the frame grabber via a 34-pin flat cable:
Installation within a host PC:
Production line using TTL Trigger Board (example):
Example: Frame grabber with attached TTL Trigger Board within a sample production line
|
Trigger System Documentation |
|
For detailed information on how you can use your Opto Trigger 5 for various tasks within a trigger system, refer to the Trigger System documentation. |
|
Applet-Specific Trigger Settings |
|
How the individual inputs and outputs of the trigger extension board are employed you can configure via the applet you are using. Please refer to the documentation of your specific applet. |