Gain Auto#
The pixel data for the auto function can come from one or multiple auto function ROIs.
If you want to use Gain Auto and Exposure Auto at the same time, use the Auto Function Profile feature to specify how the effects of both are balanced.
To adjust the gain manually, use the Gain feature.
Using the Feature#
Enabling or Disabling Gain Auto#
To enable or disable the Gain Auto auto function:
- Assign at least one auto function ROI to the Gain Auto auto function.
Make sure the auto function ROI overlaps the image ROI, either partially or completely. - Set the
GainAuto
parameter to one of the following operating modes:Once
: The camera adjusts the gain until the specified target brightness value has been reached. When this has been achieved, or after a maximum of 30 calculation cycles, the camera sets the auto function to [Off` and applies the gain resulting from the last calculation to all following images.Continuous
: The camera adjusts the gain continuously while images are being acquired.Off
: Disables the Gain Auto auto function. The gain remains at the value resulting from the last automatic or manual adjustment.
Info
When the camera is capturing images continuously, the auto function takes effect with a short delay. The first few images may not be affected by the auto function.
Specifying Lower and Upper Limits#
The auto function adjusts the Gain
parameter value within limits specified by you.
To change the limits, set the AutoGainLowerLimit
and the AutoGainUpperLimit
parameters to the desired values.
Example: Assume you have set the AutoGainLowerLimit
parameter to 2 and the AutoGainUpperLimit
parameter to 6. During the automatic adjustment process, the gain will never be lower than 2 and never higher than 6.
Specifying the Target Brightness Value#
The auto function adjusts the gain until a target brightness value, i.e., an average gray value, has been reached.
To specify the target value, use the AutoTargetBrightness
parameter.
Info
- The target value calculation does not include other image optimizations, e.g., Gamma. Depending on the image optimizations set, images output by the camera may have a significantly lower or higher average gray value than indicated by the target value.
- The camera also uses the
AutoTargetBrightness
parameter to control the Exposure Auto auto function. If you want to use Gain Auto and Exposure Auto at the same time, use the Auto Function Profile feature to specify how the effects of both are balanced. - On some camera models, you can use the Remove Parameter Limits feature to increase the target value parameter limits.
On Basler ace GigE camera models, you can also specify a Gray Value Adjustment Damping factor. On Basler dart and pulse camera models, you can specify a Brightness Adjustment Damping factor.
When a damping factor is used, the target value is reached more slowly.
Sample Code#
ace Classic/U/L GigE Cameras#
// Set the the Gain Auto auto function to its minimum lower limit
// and its maximum upper limit
double minLowerLimit = camera.AutoGainRawLowerLimit.GetMin();
double maxUpperLimit = camera.AutoGainRawUpperLimit.GetMax();
camera.AutoGainRawLowerLimit.SetValue(minLowerLimit);
camera.AutoGainRawUpperLimit.SetValue(maxUpperLimit);
// Specify the target value
camera.AutoTargetValue.SetValue(150);
// Select auto function ROI 1
camera.AutoFunctionAOISelector.SetValue(AutoFunctionAOISelector_AOI1);
// Enable the 'Intensity' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.AutoFunctionAOIUsageIntensity.SetValue(true);
// Enable Gain Auto by setting the operating mode to Continuous
camera.GainAuto.SetValue(GainAuto_Continuous);
INodeMap& nodemap = camera.GetNodeMap();
// Set the the Gain Auto auto function to its minimum lower limit
// and its maximum upper limit
double minLowerLimit = CFloatParameter(nodemap, "AutoGainRawLowerLimit").GetMin();
double maxUpperLimit = CFloatParameter(nodemap, "AutoGainRawUpperLimit").GetMax();
CFloatParameter(nodemap, "AutoGainRawLowerLimit").SetValue(minLowerLimit);
CFloatParameter(nodemap, "AutoGainRawUpperLimit").SetValue(maxUpperLimit);
// Specify the target value
CIntegerParameter(nodemap, "AutoTargetValue").SetValue(150);
// Select auto function ROI 1
CEnumParameter(nodemap, "AutoFunctionAOISelector").SetValue("AOI1");
// Enable the 'Intensity' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionAOIUsageIntensity").SetValue(true);
// Enable Gain Auto by setting the operating mode to Continuous
CEnumParameter(nodemap, "GainAuto").SetValue("Continuous");
// Set the the Gain Auto auto function to its minimum lower limit
// and its maximum upper limit
double minLowerLimit = camera.Parameters[PLCamera.AutoGainRawLowerLimit].GetMinimum();
double maxUpperLimit = camera.Parameters[PLCamera.AutoGainRawUpperLimit].GetMaximum();
camera.Parameters[PLCamera.AutoGainRawLowerLimit].SetValue(minLowerLimit);
camera.Parameters[PLCamera.AutoGainRawUpperLimit].SetValue(maxUpperLimit);
// Specify the target value
camera.Parameters[PLCamera.AutoTargetValue].SetValue(150);
// Select auto function ROI 1
camera.Parameters[PLCamera.AutoFunctionAOISelector].SetValue(PLCamera.AutoFunctionAOISelector.AOI1);
// Enable the 'Intensity' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionAOIUsageIntensity].SetValue(true);
// Enable Gain Auto by setting the operating mode to Continuous
camera.Parameters[PLCamera.GainAuto].SetValue(PLCamera.GainAuto.Continuous);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double minLowerLimit = 0;
double maxUpperLimit = 0;
/* Set the the Gain Auto auto function to its minimum lower limit */
/* and its maximum upper limit */
errRes = PylonDeviceGetFloatFeatureMin(hdev, "AutoGainRawLowerLimit", &minLowerLimit);
CHECK(errRes);
errRes = PylonDeviceGetFloatFeatureMax(hdev, "AutoGainRawUpperLimit", &maxUpperLimit);
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "AutoGainRawLowerLimit", minLowerLimit);
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "AutoGainRawUpperLimit", maxUpperLimit);
CHECK(errRes);
/* Specify the target value */
errRes = PylonDeviceSetIntegerFeature(hdev, "AutoTargetValue", 150);
CHECK(errRes);
/* Select auto function ROI 1 */
errRes = PylonDeviceFeatureFromString(hdev, "AutoFunctionAOISelector", "AOI1");
CHECK(errRes);
/* Enable the 'Intensity' auto function (Gain Auto + Exposure Auto) */
/* for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionAOIUsageIntensity", 1);
CHECK(errRes);
/* Enable Gain Auto by setting the operating mode to Continuous */
errRes = PylonDeviceFeatureFromString(hdev, "GainAuto", "Continuous");
CHECK(errRes);
Other Cameras#
// Set the the Gain Auto auto function to its minimum lower limit
// and its maximum upper limit
double minLowerLimit = camera.AutoGainLowerLimit.GetMin();
double maxUpperLimit = camera.AutoGainUpperLimit.GetMax();
camera.AutoGainLowerLimit.SetValue(minLowerLimit);
camera.AutoGainUpperLimit.SetValue(maxUpperLimit);
// Specify the target value
camera.AutoTargetBrightness.SetValue(0.6);
// Select auto function ROI 1
camera.AutoFunctionROISelector.SetValue(AutoFunctionROISelector_ROI1);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.AutoFunctionROIUseBrightness.SetValue(true);
// Enable Gain Auto by setting the operating mode to Continuous
camera.GainAuto.SetValue(GainAuto_Continuous);
INodeMap& nodemap = camera.GetNodeMap();
// Set the the Gain Auto auto function to its minimum lower limit
// and its maximum upper limit
double minLowerLimit = CFloatParameter(nodemap, "AutoGainLowerLimit").GetMin();
double maxUpperLimit = CFloatParameter(nodemap, "AutoGainUpperLimit").GetMax();
CFloatParameter(nodemap, "AutoGainLowerLimit").SetValue(minLowerLimit);
CFloatParameter(nodemap, "AutoGainUpperLimit").SetValue(maxUpperLimit);
// Specify the target value
CFloatParameter(nodemap, "AutoTargetBrightness").SetValue(0.6);
// Select auto function ROI 1
CEnumParameter(nodemap, "AutoFunctionROISelector").SetValue("ROI1");
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
CBooleanParameter(nodemap, "AutoFunctionROIUseBrightness").SetValue(true);
// Enable Gain Auto by setting the operating mode to Continuous
CEnumParameter(nodemap, "GainAuto").SetValue("Continuous");
// Set the the Gain Auto auto function to its minimum lower limit
// and its maximum upper limit
double minLowerLimit = camera.Parameters[PLCamera.AutoGainLowerLimit].GetMinimum();
double maxUpperLimit = camera.Parameters[PLCamera.AutoGainUpperLimit].GetMaximum();
camera.Parameters[PLCamera.AutoGainLowerLimit].SetValue(minLowerLimit);
camera.Parameters[PLCamera.AutoGainUpperLimit].SetValue(maxUpperLimit);
// Specify the target value
camera.Parameters[PLCamera.AutoTargetBrightness].SetValue(0.6);
// Select auto function ROI 1
camera.Parameters[PLCamera.AutoFunctionROISelector].SetValue(PLCamera.AutoFunctionROISelector.ROI1);
// Enable the 'Brightness' auto function (Gain Auto + Exposure Auto)
// for the auto function ROI selected
camera.Parameters[PLCamera.AutoFunctionROIUseBrightness].SetValue(true);
// Enable Gain Auto by setting the operating mode to Continuous
camera.Parameters[PLCamera.GainAuto].SetValue(PLCamera.GainAuto.Continuous);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double minLowerLimit = 0;
double maxUpperLimit = 0;
/* Set the the Gain Auto auto function to its minimum lower limit */
/* and its maximum upper limit */
errRes = PylonDeviceGetFloatFeatureMin(hdev, "AutoGainLowerLimit", &minLowerLimit);
CHECK(errRes);
errRes = PylonDeviceGetFloatFeatureMax(hdev, "AutoGainUpperLimit", &maxUpperLimit);
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "AutoGainLowerLimit", minLowerLimit);
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "AutoGainUpperLimit", maxUpperLimit);
CHECK(errRes);
/* Specify the target value */
errRes = PylonDeviceSetFloatFeature(hdev, "AutoTargetBrightness", 0.6);
CHECK(errRes);
/* Select auto function ROI 1 */
errRes = PylonDeviceFeatureFromString(hdev, "AutoFunctionROISelector", "ROI1");
CHECK(errRes);
/* Enable the 'Brightness' auto function (Gain Auto + Exposure Auto) */
/* for the auto function ROI selected */
errRes = PylonDeviceSetBooleanFeature(hdev, "AutoFunctionROIUseBrightness", 1);
CHECK(errRes);
/* Enable Gain Auto by setting the operating mode to Continuous */
errRes = PylonDeviceFeatureFromString(hdev, "GainAuto", "Continuous");
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.