Gain#
Increasing the gain increases all pixel values of the images.
To adjust the gain value automatically, use the Gain Auto feature.
Using the Feature#
Analog and Digital Gain#
The gain is an amplification factor applied to all pixel values of the acquired images. There are different types of gains:
- Analog gain is applied before the signal from the camera sensor is converted into digital values.
- Digital gain is applied after the conversion, i.e., it is basically a multiplication of the digitized values.
Depending on your camera model, the mechanisms to control the gain can vary:
- For some cameras, gain control is analog up to and including a certain threshold. Above the threshold, gain control is digital.
- For some cameras, gain control is entirely digital or analog.
- For some cameras, you can use the
GainSelector
parameter to manually switch between analog and digital gain.
Choosing the Gain Type#
On some camera models, the GainSelector
parameter is available. This parameter allows you to apply a universal gain, which can be analog, digital, or both, depending on your camera model and the sensor used. The GainSelector
parameter also allows you to manually switch between analog and digital gain (if available).
On racer 2 L cameras, the GainSelector
parameter can be used to apply the gain to a specific sensor line if the camera is operated in Dual Line sensor acquisition mode.
You can set the GainSelector
parameter to one of the following values, if available:
All
: A universal gain is applied.AnalogAll
: An analog gain is applied.DigitalAll
: A digital gain is applied.Line1
: A digital gain is applied to line 1.Line2
: A digital gain is applied to line 2.
Info
For racer 2 L cameras, consider the following:
- The gain value specified for line 2 only becomes effective if the Dual Line sensor acquisition mode is enabled.
- The gain value finally applied to line 1 and line 2 is the sum of the gain value specified for
All
plus the gain value specified forLine1
orLine2
respectively.
Conversion Gain Mode#
On a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras, the BslConversionGainMode
parameter is available. It allows you to select one of the following conversion gain modes:
High
: Enables the High Conversion Gain (HCG) mode.
HCG helps to improve image quality in low light conditions. The sensitivity is increased and the readout noise reduced, which results in an improved signal-to-noise ratio, but a lower dynamic range.Low
: Enables the Low Conversion Gain (LCG) mode.
LCG is recommended for normal to bright light conditions. The saturation capacity is increased and the dynamic range is higher.
"Raw" and Absolute Gain Values#
On some camera models, the gain must be entered as a "raw" value on an integer scale. The camera needs the raw value for its internal processing mechanism. The raw value, however, isn't the same as the actual gain value, which is expressed in decibels (dB).
In the camera-specific Gain Properties table, you can find a formula to calculate the absolute gain (in dB) from the raw gain value.
Additional Parameters#
On boA13440-17cm cameras, the BslGainTopLeft
, BslGainTopRight
, BslGainBottomLeft
, and BslGainBottomRight
parameters are available. You can use these parameters to increase the brightness individually in each of the four quadrants of the image. This can be useful to compensate for differences in the image brightness.
The brightness in each quadrant can be increased linearly by up to 5 % (digital gain).
Setting the Gain#
- Set the
GainAuto
parameter toOff
. - If available, set the
GainSelector
parameter to the desired gain type, e.g.,All
. - If available, set the
BslConversionGain
parameter to the desired conversion gain mode, e.g.,High
. - Set the
Gain
parameter to the desired value.
The minimum and maximum parameter values vary depending on the camera model, the pixel format chosen, and the Binning settings.
Specifics#
Gain Properties#
Camera Model | Gain Control Mechanism | Threshold | Gain Must be Entered as | Formula to Calculate Gain from Raw Gain Values |
---|---|---|---|---|
a2A640-240gmSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A640-240umSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1280-80gmSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1280-125umSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-51gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-51gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-51gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-51gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-160ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-160ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-160umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-160umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-165g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A1920-165g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-35gmSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-37gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-37gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-37gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-37gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-110umSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-114g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-114g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-114ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-114ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-114umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2048-114umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2440-98g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2440-98g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-23gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-23gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-23gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-23gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-75ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-75ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-75umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-75umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-105g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-105g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-120cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-120cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-210cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2448-210cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2560-20gmSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2560-70umSWIR | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2590-22gcBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2590-22gcPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2590-22gmBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2590-22gmPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2590-60ucBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2590-60ucPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2590-60umBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2590-60umPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A2600-20gcBAS | Digital gain only | 0 | dB | N/A |
a2A2600-20gcPRO | Digital gain only | 0 | dB | N/A |
a2A2600-20gmBAS | Digital gain only | 0 | dB | N/A |
a2A2600-20gmPRO | Digital gain only | 0 | dB | N/A |
a2A2600-64ucBAS | Digital gain only | 0 | dB | N/A |
a2A2600-64ucPRO | Digital gain only | 0 | dB | N/A |
a2A2600-64umBAS | Digital gain only | 0 | dB | N/A |
a2A2600-64umPRO | Digital gain only | 0 | dB | N/A |
a2A2840-14gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-14gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-14gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-14gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-14gmUV | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-48ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-48ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-48umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-48umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-48umUV | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-67g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-67g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-67g5mUV | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-86cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A2840-86cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A3536-9gcBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-9gcPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-9gmBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-9gmPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-31ucBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-31ucPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-31umBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-31umPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-42g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3536-42g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-13gcBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-13gcPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-13gmBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-13gmPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-45ucBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-45ucPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-45umBAS | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A3840-45umPRO | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
a2A4096-9gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-9gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-9gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-9gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-30ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-30ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-30umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-30umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-44g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-44g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-67cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4096-67cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4200-12gcBAS | Digital gain only | 0 | dB | N/A |
a2A4200-12gcPRO | Digital gain only | 0 | dB | N/A |
a2A4200-12gmBAS | Digital gain only | 0 | dB | N/A |
a2A4200-12gmPRO | Digital gain only | 0 | dB | N/A |
a2A4200-40ucBAS | Digital gain only | 0 | dB | N/A |
a2A4200-40ucPRO | Digital gain only | 0 | dB | N/A |
a2A4200-40umBAS | Digital gain only | 0 | dB | N/A |
a2A4200-40umPRO | Digital gain only | 0 | dB | N/A |
a2A4504-5gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-5gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-5gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-5gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-18ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-18ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-18umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-18umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-27g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-27g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-42cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4504-42cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A4508-6gcBAS | Digital gain only | 0 | dB | N/A |
a2A4508-6gcPRO | Digital gain only | 0 | dB | N/A |
a2A4508-6gmBAS | Digital gain only | 0 | dB | N/A |
a2A4508-6gmPRO | Digital gain only | 0 | dB | N/A |
a2A4508-20ucBAS | Digital gain only | 0 | dB | N/A |
a2A4508-20ucPRO | Digital gain only | 0 | dB | N/A |
a2A4508-20umBAS | Digital gain only | 0 | dB | N/A |
a2A4508-20umPRO | Digital gain only | 0 | dB | N/A |
a2A5060-4gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5060-4gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5060-15ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5060-15umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5060-21g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5060-21g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-7gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-7gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-7gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-7gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-23ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-23ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-23umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-23umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-34g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-34g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-52cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5320-52cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-4gcBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-4gcPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-4gmBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-4gmPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-15ucBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-15ucPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-15umBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-15umPRO | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-22g5cBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-22g5mBAS | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-35cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
a2A5328-35cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA640-121gm | Above the threshold, analog gain automatically switches to digital gain | N/A | Raw | Gain = 0.0359 * GainRaw (Sony ICX618 replacement) |
acA640-300gc | Digital Control only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA640-300gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA640-750uc | Digital gain only | - | dB | N/A |
acA640-750um | Digital gain only | - | dB | N/A |
acA720-290gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA720-290gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA720-520uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA720-520um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA800-200gc | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA800-200gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA800-510uc | Digital gain only | - | dB | N/A |
acA800-510um | Digital gain only | - | dB | N/A |
acA1280-60gc | Gain control settable via GainSelector parameter. | - | Raw | Analog Gain: - Gain is 0 when GainRaw is set to 0 - Gain is 3.5 when GainRaw is set to 1 - Gain is 6 when GainRaw is set to 2 - Gain is 9.5 when GainRaw is set to 3 Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32 - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32 |
acA1280-60gm | Gain control settable via GainSelector parameter. | - | Raw | Analog Gain: - Gain is 0 when GainRaw is set to 0 - Gain is 3.5 when GainRaw is set to 1 - Gain is 6 when GainRaw is set to 2 - Gain is 9.5 when GainRaw is set to 3 Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32 - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32 |
acA1300-60gc | Gain control settable via GainSelector parameter. | - | Raw | Analog Gain: - Gain is 0 when GainRaw is set to 0 - Gain is 3.5 when GainRaw is set to 1 - Gain is 6 when GainRaw is set to 2 - Gain is 9.5 when GainRaw is set to 3 Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32 - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32 |
acA1300-60gm | Gain control settable via GainSelector parameter. | - | Raw | Analog Gain: - Gain is 0 when GainRaw is set to 0 - Gain is 3.5 when GainRaw is set to 1 - Gain is 6 when GainRaw is set to 2 - Gain is 9.5 when GainRaw is set to 3 Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32 - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32 |
acA1300-60gmNIR | Gain control settable via GainSelector parameter. | - | Raw | Analog Gain: - Gain is 0 when GainRaw is set to 0 - Gain is 3.5 when GainRaw is set to 1 - Gain is 6 when GainRaw is set to 2 - Gain is 9.5 when GainRaw is set to 3 Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32 - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32 |
acA1300-75gc | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA1300-75gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA1300-200uc | Digital gain only | - | dB | N/A |
acA1300-200um | Digital gain only | - | dB | N/A |
acA1440-73gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA1440-73gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA1440-220uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1440-220um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1600-20gc | Above the threshold, analog gain automatically switches to digital gain | 511 | Raws | Gain = 0.0359 * GainRaw |
acA1600-20uc | Above the threshold, analog gain automatically switches to digital gain | 10.1 | dB | N/A |
acA1600-60gc | Gain control settable via GainSelector parameter | - | Raw | Analog Gain: - Gain is 3.5 when GainRaw is set to 1 - Gain is 6 when GainRaw is set to 2 - Gain is 9.5 when GainRaw is set to 3 Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32 - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32 |
acA1600-60gm | Gain control settable via GainSelector parameter | - | Raw | Analog Gain: - Gain is 3.5 when GainRaw is set to 1 - Gain is 6 when GainRaw is set to 2 - Gain is 9.5 when GainRaw is set to 3 Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32 - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32 |
acA1920-25gc | Above the threshold, analog gain automatically switches to digital gain | 19 | Raw | See this graph for approximate values. |
acA1920-25gm | Above the threshold, analog gain automatically switches to digital gain | 19 | Raw | See this graph for approximate values. |
acA1920-25uc | Digital gain only | - | dB | N/A |
acA1920-25um | Digital gain only | - | dB | N/A |
acA1920-40gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA1920-40gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA1920-40uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1920-40ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1920-40um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1920-40umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1920-48gc | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA1920-48gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA1920-50gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA1920-50gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA1920-150uc | Digital gain only | - | dB | N/A |
acA1920-150um | Digital gain only | - | dB | N/A |
acA1920-155uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1920-155ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1920-155um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA1920-155umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2000-50gc | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 32) |
acA2000-50gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 32) |
acA2000-165uc | Digital gain only | - | dB | N/A |
acA2000-165um | Digital gain only | - | dB | N/A |
acA2040-25gc | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 32) |
acA2040-25gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 32) |
acA2040-25gmNIR | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 32) |
acA2040-35gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA2040-35gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA2040-55uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2040-55um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2040-90uc | Digital gain only | - | dB | N/A |
acA2040-90um | Digital gain only | - | dB | N/A |
acA2040-90umNIR | Digital gain only | - | dB | N/A |
acA2040-120uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2040-120um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-20gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA2440-20gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA2440-35uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-35ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-35um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-35umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-75uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-75ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-75um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2440-75umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA2500-14gc | Above the threshold, analog gain automatically switches to digital gain | 19 | Raw | See this graph for approximate values. |
acA2500-14gm | Above the threshold, analog gain automatically switches to digital gain | 19 | Raw | See this graph for approximate values. |
acA2500-14uc | Digital gain only | - | dB | N/A |
acA2500-14um | Digital gain only | - | dB | N/A |
acA2500-20gc | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA2500-20gcMED | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA2500-20gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA2500-20gmMED | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 136) |
acA2500-60uc | Digital gain only | - | dB | N/A |
acA2500-60um | Digital gain only | - | dB | N/A |
acA3088-16gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA3088-16gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA3088-57uc | Analog gain only | - | dB | N/A |
acA3088-57ucMED | Analog gain only | - | dB | N/A |
acA3088-57um | Analog gain only | - | dB | N/A |
acA3088-57umMED | Analog gain only | - | dB | N/A |
acA3800-10gc | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 32) |
acA3800-10gm | Digital gain only | - | Raw | Gain = 20 * log10 (GainRaw / 32) |
acA3800-14uc | Digital gain only | - | dB | N/A |
acA3800-14um | Digital gain only | - | dB | N/A |
acA4024-8gc | Analog gain only | - | Raw | Gain = -20 * log10 ((2048-GainRaw) / 2048) |
acA4024-8gm | Analog gain only | - | Raw | Gain = -20 * log10 ((2048-GainRaw) / 2048) |
acA4024-29uc | Analog gain only | - | dB | N/A |
acA4024-29um | Analog gain only | - | dB | N/A |
acA4096-11gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA4096-11gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA4096-30uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4096-30ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4096-30um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4096-30umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4096-40uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4096-40ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4096-40um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4096-40umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-8gc | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA4112-8gm | Above the threshold, analog gain automatically switches to digital gain | 240 | Raw | Gain = 0.1 * GainRaw |
acA4112-20uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-20ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-20um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-20umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-30uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-30ucMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-30um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA4112-30umMED | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
acA5472-5gc | Analog gain only | - | Raw | Gain = -20 * log10 ((2048-GainRaw) / 2048) |
acA5472-5gm | Analog gain only | - | Raw | Gain = -20 * log10 ((2048-GainRaw) / 2048) |
acA5472-17uc | Analog gain only | - | dB | N/A |
acA5472-17ucMED | Analog gain only | - | dB | N/A |
acA5472-17um | Analog gain only | - | dB | N/A |
acA5472-17umMED | Analog gain only | - | dB | N/A |
boA1936-400cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA1936-400cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA2448-250cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA2448-250cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA2832-190cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA2832-190cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4096-93cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4096-93cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4096-180cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4096-180cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4112-68cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4112-68cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4500-45cc | Combination of analog and digital gain | - | dB | N/A |
boA4500-45cm | Combination of analog and digital gain | - | dB | N/A |
boA4504-100cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA4504-100cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA5120-150cc | Digital gain only | - | dB | N/A |
boA5120-150cm | Digital gain only | - | dB | N/A |
boA5120-230cc | Digital gain only | - | dB | N/A |
boA5120-230cm | Digital gain only | - | dB | N/A |
boA5320-150cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA5320-150cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA5328-100cc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA5328-100cm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
boA6500-36cc | Combination of analog and digital gain | - | dB | N/A |
boA6500-36cm | Combination of analog and digital gain | - | dB | N/A |
boA8100-16cc | Combination of analog and digital gain | - | dB | N/A |
boA8100-16cm | Combination of analog and digital gain | - | dB | N/A |
boA9344-30cc | Digital gain only | - | dB | N/A |
boA9344-30cm | Digital gain only | - | dB | N/A |
boA9344-70cc | Digital gain only | - | dB | N/A |
boA9344-70cm | Digital gain only | - | dB | N/A |
boA13440-17cm | Analog gain only | - | dB | N/A |
daA720-520uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA720-520um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA1280-54uc | Digital gain only | - | dB | N/A |
daA1280-54um | Digital gain only | - | dB | N/A |
daA1440-220uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA1440-220um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA1600-60uc | Digital gain only | - | dB | N/A |
daA1600-60um | Digital gain only | - | dB | N/A |
daA1920-15um | Digital gain only | - | dB | N/A |
daA1920-30uc | Digital gain only | - | dB | N/A |
daA1920-30um | Digital gain only | - | dB | N/A |
daA1920-160uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA1920-160um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA2448-70uc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA2448-70um | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
daA2500-14uc | Digital gain only | - | dB | N/A |
daA2500-14um | Digital gain only | - | dB | N/A |
daA3840-45uc | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
daA3840-45um | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
dmA720-290gc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA720-290gm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA1440-73gc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA1440-73gm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA1920-51gc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA1920-51gm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA2448-23gc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA2448-23gm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA2840-14gc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA2840-14gm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA3536-9gc | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
dmA3536-9gm | Above the threshold, analog gain automatically switches to digital gain | 30 | dB | N/A |
dmA4096-9gc | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
dmA4096-9gm | Above the threshold, analog gain automatically switches to digital gain | 24 | dB | N/A |
puA1280-54uc | Digital gain only | - | dB | N/A |
puA1280-54um | Digital gain only | - | dB | N/A |
puA1600-60uc | Digital gain only | - | dB | N/A |
puA1600-60um | Digital gain only | - | dB | N/A |
puA1920-30uc | Digital gain only | - | dB | N/A |
puA1920-30um | Digital gain only | - | dB | N/A |
puA2500-14uc | Digital gain only | - | dB | N/A |
puA2500-14um | Digital gain only | - | dB | N/A |
r2L2048-29gc | Digital gain only | - | dB | N/A |
r2L2048-58gm | Digital gain only | - | dB | N/A |
r2L2048-62cc | Digital gain only | - | dB | N/A |
r2L2048-62g5c | Digital gain only | - | dB | N/A |
r2L2048-172cm | Digital gain only | - | dB | N/A |
r2L2048-172g5m | Digital gain only | - | dB | N/A |
r2L4096-14gc | Digital gain only | - | dB | N/A |
r2L4096-29gm | Digital gain only | - | dB | N/A |
r2L4096-42cc | Digital gain only | - | dB | N/A |
r2L4096-42g5c | Digital gain only | - | dB | N/A |
r2L4096-84cm | Digital gain only | - | dB | N/A |
r2L4096-84g5m | Digital gain only | - | dB | N/A |
r2L8192-200cm | Digital gain only | - | dB | N/A |
r2L16384-120cm | Digital gain only | - | dB | N/A |
Gain Values#
Info
On some camera models, you can use the Remove Parameter Limits feature to increase the gain parameter limits.
Camera Model | Minimum Gain Setting | Minimum Gain Setting with Vertical Binning Enabled | Maximum Gain Setting (8-bit Pixel Formats) | Maximum Gain Setting (10-bit Pixel Formats) | Maximum Gain Setting (12-bit Pixel Formats) |
---|---|---|---|---|---|
a2A640-240gmSWIR | 0 | 0 | 42 | 42 | 42 |
a2A640-240umSWIR | 0 | 0 | 42 | 42 | 42 |
a2A1280-80gmSWIR | 0 | 0 | 42 | 42 | 42 |
a2A1280-125umSWIR | 0 | 0 | 42 | 42 | 42 |
a2A1920-51gcBAS | 0 | - | 48 | 48 | 48 |
a2A1920-51gcPRO | 0 | - | 48 | 48 | 48 |
a2A1920-51gmBAS | 0 | 0 | 48 | 48 | 48 |
a2A1920-51gmPRO | 0 | 0 | 48 | 48 | 48 |
a2A1920-160ucBAS | 0 | - | 48 | 48 | 48 |
a2A1920-160ucPRO | 0 | - | 48 | 48 | 48 |
a2A1920-160umBAS | 0 | 0 | 48 | 48 | 48 |
a2A1920-160umPRO | 0 | 0 | 48 | 48 | 48 |
a2A1920-165g5cBAS | 0 | - | 48 | 48 | 48 |
a2A1920-165g5mBAS | 0 | 0 | 48 | 48 | 48 |
a2A2048-35gmSWIR | 0 | 0 | 42 | 42 | 42 |
a2A2048-37gcBAS | 0 | - | - | 48 | 48 |
a2A2048-37gcPRO | 0 | - | - | 48 | 48 |
a2A2048-37gmBAS | 0 | 0 | 48 | - | 48 |
a2A2048-37gmPRO | 0 | 0 | 48 | - | 48 |
a2A2048-110umSWIR | 0 | 0 | 42 | 42 | 42 |
a2A2048-114g5cBAS | 0 | - | - | 48 | 48 |
a2A2048-114g5mBAS | 0 | 0 | 48 | - | 48 |
a2A2048-114ucBAS | 0 | - | - | 48 | 48 |
a2A2048-114ucPRO | 0 | - | - | 48 | 48 |
a2A2048-114umBAS | 0 | 0 | 48 | - | 48 |
a2A2048-114umPRO | 0 | 0 | 48 | - | 48 |
a2A2440-98g5cBAS | 0 | - | 48 | 48 | 48 |
a2A2440-98g5mBAS | 0 | 0 | 48 | 48 | 48 |
a2A2448-23gcBAS | 0 | - | - | 48 | 48 |
a2A2448-23gcPRO | 0 | - | - | 48 | 48 |
a2A2448-23gmBAS | 0 | 0 | 48 | - | 48 |
a2A2448-23gmPRO | 0 | 0 | 48 | - | 48 |
a2A2448-75ucBAS | 0 | - | - | 48 | 48 |
a2A2448-75ucPRO | 0 | - | - | 48 | 48 |
a2A2448-75umBAS | 0 | 0 | 48 | - | 48 |
a2A2448-75umPRO | 0 | 0 | 48 | - | 48 |
a2A2448-105g5cBAS | 0 | - | - | 48 | 48 |
a2A2448-105g5mBAS | 0 | 0 | 48 | - | 48 |
a2A2448-120cc | 0 | - | 48 | 48 | 48 |
a2A2448-120cm | 0 | 0 | 48 | 48 | 48 |
a2A2448-210cc | 0 | - | 48 | 48 | 48 |
a2A2448-210cm | 0 | 0 | 48 | 48 | 48 |
a2A2560-20gmSWIR | 0 | 0 | 42 | 42 | 42 |
a2A2560-70umSWIR | 0 | 0 | 42 | 42 | 42 |
a2A2590-22gcBAS | 0 | - | 48 | 48 | 48 |
a2A2590-22gcPRO | 0 | - | 48 | 48 | 48 |
a2A2590-22gmBAS | 0 | 0 | 48 | 48 | 48 |
a2A2590-22gmPRO | 0 | 0 | 48 | 48 | 48 |
a2A2590-60ucBAS | 0 | - | 48 | 48 | 48 |
a2A2590-60ucPRO | 0 | - | 48 | 48 | 48 |
a2A2590-60umBAS | 0 | 0 | 48 | 48 | 48 |
a2A2590-60umPRO | 0 | 0 | 48 | 48 | 48 |
a2A2600-20gcBAS | 0 | - | 36 | 36 | 36 |
a2A2600-20gcPRO | 0 | - | 36 | 36 | 36 |
a2A2600-20gmBAS | 0 | 0 | 36 | 36 | 36 |
a2A2600-20gmPRO | 0 | 0 | 36 | 36 | 36 |
a2A2600-64ucBAS | 0 | - | 36 | 36 | 36 |
a2A2600-64ucPRO | 0 | - | 36 | 36 | 36 |
a2A2600-64umBAS | 0 | 0 | 36 | 36 | 36 |
a2A2600-64umPRO | 0 | 0 | 36 | 36 | 36 |
a2A2840-14gcBAS | 0 | - | - | 48 | 48 |
a2A2840-14gcPRO | 0 | - | - | 48 | 48 |
a2A2840-14gmBAS | 0 | 0 | 48 | - | 48 |
a2A2840-14gmPRO | 0 | 0 | 48 | - | 48 |
a2A2840-14gmUV | 0 | 0 | 48 | 48 | 48 |
a2A2840-48ucBAS | 0 | - | - | 48 | 48 |
a2A2840-48ucPRO | 0 | - | - | 48 | 48 |
a2A2840-48umBAS | 0 | 0 | 48 | - | 48 |
a2A2840-48umPRO | 0 | 0 | 48 | - | 48 |
a2A2840-48umUV | 0 | 0 | 48 | 48 | 48 |
a2A2840-67g5cBAS | 0 | - | - | 48 | 48 |
a2A2840-67g5mBAS | 0 | 0 | 48 | - | 48 |
a2A2840-67g5mUV | 0 | 0 | 48 | 48 | 48 |
a2A2840-86cc | 0 | - | 48 | 48 | 48 |
a2A2840-86cm | 0 | 0 | 48 | - | 48 |
a2A3536-9gcBAS | 0 | - | 48 | 48 | 48 |
a2A3536-9gcPRO | 0 | - | 48 | 48 | 48 |
a2A3536-9gmBAS | 0 | 0 | 48 | 48 | 48 |
a2A3536-9gmPRO | 0 | 0 | 48 | 48 | 48 |
a2A3536-31ucBAS | 0 | - | 48 | 48 | 48 |
a2A3536-31ucPRO | 0 | - | 48 | 48 | 48 |
a2A3536-31umBAS | 0 | 0 | 48 | 48 | 48 |
a2A3536-31umPRO | 0 | 0 | 48 | 48 | 48 |
a2A3536-42g5cBAS | 0 | - | 48 | 48 | 48 |
a2A3536-42g5mBAS | 0 | 0 | 48 | 48 | 48 |
a2A3840-13gcBAS | 0 | - | 48 | 48 | 48 |
a2A3840-13gcPRO | 0 | - | 48 | 48 | 48 |
a2A3840-13gmBAS | 0 | 0 | 48 | 48 | 48 |
a2A3840-13gmPRO | 0 | 0 | 48 | 48 | 48 |
a2A3840-45ucBAS | 0 | - | 48 | 48 | 48 |
a2A3840-45ucPRO | 0 | - | 48 | 48 | 48 |
a2A3840-45umBAS | 0 | 0 | 48 | 48 | 48 |
a2A3840-45umPRO | 0 | 0 | 48 | 48 | 48 |
a2A4096-9gcBAS | 0 | - | - | 48 | 48 |
a2A4096-9gcPRO | 0 | - | - | 48 | 48 |
a2A4096-9gmBAS | 0 | 0 | 48 | - | 48 |
a2A4096-9gmPRO | 0 | 0 | 48 | - | 48 |
a2A4096-30ucBAS | 0 | - | - | 48 | 48 |
a2A4096-30ucPRO | 0 | - | - | 48 | 48 |
a2A4096-30umBAS | 0 | 0 | 48 | - | 48 |
a2A4096-30umPRO | 0 | 0 | 48 | - | 48 |
a2A4096-44g5cBAS | 0 | - | - | 48 | 48 |
a2A4096-44g5mBAS | 0 | 0 | 48 | - | 48 |
a2A4096-67cc | 0 | - | 48 | 48 | 48 |
a2A4096-67cm | 0 | 0 | 48 | 48 | 48 |
a2A4200-12gcBAS | 0 | - | 36 | 36 | 36 |
a2A4200-12gcPRO | 0 | - | 36 | 36 | 36 |
a2A4200-12gmBAS | 0 | 0 | 36 | 36 | 36 |
a2A4200-12gmPRO | 0 | 0 | 36 | 36 | 36 |
a2A4200-40ucBAS | 0 | - | 36 | 36 | 36 |
a2A4200-40ucPRO | 0 | - | 36 | 36 | 36 |
a2A4200-40umBAS | 0 | 0 | 36 | 36 | 36 |
a2A4200-40umPRO | 0 | 0 | 36 | 36 | 36 |
a2A4504-5gcBAS | 0 | - | - | 48 | 48 |
a2A4504-5gcPRO | 0 | - | - | 48 | 48 |
a2A4504-5gmBAS | 0 | 0 | 48 | - | 48 |
a2A4504-5gmPRO | 0 | 0 | 48 | - | 48 |
a2A4504-18ucBAS | 0 | - | - | 48 | 48 |
a2A4504-18ucPRO | 0 | - | - | 48 | 48 |
a2A4504-18umBAS | 0 | 0 | 48 | - | 48 |
a2A4504-18umPRO | 0 | 0 | 48 | - | 48 |
a2A4504-27g5cBAS | 0 | - | - | 48 | 48 |
a2A4504-27g5mBAS | 0 | 0 | 48 | - | 48 |
a2A4504-42cc | 0 | - | 48 | 48 | 48 |
a2A4504-42cm | 0 | 0 | 48 | 48 | 48 |
a2A4508-6gcBAS | 0 | - | 36 | 36 | 36 |
a2A4508-6gcPRO | 0 | - | 36 | 36 | 36 |
a2A4508-6gmBAS | 0 | 0 | 36 | 36 | 36 |
a2A4508-6gmPRO | 0 | 0 | 36 | 36 | 36 |
a2A4508-20ucBAS | 0 | - | 36 | 36 | 36 |
a2A4508-20ucPRO | 0 | - | 36 | 36 | 36 |
a2A4508-20umBAS | 0 | 0 | 36 | 36 | 36 |
a2A4508-20umPRO | 0 | 0 | 36 | 36 | 36 |
a2A5060-4gcBAS | 0 | - | - | 48 | 48 |
a2A5060-4gmBAS | 0 | 0 | 48 | - | 48 |
a2A5060-15ucBAS | 0 | - | - | 48 | 48 |
a2A5060-15umBAS | 0 | 0 | 48 | - | 48 |
a2A5060-21g5cBAS | 0 | - | - | 48 | 48 |
a2A5060-21g5mBAS | 0 | 0 | 48 | - | 48 |
a2A5320-7gcBAS | 0 | - | - | 48 | 48 |
a2A5320-7gcPRO | 0 | - | - | 48 | 48 |
a2A5320-7gmBAS | 0 | 0 | 48 | - | 48 |
a2A5320-7gmPRO | 0 | 0 | 48 | - | 48 |
a2A5320-23ucBAS | 0 | - | - | 48 | 48 |
a2A5320-23ucPRO | 0 | - | - | 48 | 48 |
a2A5320-23umBAS | 0 | 0 | 48 | - | 48 |
a2A5320-23umPRO | 0 | 0 | 48 | - | 48 |
a2A5320-34g5cBAS | 0 | - | - | 48 | 48 |
a2A5320-34g5mBAS | 0 | 0 | 48 | - | 48 |
a2A5320-52cc | 0 | - | 48 | 48 | 48 |
a2A5320-52cm | 0 | 0 | 48 | 48 | 48 |
a2A5328-4gcBAS | 0 | - | - | 48 | 48 |
a2A5328-4gcPRO | 0 | - | - | 48 | 48 |
a2A5328-4gmBAS | 0 | 0 | 48 | - | 48 |
a2A5328-4gmPRO | 0 | 0 | 48 | - | 48 |
a2A5328-15ucBAS | 0 | - | - | 48 | 48 |
a2A5328-15ucPRO | 0 | - | - | 48 | 48 |
a2A5328-15umBAS | 0 | 0 | 48 | - | 48 |
a2A5328-15umPRO | 0 | 0 | 48 | - | 48 |
a2A5328-22g5cBAS | 0 | - | - | 48 | 48 |
a2A5328-22g5mBAS | 0 | 0 | 48 | - | 48 |
a2A5328-35cc | 0 | - | 48 | 48 | 48 |
a2A5328-35cm | 0 | 0 | 48 | 48 | 48 |
acA640-121gm | 0 | 0 | 1023 | - | 600 |
acA640-300gc | 136 | - | 542 | 542 | - |
acA640-300gm | 136 | 136 | 542 | 542 | - |
acA640-750uc | 0 | - | 12 | 12 | - |
acA640-750um | 0 | 0 | 12 | 12 | - |
acA720-290gc | 0 | - | 360 | - | 240 |
acA720-290gm | 0 | 0 | 360 | - | 240 |
acA720-520uc | 0 | - | 36 | - | 24 |
acA720-520um | 0 | 0 | 36 | - | 24 |
acA800-200gc | 136 | - | 542 | 542 | - |
acA800-200gm | 136 | 136 | 542 | 542 | - |
acA800-510uc | 0 | - | 12 | 12 | - |
acA800-510um | 0 | 0 | 12 | 12 | - |
acA1280-60gc | 0 | - | - | - | 3/95a |
acA1280-60gm | 0 | 0 | - | - | 3/95a |
acA1300-60gc | 0 | - | - | - | 3/95a |
acA1300-60gm | 0 | 0 | - | - | 3/95a |
acA1300-60gmNIR | 0 | 0 | - | - | 3/95a |
acA1300-75gc | 136 | - | 542 | 542 | - |
acA1300-75gm | 136 | 136 | 542 | 542 | - |
acA1300-200uc | 0 | - | 12 | 12 | - |
acA1300-200um | 0 | 0 | 12 | 12 | - |
acA1440-73gc | 0 | - | 360 | - | 240 |
acA1440-73gm | 0 | 0 | 360 | - | 240 |
acA1440-220uc | 0 | - | 36 | - | 24 |
acA1440-220um | 0 | 0 | 36 | - | 24 |
acA1600-20gc | 230 | - | 850 | - | 400 |
acA1600-20uc | 0 | - | 22.25800 | - | 6.10300 |
acA1600-60gc | 1/0a | - | - | - | 3/95a |
acA1600-60gm | 1/0a | 1/0a | - | - | 3/95a |
acA1920-25gc | 0 | - | 63 | - | 63 |
acA1920-25gm | 0 | 0 | 63 | - | 63 |
acA1920-25uc | 0 | - | 23.79814 | - | 23.79814 |
acA1920-25um | 0 | 0 | 23.79814 | - | 23.79814 |
acA1920-40gc | 0 | 0 | 360 | - | 240 |
acA1920-40gm | 0 | 0 | 360 | - | 240 |
acA1920-40uc | 0 | - | 36 | - | 24 |
acA1920-40ucMED | 0 | 0 | 36 | - | 24 |
acA1920-40um | 0 | 0 | 36 | – | 24 |
acA1920-40umMED | 0 | 0 | 36 | - | 24 |
acA1920-48gc | 136 | - | 542 | 542 | - |
acA1920-48gm | 136 | 136 | 542 | 542 | - |
acA1920-50gc | 0 | - | 360 | - | 240 |
acA1920-50gm | 0 | 0 | 360 | - | 240 |
acA1920-150uc | 0 | - | 12 | 12 | - |
acA1920-150um | 0 | 0 | 12 | 12 | - |
acA1920-155uc | 0 | - | 36 | - | 24 |
acA1920-155ucMED | 0 | - | 36 | - | 24 |
acA1920-155um | 0 | 0 | 36 | - | 24 |
acA1920-155umMED | 0 | 0 | 36 | - | 24 |
acA2000-50gc | 36 | - | 512 | - | 512 |
acA2000-50gm | 36 | 33 | 512 | - | 512 |
acA2000-165uc | 0 | - | 23.59350 | - | 23.59350 |
acA2000-165um | 0 | 0 | 23.59350 | - | 23.59350 |
acA2040-25gc | 36 | - | 512 | - | 512 |
acA2040-25gm | 36 | 33 | 512 | - | 512 |
acA2040-25gmNIR | 36 | 33 | 512 | - | 512 |
acA2040-35gc | 0 | - | 360 | - | 240 |
acA2040-35gm | 0 | 0 | 360 | - | 240 |
acA2040-55uc | 0 | - | 36 | - | 24 |
acA2040-55um | 0 | 0 | 36 | - | 24 |
acA2040-90uc | 0 | - | 23.59350 | - | 23.59350 |
acA2040-90um | 0 | 0 | 23.59350 | - | 23.59350 |
acA2040-90umNIR | 0 | 0 | 23.59350 | - | 23.59350 |
acA2040-120uc | 0 | - | 36 | - | 24 |
acA2040-120um | 0 | 0 | 36 | - | 24 |
acA2440-20gc | 0 | - | 360 | - | 240 |
acA2440-20gm | 0 | 0 | 360 | - | 240 |
acA2440-35uc | 0 | - | 36 | - | 24 |
acA2440-35ucMED | 0 | - | 36 | - | 24 |
acA2440-35um | 0 | 0 | 36 | - | 24 |
acA2440-35umMED | 0 | 0 | 36 | - | 24 |
acA2440-75uc | 0 | - | 36 | - | 24 |
acA2440-75ucMED | 0 | 0 | 36 | - | 24 |
acA2440-75um | 0 | 0 | 36 | - | 24 |
acA2440-75umMED | 0 | - | 36 | - | 24 |
acA2500-14gc | 0 | - | 63 | - | 63 |
acA2500-14gm | 0 | 0 | 63 | - | 63 |
acA2500-14uc | 0 | - | 23.79814 | - | 23.79814 |
acA2500-14um | 0 | 0 | 23.79814 | - | 23.79814 |
acA2500-20gc | 136 | 136 | 542 | 542 | - |
acA2500-20gcMED | 136 | - | 542 | 542 | - |
acA2500-20gm | 136 | 136 | 542 | 542 | - |
acA2500-20gmMED | 136 | 136 | 542 | 542 | - |
acA2500-60uc | 0 | - | 12 | 12 | - |
acA2500-60um | 0 | 0 | 12 | 12 | - |
acA3088-16gc | 0 | - | 360 | - | 240 |
acA3088-16gm | 0 | 0 | 360 | - | 240 |
acA3088-57uc | 0 | - | 36 | - | 24 |
acA3088-57ucMED | 0 | - | 36 | - | 24 |
acA3088-57um | 0 | 0 | 36 | - | 24 |
acA3088-57umMED | 0 | 0 | 36 | - | 24 |
acA3800-10gc | 33 | - | 255 | - | 255 |
acA3800-10gm | 33 | 33 | 255 | - | 255 |
acA3800-14uc | 0 | - | 16.67569 | - | 16.67569 |
acA3800-14um | 0 | 0 | 16.67569 | - | 16.67569 |
acA4024-8gc | 0 | - | 1957 | - | 1957 |
acA4024-8gm | 0 | 0 | 1957 | - | 1957 |
acA4024-29uc | 0 | - | 27 | - | 27 |
acA4024-29um | 0 | 0 | 27 | - | 27 |
acA4096-11gc | 0 | 0 | 36 | - | 24 |
acA4096-11gm | 0 | 0 | 36 | - | 24 |
acA4096-30uc | 0 | - | 36 | - | 24 |
acA4096-30ucMED | 0 | - | 36 | - | 24 |
acA4096-30um | 0 | 0 | 36 | - | 24 |
acA4096-30umMED | 0 | 0 | 36 | - | 24 |
acA4096-40uc | 0 | - | 36 | - | 24 |
acA4096-40ucMED | 0 | - | 36 | - | 24 |
acA4096-40um | 0 | 0 | 36 | - | 24 |
acA4096-40umMED | 0 | 0 | 36 | - | 24 |
acA4112-8gc | 0 | 0 | 36 | - | 24 |
acA4112-8gm | 0 | 0 | 36 | - | 24 |
acA4112-20uc | 0 | - | 36 | - | 24 |
acA4112-20ucMED | 0 | - | 36 | - | 24 |
acA4112-20um | 0 | 0 | 36 | - | 24 |
acA4112-20umMED | 0 | 0 | 36 | - | 24 |
acA4112-30uc | 0 | - | 36 | - | 24 |
acA4112-30ucMED | 0 | - | 36 | - | 24 |
acA4112-30um | 0 | 0 | 36 | - | 24 |
acA4112-30umMED | 0 | 0 | 36 | - | 24 |
acA5472-5gc | 0 | - | 1957 | - | 1957 |
acA5472-5gm | 0 | 0 | 1957 | - | 1957 |
acA5472-17uc | 0 | - | 27.04000 | - | 27.04000 |
acA5472-17ucMED | 0 | - | 27.04000 | - | 27.04000 |
acA5472-17um | 0 | 0 | 27.04000 | - | 27.04000 |
acA5472-17umMED | 0 | 0 | 27.04000 | - | 27.04000 |
boA1936-400cc | 0 | - | 48 | 48 | 48 |
boA1936-400cm | 0 | - | 48 | 48 | 48 |
boA2448-250cc | 0 | - | 48 | 48 | 48 |
boA2448-250cm | 0 | - | 48 | 48 | 48 |
boA2832-190cc | 0 | - | 48 | 48 | 48 |
boA2832-190cm | 0 | - | 48 | 48 | 48 |
boA4096-93cc | 0 | - | 48 | - | 48 |
boA4096-93cm | 0 | - | 48 | - | 48 |
boA4096-180cc | 0 | - | 48 | 48 | 48 |
boA4096-180cm | 0 | - | 48 | 48 | 48 |
boA4112-68cc | 0 | - | 48 | - | 48 |
boA4112-68cm | 0 | - | 48 | - | 48 |
boA4500-45cc | 0 | - | 18.06200 | 18.062 | 18.06200 |
boA4500-45cm | 0 | - | 18.06200 | 18.062 | 18.06200 |
boA4504-100cc | 0 | - | 48 | 48 | 48 |
boA4504-100cm | 0 | - | 48 | 48 | 48 |
boA5120-150cc | 0 | - | 24 | 24 | - |
boA5120-150cm | 0 | - | 24 | 24 | - |
boA5120-230cc | 0 | - | 24 | 24 | - |
boA5120-230cm | 0 | - | 24 | 24 | - |
boA5320-150cc | 0 | - | 48 | 48 | 48 |
boA5320-150cm | 0 | - | 48 | 48 | 48 |
boA5328-100cc | 0 | - | 48 | 48 | 48 |
boA5328-100cm | 0 | - | 48 | 48 | 48 |
boA6500-36cc | 0 | - | 18.06200 | 18.062 | 18.06200 |
boA6500-36cm | 0 | - | 18.06200 | 18.062 | 18.06200 |
boA8100-16cc | 0 | - | 18.06200 | 18.062 | 18.06200 |
boA8100-16cm | 0 | - | 18.06200 | 18.062 | 18.06200 |
boA9344-30cc | 0 | - | 24 | 24 | - |
boA9344-30cm | 0 | - | 24 | 24 | - |
boA9344-70cc | 0 | - | 24 | 24 | - |
boA9344-70cm | 0 | - | 24 | 24 | - |
boA13440-17cm | 0 | - | 36 | 36 | 36b |
daA720-520uc | 0 | - | 48 | - | 48 |
daA720-520um | 0 | 0 | 48 | - | 48 |
daA1280-54uc | 0 | 0 | 18 | - | 18 |
daA1280-54um | 0 | 0 | 18 | - | 18 |
daA1440-220uc | 0 | - | 48 | - | 48 |
daA1440-220um | 0 | 0 | 48 | - | 48 |
daA1600-60uc | 0 | 0 | 24 | - | 24 |
daA1600-60um | 0 | 0 | 24 | - | 24 |
daA1920-15um | 0 | 0 | 24 | - | 24 |
daA1920-30uc | 0 | 0 | 24 | - | 24 |
daA1920-30um | 0 | 0 | 24 | - | 24 |
daA1920-160uc | 0 | - | 48 | - | 48 |
daA1920-160um | 0 | 0 | 48 | - | 48 |
daA2448-70uc | 0 | - | 48 | - | 48 |
daA2448-70um | 0 | 0 | 48 | - | 48 |
daA2500-14uc | 0 | 0 | 24 | - | 24 |
daA2500-14um | 0 | 0 | 24 | - | 24 |
daA3840-45uc | 0 | - | 48 | - | 48 |
daA3840-45um | 0 | 0 | 48 | - | 48 |
dmA720-290gc | 0 | - | 48 | 48 | 48 |
dmA720-290gm | 0 | 0 | 48 | 48 | 48 |
dmA1440-73gc | 0 | - | 48 | 48 | 48 |
dmA1440-73gm | 0 | 0 | 48 | 48 | 48 |
dmA1920-51gc | 0 | - | 48 | 48 | 48 |
dmA1920-51gm | 0 | 0 | 48 | 48 | 48 |
dmA2448-23gc | 0 | - | - | 48 | 48 |
dmA2448-23gm | 0 | 0 | 48 | - | 48 |
dmA2840-14gc | 0 | - | - | 48 | 48 |
dmA2840-14gm | 0 | 0 | 48 | - | 48 |
dmA3536-9gc | 0 | - | 48 | 48 | 48 |
dmA3536-9gm | 0 | 0 | 48 | 48 | 48 |
dmA4096-9gc | 0 | - | - | 48 | 48 |
dmA4096-9gm | 0 | 0 | 48 | - | 48 |
puA1280-54uc | 0 | 0 | 18 | - | 18 |
puA1280-54um | 0 | 0 | 18 | - | 18 |
puA1600-60uc | 0 | 0 | 24 | - | 24 |
puA1600-60um | 0 | 0 | 24 | - | 24 |
puA1920-30uc | 0 | 0 | 24 | - | 24 |
puA1920-30um | 0 | 0 | 24 | - | 24 |
puA2500-14uc | 0 | 0 | 24 | - | 24 |
puA2500-14um | 0 | 0 | 24 | - | 24 |
r2L2048-29gc | 0 | - | 36 | 36 | 36 |
r2L2048-58gm | 0 | - | 36 | 36 | 36 |
r2L2048-62cc | 0 | - | 36 | 36 | 36 |
r2L2048-62g5c | 0 | - | 36 | 36 | 36 |
r2L2048-172cm | 0 | - | 36 | 36 | 36 |
r2L2048-172g5m | 0 | - | 36 | 36 | 36 |
r2L4096-14gc | 0 | - | 36 | 36 | 36 |
r2L4096-29gm | 0 | - | 36 | 36 | 36 |
r2L4096-42cc | 0 | - | 36 | 36 | 36 |
r2L4096-42g5c | 0 | - | 36 | 36 | 36 |
r2L4096-84cm | 0 | - | 36 | 36 | 36 |
r2L4096-84g5m | 0 | - | 36 | 36 | 36 |
r2L8192-200cm | 0 | - | - | - | 36 |
r2L16384-120cm | 0 | - | - | 36 | - |
-
Analog gain / digital gain.
-
Also valid when the pixel format is set to a 14-bit format.
Sample Code#
ace Classic/U/L GigE Cameras#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Set the "raw" gain value to 400 */
/* If you want to know the resulting gain in dB, use the formula given in this topic */
errRes = PylonDeviceSetIntegerFeature(hdev, "GainRaw", 400);
CHECK(errRes);
Other Cameras#
// Select the type of gain
camera.GainSelector.SetValue(GainSelector_All);
// Set the conversion gain mode to High
// Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
camera.BslConversionGainMode.SetValue(BslConversionGainMode_High);
// Set the gain to 4.2 dB
camera.Gain.SetValue(4.2);
// Increase the gain in the top-left quadrant of the image by 3 %
// Note: Available on boA13440-17cm cameras only
camera.BslGainTopLeft.SetValue(1.03);
INodeMap& nodemap = camera.GetNodeMap();
// Select the type of gain
CEnumParameter(nodemap, "GainSelector").SetValue("All");
// Set the conversion gain mode to High
// Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
CEnumParameter(nodemap, "BslConversionGainMode").SetValue("High");
// Set the gain to 4.2 dB
CFloatParameter(nodemap, "Gain").SetValue(4.2);
// Increase the gain in the top-left quadrant of the image by 3 %
// Note: Available on boA13440-17cm cameras only
CFloatParameter(nodemap, "BslGainTopLeft").SetValue(1.03);
// Select the type of gain
camera.Parameters[PLCamera.GainSelector].SetValue(PLCamera.GainSelector.All);
// Set the conversion gain mode to High
// Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
camera.Parameters[PLCamera.BslConversionGainMode].SetValue(PLCamera.BslConversionGainMode.High);
// Set the gain to 4.2 dB
camera.Parameters[PLCamera.Gain].SetValue(4.2);
// Increase the gain in the top-left quadrant of the image by 3 %
// Note: Available on boA13440-17cm cameras only
camera.Parameters[PLCamera.BslGainTopLeft].SetValue(1.03);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select the type of gain */
errRes = PylonDeviceFeatureFromString(hdev, "GainSelector", "All");
CHECK(errRes);
/* Set the conversion gain mode to High */
/* Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only */
errRes = PylonDeviceFeatureFromString(hdev, "BslConversionGainMode", "High");
CHECK(errRes);
/* Set the gain to 4.2 dB */
errRes = PylonDeviceSetFloatFeature(hdev, "Gain", 4.2);
CHECK(errRes);
/* Increase the gain in the top-left quadrant of the image by 3 % */
/* Note: Available on boA13440-17cm cameras only */
errRes = PylonDeviceSetFloatFeature(hdev, "BslGainTopLeft", 1.03);
CHECK(errRes);
# Select the type of gain
camera.GainSelector.Value = "All"
# Set the conversion gain mode to High
# Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
camera.BslConversionGainMode.Value = "High"
# Set the gain to 4.2 dB
camera.Gain.Value = 4.2
# Increase the gain in the top-left quadrant of the image by 3 %
# Note: Available on boA13440-17cm cameras only
camera.BslGainTopLeft.Value = 1.03
You can also use the pylon Viewer to easily set the parameters.