How To: Generate a Frequency Divider#
Assume the following:
- You want to acquire images from a Basler ace 2, boost, or dart IMX camera with a hardware trigger.
- The trigger source frequency is higher than your targeted image acquisition.
Using the Counter feature, you can create a kind of frequency divider.
For example, consider that you want to acquire an image every 15th trigger.
First, set up counter 1:
- Assign the
CounterEventSource
parameter to the desired hardware line. - Set the
CounterResetSource
parameter to ExposureActive. - Set the
CounterResetActivation
parameter toRisingEdge
. This resets the counter whenever exposure is started (exposure active rising edge). - Set the
CounterDuration
parameter to a value of 15. Every trigger input increments the counter.
Finally, set the trigger source of the Frame Start trigger to Counter 1 End.
Now, the counter generates a Counter End event once it reaches 15. The Counter End event triggers a frame start, and an image is being acquired.
Once the exposure is started, the Exposure Active signal rises, which resets the counter, and the cycle continues.