Skip to content

Line Source#

The Line Source camera feature allows you to configure which signal to output on the I/O line currently selected.

This allows you to monitor the status of the camera or to control external devices. For example, you can monitor if the camera is currently exposing or you can control external flash lighting.

For each camera output line, you can set exactly one signal.

Info

  • For the pin numbering and pin assignment of the I/O connector, see your camera topic. You can find your camera topic in the "Models" section.
  • The camera sends all output signals with a short propagation delay. The delay is usually in the microseconds range.

Using the Feature#

Setting the Line Source#

To set the line source:

  1. Set the LineSelector parameter to an I/O line configured as output, e.g., Line2.
  2. Set the LineSource parameter to one of the following values (if available):

Available Line Source Signals#

Depending on your camera model, the following line source signals are available:

Counter Active#

If available, you can use the camera's "Counter Active" signals, e.g., Counter 1 Active, to monitor the camera's Counter feature. The signal goes high when the counter has been started. The signal goes low when the counter is stopped, reset, or when it has reached its maximum value.

Exposure Active#

If available, you can use the Exposure Active signal to monitor if the camera is currently exposing. The signal goes high when exposure starts. The signal goes low when exposure ends. On rolling shutter cameras, the signal goes low when exposure for the last row has ended.

The Exposure Active signal can be used to trigger a flash.

The signal is also useful in situations where either the camera or the target object is moving. For example, assume that the camera is mounted on an arm mechanism that moves the camera to different sections of a product assembly. Typically, you don't want the camera to move during exposure. In this case, you can monitor the Exposure Active signal to know when exposure is taking place. This allows you to avoid moving the camera during that time.

Flash Window#

If available, you can use the Flash Window signal to determine when to use flash lighting. The signal goes high when you can start the flash lighting. The signal goes low when you should stop the flash lighting.

The signal indicates the period of time during a frame acquisition when all of the rows in the sensor are open for exposure.

Rolling Shutter Cameras#

On rolling shutter cameras, Basler recommends the use of flash lighting, especially when you are capturing images of fast-moving objects. Otherwise, images can be distorted due to the temporal shift between the different exposure starts of the individual rows.

The following diagram illustrates the timing of the Flash Window signal on rolling shutter cameras:

Flash Window Signal on Rolling Shutter Cameras

As shown above, on rolling shutter cameras, the Flash Window signal covers the period of time between the start of exposure of the last row (A) and the end of exposure of the first row (B).

On most rolling shutter cameras, you can calculate how long the flash window will remain open by using this formula:

Flash Window Width = Exposure Time - [ (tRow x (Image ROI Height - 1) ]

Info

On rolling shutter cameras, avoid extremely short exposure times or extremely large image ROIs. Otherwise, the exposure time for the first row may end before exposure of the last row starts, i.e., (B) occurs before (A). In that case, the Flash Window signal would always be low:

Invalid Flash Window Signal

Global Reset Release Shutter Cameras#

On Global Reset Release shutter cameras, you must use flash lighting. Otherwise, the brightness in each acquired image may vary significantly from top to bottom due to the differences in the exposure times of the rows. Also, when you are capturing images of fast-moving objects, images may be distorted due to the temporal shift between the different exposure ends of the individual rows.

The following diagram illustrates the timing of the Flash Window signal on Global Reset Release shutter cameras:

Flash Window Signal on Global Reset Release Shutter Cameras

As shown above, on Global Reset Release shutter cameras, the Flash Window signal spans the exposure time of the first row.

Global Shutter Cameras#

On global shutter cameras, the Flash Window signal is either not available or equivalent to the Exposure Active signal.

Frame Burst Active#

If available, you can use the Frame Burst Active signal to monitor if the camera is currently acquiring a series of images (a "burst" of images). The signal goes high when the acquisition of a series of images has been initialized. The signal goes low when the acquisition of a series of images has been finalized.

Serial Tx#

If available, you can use the Serial Tx signal to output serial data using the Serial Communication feature.

Sync User Output#

If available, you can use the Sync User Output signal to manually set the status of the line using the Sequencer feature.

The Sync User Output signal is similar to the User Output signal. The only difference is that Sync User Output signals can be controlled by the Sequencer feature, while the User Output signals can't.

The parameters related to the Sync User Output signals are also similar to the User Output parameters:

  • The SyncUserOutputValue parameter is the equivalent of the UserOutputValue parameter.
  • The SyncUserOutputValueAll parameter is the equivalent of the UserOutputValueAll parameter.
  • The SyncUserOutputSelector parameter is the equivalent of the UserOutputSelector parameter.

Timer Active#

You can use the camera's "Timer Active" signals, e.g., Timer 1 Active, to monitor the camera's Timer feature. The signal goes high after the delay specified. The signal goes low after the duration specified.

Info

The TimerStatus parameter, which is available on some camera models, can also take a value named TimerActive. However, this Timer Active status is different from the Timer Active signal: The signal is only high during the timer's duration, whereas the Timer Active status applies from the beginning of the timer delay until the end of the timer arm delay.

Trigger Wait#

You can use the camera's "Trigger Wait" signals, e.g., Frame Trigger Wait, to optimize triggered image acquisition and to avoid overtriggering.

Info

Trigger Wait signals go high when the camera is ready to receive trigger signals of the corresponding trigger type. When you apply the corresponding trigger signal, the Trigger Wait signal goes low. It stays low until the camera is ready to receive the next corresponding trigger signal.

For example, the Frame Trigger Wait signal goes high when the camera is ready to receive Frame Start trigger signals. When you apply a frame trigger signal, the signal goes low. It stays low until the camera is ready to receive the next Frame Start trigger signal:

Frame Trigger Wait Signal

Info

If you operate the camera with overlapping image acquisition and the Exposure Overlap Time Max feature is available on your camera model, you can use that feature to optimize the Frame Trigger Wait signal.

User Output#

You can set the status of a line by software. This can be useful to control external events or devices, e.g., a light source. For more information, see the User Output Value feature.

How to configure the output lines depends on how many User Output line sources are available on your camera model.

Configuration: One User Output Line Source Available#

If only one User Output line source is available ("User Output"):

  1. Set the LineSelector parameter to Out1.
  2. Set the LineSource parameter to UserOutput.

Now, you can use the User Output Value feature to set the status of the line by software.

Configuration: Multiple User Output Line Sources Available#

If multiple User Output line sources are available (e.g., "User Output 1" and "User Output 2"):

  1. Set the LineSelector parameter to the desired output line, e.g., Line2.
  2. If there is a user output signal assignment for your camera:

    • Set the LineSource parameter according to the signal assignment.
      Example: Assume that you selected Line 2 in step 1 and that the signal assignment is "User Output 1 → Line 2". In this case, you must set the LineSource parameter to UserOutput1.
  3. If there is no user output signal assignment for your camera, i.e., the signals are freely selectable:

    • Set the LineSource parameter to the desired line source, e.g., UserOutput1.

Now, you can use the User Output Value feature to set the status of the line by software.

Specifics#

Show all camera models

Camera Model Available Line Sources User Output Signal Assignment
a2A1920-51gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A1920-51gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A1920-51gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A1920-51gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A1920-160ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A1920-160ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A1920-160umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A1920-160umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-23gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-23gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-23gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-23gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-75ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-75ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-75umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2448-75umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-22gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-22gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-22gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-22gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-60ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-60ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-60umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2590-60umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-20gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-20gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-20gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-20gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-64ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-64ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-64umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2600-64umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-14gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-14gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-14gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-14gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-48ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-48ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-48umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A2840-48umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-13gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-13gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-13gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-13gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-45ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-45ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-45umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A3840-45umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-9gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-9gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-9gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-9gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-30ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-30ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-30umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4096-30umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-12gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-12gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-12gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-12gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-40ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-40ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-40umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4200-40umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-5gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-5gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-5gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-5gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-18ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-18ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-18umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A4504-18umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-7gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-7gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-7gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-7gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-23ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-23ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-23umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5320-23umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-4gcBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-4gcPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-4gmBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-4gmPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-15ucBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-15ucPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-15umBAS Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
a2A5328-15umPRO Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
acA640-90gc Exposure Active
Frame Trigger Wait
Aquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA640-90uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA640-121gm Exposure Active
Flash Window
Frame Trigger Wait
Aquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> line 3
acA640-300gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA640-300gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA640-750uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA640-750um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA720-290gc Exposure Time
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Time 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA720-290gm Exposure Time
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Time 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA720-520uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA720-520um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA800-200gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Time Active
User Output
Sync User Output
User Output 1 -> Line 2
User Output 2 -> Line 3
acA800-200gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Time Active
User Output
Sync User Output
User Output 1 -> Line 2
User Output 2 -> Line 3
acA800-510uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA800-510um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1280-60gc Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1280-60gm Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1300-60gc Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1300-60gm Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1300-60gmNIR Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1300-75gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1300-75gm Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1300-200uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1300-200um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1440-73gc Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1440-73gm Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1440-220uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1440-220um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1600-20gc Exposure Time
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1600-20uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1600-60gc Exposure Time
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1600-60gm Exposure Time
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1920-25gc Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1920-25gm Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA1920-25uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-25um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-40gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1920-40gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1920-40uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-40ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-40um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 → Line 2
User Output 2 → Line 3
User Output 3 → Line 4
acA1920-40umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-48gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1920-48gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1920-50gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1920-50gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA1920-150uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-150um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-155uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-155ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-155um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA1920-155umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2000-50gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2000-50gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2000-50gmNIR Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2000-165uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2000-165um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2000-165umNIR Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2040-25gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2040-25gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2040-25gmNIR Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2040-35gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2040-35gm Exposure Time
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2040-55uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2040-55um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2040-90uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2040-90um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2040-90umNIR Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2040-120uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2040-120um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-20gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2440-20gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2440-35uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-35ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-35um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-35umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-75uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-75ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-75um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2440-75umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2500-14gc Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2500-14gm Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA2500-14uc Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2500-14um Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2500-20gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2500-20gcMED Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2500-20gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2500-20gmMED Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA2500-60uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA2500-60um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA3088-16gc Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA3088-16gm Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA3088-57uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA3088-57ucMED Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA3088-57um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA3088-57umMED Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA3800-10gc Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA3800-10gm Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA3800-14uc Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA3800-14um Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4024-8gc Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA4024-8gm Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA4024-29uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4024-29um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4096-11gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA4096-11gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA4096-30uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4096-30ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 → Line 2
User Output 2 → Line 3
User Output 3 → Line 4
acA4096-30um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4096-30umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4096-40uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4096-40ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4096-40um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4096-40umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-8gc Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA4112-8gm Exposure Active
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output 2
User Output 1 -> Line 2
User Output 2 -> Line 3
acA4112-20uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-20ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-20um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-20umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-30uc Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-30ucMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-30um Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA4112-30umMED Exposure Active
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 → Line 2
User Output 2 → Line 3
User Output 3 → Line 4
acA4600-7gc Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer Active
User Output
Sync User Output
User Output -> Out 1
acA4600-10uc Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA5472-5gc Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output
User Output 1 -> Line 2
User Output 2 -> Line 3
acA5472-5gm Exposure Active
Flash Window
Frame Trigger Wait
Acquisition Trigger Wait
Timer 1 Active
User Output 1, User Output 2
Sync User Output 1, Sync User Output
User Output 1 -> Line 2
User Output 2 -> Line 3
acA5472-17uc Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA5472-17ucMED Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA5472-17um Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
acA5472-17umMED Exposure Active
Flash Window
Frame Trigger Wait
Frame Burst Trigger Wait
Timer 1 Active
User Output 1, User Output 2, User Output 3
User Output 1 -> Line 2
User Output 2 -> Line 3
User Output 3 -> Line 4
boA1936-400cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA1936-400cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA2448-250cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA2448-250cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA2832-190cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA2832-190cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4096-93cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4096-93cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4096-180cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4096-180cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4112-68cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4112-68cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4500-45cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4500-45cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4504-100cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA4504-100cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA5320-150cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA5320-150cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA5328-100cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA5328-100cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA6500-36cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA6500-36cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA8100-16cc Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
boA8100-16cm Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Serial Tx
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3
No assignment, signals freely selectable
daA1280-54uc Exposure Active
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA1280-54um Exposure Active
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA1600-60uc Exposure Active
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA1600-60um Exposure Active
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA1920-15um Flash Window
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA1920-30uc Flash Window
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA1920-30um Flash Window
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA1920-160uc Acquisition Active
Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3, User Output 4
No assignment, signals freely selectable
daA1920-160um Acquisition Active
Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3, User Output 4
No assignment, signals freely selectable
daA2448-70uc Acquisition Active
Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3, User Output 4
No assignment, signals freely selectable
daA2448-70um Acquisition Active
Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3, User Output 4
No assignment, signals freely selectable
daA2500-14uc Flash Window
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA2500-14um Flash Window
User Output 1, User Output 2
User Output 1 -> Line 1
User Output 2 -> Line 2
daA3840-45uc Acquisition Active
Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3, User Output 4
No assignment, signals freely selectable
daA3840-45um Acquisition Active
Counter 1 Active, Counter 2 Active
Exposure Active
Exposure Trigger Wait
Frame Burst Active
Frame Burst Trigger Wait
Frame Trigger Wait
Timer 1 Active, Timer 2 Active
User Output 1, User Output 2, User Output 3, User Output 4
No assignment, signals freely selectable
puA1280-54uc Line Source feature not supported Line Source feature not supported
puA1280-54um Line Source feature not supported Line Source feature not supported
puA1600-60uc Line Source feature not supported Line Source feature not supported
puA1600-60um Line Source feature not supported Line Source feature not supported
puA1920-30uc Line Source feature not supported Line Source feature not supported
puA1920-30um Line Source feature not supported Line Source feature not supported
puA2500-14uc Line Source feature not supported Line Source feature not supported
puA2500-14um Line Source feature not supported Line Source feature not supported

Sample Code#

// Select Line 2 (output line)
camera.LineSelector.SetValue(LineSelector_Line2);
// Select the Flash Window signal as the source signal for Line 2
camera.LineSource.SetValue(LineSource_FlashWindow);
INodeMap& nodemap = camera.GetNodeMap();
// Select Line 2 (output line)
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
// Select the Flash Window signal as the source signal for Line 2
CEnumParameter(nodemap, "LineSource").SetValue("FlashWindow");
// Select Line 2 (output line)
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
// Select the Flash Window signal as the source signal for Line 2
camera.Parameters[PLCamera.LineSource].SetValue(PLCamera.LineSource.FlashWindow);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select Line 2 (output line) */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
/* Select the Flash Window signal as the source signal for Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSource", "FlashWindow");
CHECK(errRes);

You can also use the pylon Viewer to easily set the parameters.