Processing Examples

VisualApplets includes numerous examples which will show the usage of operators and will provide you with implementation ideas. All examples can be found in the VisualApplets installation directory in sub-directory examples i.e. “%VASINSTALLDIR%/examples”. Testimages for simulation can be found in “%VASINSTALLDIR%/testimages”

The following sections show an overview on all examples. A brief introduction is presented as well as the folder and filename. All examples use a default hardware platform. This is the marathon VCL platform. Please find updates to the new imaFlex Quad and Penta platform for following directories and designs:

ImaFlex Quad:

  • examples\Acquisition\BasicAcquisition\iF-CXP12-Q

  • examples\Processing\ArtificialImageSource\ SimulationSource_ImageInjector.vad

  • examples\Processing\Compression\JPEG\iF-CXP12-Q examples\Processing\DMAFromPC\iF-CXP12-Q examples\Processing\Geometry\Downsampling

  • examples\Processing\Geometry\GeometricTransformation\iF-CXP12-Q

  • examples\Processing\Geometry\TapGeometrySorting\imaFlexQuad_CXP12x4_CxpCameraMultiTap.vad

  • examples\Processing\HDR_ImageComposition\HighDynamicRange_racer2L

  • examples\Processing\MultipleROIs\iF-CXP12-Q

ImaFlex Penta:

  • examples\Processing\Compression\JPEG\iF-CXP12-P

  • examples\Processing\Geometry\GeometricTransformation\iF-CXP12-P

  • examples\Processing\Geometry\TapGeometrySorting\ imaFlexPenta_CXP12x4_CxpCameraMultiTap.vad

  • examples\Processing\MultipleROIs\iF-CXP12-P

Most of all examples can easily be converted to other hardware platforms. See 'Target Hardware Porting' for more information on how to switch the hardware platform.