Pixel Format#
There are different pixel formats depending on the model of your camera and whether it is a color or a mono camera.
Info
Detailed information about pixel formats can be found in the GenICam Pixel Format Naming Convention 2.1.
Using the Feature#
Choosing a Pixel Format#
To choose a pixel format:
- Make sure the camera is idle, i.e., not capturing images.
- Set the
PixelFormat
parameter to one of the following values (if available):MonoXX
(e.g.,Mono10
,Mono12p
)BayerXXYY
(e.g.,BayerBG10
,BayerGR12
)YCbCrXXX
,YUVXXX
RGB8
,BGR8
BiColor BGRG8
,BiColor RGBG8
Determining the Pixel Format#
To determine the pixel format currently used by the camera, get the value of the PixelFormat
parameter.
Available Pixel Formats#
Info
- If the Sensor Bit Depth feature is available on your camera model, you can set the bit depth of the data output by the sensor independently of the pixel format. For example, you can configure the camera to output 8-bit image data based on 12-bit sensor data (pixel format = Mono 8, sensor bit depth = 12 bit).
- If the Transfer Bit Depth feature is available on your camera model, you can set the bit depth used for internal image processing independently of the pixel format. For example, you can configure the camera to output 8-bit image data based on data with a transfer bit depth of 10 bit (pixel format = Mono 8, transfer bit depth = 10 bit).
- For a list of the enumeration values, see the pylon API Documentation.
Mono Formats#
If a monochrome camera uses one of the mono pixel formats, it outputs 8, 10, 12, or 14 bits of data per pixel.
If a color camera uses one of the mono pixel formats, the values for each pixel are first converted to the YCbCr color model. The Y component of this model represents a brightness value and is equivalent to the value that would be derived from a pixel in a monochrome sensor. So in essence, when a color camera is set to, e.g., Mono 8, it outputs an 8-bit monochrome image.
Which mono formats are available depends on your camera model.
Bayer Formats#
Color cameras are equipped with a Bayer color filter and can output color images based on Bayer pixel formats.
If a color camera uses one of the Bayer pixel formats, it outputs 8, 10, or 12 bits of data per pixel. Each pixel is filtered to record only one of the colors red, green, and blue. The pixel data is not processed or interpolated in any way. This type of pixel data is sometimes referred to as "raw" output.
Which Bayer formats are available depends on your camera model.
YCbCr Formats#
Color cameras can also output color images based on pixel data in YCbCr (or YUV) format.
If a color camera uses this format, each pixel value in the captured image goes through a conversion process as it exits the sensor and passes through the camera. This process yields Y, Cb, and Cr color information for each pixel value.
RGB and BGR Formats#
When a color camera uses the RGB 8 or BGR 8 pixel format, the camera outputs 8 bit of red data, 8 bit of green data, and 8 bit of blue data for each pixel in the acquired frame.
The pixel formats differ by the output sequences for the color data (red, green, blue or blue, green, red).
BiColor BGRG and RGBG Formats#
The color cameras with BiColor pixel formats are equipped with a color filter array as displayed in the example figure below. The color filter array of the sensor has the red and blue color components on the first line, and the green component on the second line.
The camera combines this color information and outputs the data as shown in the example figure below.
If a color camera uses one of the BiColor pixel formats, it outputs 8 bit of data per pixel. Each pixel is filtered to record only one of the colors red, green, and blue. The pixel data is not processed or interpolated in any way. This type of pixel data is sometimes referred to as "raw" output. The pixel formats differ by the output sequences for the color data (blue, green, red, green or red, green, blue, green).
Which BiColor formats are available depends on your camera model.
Maximum Pixel Bit Depth#
The maximum pixel bit depth is defined by the pixel format with the highest bit depth among the pixel formats available on your camera.
Example: If the available pixel formats for your camera are Mono 8 and Mono 12, the maximum pixel bit depth of the camera is 12 bit.
Unpacked and Packed Pixel Formats#
When a camera uses an unpacked pixel format (e.g., Bayer 12), pixel data is always 8-bit aligned. Padding bits (zeros) are inserted as necessary to reach the next 8-bit boundary.
Example (simplified):
Assume that you have chosen a 12-bit unpacked pixel format. The camera outputs 16 bits per pixel: 12 bits of pixel data and 4 padding bits to reach the next 8-bit boundary.
When a camera uses a packed pixel format (e.g., Bayer 12p), pixel data is not aligned. This means that no padding bits are inserted and that one byte can contain data of multiple pixels.
Example (simplified):
Assume that you have chosen a 12-bit packed pixel format. The camera outputs 12 bits per pixel. As a consequence, data for two pixels is always spread over 3 bytes.
Info
The exact data alignment depends on the pixel format. You can find detailed information in the GenICam Pixel Format Naming Convention 2.1.
Specifics#
Camera Model | Available Pixel Formats |
---|---|
a2A640-240gmSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A640-240umSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A1280-80gmSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A1280-125umSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A1920-51gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A1920-51gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A1920-51gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A1920-51gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A1920-160ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A1920-160ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A1920-160umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A1920-160umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A1920-165g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A1920-165g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2048-35gmSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2048-110umSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2440-98g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2440-98g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2448-23gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2448-23gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2448-23gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2448-23gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2448-75ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2448-75ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2448-75umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2448-75umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2448-105g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2448-105g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2448-120cc | Mono 8 Mono 10 Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
a2A2448-120cm | Mono 8 Mono 10 Mono 12 |
a2A2448-210cc | Mono 8 Mono 10 Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
a2A2448-210cm | Mono 8 Mono 10 Mono 12 |
a2A2560-20gmSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2560-70umSWIR | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2590-22gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2590-22gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2590-22gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2590-22gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2590-60ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2590-60ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2590-60umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2590-60umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2600-20gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2600-20gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2600-20gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2600-20gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2600-64ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2600-64ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2600-64umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2600-64umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-14gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2840-14gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2840-14gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-14gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-14gmUV | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-48ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2840-48ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2840-48umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-48umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-48umUV | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-67g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A2840-67g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-67g5mUV | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A2840-86cc | Mono 8 Mono 10 Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
a2A2840-86cm | Mono 8 Mono 10 Mono 12 |
a2A3536-9gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3536-9gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3536-9gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3536-9gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3536-31ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3536-31ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3536-31umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3536-31umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3536-42g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3536-42g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3840-13gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3840-13gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3840-13gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3840-13gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3840-45ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3840-45ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A3840-45umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A3840-45umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4096-9gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4096-9gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4096-9gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4096-9gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4096-30ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4096-30ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4096-30umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4096-30umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4096-44g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4096-44g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4096-67cc | Mono 8 Mono 10 Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
a2A4096-67cm | Mono 8 Mono 10 Mono 12 |
a2A4200-12gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4200-12gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4200-12gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4200-12gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4200-40ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4200-40ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4200-40umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4200-40umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4504-5gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4504-5gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4504-5gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4504-5gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4504-18ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4504-18ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4504-18umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4504-18umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4504-27g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4504-27g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4504-42cc | Mono 8 Mono 10 Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
a2A4504-42cm | Mono 8 Mono 10 Mono 12 |
a2A4508-6gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4508-6gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4508-6gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4508-6gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4508-20ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4508-20ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer GB 8a Bayer GB 10a Bayer GB 10pa Bayer GB 12a Bayer GB 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A4508-20umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A4508-20umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5060-4gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5060-4gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5060-15ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5060-15umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5060-21g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5060-21g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5320-7gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5320-7gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5320-7gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5320-7gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5320-23ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5320-23ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5320-23umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5320-23umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5320-34g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5320-34g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5320-52cc | Mono 8 Mono 10 Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
a2A5320-52cm | Mono 8 Mono 10 Mono 12 |
a2A5328-4gcBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5328-4gcPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5328-4gmBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5328-4gmPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5328-15ucBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5328-15ucPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5328-15umBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5328-15umPRO | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5328-22g5cBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
a2A5328-22g5mBAS | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
a2A5328-35cc | Mono 8 Mono 10 Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
a2A5328-35cm | Mono 8 Mono 10 Mono 12 |
acA640-121gm | Mono 8 Mono 12 Mono 12 Packed |
acA640-300gc | Mono 8 Bayer BG 8a Bayer BG 10a Bayer BG 10 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA640-300gm | Mono 8 Mono 10 Mono 10 Packed |
acA640-750uc | Mono 8 Bayer BG 8a Bayer BG 10a Bayer BG 10pa RGB 8 BGR 8 YCbCr422_8 |
acA640-750um | Mono 8 Mono 10 Mono 10p |
acA720-290gc | Mono 8 Bayer RG 8 Bayer RG 12 Bayer RG 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA720-290gm | Mono 8 Mono 12 Mono 12 Packed |
acA720-520uc | Mono 8 Bayer BG 8a Bayer BG 10a Bayer BG 10pa RGB 8 BGR 8 YCbCr422_8 |
acA720-520um | Mono 8 Mono 12 Mono 12p |
acA800-200gc | Mono 8 Bayer BG 8 Bayer BG 10 Bayer BG 10 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA800-200gm | Mono 8 Mono 10 Mono 10 Packed |
acA800-510uc | Mono 8 Bayer BG 8a Bayer BG 10a Bayer BG 10pa RGB 8 BGR 8 YCbCr422_8 |
acA800-510um | Mono 8 Mono 10 Mono 10p |
acA1280-60gc | Mono 8 Bayer BG 8 Bayer BG 12b Bayer BG 12 Packedb YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1280-60gm | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1300-60gc | Mono 8 Bayer RG 8 Bayer RG 12b Bayer RG 12 Packedb YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1300-60gm | Mono 8 Mono 12 Mono 12 Packed |
acA1300-60gmNIR | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1300-75gc | Mono 8 Bayer BG 8a Bayer BG 10a Bayer BG 10 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1300-75gm | Mono 8 Mono 10 Mono 10 Packed |
acA1300-200uc | Mono 8 Bayer BG 8a Bayer BG 10a Bayer BG 10pa RGB 8 BGR 8 YCbCr422_8 |
acA1300-200um | Mono 8 Mono 10 Mono 10p |
acA1440-73gc | Mono 8 Bayer RG 8a Bayer RG 12]a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1440-73gm | Mono 8 Mono 12 Mono 12 Packed |
acA1440-220uc | Mono 8 Bayer BG 8a Bayer BG 10a Bayer BG 10pa RGB 8 BGR 8 YCbCr422_8 |
acA1440-220um | Mono 8 Mono 12 Mono 12p |
acA1600-20gc | Mono 8 Bayer RG 8 Bayer RG 12 Bayer RG 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1600-20uc | Mono 8 Bayer BG 8 Bayer BG 12 Bayer BG 12p RGB 8 BGR 8 YCbCr422_8 |
acA1600-60gc | Mono 8 Bayer RG 8 Bayer RG 12b Bayer RG 12 Packedb YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1600-60gm | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1920-25gc | Mono 8 Bayer BG 8 Bayer BG 12 Bayer BG 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1920-25gm | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1920-25uc | Mono 8 Bayer GB 8 Bayer GB 12 Bayer GB 12p YCbCr422_8 |
acA1920-25um | Mono 8 Mono 12 Mono 12p |
acA1920-40gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1920-40gm | Mono 8 Mono 12 Mono 12 Packed |
acA1920-40uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA1920-40ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA1920-40um | Mono 8 Mono 12 Mono 12p |
acA1920-40umMED | Mono 8 Mono 12 Mono 12 Packed |
acA1920-48gc | Mono 8 Bayer RG 8a Bayer RG 10a Bayer RG 10 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1920-48gm | Mono 8 Mono 10 Mono 10 Packed |
acA1920-50gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA1920-50gm | Mono 8 Mono 12 Mono 12 Packed |
acA1920-150uc | Mono 8 Bayer RG 8a Bayer RG 10a Bayer RG 10pa RGB 8 BGR 8 YCbCr422_8 |
acA1920-150um | Mono 8 Mono 10 Mono 10p |
acA1920-155uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA1920-155ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA1920-155um | Mono 8 Mono 12 Mono 12p |
acA1920-155umMED | Mono 8 Mono 12 Mono 12 Packed |
acA2000-50gc | Mono 8 Bayer GR 8 Bayer GR 12 Bayer GR 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2000-50gm | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2000-165uc | Bayer BG 8 Bayer BG 12 Bayer BG 12p |
acA2000-165um | Mono 8 Mono 12 Mono 12p |
acA2040-25gc | Mono 8 Bayer GR 8 Bayer GR 12 Bayer GR 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2040-25gm | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2040-25gmNIR | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2040-35gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2040-35gm | Mono 8 Mono 12 Mono 12 Packed |
acA2040-55uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA2040-55um | Mono 8 Mono 12 Mono 12p |
acA2040-90uc | Bayer BG 8 Bayer BG 12 Bayer BG 12p |
acA2040-90um | Mono 8 Mono 12 Mono 12p |
acA2040-90umNIR | Mono 8 Mono 12 Mono 12 Packed |
acA2040-120uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA2040-120um | Mono 8 Mono 12 Mono 12p |
acA2440-20gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2440-20gm | Mono 8 Mono 12 Mono 12 Packed |
acA2440-35uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA2440-35ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA2440-35um | Mono 8 Mono 12 Mono 12p |
acA2440-35umMED | Mono 8 Mono 12 Mono 12 Packed |
acA2440-75uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA2440-75ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA2440-75um | Mono 8 Mono 12 Mono 12p |
acA2440-75umMED | Mono 8 Mono 12 Mono 12 Packed |
acA2500-14gc | Mono 8 Bayer GB 8 Bayer GB 12 Bayer GB 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2500-14gm | Mono 8 Mono 12 Mono 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2500-14uc | Mono 8 Bayer GB 8 Bayer GB 12 Bayer GB 12p YCbCr422_8 |
acA2500-14um | Mono 8 Mono 12 Mono 12p |
acA2500-20gc | Mono 8 Bayer RG 8a YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2500-20gcMED | Mono 8 Bayer RG 8a Bayer RG 10a Bayer RG 10 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA2500-20gm | Mono 8 Mono 10 Mono 10 Packed |
acA2500-20gmMED | Mono 8 Mono 10 Mono 10 Packed |
acA2500-60uc | Mono 8 Bayer RG 8a Bayer RG 10a Bayer RG 10pa RGB 8 BGR 8 YCbCr422_8 |
acA2500-60um | Mono 8 Mono 10 Mono 10p |
acA3088-16gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA3088-16gm | Mono 8 Mono 12 Mono 12 Packed |
acA3088-57uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA3088-57ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA3088-57um | Mono 8 Mono 12 Mono 12p |
acA3088-57umMED | Mono 8 Mono 12 Mono 12 Packed |
acA3800-10gc | Mono 8 Bayer BG 8 Bayer BG 12 Bayer BG 12 Packed YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA3800-10gm | Mono 8 Mono 12 Mono 12 Packed |
acA3800-14uc | Mono 8 Bayer BG 8 Bayer BG 12 Bayer BG 12p YCbCr422_8 |
acA3800-14um | Mono 8 Mono 12 Mono 12p |
acA4024-8gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA4024-8gm | Mono 8 Mono 12 Mono 12 Packed |
acA4024-29uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA4024-29um | Mono 8 Mono 12 Mono 12p |
acA4096-11gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA4096-11gm | Mono 8 Mono 12 Mono 12 Packed |
acA4096-30uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA4096-30ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA4096-30um | Mono 8 Mono 12 Mono 12p |
acA4096-30umMED | Mono 8 Mono 12 Mono 12 Packed |
acA4096-40uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA4096-40ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA4096-40um | Mono 8 Mono 12 Mono 12p |
acA4096-40umMED | Mono 8 Mono 12 Mono 12 Packed |
acA4112-8gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA4112-8gm | Mono8 Mono 12 Mono 12 Packed |
acA4112-20uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA4112-20ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA4112-20um | Mono 8 Mono 12 Mono 12p |
acA4112-20umMED | Mono 8 Mono 12 Mono 12 Packed |
acA4112-30uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA4112-30ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA4112-30um | Mono 8 Mono 12 Mono 12p |
acA4112-30umMED | Mono 8 Mono 12 Mono 12 Packed |
acA5472-5gc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda YUV 4:2:2 Packed YUV 4:2:2 (YUYV) Packed |
acA5472-5gm | Mono 8 Mono 12 Mono 12 Packed |
acA5472-17uc | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
acA5472-17ucMED | Mono 8 Bayer RG 8a Bayer RG 12a Bayer RG 12 Packeda RGB 8 BGR 8 YCbCr422_8 |
acA5472-17um | Mono 8 Mono 12 Mono 12p |
acA5472-17umMED | Mono 8 Mono 12 Mono 12 Packed |
boA1936-400cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA1936-400cm | Mono 8 Mono 10 Mono 12 |
boA2448-250cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA2448-250cm | Mono 8 Mono 10 Mono 12 |
boA2832-190cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA2832-190cm | Mono 8 Mono 10 Mono 12 |
boA4096-93cc | Mono 8 Mono 10 Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422 |
boA4096-93cm | Mono 8 Mono 10 Mono 12 |
boA4096-180cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA4096-180cm | Mono 8 Mono 10 Mono 12 |
boA4112-68cc | Mono 8 Mono 10 Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422 |
boA4112-68cm | Mono 8 Mono 10 Mono 12 |
boA4500-45cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA4500-45cm | Mono 8 Mono 10 Mono 12 |
boA4504-100cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA4504-100cm | Mono 8 Mono 10 Mono 12 |
boA5120-150cc | Mono 8 Mono 10d Bayer GB 8 Bayer GB 10d |
boA5120-150cm | Mono 8 Mono 10d |
boA5120-230cc | Mono 8 Mono 10d Bayer GB 8 Bayer GB 10d |
boA5120-230cm | Mono 8 Mono 10d |
boA5320-150cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA5320-150cm | Mono 8 Mono 10 Mono 12 |
boA5328-100cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA5328-100cm | Mono 8 Mono 10 Mono 12 |
boA6500-36cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA6500-36cm | Mono 8 Mono 10 Mono 12 |
boA8100-16cc | Mono 8 Mono 10 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 12a RGB 8 YUV422_8 |
boA8100-16cm | Mono 8 Mono 10 Mono 12 |
boA9344-30cc | Mono 8 Mono 10d Bayer BG 8 Bayer BG 10d |
boA9344-30cm | Mono 8 Mono 10d |
boA9344-70cc | Mono 8 Mono 10d Bayer BG 8 Bayer BG 10d |
boA9344-70cm | Mono 8 Mono 10d |
boA13440-17cm | Mono 8 Mono 10 Mono 12 Mono 14 |
daA720-520uc | Mono 8 Mono 12 Mono 12p Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
daA720-520um | Mono 8 Mono 12 Mono 12p |
daA1280-54uc | Bayer 8 Bayer 12 RGB 8c YCbCr422_8c |
daA1280-54um | Mono 8 Mono 12 |
daA1440-220uc | Mono 8 Mono 12 Mono 12p Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
daA1440-220um | Mono 8 Mono 12 Mono 12p |
daA1600-60uc | Bayer 8a Bayer 12ab RGB 8c YCbCr422_8c |
daA1600-60um | Mono 8 Mono 12b |
daA1920-15um | Mono 8 Mono 12 |
daA1920-30uc | Bayer 8a Bayer 12a RGB 8c YCbCr422_8c |
daA1920-30um | Mono 8 Mono 12 |
daA1920-160uc | Mono 8 Mono 12 Mono 12p Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
daA1920-160um | Mono 8 Mono 12 Mono 12p |
daA2448-70uc | Mono 8 Mono 12 Mono 12p Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
daA2448-70um | Mono 8 Mono 12 Mono 12p |
daA2500-14uc | Bayer 8a Bayer 12a RGB 8c YCbCr422_8c |
daA2500-14um | Mono 8 Mono 12 |
daA3840-45uc | Mono 8 Mono 12 Mono 12p Bayer RG 8a Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
daA3840-45um | Mono 8 Mono 12 Mono 12p |
dmA720-290gc | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
dmA720-290gm | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
dmA1440-73gc | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
dmA1440-73gm | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
dmA1920-51gc | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
dmA1920-51gm | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
dmA3536-9gc | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p Bayer RG 8a Bayer RG 10a Bayer RG 10pa Bayer RG 12a Bayer RG 12pa RGB 8 BGR 8 YCbCr422_8 |
dmA3536-9gm | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
puA1280-54uc | Bayer 8 Bayer 12 RGB 8c YCbCr422_8c |
puA1280-54um | Mono 8 Mono 12 |
puA1600-60uc | Bayer 8a Bayer 12ab RGB 8c YCbCr422_8c |
puA1600-60um | Mono 8 Mono 12b |
puA1920-30uc | Bayer 8a Bayer 12a RGB 8c YCbCr422_8c |
puA1920-30um | Mono 8 Mono 12 |
puA2500-14uc | Bayer 8a Bayer 12a RGB 8c YCbCr422_8c |
puA2500-14um | Mono 8 Mono 12 |
r2L2048-29gc | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p RGB 8 BGR 8 YCbCr422_8 |
r2L2048-58gm | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
r2L2048-62cc | Mono 8 Mono 10 Mono 12 RGB 8 YUV422_8 |
r2L2048-62g5c | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p RGB 8 BGR 8 YCbCr422_8 |
r2L2048-172cm | Mono 8 Mono 10 Mono 12 |
r2L2048-172g5m | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
r2L4096-14gc | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p RGB 8 BGR 8 YCbCr422_8 BiColor BGRG 8 BiColor RGBG 8 |
r2L4096-29gm | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
r2L4096-42cc | Mono 8 Mono 10 Mono 12 RGB 8 YUV422_8 |
r2L4096-42g5c | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p RGB 8 BGR 8 YCbCr422_8 BiColor BGRG 8 BiColor RGBG 8 |
r2L4096-84cm | Mono 8 Mono 10 Mono 12 |
r2L4096-84g5m | Mono 8 Mono 10 Mono 10p Mono 12 Mono 12p |
r2L8192-200cm | Mono 8 Mono 10 Mono 12 |
r2L16384-120cm | Mono 8 Mono 10 Mono 12b |
-
If you enable the Reverse X and Reverse Y feature, the actual Bayer color filter alignment changes.
-
12-bit image data based on 10-bit sensor data.
-
By default, YCbCr422 and RGB 8 images are acquired in sRGB color space. You can use the BslColorSpaceMode parameter to change the color space to RGB.
-
When using 10-bit pixel formats, especially with a large image ROI, you may not be able to reach the desired frame rate. This is due to bandwidth limitations (maximum PCIe transfer rate). To solve this, start the pylon Viewer, navigate to Device Transport Layer > Image Format Control using the feature tree, and enable the Output Packed Formats option. Now, image output is packed, which requires less bandwidth.
Sample Code#
You can also use the pylon Viewer to easily set the parameters.