Skip to content

Pixel Format#

The Pixel Format camera feature allows you to choose the format of the image data transmitted by the camera.

There are different pixel formats depending on the model of your camera and whether it is a color or a mono camera.

Info

Detailed information about pixel formats can be found in the GenICam Pixel Format Naming Convention 2.1.

Using the Feature#

Choosing a Pixel Format#

To choose a pixel format:

  1. Make sure the camera is idle, i.e., not capturing images.
  2. Set the PixelFormat parameter to one of the following values (if available):

Determining the Pixel Format#

To determine the pixel format currently used by the camera, get the value of the PixelFormat parameter.

Available Pixel Formats#

Info

  • If the Sensor Bit Depth feature is available on your camera model, you can set the bit depth of the data output by the sensor independently of the pixel format. For example, you can configure the camera to output 8-bit image data based on 12-bit sensor data (pixel format = Mono 8, sensor bit depth = 12 bit).
  • If the Transfer Bit Depth feature is available on your camera model, you can set the bit depth used for internal image processing independently of the pixel format. For example, you can configure the camera to output 8-bit image data based on data with a transfer bit depth of 10 bit (pixel format = Mono 8, transfer bit depth = 10 bit).
  • For a list of the enumeration values, see the pylon API Documentation.

Mono Formats#

If a monochrome camera uses one of the mono pixel formats, it outputs 8, 10, or 12 bits of data per pixel.

If a color camera uses one of the mono pixel formats, the values for each pixel are first converted to the YCbCr color model. The Y component of this model represents a brightness value and is equivalent to the value that would be derived from a pixel in a monochrome sensor. So in essence, when a color camera is set to, e.g., Mono 8, it outputs an 8-bit monochrome image.

Which mono formats are available depends on your camera model.

Bayer Formats#

Color cameras are equipped with a Bayer color filter and can output color images based on Bayer pixel formats.

If a color camera uses one of the Bayer pixel formats, it outputs 8, 10, or 12 bits of data per pixel. Each pixel is filtered to record only one of the colors red, green, and blue. The pixel data is not processed or interpolated in any way. This type of pixel data is sometimes referred to as "raw" output.

Which Bayer formats are available depends on your camera model.

YCbCr Formats#

Color cameras can also output color images based on pixel data in YCbCr (or YUV) format.

If a color camera uses this format, each pixel value in the captured image goes through a conversion process as it exits the sensor and passes through the camera. This process yields Y, Cb, and Cr color information for each pixel value.

RGB and BGR Formats#

When a color camera uses the RGB 8 or BGR 8 pixel format, the camera outputs 8 bit of red data, 8 bit of green data, and 8 bit of blue data for each pixel in the acquired frame.

The pixel formats differ by the output sequences for the color data (red, green, blue or blue, green, red).

Maximum Pixel Bit Depth#

The maximum pixel bit depth is defined by the pixel format with the highest bit depth among the pixel formats available on your camera.

Example: If the available pixel formats for your camera are Mono 8 and Mono 12, the maximum pixel bit depth of the camera is 12 bit.

Unpacked and Packed Pixel Formats#

When a camera uses an unpacked pixel format (e.g., Bayer 12), pixel data is always 8-bit aligned. Padding bits (zeros) are inserted as necessary to reach the next 8-bit boundary.

Example (simplified):

Assume that you have chosen a 12-bit unpacked pixel format. The camera outputs 16 bits per pixel: 12 bits of pixel data and 4 padding bits to reach the next 8-bit boundary.

Unpacked Pixel Formats

When a camera uses a packed pixel format (e.g., Bayer 12p), pixel data is not aligned. This means that no padding bits are inserted and that one byte can contain data of multiple pixels.

Example (simplified):

Assume that you have chosen a 12-bit packed pixel format. The camera outputs 12 bits per pixel. As a consequence, data for two pixels is always spread over 3 bytes.

Packed Pixel Formats

Info

The exact data alignment depends on the pixel format. You can find detailed information in the GenICam Pixel Format Naming Convention 2.1.

Specifics#

Show all camera models

Camera Model Available Pixel Formats
a2A1920-51gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A1920-51gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A1920-51gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A1920-51gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A1920-160ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A1920-160ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A1920-160umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A1920-160umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A1920-165g5cBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A1920-165g5mBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2448-23gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2448-23gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2448-23gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2448-23gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2448-75ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2448-75ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2448-75umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2448-75umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2448-105g5cBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2448-105g5mBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2590-22gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2590-22gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2590-22gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2590-22gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2590-60ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2590-60ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2590-60umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2590-60umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2600-20gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2600-20gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2600-20gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2600-20gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2600-64ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2600-64ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2600-64umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2600-64umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2840-14gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2840-14gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2840-14gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2840-14gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2840-48ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2840-48ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2840-48umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2840-48umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A2840-67g5cBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A2840-67g5mBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A3840-13gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A3840-13gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A3840-13gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A3840-13gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A3840-45ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A3840-45ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A3840-45umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A3840-45umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4096-9gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4096-9gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4096-9gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4096-9gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4096-30ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4096-30ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4096-30umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4096-30umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4096-44g5cBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4096-44g5mBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4200-12gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4200-12gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4200-12gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4200-12gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4200-40ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4200-40ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer GB 8a
Bayer GB 10a
Bayer GB 10pa
Bayer GB 12a
Bayer GB 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4200-40umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4200-40umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4504-5gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4504-5gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4504-5gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4504-5gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4504-18ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4504-18ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4504-18umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4504-18umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A4504-27g5cBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A4504-27g5mBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5320-7gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5320-7gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5320-7gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5320-7gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5320-23ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5320-23ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5320-23umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5320-23umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5320-34g5cBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5320-34g5mBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5328-4gcBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5328-4gcPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5328-4gmBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5328-4gmPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5328-15ucBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5328-15ucPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5328-15umBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5328-15umPRO Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
a2A5328-22g5cBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 10pa
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
a2A5328-22g5mBAS Mono 8
Mono 10
Mono 10p
Mono 12
Mono 12p
acA640-90gc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12
YUV 4:2:2 (YUYV) Packed
acA640-90uc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA640-121gm Mono 8
Mono 12
Mono 12 Packed
acA640-300gc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA640-300gm Mono 8
Mono 10
Mono 10 Packed
acA640-750uc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA640-750um Mono 8
Mono 10
Mono 10 Packed
acA720-290gc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA720-290gm Mono 8
Mono 12
Mono 12 Packed
acA720-520uc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA720-520um Mono 8
Mono 12
Mono 12 Packed
acA800-200gc Mono 8
Bayer BG 8
Bayer BG 10
Bayer BG 10 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA800-200gm Mono 8
Mono 10
Mono 10 Packed
acA800-510uc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA800-510um Mono 8
Mono 10
Mono 10 Packed
acA1280-60gc Mono 8
Bayer BG 8
Bayer BG 12b
Bayer BG 12 Packedb
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1280-60gm Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1300-60gc Mono 8
Bayer RG 8
Bayer RG 12b
Bayer RG 12 Packedb
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1300-60gm Mono 8
Mono 12
Mono 12 Packed
acA1300-60gmNIR Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1300-75gc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1300-75gm Mono 8
Mono 10
Mono 10 Packed
acA1300-200uc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA1300-200um Mono 8
Mono 10
Mono 10 Packed
acA1440-73gc Mono 8
Bayer RG 8a
Bayer RG 12]a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1440-73gm Mono 8
Mono 12
Mono 12 Packed
acA1440-220uc Mono 8
Bayer BG 8a
Bayer BG 10a
Bayer BG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA1440-220um Mono 8
Mono 12
Mono 12 Packed
acA1600-20gc Mono 8
Bayer RG 8
Bayer RG 12
Bayer RG 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1600-20uc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
RGB 8
BGR 8
YCbCr422_8
acA1600-60gc Mono 8
Bayer RG 8
Bayer RG 12b
Bayer RG 12 Packedb
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1600-60gm Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1920-25gc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1920-25gm Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1920-25uc Mono 8
Bayer GB 8
Bayer GB 12
Bayer GB 12 Packed
YCbCr422_8
acA1920-25um Mono 8
Mono 12
Mono 12 Packed
acA1920-40gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1920-40gm Mono 8
Mono 12
Mono 12 Packed
acA1920-40uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA1920-40ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA1920-40um Mono 8
Mono 12
Mono 12 Packed
acA1920-40umMED Mono 8
Mono 12
Mono 12 Packed
acA1920-48gc Mono 8
Bayer RG 8a
Bayer RG 10a
Bayer RG 10 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1920-48gm Mono 8
Mono 10
Mono 10 Packed
acA1920-50gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA1920-50gm Mono 8
Mono 12
Mono 12 Packed
acA1920-150uc Mono 8
Bayer RG 8a
Bayer RG 10a
Bayer RG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA1920-150um Mono 8
Mono 10
Mono 10 Packed
acA1920-155uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA1920-155ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA1920-155um Mono 8
Mono 12
Mono 12 Packed
acA1920-155umMED Mono 8
Mono 12
Mono 12 Packed
acA2000-50gc Mono 8
Bayer GR 8
Bayer GR 12
Bayer GR 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2000-50gm Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2000-165uc Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
acA2000-165um Mono 8
Mono 12
Mono 12 Packed
acA2040-25gc Mono 8
Bayer GR 8
Bayer GR 12
Bayer GR 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2040-25gm Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2040-25gmNIR Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2040-35gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2040-35gm Mono 8
Mono 12
Mono 12 Packed
acA2040-55uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA2040-55um Mono 8
Mono 12
Mono 12 Packed
acA2040-90uc Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
acA2040-90um Mono 8
Mono 12
Mono 12 Packed
acA2040-90umNIR Mono 8
Mono 12
Mono 12 Packed
acA2040-120uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA2040-120um Mono 8
Mono 12
Mono 12 Packed
acA2440-20gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2440-20gm Mono 8
Mono 12
Mono 12 Packed
acA2440-35uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA2440-35ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA2440-35um Mono 8
Mono 12
Mono 12 Packed
acA2440-35umMED Mono 8
Mono 12
Mono 12 Packed
acA2440-75uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA2440-75ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA2440-75um Mono 8
Mono 12
Mono 12 Packed
acA2440-75umMED Mono 8
Mono 12
Mono 12 Packed
acA2500-14gc Mono 8
Bayer GB 8
Bayer GB 12
Bayer GB 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2500-14gm Mono 8
Mono 12
Mono 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2500-14uc Mono 8
Bayer GB 8
Bayer GB 12
Bayer GB 12 Packed
YCbCr422_8
acA2500-14um Mono 8
Mono 12
Mono 12 Packed
acA2500-20gc Mono 8
Bayer RG 8a
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2500-20gcMED Mono 8
Bayer RG 8a
Bayer RG 10a
Bayer RG 10 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA2500-20gm Mono 8
Mono 10
Mono 10 Packed
acA2500-20gmMED Mono 8
Mono 10
Mono 10 Packed
acA2500-60uc Mono 8
Bayer RG 8a
Bayer RG 10a
Bayer RG 10 Packeda
RGB 8
BGR 8
YCbCr422_8
acA2500-60um Mono 8
Mono 10
Mono 10 Packed
acA3088-16gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA3088-16gm Mono 8
Mono 12
Mono 12 Packed
acA3088-57uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA3088-57ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA3088-57um Mono 8
Mono 12
Mono 12 Packed
acA3088-57umMED Mono 8
Mono 12
Mono 12 Packed
acA3800-10gc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA3800-10gm Mono 8
Mono 12
Mono 12 Packed
acA3800-14uc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
YCbCr422_8
acA3800-14um Mono 8
Mono 12
Mono 12 Packed
acA4024-8gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA4024-8gm Mono 8
Mono 12
Mono 12 Packed
acA4024-29uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4024-29um Mono 8
Mono 12
Mono 12 Packed
acA4096-11gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA4096-11gm Mono 8
Mono 12
Mono 12 Packed
acA4096-30uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4096-30ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4096-30um Mono 8
Mono 12
Mono 12 Packed
acA4096-30umMED Mono 8
Mono 12
Mono 12 Packed
acA4096-40uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4096-40ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4096-40um Mono 8
Mono 12
Mono 12 Packed
acA4096-40umMED Mono 8
Mono 12
Mono 12 Packed
acA4112-8gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA4112-8gm Mono8
Mono 12
Mono 12 Packed
acA4112-20uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4112-20ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4112-20um Mono 8
Mono 12
Mono 12 Packed
acA4112-20umMED Mono 8
Mono 12
Mono 12 Packed
acA4112-30uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4112-30ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA4112-30um Mono 8
Mono 12
Mono 12 Packed
acA4112-30umMED Mono 8
Mono 12
Mono 12 Packed
acA4600-7gc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA4600-10uc Mono 8
Bayer BG 8
Bayer BG 12
Bayer BG 12 Packed
YCbCr422_8
acA5472-5gc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
YUV 4:2:2 Packed
YUV 4:2:2 (YUYV) Packed
acA5472-5gm Mono 8
Mono 12
Mono 12 Packed
acA5472-17uc Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA5472-17ucMED Mono 8
Bayer RG 8a
Bayer RG 12a
Bayer RG 12 Packeda
RGB 8
BGR 8
YCbCr422_8
acA5472-17um Mono 8
Mono 12
Mono 12 Packed
acA5472-17umMED Mono 8
Mono 12
Mono 12 Packed
boA1936-400cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA1936-400cm Mono 8
Mono 10
Mono 12
boA2448-250cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA2448-250cm Mono 8
Mono 10
Mono 12
boA2832-190cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA2832-190cm Mono 8
Mono 10
Mono 12
boA4096-93cc Mono 8
Mono 10
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422
boA4096-93cm Mono 8
Mono 10
Mono 12
boA4096-180cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA4096-180cm Mono 8
Mono 10
Mono 12
boA4112-68cc Mono 8
Mono 10
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422
boA4112-68cm Mono 8
Mono 10
Mono 12
boA4500-45cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA4500-45cm Mono 8
Mono 10
Mono 12
boA4504-100cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA4504-100cm Mono 8
Mono 10
Mono 12
boA5320-150cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA5320-150cm Mono 8
Mono 10
Mono 12
boA5328-100cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA5328-100cm Mono 8
Mono 10
Mono 12
boA6500-36cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA6500-36cm Mono 8
Mono 10
Mono 12
boA8100-16cc Mono 8
Mono 10
Mono 12p
Bayer RG 8a
Bayer RG 10a
Bayer RG 12a
RGB 8
YUV422_8
boA8100-16cm Mono 8
Mono 10
Mono 12
daA720-520uc Mono 8
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
daA720-520um Mono 8
Mono 12
Mono 12p
daA1280-54uc Bayer 8
Bayer 12
RGB 8c
YCbCr422_8c
daA1280-54um Mono 8
Mono 12
daA1440-220uc Mono 8
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
daA1440-220um Mono 8
Mono 12
Mono 12p
daA1600-60uc Bayer 8a
Bayer 12ab
RGB 8c
YCbCr422_8c
daA1600-60um Mono 8
Mono 12b
daA1920-15um Mono 8
Mono 12
daA1920-30uc Bayer 8a
Bayer 12a
RGB 8c
YCbCr422_8c
daA1920-30um Mono 8
Mono 12
daA1920-160uc Mono 8
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
daA1920-160um Mono 8
Mono 12
Mono 12p
daA2448-70uc Mono 8
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
daA2448-70um Mono 8
Mono 12
Mono 12p
daA2500-14uc Bayer 8a
Bayer 12a
RGB 8c
YCbCr422_8c
daA2500-14um Mono 8
Mono 12
daA3840-45uc Mono 8
Mono 12
Mono 12p
Bayer RG 8a
Bayer RG 12a
Bayer RG 12pa
RGB 8
BGR 8
YCbCr422_8
daA3840-45um Mono 8
Mono 12
Mono 12p
puA1280-54uc Bayer 8
Bayer 12
RGB 8c
YCbCr422_8c
puA1280-54um Mono 8
Mono 12
puA1600-60uc Bayer 8a
Bayer 12ab
RGB 8c
YCbCr422_8c
puA1600-60um Mono 8
Mono 12b
puA1920-30uc Bayer 8a
Bayer 12a
RGB 8c
YCbCr422_8c
puA1920-30um Mono 8
Mono 12
puA2500-14uc Bayer 8a
Bayer 12a
RGB 8c
YCbCr422_8c
puA2500-14um Mono 8
Mono 12

  1. If you enable the Reverse X and Reverse Y feature, the actual Bayer color filter alignment changes.

  2. 12-bit image data based on 10-bit sensor data.

  3. By default, YCbCr422 and RGB 8 images are acquired in sRGB color space. You can use the BslColorSpaceMode parameter to change the color space to RGB.

Sample Code#

// Set the pixel format to Mono 8
camera.PixelFormat.SetValue(PixelFormat_Mono8);
INodeMap& nodemap = camera.GetNodeMap();
// Set the pixel format to Mono 8
CEnumParameter(nodemap, "PixelFormat").SetValue("Mono8");
// Set the pixel format to Mono 8
camera.Parameters[PLCamera.PixelFormat].SetValue(PLCamera.PixelFormat.Mono8);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Set the pixel format to Mono 8 */
errRes = PylonDeviceFeatureFromString(hdev, "PixelFormat", "Mono8");
CHECK(errRes);

You can also use the pylon Viewer to easily set the parameters.