Reverse X and Reverse Y#
Reverse X is available on all camera models. Reverse Y is available on selected camera models.
Using the Feature#
Enabling Reverse X#
To enable Reverse X, set the ReverseX
parameter to true
.
The camera mirrors the image horizontally:
Enabling Reverse Y#
On some camera models, the Reverse Y feature is also available.
To enable Reverse Y, set the ReverseY
parameter to true
.
The camera mirrors the image vertically:
Using Image ROIs or Auto Function ROIs with Reverse X or Reverse Y#
If you have specified an image ROI or auto function ROI while using Reverse X or Reverse Y, it depends on your camera model whether the position of the ROI relative to the sensor adapts to the mirrored image or not.
Self-Adapting ROI#
On some camera models, the position of the ROI relative to the sensor adapts to the mirrored image when you use the Reverse X or the Reverse Y feature. The camera captures the same portions of the image.
No Self-Adapting ROI#
On some camera models, the position of the ROI relative to the sensor remains the same. As a consequence, the camera captures different portions of the image depending on whether the Reverse X or the Reverse Y feature are enabled:
Effective Bayer Filter Alignments (Color Cameras Only)#
Depending on your camera model, the Bayer filter alignment changes when Reverse X, Reverse Y, or both are used.
For example, if you use a camera with a physical Bayer BG filter alignment and enable Reverse X, the actual Bayer filter alignment will be Bayer GB. The PixelFormat
parameter value changes accordingly.
Specifics#
Camera Model | Available Directions | Self-Adapting ROI | Changes in Bayer Filter Alignment |
---|---|---|---|
a2A640-240gmSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A640-240umSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A1280-80gmSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A1280-125umSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A1920-51gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A1920-51gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A1920-51gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A1920-51gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A1920-160ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A1920-160ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A1920-160umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A1920-160umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A1920-165g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A1920-165g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2048-35gmSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2048-110umSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2440-98g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2440-98g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2448-23gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2448-23gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2448-23gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2448-23gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2448-75ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2448-75ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2448-75umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2448-75umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2448-105g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2448-105g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2448-120cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2448-120cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2448-210cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2448-210cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2560-20gmSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2560-70umSWIR | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2590-22gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2590-22gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2590-22gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2590-22gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2590-60ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2590-60ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2590-60umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2590-60umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2600-20gcBAS | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A2600-20gcPRO | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A2600-20gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2600-20gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2600-64ucBAS | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A2600-64ucPRO | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A2600-64umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2600-64umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-14gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2840-14gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2840-14gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-14gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-14gmUV | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-48ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2840-48ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2840-48umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-48umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-48umUV | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-67g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2840-67g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-67g5mUV | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A2840-86cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A2840-86cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3536-9gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3536-9gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3536-9gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3536-9gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3536-31ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3536-31ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3536-31umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3536-31umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3536-42g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3536-42g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3840-13gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3840-13gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3840-13gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3840-13gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3840-45ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3840-45ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A3840-45umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A3840-45umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4096-9gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4096-9gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4096-9gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4096-9gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4096-30ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4096-30ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4096-30umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4096-30umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4096-44g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4096-44g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4096-67cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4096-67cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4200-12gcBAS | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4200-12gcPRO | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4200-12gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4200-12gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4200-40ucBAS | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4200-40ucPRO | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4200-40umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4200-40umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4504-5gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4504-5gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4504-5gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4504-5gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4504-18ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4504-18ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4504-18umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4504-18umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4504-27g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4504-27g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4504-42cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A4504-42cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4508-6gcBAS | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4508-6gcPRO | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4508-6gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4508-6gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4508-20ucBAS | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4508-20ucPRO | Reverse X Reverse Y | Yes | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
a2A4508-20umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A4508-20umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5060-4gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5060-4gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5060-15ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5060-15umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5060-21g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5060-21g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5320-7gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5320-7gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5320-7gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5320-7gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5320-23ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5320-23ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5320-23umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5320-23umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5320-34g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5320-34g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5320-52cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5320-52cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5328-4gcBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5328-4gcPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5328-4gmBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5328-4gmPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5328-15ucBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5328-15ucPRO | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5328-15umBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5328-15umPRO | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5328-22g5cBAS | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5328-22g5mBAS | Reverse X Reverse Y | Yes | N/A (mono camera) |
a2A5328-35cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
a2A5328-35cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
acA640-121gm | Reverse X | No | N/A (mono camera) |
acA640-300gc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA640-300gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA640-750uc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA640-750um | Reverse X Reverse Y | No | N/A (mono camera) |
acA720-290gc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA720-290gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA720-520uc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA720-520um | Reverse X Reverse Y | No | N/A (mono camera) |
acA800-200gc | Reverse X Reverse Y | No | N/A (mono camera) |
acA800-200gm | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA800-510uc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA800-510um | Reverse X Reverse Y | No | N/A (mono camera) |
acA1280-60gc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA1280-60gm | Reverse X | No | N/A (mono camera) |
acA1300-60gc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA1300-60gm | Reverse X | No | N/A (mono camera) |
acA1300-60gmNIR | Reverse X | No | N/A (mono camera) |
acA1300-75gc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA1300-75gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA1300-200uc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA1300-200um | Reverse X Reverse Y | No | N/A (mono camera) |
acA1440-73gc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA1440-73gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA1440-220uc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA1440-220um | Reverse X Reverse Y | No | N/A (mono camera) |
acA1600-20gc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA1600-20uc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA1600-60gc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA1600-60gm | Reverse X | No | N/A (mono camera) |
acA1920-25gc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA1920-25gm | Reverse X | No | N/A (mono camera) |
acA1920-25uc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA1920-25um | Reverse X | No | N/A (mono camera) |
acA1920-40gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA1920-40gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA1920-40uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA1920-40ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA1920-40um | Reverse X Reverse Y | No | N/A (mono camera) |
acA1920-40umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA1920-48gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA1920-48gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA1920-50gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA1920-50gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA1920-150uc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA1920-150um | Reverse X Reverse Y | No | N/A (mono camera) |
acA1920-155uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA1920-155ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA1920-155um | Reverse X Reverse Y | No | N/A (mono camera) |
acA1920-155umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA2000-50gc | Reverse X Reverse Y | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA2000-50gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA2000-165uc | Reverse X Reverse Y | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA2000-165um | Reverse X Reverse Y | No | N/A (mono camera) |
acA2040-25gc | Reverse X Reverse Y | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA2040-25gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA2040-25gmNIR | Reverse X Reverse Y | No | N/A (mono camera) |
acA2040-35gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2040-35gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA2040-55uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2040-55um | Reverse X Reverse Y | No | N/A (mono camera) |
acA2040-90uc | Reverse X Reverse Y | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA2040-90um | Reverse X Reverse Y | No | N/A (mono camera) |
acA2040-90umNIR | Reverse X Reverse Y | No | N/A (mono camera) |
acA2040-120uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2040-120um | Reverse X Reverse Y | No | N/A (mono camera) |
acA2440-20gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2440-20gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA2440-35uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2440-35ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2440-35um | Reverse X Reverse Y | No | N/A (mono camera) |
acA2440-35umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA2440-75uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2440-75ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA2440-75um | Reverse X Reverse Y | No | N/A (mono camera) |
acA2440-75umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA2500-14gc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA2500-14gm | Reverse X | No | N/A (mono camera) |
acA2500-14uc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA2500-14um | Reverse X | No | N/A (mono camera) |
acA2500-20gc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA2500-20gcMED | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA2500-20gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA2500-20gmMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA2500-60uc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA2500-60um | Reverse X Reverse Y | No | N/A (mono camera) |
acA3088-16gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA3088-16gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA3088-57uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA3088-57ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA3088-57um | Reverse X Reverse Y | No | N/A (mono camera) |
acA3088-57umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA3800-10gc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA3800-10gm | Reverse X | No | N/A (mono camera) |
acA3800-14uc | Reverse X | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
acA3800-14um | Reverse X | No | N/A (mono camera) |
acA4024-8gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4024-8gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA4024-29uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4024-29um | Reverse X Reverse Y | No | N/A (mono camera) |
acA4096-11gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4096-11gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA4096-30uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4096-30ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4096-30um | Reverse X Reverse Y | No | N/A (mono camera) |
acA4096-30umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA4096-40uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4096-40ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4096-40um | Reverse X Reverse Y | No | N/A (mono camera) |
acA4096-40umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA4112-8gc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4112-8gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA4112-20uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4112-20ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4112-20um | Reverse X Reverse Y | No | N/A (mono camera) |
acA4112-20umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA4112-30uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4112-30ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA4112-30um | Reverse X Reverse Y | No | N/A (mono camera) |
acA4112-30umMED | Reverse X Reverse Y | No | N/A (mono camera) |
acA5472-5gc | Reverse X Reverse Y | No | Default: BG Reverse X enabled: GB Reverse Y enabled: GR Reverse X and Reverse Y enabled: RG |
acA5472-5gm | Reverse X Reverse Y | No | N/A (mono camera) |
acA5472-17uc | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA5472-17ucMED | Reverse X Reverse Y | No | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
acA5472-17um | Reverse X Reverse Y | No | N/A (mono camera) |
acA5472-17umMED | Reverse X Reverse Y | No | N/A (mono camera) |
boA1936-400cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA1936-400cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA2448-250cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA2448-250cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA2832-190cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA2832-190cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA4096-93cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA4096-93cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA4096-180cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA4096-180cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA4112-68cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA4112-68cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA4500-45cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA4500-45cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA4504-100cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA4504-100cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA5120-150cc | Reverse X and Reverse Y feature not supported | N/A | N/A |
boA5120-150cm | Reverse X Reverse Y | No | N/A (mono camera) |
boA5120-230cc | Reverse X and Reverse Y feature not supported | N/A | N/A |
boA5120-230cm | Reverse X and Reverse Y feature not supported | N/A | N/A |
boA5320-150cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA5320-150cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA5328-100cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA5328-100cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA6500-36cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA6500-36cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA8100-16cc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
boA8100-16cm | Reverse X Reverse Y | Yes | N/A (mono camera) |
boA9344-30cc | Reverse X and Reverse Y feature not supported | N/A | N/A |
boA9344-30cm | Reverse X and Reverse Y feature not supported | N/A | N/A |
boA9344-70cc | Reverse X and Reverse Y feature not supported | N/A | N/A |
boA9344-70cm | Reverse X and Reverse Y feature not supported | N/A | N/A |
boA13440-17cm | Reverse X and Reverse Y feature not supported | Reverse X and Reverse Y feature not supported | N/A (mono camera) |
daA720-520uc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
daA720-520um | Reverse X Reverse Y | Yes | N/A (mono camera) |
daA1280-54uc | Reverse X Reverse Y | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
daA1280-54um | Reverse X Reverse Y | No | N/A (mono camera) |
daA1440-220uc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
daA1440-220um | Reverse X Reverse Y | Yes | N/A (mono camera) |
daA1600-60uc | Reverse X Reverse Y | No | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
daA1600-60um | Reverse X Reverse Y | No | N/A (mono camera) |
daA1920-15um | Reverse X Reverse Y | No | N/A (mono camera) |
daA1920-30uc | Reverse X Reverse Y | No | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
daA1920-30um | Reverse X Reverse Y | No | N/A (mono camera) |
daA1920-160uc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
daA1920-160um | Reverse X Reverse Y | Yes | N/A (mono camera) |
daA2448-70uc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
daA2448-70um | Reverse X Reverse Y | Yes | N/A (mono camera) |
daA2500-14uc | Reverse X Reverse Y | No | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
daA2500-14um | Reverse X Reverse Y | No | N/A (mono camera) |
daA3840-45uc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
daA3840-45um | Reverse X Reverse Y | Yes | N/A (mono camera) |
dmA720-290gc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
dmA720-290gm | Reverse X Reverse Y | Yes | N/A (mono camera) |
dmA1440-73gc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
dmA1440-73gm | Reverse X Reverse Y | Yes | N/A (mono camera) |
dmA1920-51gc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
dmA1920-51gm | Reverse X Reverse Y | Yes | N/A (mono camera) |
dmA3536-9gc | Reverse X Reverse Y | Yes | Default: RG Reverse X enabled: GR Reverse Y enabled: GB Reverse X and Reverse Y enabled: BG |
dmA3536-9gm | Reverse X Reverse Y | Yes | N/A (mono camera) |
puA1280-54uc | Reverse X Reverse Y | No | Reverse X and Reverse Y don't affect Bayer filter alignment |
puA1280-54um | Reverse X Reverse Y | No | N/A (mono camera) |
puA1600-60uc | Reverse X Reverse Y | No | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
puA1600-60um | Reverse X Reverse Y | No | N/A (mono camera) |
puA1920-30uc | Reverse X Reverse Y | No | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
puA1920-30um | Reverse X Reverse Y | No | N/A (mono camera) |
puA2500-14uc | Reverse X Reverse Y | No | Default: GB Reverse X enabled: BG Reverse Y enabled: RG Reverse X and Reverse Y enabled: GR |
puA2500-14um | Reverse X Reverse Y | No | N/A (mono camera) |
r2L2048-29gc | Reverse X | Yes | N/A |
r2L2048-58gm | Reverse X | Yes | N/A (mono camera) |
r2L2048-62cc | Reverse X | Yes | N/A |
r2L2048-62g5c | Reverse X | Yes | N/A |
r2L2048-172cm | Reverse X | Yes | N/A (mono camera) |
r2L2048-172g5m | Reverse X | Yes | N/A (mono camera) |
r2L4096-14gc | Reverse X | Yes | N/A |
r2L4096-29gm | Reverse X | Yes | N/A (mono camera) |
r2L4096-42cc | Reverse X | Yes | N/A |
r2L4096-42g5c | Reverse X | Yes | N/A |
r2L4096-84cm | Reverse X | Yes | N/A (mono camera) |
r2L4096-84g5m | Reverse X | Yes | N/A (mono camera) |
r2L8192-200cm | Reverse X | Yes | N/A (mono camera) |
r2L16384-120cm | Reverse X | Yes | N/A (mono camera) |
Sample Code#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Enable Reverse X */
errRes = PylonDeviceSetBooleanFeature(hdev, "ReverseX", 1);
CHECK(errRes);
/* Enable Reverse Y, if available */
errRes = PylonDeviceSetBooleanFeature(hdev, "ReverseY", 1);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.