Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Temperature State#

The Temperature State camera feature indicates whether the camera's internal temperature is normal or too high.

When the temperature is too high, immediate cooling is required.

Use the Device Temperature feature to determine the camera's current temperature.

Using the Feature#

How It Works#

Information about the internal temperature is provided by the following parameters:

  • The DeviceTemperature parameter value shows the current temperature at various locations within the camera. For more information, see the Device Temperature topic.
  • The TemperatureState parameter value tells you the camera's current internal temperature state:
    • Ok: The device temperature is within the normal operating temperature range.
    • Critical: The device temperature is close to or at the allowed maximum. Provide cooling.
    • Error: The device temperature is above the allowed maximum. Provide cooling immediately.

Depending on your camera model, the following additional parameters are available:

  • The BslTemperatureStatusErrorCount parameter indicates how often the temperature state changed to Error.
  • The BslTemperatureMax parameter indicates the maximum temperature the camera reached during operation.

When the TemperatureState parameter value is Critical or Error, the camera provides a set of mechanisms that alert the user and help to protect the camera.

The mechanisms take effect at different device temperatures, depending on the alert level and on whether the camera is heating up or cooling down.

Info

Normal camera operation requires that the temperature state stays at Ok and the housing temperature stays within the allowed range. To ensure this, follow the guidelines set out in the "Environmental Requirements" section of your camera topic. You can find your camera topic in the "Models" section.

At elevated temperatures, the camera may get damaged, the camera's lifetime is shortened, and image quality can degrade. The lifetime is also shortened by frequent high-temperature incidents.

Heating Path and Cooling Path

Heating Path#

Critical Temperature Threshold#

When the device temperature reaches the critical temperature threshold, the camera is close to becoming too hot.

In this situation, the following happens:

  • The TemperatureState parameter value changes to Critical.
  • The camera sends a Critical Temperature event.

Info

Another Critical Temperature event can only be sent after the device temperature has fallen to at least 4 °C below the critical temperature threshold.

Over Temperature Threshold#

When the device temperature reaches the over temperature threshold, the camera is too hot. The camera must be cooled immediately. Otherwise, the camera may get irreversibly damaged.

In this situation, the following happens:

  • The TemperatureState parameter value changes to Error.
  • The camera's current draw reduces.
  • Image acquisition changes:
    • On ace 2, boost, dart M/R, and racer 2 cameras, image acquisition stops and can't be started until the device has cooled down.
    • On other cameras, test image 2 appears.
  • The camera sends an Over Temperature event.
  • If the Error Code feature is available on your camera model, the camera reports an over temperature error code.
  • If available, the BslTemperatureStatusErrorCount parameter increases by 1.

Info

Another Over Temperature event can only be sent after the device temperature has fallen to at least 4 °C below the over temperature threshold.

Cooling Path#

Over Temperature Threshold#

When the device temperature falls below the over temperature threshold, the following happens:

  • The TemperatureState parameter value changes from Error to Critical.

When the device temperature falls to 4 °C below the over temperature threshold, the following happens:

  • On ace 2, boost, dart M/R, and racer 2 cameras, image acquisition can be started again.
  • On other cameras, test image 2 disappears. Image acquisition resumes with the same settings and features as before the camera entered the Error state. The exception is the Sequencer feature which you have to re-enable manually.
Critical Temperature Threshold#

When the device temperature falls below the critical temperature threshold, the following happens:

  • The TemperatureState parameter value changes to Ok.

The camera's temperature state and internal temperature are normal and therefore allow normal camera operation.

Determining the Temperature State#

  1. Get the TemperatureState parameter value.
  2. If the parameter value is Critical or Error, you must cool the camera until the parameter value is Ok.

To make full use of the Temperature State feature:

  • Use the Device Temperature feature to determine the exact core board or sensor board temperature.
  • Enable the Event Notification feature to receive events whenever the camera gets too hot.
  • If the Error Code feature is available on your camera model, read the LastError parameter value to determine whether the camera was too hot.

Specifics#

Show all camera models

Camera Model Critical Temperature Threshold Over Temperature Threshold Additional Parameters
a2A640-240gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A640-240umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1280-80gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1280-125umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gcIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gmIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-165g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-165g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-35gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-37gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-37gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-37gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-37gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-110umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-114g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-114g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-114ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-114ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-114umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-114umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-173cmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2440-98g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2440-98g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gcIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gmIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-105g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-105g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-120cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-120cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-210cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-210cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2560-20gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2560-70umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2560-131cmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gcIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gmIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gmUV 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48umUV 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-67g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-67g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-67g5mUV 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-86cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-86cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-9gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-9gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-9gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-9gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-31ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-31ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-31umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-31umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-42g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3536-42g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gcIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gmIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-44g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-44g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-67cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-67cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gcIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gmIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-27g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-27g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-42cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-42cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-4gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-4gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-15ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-15umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-21g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-21g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-35cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5060-35cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gcIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gmip67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-34g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-34g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-52cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-52cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gcIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gmIP67 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-22g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-22g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-35cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-35cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
acA640-121gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA640-300gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA640-300gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA640-750uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA640-750um 75 °C (167 °F) 81 °C (177.8 °F) None
acA720-290gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA720-290gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA720-520uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA720-520um 75 °C (167 °F) 81 °C (177.8 °F) None
acA800-200gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA800-200gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA800-510uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA800-510um 75 °C (167 °F) 81 °C (177.8 °F) None
acA1280-60gc Temperature State feature not supported Temperature State feature not supported None
acA1280-60gm Temperature State feature not supported Temperature State feature not supported None
acA1300-60gc Temperature State feature not supported Temperature State feature not supported None
acA1300-60gm Temperature State feature not supported Temperature State feature not supported None
acA1300-60gmNIR Temperature State feature not supported Temperature State feature not supported None
acA1300-75gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1300-75gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1300-200uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA1300-200um 75 °C (167 °F) 81 °C (177.8 °F) None
acA1440-73gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1440-73gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1440-220uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA1440-220um 75 °C (167 °F) 81 °C (177.8 °F) None
acA1600-20gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1600-20uc Temperature State feature not supported Temperature State feature not supported None
acA1600-60gc Temperature State feature not supported Temperature State feature not supported None
acA1600-60gm Temperature State feature not supported Temperature State feature not supported None
acA1920-25gc Temperature State feature not supported Temperature State feature not supported None
acA1920-25gm Temperature State feature not supported Temperature State feature not supported None
acA1920-25uc Temperature State feature not supported Temperature State feature not supported None
acA1920-25um Temperature State feature not supported Temperature State feature not supported None
acA1920-40gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1920-40gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1920-40uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-40ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-40um 75 °C (167.0 °F) 81 °C (177.8 °F) None
acA1920-40umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-48gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1920-48gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1920-50gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1920-50gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA1920-150uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-150um 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-155uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-155ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-155um 75 °C (167 °F) 81 °C (177.8 °F) None
acA1920-155umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA2000-50gc Temperature State feature not supported Temperature State feature not supported None
acA2000-50gm Temperature State feature not supported Temperature State feature not supported None
acA2000-165uc Temperature State feature not supported Temperature State feature not supported None
acA2000-165um Temperature State feature not supported Temperature State feature not supported None
acA2040-25gc Temperature State feature not supported Temperature State feature not supported None
acA2040-25gm Temperature State feature not supported Temperature State feature not supported None
acA2040-25gmNIR Temperature State feature not supported Temperature State feature not supported None
acA2040-35gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2040-35gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2040-55uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA2040-55um 75 °C (167 °F) 81 °C (177.8 °F) None
acA2040-90uc Temperature State feature not supported Temperature State feature not supported None
acA2040-90um Temperature State feature not supported Temperature State feature not supported None
acA2040-90umNIR Temperature State feature not supported Temperature State feature not supported None
acA2040-120uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA2040-120um 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-20gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2440-20gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2440-35uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-35ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-35um 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-35umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-75uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-75ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-75um 75 °C (167 °F) 81 °C (177.8 °F) None
acA2440-75umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA2500-14gc Temperature State feature not supported Temperature State feature not supported None
acA2500-14gm Temperature State feature not supported Temperature State feature not supported None
acA2500-14uc Temperature State feature not supported Temperature State feature not supported None
acA2500-14um Temperature State feature not supported Temperature State feature not supported None
acA2500-20gc 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2500-20gcMED 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2500-20gm 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2500-20gmMED 72 °C (161.6 °F) 78 °C (172.4 °F) None
acA2500-60uc 75 °C (167 °F) 81 °C (177.8 °F) None
acA2500-60um 75 °C (167 °F) 81 °C (177.8 °F) None
acA3088-16gc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA3088-16gm The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA3088-57uc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA3088-57ucMED 290 °C (554 °F) 300 °C (572 °F) None
acA3088-57um The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA3088-57umMED 290 °C (554 °F) 300 °C (572 °F) None
acA3800-10gc Temperature State feature not supported Temperature State feature not supported None
acA3800-10gm Temperature State feature not supported Temperature State feature not supported None
acA3800-14uc Temperature State feature not supported Temperature State feature not supported None
acA3800-14um Temperature State feature not supported Temperature State feature not supported None
acA4024-8gc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA4024-8gm The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA4024-29uc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA4024-29um The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA4096-11gc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA4096-11gm The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. - None
acA4096-30uc 80 °C (176 °F) 86 °C (186.8 °F) None
acA4096-30ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA4096-30um 80 °C (176 °F) 86 °C (186.8 °F) None
acA4096-30umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA4096-40uc 80 °C (176 °F) 86 °C (186.8 °F) None
acA4096-40ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA4096-40um 80 °C (176 °F) 86 °C (186.8 °F) None
acA4096-40umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA4112-8gc 79 °C (174.2 °F) 85 °C (185 °F) None
acA4112-8gm 79 °C (174.2 °F) 85 °C (185 °F) None
acA4112-20uc 80 °C (176 °F) 86 °C (186.8 °F) None
acA4112-20ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA4112-20um 80 °C (176 °F) 86 °C (186.8 °F) None
acA4112-20umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA4112-30uc 80 °C (176 °F) 86 °C (186.8 °F) None
acA4112-30ucMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA4112-30um 80 °C (176 °F) 86 °C (186.8 °F) None
acA4112-30umMED 75 °C (167 °F) 81 °C (177.8 °F) None
acA5472-5gc 71 °C (159.8 °F) 77 °C (170.6 °F) None
acA5472-5gm 71 °C (159.8 °F) 77 °C (170.6 °F) None
acA5472-17uc 74 °C (174.2 °F) 80 °C (176 °F) None
acA5472-17ucMED 74 °C (174.2 °F) 80 °C (176 °F) None
acA5472-17um 74 °C (165.2 °F) 80 °C (176 °F) None
acA5472-17umMED 74 °C (174.2 °F) 80 °C (176 °F) None
boA1936-400cc 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
boA1936-400cm 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
boA2448-250cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA2448-250cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA2832-190cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA2832-190cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA4096-93cc Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA4096-93cm Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA4096-180cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA4096-180cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA4112-68cc Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA4112-68cm Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA4500-45cc Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA4500-45cm Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA4504-100cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA4504-100cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5120-150cc 86 °C (186.8 °F) 90 °C (194 °F) None
boA5120-150cm 86 °C (186.8 °F) 90 °C (194 °F) None
boA5120-230cc 86 °C (186.8 °F) 90 °C (194 °F) None
boA5120-230cm 86 °C (186.8 °F) 90 °C (194 °F) None
boA5320-150cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5320-150cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5328-100cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5328-100cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87 °C (188.6 °F) / 90 °C (194 °F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA6500-36cc Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA6500-36cm Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA8100-16cc Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA8100-16cm Temperature State feature not supported Temperature State feature not supported BslTemperatureMax
BslTemperatureStatusErrorCount
boA9344-30cc 86 °C (186.8 °F) 90 °C (194 °F) None
boA9344-30cm 86 °C (186.8 °F) 90 °C (194 °F) None
boA9344-70cc 86 °C (186.8 °F) 90 °C (194 °F) None
boA9344-70cm 86 °C (186.8 °F) 90 °C (194 °F) None
boA13440-17cm 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA720-520uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA720-520um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1280-54uc Temperature State feature not supported Temperature State feature not supported None
daA1280-54um Temperature State feature not supported Temperature State feature not supported None
daA1440-220uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1440-220um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1600-60uc Temperature State feature not supported Temperature State feature not supported None
daA1600-60um Temperature State feature not supported Temperature State feature not supported None
daA1920-15um Temperature State feature not supported Temperature State feature not supported None
daA1920-30uc Temperature State feature not supported Temperature State feature not supported None
daA1920-30um Temperature State feature not supported Temperature State feature not supported None
daA1920-160uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1920-160um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA2448-70uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA2448-70um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA2500-14uc Temperature State feature not supported Temperature State feature not supported None
daA2500-14um Temperature State feature not supported Temperature State feature not supported None
daA3840-45uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA3840-45um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA720-290gc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA720-290gm 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1440-73gc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1440-73gm 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1920-51gc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1920-51gm 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA2048-37gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA2048-37gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA2448-23gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA2448-23gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA2840-14gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA2840-14gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA3536-9gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA3536-9gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA4096-9gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA4096-9gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
puA1280-54uc Temperature State feature not supported Temperature State feature not supported None
puA1280-54um Temperature State feature not supported Temperature State feature not supported None
puA1600-60uc Temperature State feature not supported Temperature State feature not supported None
puA1600-60um Temperature State feature not supported Temperature State feature not supported None
puA1920-30uc Temperature State feature not supported Temperature State feature not supported None
puA1920-30um Temperature State feature not supported Temperature State feature not supported None
puA2500-14uc Temperature State feature not supported Temperature State feature not supported None
puA2500-14um Temperature State feature not supported Temperature State feature not supported None
r2L2048-29gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-58gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-62cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-62g5c 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-172cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-172g5m 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-14gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-29gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-42cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-42g5c 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-84cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-84g5m 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L8192-80cc 67 °C (152.6 °F) 72 °C (161.6 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L8192-240cm 67 °C (152.6 °F) 72 °C (161.6 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L16384-60cc 67 °C (152.6 °F) 72 °C (161.6 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L16384-120cm 67 °C (152.6 °F) 72 °C (161.6 °F) BslTemperatureMax
BslTemperatureStatusErrorCount

  1. 1 CXP with PoCXP / 1 CXP via AUX power or 2 CXP

Sample Code#

ace 2, boost, dart M/R, and racer 2 Cameras#
// Get the current temperature state
BslTemperatureStatusEnums e = camera.BslTemperatureStatus.GetValue();
// Get the maximum temperature the camera reached during operation
double temperatureMax = camera.BslTemperatureMax.GetValue();
// Determine how often the temperature state changed to Error
int64_t i = camera.BslTemperatureStatusErrorCount.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Get the current temperature state
String_t e = CEnumParameter(nodemap, "BslTemperatureStatus").GetValue();
// Get the maximum temperature the camera reached during operation
double temperatureMax = CFloatParameter(nodemap, "BslTemperatureMax").GetValue();
// Determine how often the temperature state changed to Error
int64_t i = CIntegerParameter(nodemap, "BslTemperatureStatusErrorCount").GetValue();
// Get the current temperature state
string e = camera.Parameters[PLCamera.BslTemperatureStatus].GetValue();
// Get the maximum temperature the camera reached during operation
double temperatureMax = camera.Parameters[PLCamera.BslTemperatureMax].GetValue();
// Determine how often the temperature state changed to Error
Int64 i = camera.Parameters[PLCamera.BslTemperatureStatusErrorCount].GetValue();
size_t len = 0;
char e_str[64] = {0};
double temperatureMax = 0;
int64_t i = 0;
/* Get the current temperature state */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "BslTemperatureStatus", e_str, &len);
CHECK(errRes);
/* Get the maximum temperature the camera reached during operation */
errRes = PylonDeviceGetFloatFeature(hdev, "BslTemperatureMax", &temperatureMax);
CHECK(errRes);
/* Determine how often the temperature state changed to Error */
errRes = PylonDeviceGetIntegerFeature(hdev, "BslTemperatureStatusErrorCount", &i);
CHECK(errRes);
# Get the current temperature state
e = camera.BslTemperatureStatus.Value
# Get the maximum temperature the camera reached during operation
temperatureMax = camera.BslTemperatureMax.Value
# Determine how often the temperature state changed to Error
i = camera.BslTemperatureStatusErrorCount.Value
Other Cameras#
// Get the current temperature state
TemperatureStateEnums e = camera.TemperatureState.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Get the current temperature state
String_t e = CEnumParameter(nodemap, "TemperatureState").GetValue();
// Get the current temperature state
string e = camera.Parameters[PLCamera.TemperatureState].GetValue();
size_t len = 0;
char e_str[64] = {0};
/* Get the current temperature state */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "TemperatureState", e_str, &len);
CHECK(errRes);
# Get the current temperature state
e = camera.TemperatureState.Value

You can also use the pylon Viewer to easily set the parameters.