Trigger Selector#
Once selected, you can use the trigger type for a number of camera configuration tasks, e.g., enabling hardware triggering.
Using the Feature#
Selecting a Trigger Type#
To select a trigger type, set the TriggerSelector
parameter to one of the following values (if available):
FrameStart
FrameEnd
FrameActive
FrameBurstStart
FrameBurstEnd
FrameBurstActive
ExposureStart
ExposureEnd
ExposureActive
Common Tasks#
Once you have selected a trigger type, you can do the following:
Task | Feature |
---|---|
Enabling or disabling the selected trigger | Trigger Mode |
Configuring how the selected trigger can be triggered | Trigger Source |
Defining which signal transition activates the selected trigger | Trigger Activation |
Configuring a delay between the receipt of a trigger signal and the moment when the trigger selected becomes effective | Trigger Delay |
Available Trigger Types#
Frame Burst Start (= Acquisition Start), End, and Active Trigger#
Info
The Frame Burst Start trigger and the Acquisition Start trigger are identical, only the names differ. The naming depends on your camera model. In the following, the term "Frame Burst Start trigger" is used to describe both types.
If available, you can use the Frame Burst Start, End, and Active triggers to control the acquisition of a series of images (a "burst" of images).
The number of images per series is specified by the AcquisitionBurstFrameCount
parameter. The maximum number of images per series depends on your camera model.
By default, these triggers are disabled, and the camera acquires single images only.
If you enable these triggers and the camera receives the corresponding signal via the trigger source configured, the following happens:
- Frame Burst Start: The camera initializes the acquisition of a series of images.
If the Frame Start trigger is enabled, the camera is now ready to receive Frame Start trigger signals.
If the Frame Start trigger is disabled and the Exposure Start trigger is enabled, the camera automatically initializes the next image.
If the Frame Start trigger is disabled and the Exposure Start trigger is also disabled or not available, the camera automatically acquires the entire series of images. - Frame Burst End: The camera finalizes the acquisition of a series of images.
If this trigger is disabled or not available, the camera automatically finalizes the series after the last image acquisition. - Frame Burst Active: When the trigger signal rises, the camera generates a Frame Burst Start trigger signal. When the trigger signal falls, the camera generates a Frame Burst End trigger signal. You can change this behavior using the Trigger Activation feature.
Frame Start, End, and Active Trigger#
Info
- If you want to use any of these triggers, the exposure mode must be set to
Timed
orTriggerWidth
.
If available, you can use the Frame Start, End, and Active triggers to control the acquisition of a single image. These are the trigger types used most commonly. In most image applications, you will only need to configure these trigger types.
By default, these triggers are disabled, and the camera controls image acquisition automatically.
If you enable these triggers and the camera receives the corresponding signal via the trigger source configured, the following happens:
- Frame Start: The camera initializes the acquisition of one image.
If the Exposure Start trigger is enabled, the camera is now ready to receive Exposure Start trigger signals.
If the Exposure Start trigger is not available or disabled, the camera automatically starts exposing the image. Note that in this case, exposure starts with a delay (see exposure start delay). - Frame End: The camera finalizes the acquisition of one image.
If this trigger is disabled or not available, the camera automatically finalizes image acquisition after exposure. - Frame Active: When the trigger signal rises, the camera generates a Frame Start trigger signal. When the trigger signal falls, the camera generates a Frame End trigger signal. You can change this behavior using the Trigger Activation feature.
Exposure Start, End, and Active Trigger#
If available, you can use the Exposure Start, End, and Active triggers to control the exposure of a single image.
Info
- If you want to use any of these triggers, the exposure mode must be set to
TriggerControlled
. - If the exposure mode is set to
Timed
orTriggerWidth
, these triggers can't be enabled, i.e., theirTriggerMode
setting will permanently be set toOff
. - If you want to use the Exposure Start and End triggers, you must enable both for them to work.
By default, these triggers are disabled, and the camera exposes images automatically.
If you enable these triggers, set the exposure mode to TriggerControlled
, and the camera receives the corresponding signal via the trigger source configured, the following happens:
- Exposure Start: The camera starts exposing one image.
- Exposure End: The camera stops exposing one image.
- Exposure Active: When the trigger signal rises, the camera generates an Exposure Start trigger signal. When the trigger signal falls, the camera generates an Exposure End trigger signal. You can change this behavior using the Trigger Activation feature.
Using the Trigger Types#
Use Case 1: Frame Burst Triggering#
Assume you want to trigger the acquisition of a series of images with only one trigger signal.
To achieve this, enable the Frame Burst Start trigger and disable all other available trigger types. Also, set the AcquisitionBurstFrameCount
parameter to 3.
This way, every time the camera successfully receives a Frame Burst Start trigger signal, the camera automatically acquires a complete series of three images.
Afterwards, the camera waits for the next Frame Burst Start trigger signal. On the next trigger signal, the camera acquires another 3 images, and so on.
Info
On some cameras, the High Speed burst mode is available. This mode offers higher frame rates during a burst.
Use Case 2: Exposure Triggering Using Two Input Lines#
Assume that you want to control the length of exposure via external trigger signals on two input lines. Also assume that the Exposure Start and Exposure End triggers are available on your camera.
In this case, set the exposure mode to TriggerControlled
and enable the Exposure Start and Exposure End triggers.
Then, set the trigger source for the Exposure Start trigger to Line 1 and the trigger source for the Exposure End trigger to Line 2.
Now, you can start the exposure by applying a hardware trigger signal on Line 1 and stop the exposure by applying a hardware trigger signal on Line 2.
Specifics#
Camera Model | Available Trigger Types | Maximum Number of Images per Series |
---|---|---|
a2A640-240gmSWIR | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A640-240umSWIR | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1280-80gmSWIR | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1280-125umSWIR | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-51gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-51gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-51gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-51gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-160ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-160ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-160umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-160umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-165g5cBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A1920-165g5mBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-23gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-23gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-23gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-23gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-75ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-75ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-75umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-75umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-105g5cBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2448-105g5mBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-22gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-22gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-22gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-22gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-60ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-60ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-60umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2590-60umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-20gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-20gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-20gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-20gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-64ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-64ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-64umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2600-64umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-14gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-14gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-14gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-14gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-48ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-48ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-48umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-48umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-67g5cBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A2840-67g5mBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-13gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-13gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-13gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-13gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-45ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-45ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-45umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A3840-45umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-9gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-9gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-9gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-9gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-30ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-30ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-30umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-30umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-44g5cBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4096-44g5mBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-12gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-12gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-12gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-12gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-40ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-40ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-40umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4200-40umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-5gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-5gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-5gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-5gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-18ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-18ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-18umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-18umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-27g5cBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A4504-27g5mBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-7gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-7gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-7gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-7gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-23ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-23ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-23umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-23umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-34g5cBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5320-34g5mBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-4gcBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-4gcPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-4gmBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-4gmPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-15ucBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-15ucPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-15umBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-15umPRO | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-22g5cBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
a2A5328-22g5mBAS | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023a |
acA640-90gc | Frame Start Aquisition Start | 255 |
acA640-90uc | Frame Start Frame Burst Start | 255 |
acA640-121gm | Frame Start Aquisition Start | 255 |
acA640-300gc | Frame Start Acquisition Start | 255 |
acA640-300gm | Frame Start Aquisition Start | 255 |
acA640-750uc | Frame Start Frame Burst Start | 255 |
acA640-750um | Frame Start Frame Burst Start | 255 |
acA720-290gc | Frame Start Acquisition Start | 255 |
acA720-290gm | Frame Start Acquisition Start | 255 |
acA720-520uc | Frame Start Frame Burst Start | 255 |
acA720-520um | Frame Start Frame Burst Start | 255 |
acA800-200gc | Frame Start Acquisition Start | 255 |
acA800-200gm | Frame Start Acquisition Start | 255 |
acA800-510uc | Frame Start Frame Burst Start | 255 |
acA800-510um | Frame Start Frame Burst Start | 255 |
acA1280-60gc | Frame Start Acquisition Start | 255 |
acA1280-60gm | Frame Start Acquisition Start | 255 |
acA1300-60gc | Frame Start Acquisition Start | 255 |
acA1300-60gm | Frame Start Acquisition Start | 255 |
acA1300-60gmNIR | Frame Start Acquisition Start | 255 |
acA1300-75gc | Frame Start Acquisition Start | 255 |
acA1300-75gm | Frame Start Acquisition Start | 255 |
acA1300-200uc | Frame Start Frame Burst Start | 255 |
acA1300-200um | Frame Start Frame Burst Start | 255 |
acA1440-73gc | Frame Start Acquisition Start | 255 |
acA1440-73gm | Frame Start Acquisition Start | 255 |
acA1440-220uc | Frame Start Frame Burst Start | 255 |
acA1440-220um | Frame Start Frame Burst Start | 255 |
acA1600-20gc | Frame Start Acquisition Start | 255 |
acA1600-20uc | Frame Start Frame Burst Start | 255 |
acA1600-60gc | Frame Start Acquisition Start | 255 |
acA1600-60gm | Frame Start Acquisition Start | 255 |
acA1920-25gc | Frame Start Acquisition Start | 255 |
acA1920-25gm | Frame Start Acquisition Start | 255 |
acA1920-25uc | Frame Start Frame Burst Start | 255 |
acA1920-25um | Frame Start Frame Burst Start | 255 |
acA1920-40gc | Frame Start Acquisition Start | 255 |
acA1920-40gm | Frame Start Acquisition Start | 255 |
acA1920-40uc | Frame Start Frame Burst Start | 255 |
acA1920-40ucMED | Frame Start Frame Burst Start | 255 |
acA1920-40um | Frame Start Frame Burst Start | 255 |
acA1920-40umMED | Frame Start Frame Burst Start | 255 |
acA1920-48gc | Frame Start Acquisition Start | 255 |
acA1920-48gm | Frame Start Acquisition Start | 255 |
acA1920-50gc | Frame Start Acquisition Start | 255 |
acA1920-50gm | Frame Start Acquisition Start | 255 |
acA1920-150uc | Frame Start Frame Burst Start | 255 |
acA1920-150um | Frame Start Frame Burst Start | 255 |
acA1920-155uc | Frame Start Frame Burst Start | 255 |
acA1920-155ucMED | Frame Start Frame Burst Start | 255 |
acA1920-155um | Frame Start Frame Burst Start | 255 |
acA1920-155umMED | Frame Start Frame Burst Start | 255 |
acA2000-50gc | Frame Start Acquisition Start | 65535 |
acA2000-50gm | Frame Start Acquisition Start | 65535 |
acA2000-165uc | Frame Start Frame Burst Start | 255 |
acA2000-165um | Frame Start Frame Burst Start | 255 |
acA2040-25gc | Frame Start Acquisition Start | 65535 |
acA2040-25gm | Frame Start Acquisition Start | 65535 |
acA2040-25gmNIR | Frame Start Acquisition Start | 65535 |
acA2040-35gc | Frame Start Acquisition Start | 255 |
acA2040-35gm | Frame Start Acquisition Start | 255 |
acA2040-55uc | Frame Start Frame Burst Start | 255 |
acA2040-55um | Frame Start Frame Burst Start | 255 |
acA2040-90uc | Frame Start Frame Burst Start | 255 |
acA2040-90um | Frame Start Frame Burst Start | 255 |
acA2040-90umNIR | Frame Start Frame Burst Start | 255 |
acA2040-120uc | Frame Start Frame Burst Start | 255 |
acA2040-120um | Frame Start Frame Burst Start | 255 |
acA2440-20gc | Frame Start Acquisition Start | 255 |
acA2440-20gm | Frame Start Acquisition Start | 255 |
acA2440-35uc | Frame Start Frame Burst Start | 255 |
acA2440-35ucMED | Frame Start Frame Burst Start | 255 |
acA2440-35um | Frame Start Frame Burst Start | 255 |
acA2440-35umMED | Frame Start Frame Burst Start | 255 |
acA2440-75uc | Frame Start Frame Burst Start | 255 |
acA2440-75ucMED | Frame Start Frame Burst Start | 255 |
acA2440-75um | Frame Start Frame Burst Start | 255 |
acA2440-75umMED | Frame Start Frame Burst Start | 255 |
acA2500-14gc | Frame Start Acquisition Start | 255 |
acA2500-14gm | Frame Start Acquisition Start | 255 |
acA2500-14uc | Frame Start Frame Burst Start | 255 |
acA2500-14um | Frame Start Frame Burst Start | 255 |
acA2500-20gc | Frame Start Acquisition Start | 255 |
acA2500-20gcMED | Frame Start Acquisition Start | 255 |
acA2500-20gm | Frame Start Acquisition Start | 255 |
acA2500-20gmMED | Frame Start Acquisition Start | 255 |
acA2500-60uc | Frame Start Frame Burst Start | 255 |
acA2500-60um | Frame Start Frame Burst Start | 255 |
acA3088-16gc | Frame Start Acquisition Start | 255 |
acA3088-16gm | Frame Start Acquisition Start | 255 |
acA3088-57uc | Frame Start Frame Burst Start | 255 |
acA3088-57ucMED | Frame Start Frame Burst Start | 255 |
acA3088-57um | Frame Start Frame Burst Start | 255 |
acA3088-57umMED | Frame Start Frame Burst Start | 255 |
acA3800-10gc | Frame Start Acquisition Start | 255 |
acA3800-10gm | Frame Start Acquisition Start | 255 |
acA3800-14uc | Frame Start Frame Burst Start | 255 |
acA3800-14um | Frame Start Frame Burst Start | 255 |
acA4024-8gc | Frame Start Acquisition Start | 255 |
acA4024-8gm | Frame Start Acquisition Start | 255 |
acA4024-29uc | Frame Start Frame Burst Start | 255 |
acA4024-29um | Frame Start Frame Burst Start | 255 |
acA4096-11gc | Frame Start Acquisition Start | 255 |
acA4096-11gm | Frame Start Acquisition Start | 255 |
acA4096-30uc | Frame Start Frame Burst Start | 255 |
acA4096-30ucMED | Frame Start Frame Burst Start | 255 |
acA4096-30um | Frame Start Frame Burst Start | 255 |
acA4096-30umMED | Frame Start Frame Burst Start | 255 |
acA4096-40uc | Frame Start Frame Burst Start | 255 |
acA4096-40ucMED | Frame Start Frame Burst Start | 255 |
acA4096-40um | Frame Start Frame Burst Start | 255 |
acA4096-40umMED | Frame Start Frame Burst Start | 255 |
acA4112-8gc | Frame Start Acquisition Start | 255 |
acA4112-8gm | Frame Start Acquisition Start | 255 |
acA4112-20uc | Frame Start Frame Burst Start | 255 |
acA4112-20ucMED | Frame Start Frame Burst Start | 255 |
acA4112-20um | Frame Start Frame Burst Start | 255 |
acA4112-20umMED | Frame Start Frame Burst Start | 255 |
acA4112-30uc | Frame Start Frame Burst Start | 255 |
acA4112-30ucMED | Frame Start Frame Burst Start | 255 |
acA4112-30um | Frame Start Frame Burst Start | 255 |
acA4112-30umMED | Frame Start Frame Burst Start | 255 |
acA4600-7gc | Frame Start Acquisition Start | 255 |
acA4600-10uc | Frame Start Frame Burst Start | 255 |
acA5472-5gc | Frame Start Acquisition Start | 255 |
acA5472-5gm | Frame Start Acquisition Start | 255 |
acA5472-17uc | Frame Start Frame Burst Start | 255 |
acA5472-17ucMED | Frame Start Frame Burst Start | 255 |
acA5472-17um | Frame Start Frame Burst Start | 255 |
acA5472-17umMED | Frame Start Frame Burst Start | 255 |
boA1936-400cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA1936-400cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA2448-250cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA2448-250cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA2832-190cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA2832-190cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4096-93cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4096-93cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4096-180cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4096-180cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4112-68cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4112-68cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4500-45cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4500-45cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4504-100cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA4504-100cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA5320-150cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA5320-150cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA5328-100cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA5328-100cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA6500-36cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA6500-36cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA8100-16cc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
boA8100-16cm | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA720-520uc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA720-520um | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA1280-54uc | Frame Start | N/A |
daA1280-54um | Frame Start | N/A |
daA1440-220uc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA1440-220um | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA1600-60uc | Frame Start | N/A |
daA1600-60um | Frame Start | N/A |
daA1920-15um | Frame Start | N/A |
daA1920-30uc | Frame Start | N/A |
daA1920-30um | Frame Start | N/A |
daA1920-160uc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA1920-160um | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA2448-70uc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA2448-70um | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA2500-14uc | Frame Start | N/A |
daA2500-14um | Frame Start | N/A |
daA3840-45uc | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
daA3840-45um | Frame Start Frame End Frame Active Frame Burst Start Frame Burst End Frame Burst Active Exposure Start Exposure End Exposure Active | 1023 |
puA1280-54uc | Frame Start | N/A |
puA1280-54um | Frame Start | N/A |
puA1600-60uc | Frame Start | N/A |
puA1600-60um | Frame Start | N/A |
puA1920-30uc | Frame Start | N/A |
puA1920-30um | Frame Start | N/A |
puA2500-14uc | Frame Start | N/A |
puA2500-14um | Frame Start | N/A |
-
Only valid in Standard burst mode. In High Speed burst mode, the maximum number of images per series is considerably lower and depends on the size of the image ROI. To determine the actual number, enable the High Speed burst mode and determine the maximum value of the
AcquisitionBurstFrameCount
parameter. The maximum value automatically adapts to the current image ROI settings.
Sample Code#
ace Classic/U/L GigE Cameras#
// Select and enable the Frame Start trigger
camera.TriggerSelector.SetValue(TriggerSelector_FrameStart);
camera.TriggerMode.SetValue(TriggerMode_On);
// Select and enable the Acquisition Start trigger
camera.TriggerSelector.SetValue(TriggerSelector_AcquisitionStart);
camera.TriggerMode.SetValue(TriggerMode_On);
// Set the number of images to be acquired per Acquisition Start trigger signal to 3
camera.AcquisitionFrameCount.SetValue(3);
INodeMap& nodemap = camera.GetNodeMap();
// Select and enable the Frame Start trigger
CEnumParameter(nodemap, "TriggerSelector").SetValue("FrameStart");
CEnumParameter(nodemap, "TriggerMode").SetValue("On");
// Select and enable the Acquisition Start trigger
CEnumParameter(nodemap, "TriggerSelector").SetValue("AcquisitionStart");
CEnumParameter(nodemap, "TriggerMode").SetValue("On");
// Set the number of images to be acquired per Acquisition Start trigger signal to 3
CIntegerParameter(nodemap, "AcquisitionFrameCount").SetValue(3);
// Select and enable the Frame Start trigger
camera.Parameters[PLCamera.TriggerSelector].SetValue(PLCamera.TriggerSelector.FrameStart);
camera.Parameters[PLCamera.TriggerMode].SetValue(PLCamera.TriggerMode.On);
// Select and enable the Acquisition Start trigger
camera.Parameters[PLCamera.TriggerSelector].SetValue(PLCamera.TriggerSelector.AcquisitionStart);
camera.Parameters[PLCamera.TriggerMode].SetValue(PLCamera.TriggerMode.On);
// Set the number of images to be acquired per Acquisition Start trigger signal to 3
camera.Parameters[PLCamera.AcquisitionFrameCount].SetValue(3);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select and enable the Frame Start trigger */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSelector", "FrameStart");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "TriggerMode", "On");
CHECK(errRes);
/* Select and enable the Acquisition Start trigger */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSelector", "AcquisitionStart");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "TriggerMode", "On");
CHECK(errRes);
/* Set the number of images to be acquired per Acquisition Start trigger signal to 3 */
errRes = PylonDeviceSetIntegerFeature(hdev, "AcquisitionFrameCount", 3);
CHECK(errRes);
Other Cameras#
// Select and enable the Frame Start trigger
camera.TriggerSelector.SetValue(TriggerSelector_FrameStart);
camera.TriggerMode.SetValue(TriggerMode_On);
// Select and enable the Frame Burst Start trigger
camera.TriggerSelector.SetValue(TriggerSelector_FrameBurstStart);
camera.TriggerMode.SetValue(TriggerMode_On);
// Set the number of images to be acquired per Frame Burst Start trigger signal to 3
camera.AcquisitionBurstFrameCount.SetValue(3);
INodeMap& nodemap = camera.GetNodeMap();
// Select and enable the Frame Start trigger
CEnumParameter(nodemap, "TriggerSelector").SetValue("FrameStart");
CEnumParameter(nodemap, "TriggerMode").SetValue("On");
// Select and enable the Frame Burst Start trigger
CEnumParameter(nodemap, "TriggerSelector").SetValue("FrameBurstStart");
CEnumParameter(nodemap, "TriggerMode").SetValue("On");
// Set the number of images to be acquired per Frame Burst Start trigger signal to 3
CIntegerParameter(nodemap, "AcquisitionBurstFrameCount").SetValue(3);
// Select and enable the Frame Start trigger
camera.Parameters[PLCamera.TriggerSelector].SetValue(PLCamera.TriggerSelector.FrameStart);
camera.Parameters[PLCamera.TriggerMode].SetValue(PLCamera.TriggerMode.On);
// Select and enable the Frame Burst Start trigger
camera.Parameters[PLCamera.TriggerSelector].SetValue(PLCamera.TriggerSelector.FrameBurstStart);
camera.Parameters[PLCamera.TriggerMode].SetValue(PLCamera.TriggerMode.On);
// Set the number of images to be acquired per Frame Burst Start trigger signal to 3
camera.Parameters[PLCamera.AcquisitionBurstFrameCount].SetValue(3);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select and enable the Frame Start trigger */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSelector", "FrameStart");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "TriggerMode", "On");
CHECK(errRes);
/* Select and enable the Frame Burst Start trigger */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSelector", "FrameBurstStart");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "TriggerMode", "On");
CHECK(errRes);
/* Set the number of images to be acquired per Frame Burst Start trigger signal to 3 */
errRes = PylonDeviceSetIntegerFeature(hdev, "AcquisitionBurstFrameCount", 3);
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.