Trigger Source#
You can select, e.g., an input line or a software command as a trigger source.
Using the Feature#
To configure how a trigger can be triggered:
- Set the
TriggerSelector
parameter to the desired trigger type, e.g.,FrameStart
. - Set the
TriggerSource
parameter to one of the following values (if available):Line1
,Line2
,Line3
,Line4
: The trigger selected can be triggered by applying an electrical signal to I/O line 1, 2, 3, or 4.
If the I/O line is a GPIO line, the line must be configured for input.Software
: The trigger selected can be triggered by executing aTriggerSoftware
command.SoftwareSignal1
,SoftwareSignal2
,SoftwareSignal3
: The trigger selected can be triggered using the Software Signal Pulse feature.Action1
: The trigger selected can be triggered using the Action Commands feature.Counter1Active
,Counter2Active
: The trigger selected can be triggered using the Counter feature. The trigger signal will be high (1) as long as the given counter is counting and low (0) as long as it is not counting.Counter1Start
,Counter2Start
: The trigger selected can be triggered using the Counter feature. A trigger signal is sent whenever the given counter starts counting.Counter1End
,Counter2End
: The trigger selected can be triggered using the Counter feature. A trigger signal is sent whenever the given counter stops counting.Timer1Active
,Timer2Active
: The trigger selected can be triggered using the Timer feature. The trigger signal will be high (1) as long as the given timer is running and low (0) as long as it is not running.Timer1End
,Timer2End
: The trigger selected can be triggered using the Timer feature. A trigger signal is sent whenever the given timer has elapsed.PeriodicSignal1
: The trigger selected can be triggered using the Periodic Signal feature. A trigger signal is sent repeatedly. Its period is defined by theBslPeriodicSignalPeriod
parameter.-
CXPTrigger0
,CXPTrigger1
: The trigger selected can be triggered by receiving a trigger signal from a CXP-12 interface card.You can find information about configuring the interface card in the Configuring a CXP-12 Interface Card topic. Triggering the camera via the interface card has the following advantages:
- A short trigger delay.
The trigger accuracy is less than 0.5 µs when using CXP-10 or CXP-12. It is less than 1 µs when using CXP-6, CXP-5, or CXP-3. - The generated I/O trigger packets are transmitted to the camera via the CoaXPress data cable. This may be useful for your cable setup.
The
CXPTrigger0
andCXPTrigger1
triggers correspond to theLinkTrigger0
andLinkTrigger1
trigger packet definitions in the CoaXPress Standard version 2.0. In version 1.x,LinkTrigger0
is called "rising edge" andLinkTrigger1
is called "falling edge". - A short trigger delay.
Specifics#
Camera Model | Available Hardware Trigger Sources | Available Software Trigger Sources |
---|---|---|
a2A1920-51gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-51gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-51gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-51gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
acA640-90gc | Line 1 | Software Action 1 |
acA640-90uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA640-121gm | Line 1 Line 3 | Software Action 1 |
acA640-300gc | Line 1 Line 3 | Software Action 1 |
acA640-300gm | Line 1 Line 3 | Software Action 1 |
acA640-750uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA640-750um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA720-290gc | Line 1 Line 3 | Software Action 1 |
acA720-290gm | Line 1 Line 3 | Software Action 1 |
acA720-520uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA720-520um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA800-200gc | Line 1 Line 3 | Software Action 1 |
acA800-200gm | Line 1 Line 3 | Software Action 1 |
acA800-510uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA800-510um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1280-60gc | Line1 | Software |
acA1280-60gm | Line 1 | Software |
acA1300-60gc | Line 1 | Software Action 1 |
acA1300-60gm | Line 1 | Software Action 1 |
acA1300-60gmNIR | Line 1 | Software Action 1 |
acA1300-75gc | Line 1 Line 3 | Software Action 1 |
acA1300-75gm | Line 1 Line 3 | Software Action 1 |
acA1300-200uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1300-200um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1440-73gc | Line 1 Line 3 | Software Action 1 |
acA1440-73gm | Line 1 Line 3 | Software Action 1 |
acA1440-220uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1440-220um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1600-20gc | Line 1 | Software Action 1 |
acA1600-20uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1600-60gc | Line 1 | Software Action 1 |
acA1600-60gm | Line 1 | Software Action 1 |
acA1920-25gc | Line 1 | Software Action 1 |
acA1920-25gm | Line 1 | Software Action 1 |
acA1920-25uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-25um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-40gc | Line 1 Line 3 | Software Action 1 |
acA1920-40gm | Line 1 Line 3 | Software Action 1 |
acA1920-40uc | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-40ucMED | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-40um | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-40umMED | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-48gc | Line 1 Line 3 | Software Action 1 |
acA1920-48gm | Line 1 Line 3 | Software Action 1 |
acA1920-50gc | Line 1 Line 3 | Software Action 1 |
acA1920-50gm | Line 1 Line 3 | Software Action 1 |
acA1920-150uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-150um | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-155uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-155ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-155um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA1920-155umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2000-50gc | Line 1 | Software Action 1 |
acA2000-50gm | Line 1 | Software Action 1 |
acA2000-50gmNIR | Line 1 | Software Action 1 |
acA2000-165uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2000-165um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2000-165umNIR | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2040-25gc | Line 1 | Software Action 1 |
acA2040-25gm | Line 1 | Software Action 1 |
acA2040-25gmNIR | Line 1 | Software Action 1 |
acA2040-35gc | Line 1 Line 3 | Software Action 1 |
acA2040-35gm | Line 1 Line 3 | Software Action 1 |
acA2040-55uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2040-55um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2040-90uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2040-90um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2040-90umNIR | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2040-120uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2040-120um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-20gc | Line 1 Line 3 | Software Action 1 |
acA2440-20gm | Line 1 Line 3 | Software Action 1 |
acA2440-35uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-35ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-35um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-35umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-75uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-75ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-75um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2440-75umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2500-14gc | Line 1 | Software Action 1 |
acA2500-14gm | Line 1 | Software Action 1 |
acA2500-14uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2500-14um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2500-20gc | Line 1 Line 3 | Software Action 1 |
acA2500-20gcMED | Line 1 Line 3 | Software Action 1 |
acA2500-20gm | Line 1 Line 3 | Software Action 1 |
acA2500-20gmMED | Line 1 Line 3 | Software Action 1 |
acA2500-60uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA2500-60um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA3088-16gc | Line 1 Line 3 | Software Action 1 |
acA3088-16gm | Line 1 Line 3 | Software Action 1 |
acA3088-57uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA3088-57ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA3088-57um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA3088-57umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA3800-10gc | Line 1 Line 3 | Software Action 1 |
acA3800-10gm | Line 1 Line 3 | Software Action 1 |
acA3800-14uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA3800-14um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4024-8gc | Line 1 Line 3 | Software Action 1 |
acA4024-8gm | Line 1 Line 3 | Software Action 1 |
acA4024-29uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4024-29um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-11gc | Line 1 Line 3 | Software Action 1 |
acA4096-11gm | Line 1 Line 3 | Software Action 1 |
acA4096-30uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-30ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-30um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-30umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-40uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-40ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-40um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4096-40umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-8gc | Line 1 Line 3 | Software Action 1 |
acA4112-8gm | Line 1 Line 3 | Software Action 1 |
acA4112-20uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-20ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-20um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-20umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-30uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-30ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-30um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4112-30umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA4600-7gc | Line 1 | Software Action 1 |
acA4600-10uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA5472-5gc | Line 1 Line 3 | Software Action 1 |
acA5472-5gm | Line 1 Line 3 | Software Action 1 |
acA5472-17uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA5472-17ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA5472-17um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
acA5472-17umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3 (on some camera models) |
boA1936-400cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA1936-400cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2448-250cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2448-250cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2832-190cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2832-190cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-93cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-93cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-180cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-180cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4112-68cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4112-68cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4500-45cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4500-45cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4504-100cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4504-100cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5320-150cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5320-150cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5328-100cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5328-100cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA6500-36cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA6500-36cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA8100-16cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA8100-16cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
daA1280-54uc | Line 1 Line 2 | Software |
daA1280-54um | Line 1 Line 2 | Software |
daA1600-60uc | Line 1 Line 2 | Software |
daA1600-60um | Line 1 Line 2 | Software |
daA1920-15um | Line 1 Line 2 | Software |
daA1920-30uc | Line 1 Line 2 | Software |
daA1920-30um | Line 1 Line 2 | Software |
daA1920-160uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA1920-160um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA2448-70uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA2448-70um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA2500-14uc | Line 1 Line 2 | Software |
daA2500-14um | Line 1 Line 2 | Software |
daA3840-45uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA3840-45um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
puA1280-54uc | None | Software |
puA1280-54um | None | Software |
puA1600-60uc | None | Software |
puA1600-60um | None | Software |
puA1920-30uc | None | Software |
puA1920-30um | None | Software |
puA2500-14uc | None | Software |
puA2500-14um | None | Software |
Sample Code#
// Select the Frame Start trigger
camera.TriggerSelector.SetValue(TriggerSelector_FrameStart);
// Set the trigger source to Line 1
camera.TriggerSource.SetValue(TriggerSource_Line1);
INodeMap& nodemap = camera.GetNodeMap();
// Select the Frame Start trigger
CEnumParameter(nodemap, "TriggerSelector").SetValue("FrameStart");
// Set the trigger source to Line 1
CEnumParameter(nodemap, "TriggerSource").SetValue("Line1");
// Select the Frame Start trigger
camera.Parameters[PLCamera.TriggerSelector].SetValue(PLCamera.TriggerSelector.FrameStart);
// Set the trigger source to Line 1
camera.Parameters[PLCamera.TriggerSource].SetValue(PLCamera.TriggerSource.Line1);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select the Frame Start trigger */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSelector", "FrameStart");
CHECK(errRes);
/* Set the trigger source to Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSource", "Line1");
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.