Skip to content

Trigger Source#

The Trigger Source camera feature allows you to configure how the currently selected trigger can be triggered.

You can select, e.g., an input line or a software command as a trigger source.

Using the Feature#

To configure how a trigger can be triggered:

  1. Set the TriggerSelector parameter to the desired trigger type, e.g., FrameStart.
  2. Set the TriggerSource parameter to one of the following values (if available):
    • Line1, Line2, Line3, Line4: The trigger selected can be triggered by applying an electrical signal to I/O line 1, 2, 3, or 4.
      If the I/O line is a GPIO line, the line must be configured for input.
    • Software: The trigger selected can be triggered by executing a TriggerSoftware command.
    • SoftwareSignal1, SoftwareSignal2, SoftwareSignal3: The trigger selected can be triggered using the Software Signal Pulse feature.
    • Action1: The trigger selected can be triggered using the Action Commands feature.
    • Counter1Active, Counter2Active: The trigger selected can be triggered using the Counter feature. The trigger signal will be high (1) as long as the given counter is counting and low (0) as long as it is not counting.
    • Counter1Start, Counter2Start: The trigger selected can be triggered using the Counter feature. A trigger signal is sent whenever the given counter starts counting.
    • Counter1End, Counter2End: The trigger selected can be triggered using the Counter feature. A trigger signal is sent whenever the given counter stops counting.
    • Timer1Active, Timer2Active: The trigger selected can be triggered using the Timer feature. The trigger signal will be high (1) as long as the given timer is running and low (0) as long as it is not running.
    • Timer1End, Timer2End: The trigger selected can be triggered using the Timer feature. A trigger signal is sent whenever the given timer has elapsed.
    • PeriodicSignal1: The trigger selected can be triggered using the Periodic Signal feature. A trigger signal is sent repeatedly. Its period is defined by the BslPeriodicSignalPeriod parameter.
    • CXPTrigger0, CXPTrigger1: The trigger selected can be triggered by receiving a trigger signal from a CXP-12 interface card.

      You can find information about configuring the interface card in the Configuring a CXP-12 Interface Card topic. Triggering the camera via the interface card has the following advantages:

      • A short trigger delay.
        The trigger accuracy is less than 0.5 µs when using CXP-10 or CXP-12. It is less than 1 µs when using CXP-6, CXP-5, or CXP-3.
      • The generated I/O trigger packets are transmitted to the camera via the CoaXPress data cable. This may be useful for your cable setup.

      The CXPTrigger0 and CXPTrigger1 triggers correspond to the LinkTrigger0 and LinkTrigger1 trigger packet definitions in the CoaXPress Standard version 2.0. In version 1.x, LinkTrigger0 is called "rising edge" and LinkTrigger1 is called "falling edge".

Specifics#

Show all camera models

Camera Model Available Hardware Trigger Sources Available Software Trigger Sources
a2A1920-51gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A1920-51gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A1920-51gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A1920-51gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A1920-160ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A1920-160ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A1920-160umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A1920-160umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-23gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-23gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-23gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-23gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-75ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-75ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-75umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-75umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-105g5cBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2448-105g5mBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-22gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-22gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-22gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-22gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-60ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-60ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-60umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2590-60umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-20gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-20gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-20gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-20gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-64ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-64ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-64umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2600-64umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-14gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-14gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-14gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-14gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-48ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-48ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-48umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-48umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-67g5cBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A2840-67g5mBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-13gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-13gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-13gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-13gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-45ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-45ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-45umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A3840-45umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-9gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-9gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-9gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-9gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-30ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-30ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-30umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-30umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-44g5cBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4096-44g5mBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-12gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-12gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-12gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-12gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-40ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-40ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-40umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4200-40umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-5gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-5gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-5gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-5gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-18ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-18ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-18umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-18umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-27g5cBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A4504-27g5mBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-7gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-7gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-7gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-7gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-23ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-23ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-23umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-23umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-34g5cBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5320-34g5mBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-4gcBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-4gcPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-4gmBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-4gmPRO Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-15ucBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-15ucPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-15umBAS Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-15umPRO Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-22g5cBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
a2A5328-22g5mBAS Line 1
Line 2
Line 3
Action 1
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Periodic Signal 1
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
acA640-90gc Line 1 Software
Action 1
acA640-90uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA640-121gm Line 1
Line 3
Software
Action 1
acA640-300gc Line 1
Line 3
Software
Action 1
acA640-300gm Line 1
Line 3
Software
Action 1
acA640-750uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA640-750um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA720-290gc Line 1
Line 3
Software
Action 1
acA720-290gm Line 1
Line 3
Software
Action 1
acA720-520uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA720-520um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA800-200gc Line 1
Line 3
Software
Action 1
acA800-200gm Line 1
Line 3
Software
Action 1
acA800-510uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA800-510um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1280-60gc Line1 Software
acA1280-60gm Line 1 Software
acA1300-60gc Line 1 Software
Action 1
acA1300-60gm Line 1 Software
Action 1
acA1300-60gmNIR Line 1 Software
Action 1
acA1300-75gc Line 1
Line 3
Software
Action 1
acA1300-75gm Line 1
Line 3
Software
Action 1
acA1300-200uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1300-200um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1440-73gc Line 1
Line 3
Software
Action 1
acA1440-73gm Line 1
Line 3
Software
Action 1
acA1440-220uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1440-220um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1600-20gc Line 1 Software
Action 1
acA1600-20uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1600-60gc Line 1 Software
Action 1
acA1600-60gm Line 1 Software
Action 1
acA1920-25gc Line 1 Software
Action 1
acA1920-25gm Line 1 Software
Action 1
acA1920-25uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-25um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-40gc Line 1
Line 3
Software
Action 1
acA1920-40gm Line 1
Line 3
Software
Action 1
acA1920-40uc Line 1
Line 2
Line 3
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-40ucMED Line 1
Line 2
Line 3
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-40um Line 1
Line 2
Line 3
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-40umMED Line 1
Line 2
Line 3
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-48gc Line 1
Line 3
Software
Action 1
acA1920-48gm Line 1
Line 3
Software
Action 1
acA1920-50gc Line 1
Line 3
Software
Action 1
acA1920-50gm Line 1
Line 3
Software
Action 1
acA1920-150uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-150um Line 1
Line 2
Line 3
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-155uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-155ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-155um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA1920-155umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2000-50gc Line 1 Software
Action 1
acA2000-50gm Line 1 Software
Action 1
acA2000-50gmNIR Line 1 Software
Action 1
acA2000-165uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2000-165um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2000-165umNIR Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2040-25gc Line 1 Software
Action 1
acA2040-25gm Line 1 Software
Action 1
acA2040-25gmNIR Line 1 Software
Action 1
acA2040-35gc Line 1
Line 3
Software
Action 1
acA2040-35gm Line 1
Line 3
Software
Action 1
acA2040-55uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2040-55um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2040-90uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2040-90um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2040-90umNIR Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2040-120uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2040-120um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-20gc Line 1
Line 3
Software
Action 1
acA2440-20gm Line 1
Line 3
Software
Action 1
acA2440-35uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-35ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-35um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-35umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-75uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-75ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-75um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2440-75umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2500-14gc Line 1 Software
Action 1
acA2500-14gm Line 1 Software
Action 1
acA2500-14uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2500-14um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2500-20gc Line 1
Line 3
Software
Action 1
acA2500-20gcMED Line 1
Line 3
Software
Action 1
acA2500-20gm Line 1
Line 3
Software
Action 1
acA2500-20gmMED Line 1
Line 3
Software
Action 1
acA2500-60uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA2500-60um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA3088-16gc Line 1
Line 3
Software
Action 1
acA3088-16gm Line 1
Line 3
Software
Action 1
acA3088-57uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA3088-57ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA3088-57um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA3088-57umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA3800-10gc Line 1
Line 3
Software
Action 1
acA3800-10gm Line 1
Line 3
Software
Action 1
acA3800-14uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA3800-14um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4024-8gc Line 1
Line 3
Software
Action 1
acA4024-8gm Line 1
Line 3
Software
Action 1
acA4024-29uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4024-29um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-11gc Line 1
Line 3
Software
Action 1
acA4096-11gm Line 1
Line 3
Software
Action 1
acA4096-30uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-30ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-30um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-30umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-40uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-40ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-40um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4096-40umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-8gc Line 1
Line 3
Software
Action 1
acA4112-8gm Line 1
Line 3
Software
Action 1
acA4112-20uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-20ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-20um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-20umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-30uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-30ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-30um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4112-30umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA4600-7gc Line 1 Software
Action 1
acA4600-10uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA5472-5gc Line 1
Line 3
Software
Action 1
acA5472-5gm Line 1
Line 3
Software
Action 1
acA5472-17uc Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA5472-17ucMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA5472-17um Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
acA5472-17umMED Line 1
Line 3
Line 4
Software
Software Signal 1
Software Signal 2
Software Signal 3 (on some camera models)
boA1936-400cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA1936-400cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA2448-250cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA2448-250cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA2832-190cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA2832-190cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4096-93cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4096-93cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4096-180cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4096-180cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4112-68cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4112-68cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4500-45cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4500-45cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4504-100cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA4504-100cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA5320-150cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA5320-150cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA5328-100cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA5328-100cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA6500-36cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA6500-36cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA8100-16cc Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
boA8100-16cm Line 1
Line 2
Line 3
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
CXP Trigger 0
CXP Trigger 1
daA720-520uc Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA720-520um Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA1280-54uc Line 1
Line 2
Software
daA1280-54um Line 1
Line 2
Software
daA1440-220uc Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA1440-220um Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA1600-60uc Line 1
Line 2
Software
daA1600-60um Line 1
Line 2
Software
daA1920-15um Line 1
Line 2
Software
daA1920-30uc Line 1
Line 2
Software
daA1920-30um Line 1
Line 2
Software
daA1920-160uc Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA1920-160um Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA2448-70uc Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA2448-70um Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA2500-14uc Line 1
Line 2
Software
daA2500-14um Line 1
Line 2
Software
daA3840-45uc Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
daA3840-45um Line 1
Line 2
Line 3
Line 4
Counter 1 Active
Counter 1 End
Counter 1 Start
Counter 2 Active
Counter 2 End
Counter 2 Start
Timer 1 Active
Timer 1 End
Timer 2 Active
Timer 2 End
Software
Software Signal 1
Software Signal 2
Software Signal 3
puA1280-54uc None Software
puA1280-54um None Software
puA1600-60uc None Software
puA1600-60um None Software
puA1920-30uc None Software
puA1920-30um None Software
puA2500-14uc None Software
puA2500-14um None Software

Sample Code#

// Select the Frame Start trigger
camera.TriggerSelector.SetValue(TriggerSelector_FrameStart);
// Set the trigger source to Line 1
camera.TriggerSource.SetValue(TriggerSource_Line1);
INodeMap& nodemap = camera.GetNodeMap();
// Select the Frame Start trigger
CEnumParameter(nodemap, "TriggerSelector").SetValue("FrameStart");
// Set the trigger source to Line 1
CEnumParameter(nodemap, "TriggerSource").SetValue("Line1");
// Select the Frame Start trigger
camera.Parameters[PLCamera.TriggerSelector].SetValue(PLCamera.TriggerSelector.FrameStart);
// Set the trigger source to Line 1
camera.Parameters[PLCamera.TriggerSource].SetValue(PLCamera.TriggerSource.Line1);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select the Frame Start trigger */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSelector", "FrameStart");
CHECK(errRes);
/* Set the trigger source to Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSource", "Line1");
CHECK(errRes);

You can also use the pylon Viewer to easily set the parameters.