Center X and Center Y (BCON for MIPI)#
Using the Feature#
Using Center X#
To center the image horizontally, execute the BslCenterX
command.
The camera adjusts the OffsetX
parameter value to center the image ROI horizontally. This is a one-time operation. When you change the width of the image ROI, you must execute the command again.
Using Center Y#
To center the image vertically, execute the BslCenterY
command.
The camera adjusts the OffsetY
parameter value to center the image ROI vertically. This is a one-time operation. When you change the height of the image ROI, you must execute the command again.
Sample Code#
// Center the image ROI
camera.BslCenterX.Execute();
camera.BslCenterY.Execute();
INodeMap& nodemap = camera.GetNodeMap();
// Center the image ROI
CCommandParameter(nodemap, "BslCenterX").Execute();
CCommandParameter(nodemap, "BslCenterY").Execute();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Center the image ROI */
errRes = PylonDeviceExecuteCommandFeature(hdev, "BslCenterX");
CHECK(errRes);
errRes = PylonDeviceExecuteCommandFeature(hdev, "BslCenterY");
CHECK(errRes);
You can also use the pylon Viewer to easily set the parameters.