Device Information Parameters (BCON for MIPI)#
This topic describes the parameters and the information each parameter provides.
Using the Feature#
Basler BCON for MIPI camera modules provide the following device information parameters:
Parameter Name | Access (R = read-only, RW = read / write) | Description |
---|---|---|
DeviceFirmwareVersion | R | The camera's firmware version number. |
DeviceManufacturerInfo | R | The camera's manufacturer name. Usually contains an empty string. |
DeviceModelName | R | The camera's model name, e.g., acA3800-14um. |
DeviceSerialNumber | R | The camera's serial number. |
DeviceVendorName | R | The camera's vendor name, e.g., Basler. |
DeviceVersion | R | The camera's version number. |
SensorHeight | R | The actual height of the camera's sensor in pixels. |
SensorWidth | R | The actual width of the camera's sensor in pixels. |