What is OPTO Trigger 5?

OPTO Trigger 5

OPTO Trigger 5 is connected to the frame grabber via a 34-pin flat cable:

Installation within a host PC:

 

Production line using Opto Trigger 5 (example):

Example: Frame grabber with attached Opto Trigger 5 within a sample production line

 

Trigger System Documentation

 

For detailed information on how you can use your Opto Trigger 5 for various tasks within a trigger system, refer to the Trigger System documentation.

   

 

Applet-Specific Trigger Settings

 

How the individual inputs and outputs of the trigger extension board are employed you can configure via the applet you are using. Please refer to the documentation of your specific applet.