Skip to content

How Does the Multiple ROI Feature Affect the Framerate?#

The Multiple ROI feature is a standard feature of Basler ace 2 and boost R cameras.

The resulting frame rate corresponds to the frame rate of an equivalent image ROI.

For instance, consider an ace 2 with this setup:

  • Column 1 size = 1000
  • Column 2 size = 800
  • Row 1 size = 200
  • Row 2 size = 600

The resulting multiple ROI size is (1000 + 800) x (200 + 600) = 1800 x 800.

The frame rate will be the same as the frame rate of a camera with an image ROI of 1800 x 800 without the multiple ROI feature.

Back to Knowledge Articles