BoxPick

Introduction

The BoxPick module provides an out-of-the-box perception solution for robotic pick-and-place applications. It detects rectangular surfaces and determines their position, orientation and size for grasping. With the +Match extension, BoxPick can be used to detect textured rectangles with consistent orientations, such as printed product packaging, labels, brochures or books.

In addition, the module offers:

  • A dedicated page on the rc_cube Web GUI for easy setup, configuration, testing, and application tuning.
  • The definition of regions of interest to select relevant volumes in the scene (see RoiDB).
  • A load carrier detection functionality for bin-picking applications (see LoadCarrier), to provide grasps for items inside a bin only.
  • The definition of compartments inside a load carrier to provide grasps for specific volumes of the bin only.
  • Collision checking between the gripper and the load carrier and/or the point cloud.
  • Support for static and robot-mounted cameras and optional integration with the Hand-eye calibration module, to provide grasps in the user-configured external reference frame.
  • A quality value associated to each suggested grasp and related to the flatness of the grasping surface.
  • Selection of a sorting strategy to sort the returned grasps.
  • 3D visualization of the detection results with grasp points and gripper animations in the Web GUI.

Note

This module is pipeline specific. Changes to its settings or parameters only affect the respective camera pipeline and have no influence on other pipelines running on the rc_cube.

Note

In this chapter, cluster and surface are used as synonyms and identify a set of points (or pixels) with defined geometrical properties.

The module is an optional on-board module of the rc_cube and requires a separate BoxPick license to be purchased. The +Match extension requires an extra license.

Detection of items

There are two different types of models for the rectangles to be detected by the BoxPick module.

Per default, BoxPick only supports item_models of type RECTANGLE. With the +Match extension, also item models of type TEXTURED_BOX can be detected. The detection of the different item model types is described below.

Optionally, further information can be given to the BoxPick module:

  • The ID of the load carrier which contains the items to be detected.
  • A compartment inside the load carrier where to detect items.
  • The ID of the region of interest where to search for the load carriers if a load carrier is set. Otherwise, the ID of the region of interest where to search for the items.
  • The ID of a reference plane for measuring the dimensions of the detected items (see Dimensioning).
  • The current robot pose in case the camera is mounted on the robot and the chosen coordinate frame for the poses is external or the chosen region of interest is defined in the external frame.

The returned pose of a detected item is the pose of the center of the detected rectangle in the desired reference frame (pose_frame), with its z axis pointing towards the camera and the x axis aligned with the long side of the item. This pose has a 180° rotation ambiguity around the z axis, which can be resolved by using the +Match extension with a TEXTURED_BOX item model. Each detected item includes a uuid (Universally Unique Identifier) and the timestamp of the oldest image that was used to detect it.

The items are sorted according to the chosen sorting strategy (see Setting the sorting strategies).

Detection of items of type RECTANGLE

BoxPick supports multiple item_models of type RECTANGLE. Each item model is defined by its minimum and maximum size, with the minimum dimensions strictly smaller than the maximum dimensions. The dimensions should be given fairly accurately to avoid misdetections, while still considering a certain tolerance to account for possible production variations and measurement inaccuracies.

The detection of the rectangles runs in several steps. First, the point cloud is segmented into preferably plane clusters. Then, straight line segments are detected in the 2D images and projected onto the corresponding clusters. The clusters and the detected lines are visualized in the “Intermediate Result” visualization on the Web GUI’s BoxPick page. Finally, for each cluster, the set of rectangles best fitting to the detected line segments is extracted.

Detection of items of type TEXTURED_BOX (BoxPick+Match)

With the +Match extension, BoxPick additionally supports item_models of type TEXTURED_BOX. When this item model type is used, only one item model can be given for each request.

The TEXTURED_BOX item model type should be used to detect multiple rectangles that have the same texture, i.e. the same look or print, such as printed product packaging, labels, brochures or books. It is required that for all objects the texture is at the same position with respect to the object geometry. Furthermore, the texture should not be repetitive.

A TEXTURED_BOX item is defined by the item’s exact dimensions x, y and z (only z is allowed to be 0) with a tolerance dimensions_tolerance_m that indicates, how much the detected dimensions are allowed to deviate from the given dimensions. By default, a tolerance of 0.01 m is assumed. Furthermore, a template_id must be given, which will be used to refer to the specified dimensions and the textures of the detected rectangles. Additionally, the maximum possible deformation of the items max_deformation_m can be given in meters (default 0.004 m), to account for rigid or more flexible objects.

If a template_id is used for the first time, BoxPick will run the detection of rectangles as for the item model type RECTANGLE, and use the given dimensions and tolerance to specify the dimensions range. If the z dimension is given in addition to x and y, rectangles with all possible combinations of the three dimensions will be detected. From the detected rectangles, so-called views are created, which contain the shape and the image intensity values of the rectangles, and are stored in a newly created template with the given template_id. The views are created iteratively: Starting from the detected rectangle with the highest score, a view is created and then used to detect more rectangles with the same texture. Then, all remaining clusters are used to detect further rectangles by the given dimensions range and again a view is created from the best rectangle and used for further detections. Each template can store up to 10 different views, for example corresponding to different types of the same product packaging. Each view will be assigned a unique ID (view_uuid) and all rectangle items with a matching texture will be assigned the same view_uuid. That also means that all items with the same view_uuid will have consistent orientations, because the orientation of each item is aligned with its texture. The views can be displayed, deleted and the orientation of each view can be set via the Web GUI by clicking on the template or its edit symbol in the template list. Each detected item contains a field view_pose_set indicating whether the orientation of the item’s view was explicitly set or is still unset at its original random state, which has a 180° ambiguity. Additionally, a user-defined name can be set for each view, that is returned along with the view_uuid for all items and allows an easier identification of a specific view. The type of a returned item with a view_uuid will be TEXTURED_RECTANGLE.

If the template with the given template_id already exists, the existing views will be used to detect rectangles based on their texture. If additional rectangles are found with matching dimensions, but different texture, new views will be generated and added to the template. When the maximum number of views is reached, views that are matched only rarely will be deleted so that newly generated views can be added to the template and the template is kept up-to-date. To prevent a template from being updated, automatic view updating can be disabled and enabled for each template in the Web GUI by clicking on the template or the edit symbol in the template list. The dimension tolerance and the maximum deformation can also be changed there for each template. The maximum deformation determines the tolerance for the texture matching, representing possible shifts within the texture, e.g. caused by deformations of the object surface. For rigid objects the max_deformation_m should be set to a low value in meters to ensure accurate matching.

The template’s dimensions can only be specified when creating a new template. Once the template is generated, the dimensions cannot be changed and do not need to be given in the detect request. If the dimensions are still given in the request, they must match the existing dimensions in the template. However, the dimensions_tolerance_m and max_deformation_m can be set differently in every detect request and their values will also be updated in the stored template.

Dimensioning

BoxPick only detects the top surface of an item as a rectangle. To measure the full dimensions of the detected items, a reference plane on which the items are placed, e.g. a conveyor belt or a table, can be given with the dimensioning argument of the detect_items, compute_grasps and compute_grasps_extended services. dimensioning.plane_ids must contain exactly one ID of a plane that is stored in the PrimitiveDB.

For each detected item, a box is computed from the four corners of the detected rectangle, which are measured down to the reference plane. The box is the bounding box of the rectangle corners that is aligned with the reference plane.

The returned item is of type BOX (or TEXTURED_BOX with the +Match extension) and contains its dimensions in the box field instead of the rectangle field. The pose of the item is the center of the box. The returned grasps are not affected by dimensioning.

Dimensioning is not possible for TEXTURED_BOX item models for which all three dimensions are given, because the dimensions of these items are already known.

Items that lie behind the reference plane are discarded, which is reported by the return_code value 115.

Computation of grasps

The BoxPick module offers a service for computing grasps for suction grippers. The gripper is defined by its suction surface length and width.

The grasps are computed on the detected rectangular items (see Detection of items).

Optionally, further information can be given to the module in a grasp computation request:

  • The ID of the load carrier which contains the items to be grasped.
  • A compartment inside the load carrier where to compute grasps (see Load carrier compartments).
  • The ID of the 3D region of interest where to search for the load carriers if a load carrier is set. Otherwise, the ID of the 3D region of interest where to compute grasps.
  • Collision detection information: The ID of the gripper to enable collision checking and optionally a pre-grasp offset to define a pre-grasp position. Details on collision checking are given below in CollisionCheck.
  • The ID of a reference plane for measuring the dimensions of the detected items (see Dimensioning).

A grasp provided by the BoxPick module represents the recommended pose of the TCP (Tool Center Point) of the suction gripper. The grasp type is always set to SUCTION. The computed grasp pose is the center of the biggest ellipse that can be inscribed in each surface. The grasp orientation is a right-handed coordinate system and is defined such that its z axis is normal to the surface pointing inside the object at the grasp position and its x axis is directed along the maximum elongation of the ellipse. Since the x axis can have two possible directions, the one that better fits to the preferred TCP orientation (see Setting the preferred orientation of the TCP) is selected. If the run-time parameter allow_any_grasp_z_rotation is set to true, the x axis will not be forced to be aligned with the maximum elongation of the graspable ellipse, but can have any rotation around the z axis. In this case, the returned grasp will have the orientation that best fits to the preferred TCP orientation and is collision free, if collision checking is enabled.

_images/boxpick_grasp_surface.png

Fig. 20 Illustration of a suction grasp with coordinate system and ellipse representing the maximum suction surface

Each grasp includes the dimensions of the maximum suction surface available, modelled as an ellipse of axes max_suction_surface_length and max_suction_surface_width. The user is enabled to filter grasps by specifying the minimum suction surface required by the suction device in use. If the run-time parameter allow_any_grasp_z_rotation is set to true, max_suction_surface_length and max_suction_surface_width will be equal and correspond to the shortest axis of the largest graspable ellipse.

In the BoxPick module, the grasp position corresponds to the center of the detected rectangle. When BoxPick is called with item models of type RECTANGLE, the dimensions of the maximum suction surface available matches the estimated rectangle dimensions. In this case, detected rectangles with missing data or occlusions by other objects for more than 15% of their surface do not get an associated grasp.

When BoxPick is called with item models of type TEXTURED_BOX, grasps can also be computed on partly occluded boxes. The maximum suction surface available matches the free surface that is not occluded by other clusters.

Each grasp also includes a quality value, which gives an indication of the flatness of the grasping surface. The quality value varies between 0 and 1, where higher numbers correspond to a flatter reconstructed surface.

The grasp definition is complemented by a uuid (Universally Unique Identifier) and the timestamp of the oldest image that was used to compute the grasp.

Grasp sorting is performed based on the selected sorting strategy (see Setting the sorting strategies).

Setting the sorting strategies

The items and grasps returned by the service calls are sorted according to a sorting strategy which can be chosen by the user. The following sorting strategies are available and can be set in the Web GUI or using the set_sorting_strategies service call:

  • gravity: highest items or grasp points along the gravity direction are returned first,
  • surface_area: items or grasp points with the largest surface area are returned first,
  • direction: items or grasp points with the shortest distance along a defined direction vector in a given pose_frame are returned first.
  • distance_to_point: items or grasp points with the shortest or farthest (if farthest_first is true) distance from a point in a given pose_frame are returned first.

If no sorting strategy is set or default sorting is chosen in the Web GUI, sorting is done based on a combination of gravity and surface_area.

Setting the preferred orientation of the TCP

The BoxPick module determines the reachability of grasp points based on the preferred orientation of the TCP. The preferred orientation can be set via the set_preferred_orientation service or on the BoxPick page in the Web GUI. The resulting direction of the TCP’s z axis is used to reject grasps which cannot be reached by the gripper. Furthermore, the preferred orientation is used to select one grasp of several possible symmetries that is best reachable for the robot.

The preferred orientation can be set in the camera coordinate frame or in the external coordinate frame, in case a hand-eye calibration is available. If the preferred orientation is specified in the external coordinate frame and the sensor is robot mounted, the current robot pose has to be given to each object detection call. If no preferred orientation is set, the orientation of the left camera (see Coordinate frames in the rc_visard manual) will be used as the preferred orientation of the TCP.used.

Interaction with other modules

Internally, the BoxPick module depends on, and interacts with other on-board modules as listed below.

Note

All changes and configuration updates to these modules will affect the performance of the BoxPick module.

Camera and depth data

The BoxPick module makes internally use of the following data:

  • Disparity, error, and confidence images from the Stereo matching module (rc_stereomatching), in case a stereo camera is used
  • Disparity, error, and confidence images from the Blaze module (rc_blaze), in case a Basler blaze camera is used

All processed images are guaranteed to be captured after the module trigger time.

IO and Projector Control

In case the rc_cube is used in conjunction with an external random dot projector and the IO and Projector Control module (rc_iocontrol), it is recommended to connect the projector to GPIO Out 1 and set the stereo-camera module’s acquisition mode to SingleFrameOut1 (see Stereo matching parameters), so that on each image acquisition trigger an image with and without projector pattern is acquired.

Alternatively, the output mode for the GPIO output in use should be set to ExposureAlternateActive (see Description of run-time parameters).

In either case, the Auto Exposure Mode exp_auto_mode should be set to AdaptiveOut1 to optimize the exposure of both images.

Hand-eye calibration

In case the camera has been calibrated to a robot, the BoxPick module can automatically provide poses in the robot coordinate frame. For the BoxPick node’s Services, the frame of the output poses can be controlled with the pose_frame argument.

Two different pose_frame values can be chosen:

  1. Camera frame (camera). All poses provided by the modules are in the camera frame, and no prior knowledge about the pose of the camera in the environment is required. This means that the configured regions of interest and load carriers move with the camera. It is the user’s responsibility to update the configured poses if the camera frame moves (e.g. with a robot-mounted camera).
  2. External frame (external). All poses provided by the modules are in the external frame, configured by the user during the hand-eye calibration process. The module relies on the on-board Hand-eye calibration module to retrieve the sensor mounting (static or robot mounted) and the hand-eye transformation. If the mounting is static, no further information is needed. If the sensor is robot-mounted, the robot_pose is required to transform poses to and from the external frame.

Note

If no hand-eye calibration is available, all pose_frame values should be set to camera.

All pose_frame values that are not camera or external are rejected.

If the sensor is robot-mounted, the current robot_pose has to be provided depending on the value of pose_frame and the definition of the sorting direction, sorting point or preferred orientation:

  • If pose_frame is set to external, providing the robot pose is obligatory.
  • If the sorting direction is defined in external, providing the robot pose is obligatory.
  • If the distance-to-point sorting strategy is defined in external, providing the robot pose is obligatory.
  • If the preferred orientation is defined in external, providing the robot pose is obligatory.
  • In all other cases, providing the robot pose is optional.

LoadCarrier

The BoxPick module uses the load carrier detection functionality provided by the LoadCarrier module (rc_load_carrier), with the run-time parameters specified for this module. However, only one load carrier will be returned and used in case multiple matching load carriers could be found in the scene. In case multiple load carriers of the same type are visible, a 3D region of interest should be set to ensure that always the same load carrier is used for the BoxPick module.

The load carrier is used to filter false detections when BoxPick is triggered with an item model of type TEXTURED_BOX and all three dimensions x, y, z are given. In this case, 3D boxes are created internally by adding the missing dimensions to the detected rectangles and only detections corresponding to boxes which are fully inside the detected load carrier are returned.

CollisionCheck

Collision checking can be easily enabled for grasp computation of the BoxPick module by passing the ID of the used gripper and optionally a pre-grasp offset to the compute_grasps or compute_grasps_extended service call. The gripper has to be defined in the GripperDB module (see Setting a gripper) and details about collision checking are given in Collision checking within other modules.

If collision checking is enabled, only grasps which are collision free will be returned. However, the visualization images on the BoxPick page of the Web GUI also show colliding grasp points as black ellipses.

The CollisionCheck module’s run-time parameters affect the collision detection as described in CollisionCheck Parameters.

Parameters

The BoxPick module is called rc_boxpick in the REST-API and is represented in the Web GUI in the desired pipeline under Modules ‣ BoxPick. The user can explore and configure the rc_boxpick module’s run-time parameters, e.g. for development and testing, using the Web GUI or the REST-API interface.

Parameter overview

Note

The default values in the parameter table below show the values of the rc_visard. The values can be different for other sensors.

This module offers the following run-time parameters:

Table 32 The rc_boxpick module’s run-time parameters
Name Type Min Max Default Description
allow_any_grasp_z_-rotation bool false true false Whether the grasps are allowed to have arbitrary rotation instead being aligned with the major axis of the graspable ellipse
allow_untextured_-detections bool false true false Whether to return also untextured detections in case a textured box was given
check_collisions_with_-point_cloud bool false true false Whether to check for collisions between gripper and the point cloud
cluster_max_curvature float64 0.005 0.5 0.11 Maximum curvature allowed within one cluster. The smaller this value, the more clusters will be split apart.
clustering_discontinuity_-factor float64 0.1 5.0 1.0 Factor used to discriminate depth discontinuities within a patch. The smaller this value, the more clusters will be split apart.
clustering_max_surface_-rmse float64 0.0005 0.01 0.004 Maximum root-mean-square error (RMSE) in meters of points belonging to a surface
discard_cut_off_items bool false true false Whether items that are cut off by the image border, the stereo ROI, the missing stereo overlap or the 3D region of interest should be discarded
grasp_filter_orientation_-threshold float64 0.0 180.0 45.0 Maximum allowed orientation change between grasp and preferred orientation in degrees
line_sensitivity float64 0.1 1.0 0.1 Sensitivity of the line detector
manual_line_sensitivity bool false true false Indicates whether the user-defined line sensitivity should be used or the automatic one
max_grasps int32 1 100 5 Maximum number of provided grasps
min_cluster_coverage float64 0.0 0.99 0.0 Gives the minimal ratio of points per cluster that must be covered with detected items.
mode string - - Unconstrained Mode of the rectangle detection: [Unconstrained, PackedGridLayout, PackedLayers]
prefer_splits bool false true false Indicates whether rectangles are split into smaller ones when possible

Description of run-time parameters

Each run-time parameter is represented by a row on the Web GUI’s BoxPick page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI:

max_grasps (Maximum Grasps)

sets the maximum number of provided grasps.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?max_grasps=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?max_grasps=<value>

cluster_max_curvature (Cluster Maximum Curvature)

is the maximum curvature allowed within one cluster. The smaller this value, the more clusters will be split apart.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?cluster_max_curvature=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?cluster_max_curvature=<value>

clustering_discontinuity_factor (Discontinuity Factor)

is the factor used to discriminate depth discontinuities within a patch. The smaller this value, the more clusters will be split apart.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?clustering_discontinuity_factor=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?clustering_discontinuity_factor=<value>

clustering_max_surface_rmse (Maximum Surface RMSE)

is the maximum root-mean-square error (RMSE) in meters of points belonging to a surface.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?clustering_max_surface_rmse=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?clustering_max_surface_rmse=<value>

mode (Mode)

determines the mode of the rectangle detection. Possible values are Unconstrained, PackedGridLayout and PackedLayers. In PackedGridLayout mode, rectangles of a cluster are detected in a dense grid pattern. In PackedLayers mode, boxes are assumed to form layers and box detection will start searching for items at the cluster corners. Use this mode in de-palletizing applications. In Unconstrained mode (default), rectangles are detected without posing any constraints on their relative locations or their positions in the segmented cluster. Fig. 21 illustrates the modes for different scenarios.

_images/boxpick_modes_new.svg

Fig. 21 Illustration of appropriate BoxPick modes for different scenes. Modes marked with yellow are applicable but not recommended for the corresponding scene. The gray areas indicate the rectangles to be detected.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?mode=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?mode=<value>

manual_line_sensitivity (Manual Line Sensitivity)

determines whether the user-defined line sensitivity should be used to extract the lines for rectangle detection. If this parameter is set to true, the user-defined line_sensitivity value will be used. If this parameter is set to false, automatic line sensitivity will be used. This parameter should be set to true when automatic line sensitivity does not give enough lines at the box boundaries so that boxes cannot be detected. The detected line segments are visualized in the “Intermediate Result” visualization on the Web GUI’s BoxPick page.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?manual_line_sensitivity=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?manual_line_sensitivity=<value>

line_sensitivity (Line Sensitivity)

determines the line sensitivity for extracting the lines for rectangle detection, if the parameter manual_line_sensitivity is set to true. Otherwise, the value of this parameter has no effect on the rectangle detection. Higher values give more line segments, but also increase the runtime of the box detection. This parameter should be increased when boxes cannot be detected because their boundary edges are not detected. The detected line segments are visualized in the “Intermediate Result” visualization on the Web GUI’s BoxPick page.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?line_sensitivity=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?line_sensitivity=<value>

prefer_splits (Prefer Splits)

determines whether rectangles should be split into smaller ones if the smaller ones also match the given item models. This parameter should be set to true for packed box layouts in which the given item models would also match a rectangle of the size of two adjoining boxes. If this parameter is set to false, the larger rectangles will be preferred in these cases.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?prefer_splits=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?prefer_splits=<value>

min_cluster_coverage (Minimum Cluster Coverage)

determines which ratio of each segmented cluster must be covered with rectangle detections to consider the detections to be valid. If the minimum cluster coverage is not reached for a cluster, no rectangle detections will be returned for this cluster and a warning will be given. This parameter should be used to verify that all items on a layer in a de-palletizing scenario are detected.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?min_cluster_coverage=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?min_cluster_coverage=<value>

allow_untextured_detections (Only for BoxPick+Match, Allow Untextured Detections)

enables returning all rectangles matching the given template dimensions, even when they cannot be matched to an existing view or when they do not have enough texture to create a new view from them. This parameter is only used when item models of type TEXTURED_BOX are detected. Disabling this parameter leads to faster detections when used with a template for which the automatic view updating is disabled.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?allow_untextured_detections=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?allow_untextured_detections=<value>

discard_cut_off_items (Discard Cut-Off Items)

determines, whether items that are cut off by the image border, the stereo region of interest (see Stereo ROI Parameters), the missing stereo overlap between the left and right camera image, or the 3D region of interest should be discarded.

This parameter has no effect when the UNKNOWN item model type is used.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?discard_cut_off_items=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?discard_cut_off_items=<value>

grasp_filter_orientation_threshold (Grasp Orientation Threshold)

is the maximum deviation of the TCP’s z axis at the grasp point from the z axis of the TCP’s preferred orientation in degrees. Only grasp points which are within this threshold are returned. When set to zero, any deviations are valid.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?grasp_filter_orientation_threshold=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?grasp_filter_orientation_threshold=<value>

allow_any_grasp_z_rotation (Allow Any Grasp Z Rotation)

If set to true, the returned grasps are no longer forced to have their x axes aligned with the maximum elongation of the graspable ellipse, but can have any rotation around the z axis. The returned max_suction_surface_length and max_suction_surface_width will be equal and correspond to the shortest diameter of the largest graspable ellipse. This parameter enables the robot to get more options for grasping objects, especially in scenes where collisions can occur. However, since the grasp is no longer aligned with the graspable ellipse, the correct orientation for placing the object must be determined from the corresponding item’s pose.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?allow_any_grasp_z_rotation=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?allow_any_grasp_z_rotation=<value>

check_collisions_with_point_cloud (Check Collisions with Point Cloud)

This parameter is only used when collision checking is enabled by passing a gripper to the compute_grasps or compute_grasps_extended service call. If check_collisions_with_point_cloud is set to true, all grasp points will be checked for collisions between the gripper and a watertight version of the point cloud, and only grasp points at which the gripper would not collide with this point cloud will be returned.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/parameters?check_collisions_with_point_cloud=<value>
PUT http://<host>/api/v1/nodes/rc_boxpick/parameters?check_collisions_with_point_cloud=<value>

Status values

The rc_boxpick module reports the following status values:

Table 33 The rc_boxpick module’s status values
Name Description
data_acquisition_time Time in seconds required by the last active service to acquire images
grasp_computation_time Processing time of the last grasp computation in seconds
last_return_code_message Return code message of the last detection
last_return_code_value Return code value of the last detection
last_timestamp_processed The timestamp of the last processed dataset
load_carrier_detection_time Processing time of the last load carrier detection in seconds
processing_time Processing time of the last detection (including load carrier detection) in seconds
state The current state of the rc_boxpick node

The reported state can take one of the following values.

Table 34 Possible states of the BoxPick module
State name Description
IDLE The module is idle.
RUNNING The module is running and ready for load carrier detection and grasp computation.
FATAL A fatal error has occurred.

Services

The user can explore and call the rc_boxpick module’s services, e.g. for development and testing, using the REST-API interface or the rc_cube Web GUI.

The BoxPick module offers the following services.

detect_items

Triggers the detection of rectangles as described in Detection of items.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/detect_items
PUT http://<host>/api/v1/nodes/rc_boxpick/services/detect_items

Required arguments:

pose_frame: see Hand-eye calibration.

item_models: list of item models to be detected. The type of the item model must be RECTANGLE or TEXTURED_BOX. For type RECTANGLE, rectangle must be filled, while for TEXTURED_BOX, textured_box must be filled. See Detection of items for a detailed description of the item model types.

Potentially required arguments:

robot_pose: see Hand-eye calibration.

Optional arguments:

load_carrier_id: ID of the load carrier which contains the items to be detected.

load_carrier_compartment: compartment inside the load carrier where to detect items (see Load carrier compartments).

region_of_interest_id: if load_carrier_id is set, ID of the 3D region of interest where to search for the load carriers. Otherwise, ID of the 3D region of interest where to search for the items.

dimensioning: plane_ids contains the ID of the reference plane for measuring the dimensions of the detected items (see Dimensioning).

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "dimensioning": {
      "plane_ids": [
        "string"
      ]
    },
    "item_models": [
      {
        "rectangle": {
          "max_dimensions": {
            "x": "float64",
            "y": "float64"
          },
          "min_dimensions": {
            "x": "float64",
            "y": "float64"
          }
        },
        "textured_box": {
          "dimensions": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "dimensions_tolerance_m": "float64",
          "max_deformation_m": "float64",
          "template_id": "string"
        },
        "type": "string"
      }
    ],
    "load_carrier_compartment": {
      "box": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose": {
        "orientation": {
          "w": "float64",
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "position": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        }
      }
    },
    "load_carrier_id": "string",
    "pose_frame": "string",
    "region_of_interest_id": "string",
    "robot_pose": {
      "orientation": {
        "w": "float64",
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "position": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    }
  }
}

load_carriers: list of detected load carriers.

items: list of detected rectangles. If dimensioning is given, list of detected boxes.

timestamp: timestamp of the image set the detection ran on.

return_code: holds possible warnings or error codes and messages.

The definition for the response with corresponding datatypes is:

{
  "name": "detect_items",
  "response": {
    "items": [
      {
        "box": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "rectangle": {
          "x": "float64",
          "y": "float64"
        },
        "template_id": "string",
        "timestamp": {
          "nsec": "int32",
          "sec": "int32"
        },
        "type": "string",
        "uuid": "string",
        "view_name": "string",
        "view_pose_set": "bool",
        "view_uuid": "string"
      }
    ],
    "load_carriers": [
      {
        "height_open_side": "float64",
        "id": "string",
        "inner_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "outer_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "overfilled": "bool",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "rim_ledge": {
          "x": "float64",
          "y": "float64"
        },
        "rim_step_height": "float64",
        "rim_thickness": {
          "x": "float64",
          "y": "float64"
        },
        "type": "string"
      }
    ],
    "return_code": {
      "message": "string",
      "value": "int16"
    },
    "timestamp": {
      "nsec": "int32",
      "sec": "int32"
    }
  }
}

compute_grasps

Triggers the detection of rectangles and the computation of grasping poses for the detected rectangles as described in Computation of grasps.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/compute_grasps
PUT http://<host>/api/v1/nodes/rc_boxpick/services/compute_grasps

Required arguments:

pose_frame: see Hand-eye calibration.

item_models: list of item models to be detected. The type of the item model must be RECTANGLE or TEXTURED_BOX. For type RECTANGLE, rectangle must be filled, while for TEXTURED_BOX, textured_box must be filled. See Detection of items for a detailed description of the item model types.

suction_surface_length: length of the suction device grasping surface.

suction_surface_width: width of the suction device grasping surface.

Potentially required arguments:

robot_pose: see Hand-eye calibration.

Optional arguments:

load_carrier_id: ID of the load carrier which contains the items to be grasped.

load_carrier_compartment: compartment inside the load carrier where to compute grasps (see Load carrier compartments).

region_of_interest_id: if load_carrier_id is set, ID of the 3D region of interest where to search for the load carriers. Otherwise, ID of the 3D region of interest where to compute grasps.

collision_detection: see Collision checking within other modules.

dimensioning: plane_ids contains the ID of the reference plane for measuring the dimensions of the detected items (see Dimensioning).

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "collision_detection": {
      "gripper_id": "string",
      "pre_grasp_offset": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    },
    "dimensioning": {
      "plane_ids": [
        "string"
      ]
    },
    "item_models": [
      {
        "rectangle": {
          "max_dimensions": {
            "x": "float64",
            "y": "float64"
          },
          "min_dimensions": {
            "x": "float64",
            "y": "float64"
          }
        },
        "textured_box": {
          "dimensions": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "dimensions_tolerance_m": "float64",
          "max_deformation_m": "float64",
          "template_id": "string"
        },
        "type": "string"
      }
    ],
    "load_carrier_compartment": {
      "box": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose": {
        "orientation": {
          "w": "float64",
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "position": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        }
      }
    },
    "load_carrier_id": "string",
    "pose_frame": "string",
    "region_of_interest_id": "string",
    "robot_pose": {
      "orientation": {
        "w": "float64",
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "position": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    },
    "suction_surface_length": "float64",
    "suction_surface_width": "float64"
  }
}

load_carriers: list of detected load carriers.

grasps: sorted list of suction grasps.

items: list of detected rectangles corresponding to the returned grasps. If dimensioning is given, list of detected boxes.

timestamp: timestamp of the image set the detection ran on.

return_code: holds possible warnings or error codes and messages.

The definition for the response with corresponding datatypes is:

{
  "name": "compute_grasps",
  "response": {
    "grasps": [
      {
        "item_uuid": "string",
        "max_suction_surface_length": "float64",
        "max_suction_surface_width": "float64",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "quality": "float64",
        "tcp_id": "string",
        "timestamp": {
          "nsec": "int32",
          "sec": "int32"
        },
        "type": "string",
        "uuid": "string"
      }
    ],
    "items": [
      {
        "box": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "grasp_uuids": [
          "string"
        ],
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "rectangle": {
          "x": "float64",
          "y": "float64"
        },
        "template_id": "string",
        "timestamp": {
          "nsec": "int32",
          "sec": "int32"
        },
        "type": "string",
        "uuid": "string",
        "view_name": "string",
        "view_pose_set": "bool",
        "view_uuid": "string"
      }
    ],
    "load_carriers": [
      {
        "height_open_side": "float64",
        "id": "string",
        "inner_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "outer_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "overfilled": "bool",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "rim_ledge": {
          "x": "float64",
          "y": "float64"
        },
        "rim_step_height": "float64",
        "rim_thickness": {
          "x": "float64",
          "y": "float64"
        },
        "type": "string"
      }
    ],
    "return_code": {
      "message": "string",
      "value": "int16"
    },
    "timestamp": {
      "nsec": "int32",
      "sec": "int32"
    }
  }
}

compute_grasps_extended

Triggers the detection of rectangles and the computation of grasping poses for for detected rectangles in the same way as compute_grasps, but returns the item information for each grasp directly instead of as a separate list. This allows for easier parsing when item information is required for the grasps.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/compute_grasps_extended
PUT http://<host>/api/v1/nodes/rc_boxpick/services/compute_grasps_extended

See compute_grasps service.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "collision_detection": {
      "gripper_id": "string",
      "pre_grasp_offset": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    },
    "dimensioning": {
      "plane_ids": [
        "string"
      ]
    },
    "item_models": [
      {
        "rectangle": {
          "max_dimensions": {
            "x": "float64",
            "y": "float64"
          },
          "min_dimensions": {
            "x": "float64",
            "y": "float64"
          }
        },
        "textured_box": {
          "dimensions": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "dimensions_tolerance_m": "float64",
          "max_deformation_m": "float64",
          "template_id": "string"
        },
        "type": "string"
      }
    ],
    "load_carrier_compartment": {
      "box": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose": {
        "orientation": {
          "w": "float64",
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "position": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        }
      }
    },
    "load_carrier_id": "string",
    "pose_frame": "string",
    "region_of_interest_id": "string",
    "robot_pose": {
      "orientation": {
        "w": "float64",
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "position": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    },
    "suction_surface_length": "float64",
    "suction_surface_width": "float64"
  }
}

load_carriers: list of detected load carriers.

grasps: sorted list of suction grasps. Each grasp also contains the item information of the corresponding detected rectangle.

timestamp: timestamp of the image set the detection ran on.

return_code: holds possible warnings or error codes and messages.

The definition for the response with corresponding datatypes is:

{
  "name": "compute_grasps_extended",
  "response": {
    "grasps": [
      {
        "item": {
          "box": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "pose": {
            "orientation": {
              "w": "float64",
              "x": "float64",
              "y": "float64",
              "z": "float64"
            },
            "position": {
              "x": "float64",
              "y": "float64",
              "z": "float64"
            }
          },
          "pose_frame": "string",
          "rectangle": {
            "x": "float64",
            "y": "float64"
          },
          "template_id": "string",
          "type": "string",
          "uuid": "string",
          "view_name": "string",
          "view_pose_set": "bool",
          "view_uuid": "string"
        },
        "max_suction_surface_length": "float64",
        "max_suction_surface_width": "float64",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "quality": "float64",
        "tcp_id": "string",
        "timestamp": {
          "nsec": "int32",
          "sec": "int32"
        },
        "type": "string",
        "uuid": "string"
      }
    ],
    "load_carriers": [
      {
        "height_open_side": "float64",
        "id": "string",
        "inner_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "outer_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "overfilled": "bool",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "rim_ledge": {
          "x": "float64",
          "y": "float64"
        },
        "rim_step_height": "float64",
        "rim_thickness": {
          "x": "float64",
          "y": "float64"
        },
        "type": "string"
      }
    ],
    "return_code": {
      "message": "string",
      "value": "int16"
    },
    "timestamp": {
      "nsec": "int32",
      "sec": "int32"
    }
  }
}

set_preferred_orientation

Persistently stores the preferred orientation of the TCP to compute the reachability of the grasps, which is used for filtering and the grasps returned by the compute_grasps or compute_grasps_extended service (see Setting the preferred orientation of the TCP).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/set_preferred_orientation
PUT http://<host>/api/v1/nodes/rc_boxpick/services/set_preferred_orientation

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "orientation": {
      "w": "float64",
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string"
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "set_preferred_orientation",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

get_preferred_orientation

Returns the preferred orientation of the TCP to compute the reachability of the grasps, which is used for filtering the grasps returned by the compute_grasps and compute_grasps_extended service (see Setting the preferred orientation of the TCP).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/get_preferred_orientation
PUT http://<host>/api/v1/nodes/rc_boxpick/services/get_preferred_orientation
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "get_preferred_orientation",
  "response": {
    "orientation": {
      "w": "float64",
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string",
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

set_sorting_strategies

Persistently stores the sorting strategy for sorting the items and grasps (see Setting the sorting strategies).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/set_sorting_strategies
PUT http://<host>/api/v1/nodes/rc_boxpick/services/set_sorting_strategies

Only one strategy may have a weight greater than 0. If all weight values are set to 0, the module will use the default sorting strategy.

If the weight for direction is set, the vector must contain the direction vector and pose_frame must be either camera or external.

If the weight for distance_to_point is set, point must contain the sorting point and pose_frame must be either camera or external.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "direction": {
      "pose_frame": "string",
      "vector": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "weight": "float64"
    },
    "distance_to_point": {
      "farthest_first": "bool",
      "point": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose_frame": "string",
      "weight": "float64"
    },
    "gravity": {
      "weight": "float64"
    },
    "surface_area": {
      "weight": "float64"
    }
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "set_sorting_strategies",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

get_sorting_strategies

Returns the sorting strategy for sorting the items and grasps (see Setting the sorting strategies).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/get_sorting_strategies
PUT http://<host>/api/v1/nodes/rc_boxpick/services/get_sorting_strategies
This service has no arguments.

All weight values are 0 when the module uses the default sorting strategy.

The definition for the response with corresponding datatypes is:

{
  "name": "get_sorting_strategies",
  "response": {
    "direction": {
      "pose_frame": "string",
      "vector": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "weight": "float64"
    },
    "distance_to_point": {
      "farthest_first": "bool",
      "point": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose_frame": "string",
      "weight": "float64"
    },
    "gravity": {
      "weight": "float64"
    },
    "return_code": {
      "message": "string",
      "value": "int16"
    },
    "surface_area": {
      "weight": "float64"
    }
  }
}

start

Starts the module. If the command is accepted, the module moves to state RUNNING.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/start
PUT http://<host>/api/v1/nodes/rc_boxpick/services/start
This service has no arguments.

The current_state value in the service response may differ from RUNNING if the state transition is still in process when the service returns.

The definition for the response with corresponding datatypes is:

{
  "name": "start",
  "response": {
    "accepted": "bool",
    "current_state": "string"
  }
}

stop

Stops the module. If the command is accepted, the module moves to state IDLE.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/stop
PUT http://<host>/api/v1/nodes/rc_boxpick/services/stop
This service has no arguments.

The current_state value in the service response may differ from IDLE if the state transition is still in process when the service returns.

The definition for the response with corresponding datatypes is:

{
  "name": "stop",
  "response": {
    "accepted": "bool",
    "current_state": "string"
  }
}

trigger_dump

Triggers dumping of the detection that corresponds to the given timestamp, or the latest detection, if no timestamp is given. The dumps are saved to the connected USB drive.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/trigger_dump
PUT http://<host>/api/v1/nodes/rc_boxpick/services/trigger_dump

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "comment": "string",
    "timestamp": {
      "nsec": "int32",
      "sec": "int32"
    }
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "trigger_dump",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

reset_defaults

Resets all parameters of the module to its default values, as listed in above table. Also resets the sorting strategies and the preferred orientation.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_boxpick/services/reset_defaults
PUT http://<host>/api/v1/nodes/rc_boxpick/services/reset_defaults
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "reset_defaults",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

Return codes

Each service response contains a return_code, which consists of a value plus an optional message. A successful service returns with a return_code value of 0. Negative return_code values indicate that the service failed. Positive return_code values indicate that the service succeeded with additional information. The smaller value is selected in case a service has multiple return_code values, but all messages are appended in the return_code message.

The following table contains a list of common codes:

Table 35 Return codes of the BoxPick services
Code Description
0 Success
-1 An invalid argument was provided
-3 An internal timeout occurred, e.g. during box detection if the given dimension range is too large
-4 Data acquisition took longer than allowed
-8 The template has been deleted during detection
-10 New element could not be added as the maximum storage capacity of load carriers, regions of interest or template has been exceeded
-11 Sensor not connected, not supported or not ready
-12 Resource busy, e.g. when trigger_dump is called too frequently
-200 Fatal internal error
-301 More than one item model provided to the compute_grasps or compute_grasps_extended service
10 The maximum storage capacity of load carriers, regions of interest or templates has been reached
11 An existent persistent model was overwritten by the call to set_load_carrier or set_region_of_interest
100 The requested load carriers were not detected in the scene
101 No valid surfaces were found in the scene
102 The detected load carrier is empty
103 All computed grasps are in collision
112 Rejected detections of one or more clusters, because min_cluster_coverage was not reached
300 A valid robot_pose was provided as argument but it is not required
999 Additional hints for application development

BoxPick Template API

BoxPick templates are only available with the +Match extension of BoxPick. For template upload, download, listing and removal, special REST-API endpoints are provided. Templates can also be uploaded, downloaded and removed via the Web GUI. The templates include the dimensions, the views and their poses, if set. Up to 100 templates can be stored persistently on the rc_cube.

GET /templates/rc_boxpick

Get list of all rc_boxpick templates.

Template request

GET /api/v2/templates/rc_boxpick HTTP/1.1

Template response

HTTP/1.1 200 OK
Content-Type: application/json

[
  {
    "id": "string"
  }
]
Response Headers:
 
Status Codes:
Referenced Data Models:
 
GET /templates/rc_boxpick/{id}

Get a rc_boxpick template. If the requested content-type is application/octet-stream, the template is returned as file.

Template request

GET /api/v2/templates/rc_boxpick/<id> HTTP/1.1

Template response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "id": "string"
}
Parameters:
  • id (string) – id of the template (required)
Response Headers:
 
  • Content-Type – application/json application/ubjson application/octet-stream
Status Codes:
  • 200 OK – successful operation (returns Template)
  • 404 Not Found – node or template not found
Referenced Data Models:
 
PUT /templates/rc_boxpick/{id}

Create or update a rc_boxpick template.

Template request

PUT /api/v2/templates/rc_boxpick/<id> HTTP/1.1
Accept: multipart/form-data application/json

Template response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "id": "string"
}
Parameters:
  • id (string) – id of the template (required)
Form Parameters:
 
  • file – template file (required)
Request Headers:
 
  • Accept – multipart/form-data application/json
Response Headers:
 
Status Codes:
Referenced Data Models:
 
DELETE /templates/rc_boxpick/{id}

Remove a rc_boxpick template.

Template request

DELETE /api/v2/templates/rc_boxpick/<id> HTTP/1.1
Accept: application/json application/ubjson
Parameters:
  • id (string) – id of the template (required)
Request Headers:
 
  • Accept – application/json application/ubjson
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
  • 403 Forbidden – forbidden, e.g. because there is no valid license for this module.
  • 404 Not Found – node or template not found