Generic Robot Interface

The Generic Robot Interface (GRI) is an integration layer that bridges the REST-API v2 and provides a standardized way to communicate with the software modules using simple TCP socket communication on port 7100. It can be activated via a separate license .

Overview

The GRI is used in two phases. In the configuration phase, the user creates jobs and stores them under unique numeric IDs. A job contains everything needed for one operation: the module and service to call, the arguments to use, and the data to return to the robot. Jobs, and optionally hand-eye calibration configurations, are prepared once and are defined via the Web GUI or the REST-API (see Job types).

At run time, the robot triggers these jobs by their ID over a TCP socket on port 7100, exchanging fixed-size binary messages (see GRI binary protocol specification). The GRI internally manages the REST-API communication and returns the selected pose results in a format that can be chosen specifically for the robot. A typical job trigger proceeds as follows:

  1. The robot sends a trigger action (TRIGGER_JOB_SYNC or TRIGGER_JOB_ASYNC, see Actions) together with the job ID, optionally providing run-time values in the request data fields.
  2. The GRI looks up the job and translates it into the corresponding REST-API call(s) to the selected module.
  3. The results of the module, such as grasp poses, are cached by the GRI, and the first pose is returned to the robot in the chosen pose format.
  4. The robot retrieves any further results one at a time with GET_NEXT_POSE and GET_RELATED_POSE.

A job definition therefore serves as a reusable template that the robot triggers by its ID at run time. The following section describes how to define jobs; the binary protocol and the details of robot integration are described further below.

Job definition

Jobs are pre-configured tasks that can be triggered by the robot application. Each job has a unique ID and contains all the necessary information for a specific operation, e.g. computing grasps for bin picking or changing run-time parameters of a module. Once configured, the robot can execute these jobs using simple socket commands and, if applicable, receive the returned poses.

The jobs can be defined via the Web GUI or via the REST-API (see Job and HEC_config API).

In the Web GUI, a pipeline service job is created with Create Job in the Generic Robot Interface panel of the Try Out section of the respective module, using the settings currently configured there. Load Job loads a saved job back into the Try Out section for editing. When saving the job, its additional return values, dynamic arguments and mapping tables (see Returning poses and extra data) can be defined and edited with Configure Extra Data. Parameter setting jobs can be created and edited on the Web GUI’s Generic Robot Interface page.

Job types

The Generic Robot Interface supports three types of jobs, selected via the job_type field:

  • CALL_PIPELINE_SERVICE – call a service on a specific camera pipeline (e.g. to detect objects or compute grasps) and return pose data to the robot.
  • CALL_GLOBAL_SERVICE – call a service that is not tied to a pipeline (e.g. database services for regions of interest, load carriers or grippers). Returns a pose only if explicitly configured to.
  • SET_PIPELINE_PARAMETERS – set run-time parameters on a pipeline node. Returns no pose.

The fields selected_return, pose_path, additional_return and dynamic_args control which pose a job returns and how the robot can influence the call. They are described in detail in Returning poses and extra data and demonstrated on complete jobs in Worked examples.

Pipeline service job (CALL_PIPELINE_SERVICE)

This job calls a service on a specific camera pipeline, e.g. to detect objects or compute grasps, and returns pose data (e.g. grasp poses) to the robot.

Field Presence Description
job_type required the job type CALL_PIPELINE_SERVICE
name required descriptive name to distinguish jobs
pipeline required the camera pipeline to use for the job (e.g. "0")
node required the REST-API name of the pipeline node (e.g. rc_itempick)
service required the REST-API name of the service to call (e.g. compute_grasps)
args required the REST-API JSON arguments passed to the service
selected_return required the REST-API response field holding the poses to return (e.g. grasps or matches); see Choosing the returned pose: selected_return and pose_path
pose_path optional the field inside the selected_return object that holds the pose (defaults to pose); see Choosing the returned pose: selected_return and pose_path
additional_return optional extra response fields to return in data_4 through data_10; see additional_return (module to robot)
dynamic_args optional fill args from the robot request fields data_1 through data_4; see dynamic_args (robot to module)

A minimal pipeline service job definition is:

{
   "args": {
      "pose_frame": "external",
      "suction_surface_length": 0.02,
      "suction_surface_width": 0.02
   },
   "job_type": "CALL_PIPELINE_SERVICE",
   "name": "Compute Grasps",
   "node": "rc_itempick",
   "pipeline": "0",
   "selected_return": "grasps",
   "service": "compute_grasps"
}

For pipeline service jobs, the GRI adds the robot pose sent with the trigger request to the service arguments as robot_pose (position in meters, orientation as quaternion). A robot_pose given in args is overwritten. Global service jobs do not receive the robot pose.

The available values for selected_return depend on the chosen node and can be e.g. grasps or matches. Refer to the service definitions of the corresponding module for details about node, service, args and selected_return.

Global service job (CALL_GLOBAL_SERVICE)

This job calls a service that is not tied to a specific pipeline, e.g. database services for setting or retrieving regions of interest, load carriers or grippers. By default, global service jobs do not return any pose; they return a pose only if selected_return (and, typically, pose_path) is configured.

Field Presence Description
job_type required the job type CALL_GLOBAL_SERVICE
name required descriptive name to distinguish jobs
node required the REST-API name of the global node (e.g. rc_load_carrier_db)
service required the REST-API name of the service to call
args required the REST-API JSON arguments passed to the service
selected_return optional the REST-API response field holding the pose(s) to return (e.g. to retrieve gripper or TCP definitions); without it the job returns no pose; see Choosing the returned pose: selected_return and pose_path
pose_path optional the field inside the selected_return object that holds the pose (defaults to pose); see Choosing the returned pose: selected_return and pose_path
additional_return optional extra response fields to return in data_4 through data_10; see additional_return (module to robot)
dynamic_args optional fill args from the robot request fields data_1 through data_4; see dynamic_args (robot to module)

The field pipeline must not be set for global service jobs.

A minimal global service job definition is:

{
   "args": {
      "region_of_interest_2d": {
         "id": "2d_roi",
         "width": 526,
         "height": 501,
         "offset_x": 558,
         "offset_y": 307
      }
   },
   "job_type": "CALL_GLOBAL_SERVICE",
   "name": "Set 2D ROI",
   "node": "rc_roi_db",
   "service": "set_region_of_interest_2d"
}

Refer to the service definitions of the corresponding module for details about node, service and args.

Parameter setting job (SET_PIPELINE_PARAMETERS)

This job sets run-time parameters on a pipeline node, e.g. for adjusting camera or detection module settings. Parameter setting jobs do not return any pose.

Field Presence Description
job_type required the job type SET_PIPELINE_PARAMETERS
name required descriptive name to distinguish jobs
pipeline required the camera pipeline to use for the job (e.g. "0")
node required the REST-API name of the pipeline node (e.g. rc_stereomatching)
parameters required the run-time parameters to set as key-value pairs

A sample parameter setting job definition is:

{
   "job_type": "SET_PIPELINE_PARAMETERS",
   "name": "Set Stereo Parameters",
   "node": "rc_stereomatching",
   "parameters": {
      "maxdepth": 2,
      "quality": "High"
   },
   "pipeline": "0"
}

When a parameter setting job is triggered, data_1 of the response is 0 if all parameters were set and -1 otherwise; in the latter case error_code is API_RESPONSE_ERROR. Unlike for the other job types, data_1 is not a node’s return_code. GET_JOB_STATUS reports data_1 as 0 for these jobs.

Refer to the run-time parameter definitions of the corresponding module for details about node and parameters.

Returning poses and extra data

Each result that a job delivers carries one pose in the response’s pose fields (pos_x through rot_4). In addition, Protocol V1 leaves several request and response fields unused, and the job configuration uses them to exchange additional information between the robot and the REST-API:

  • selected_return and pose_path choose which pose is returned.
  • additional_return returns extra values from the REST-API response in the response fields data_4 through data_10 (module to robot, see Response body definition).
  • dynamic_args injects robot-provided values from the request fields data_1 through data_4 into the args of the REST-API call (robot to module, see Request body definition).
  • maps translates between the integers the robot exchanges and the string values the REST-API uses.

additional_return, dynamic_args and maps can also be defined and edited in the Web GUI with Configure Extra Data when saving a job.

All of these locate values inside the REST-API response or request through a json_path, which is explained first.

Locating values with json_path

A json_path addresses a single value inside the REST-API response (or, for dynamic_args, inside the request arguments). Two forms exist:

  • Object-relative (no leading dot, e.g. quality): resolved inside the primary or related object that is currently being returned by GET_NEXT_POSE / GET_RELATED_POSE.
  • Root-relative (leading dot, e.g. .timestamp.sec): resolved from the root of the entire REST-API response, which is useful for global metadata or for a parent property.

To descend into a list, use bracket notation with a zero-based index, e.g. item_models[0].type.

The following annotated response shows how each form resolves, assuming the job returns grasps as primary objects and items as related objects:

{
   "timestamp": {
      "sec": 1719900000
   },
   "grasps": [
      {
         "quality": 0.85,
         "item_uuid": "abc-123"
      }
   ],
   "items": [
      {
         "uuid": "abc-123",
         "bounding_box": { "x": 0.15 }
      }
   ]
}
  • quality (object-relative, primary scope) resolves to 0.85.
  • bounding_box.x (object-relative, related scope) resolves to 0.15.
  • .timestamp.sec (root-relative) resolves to 1719900000.

Note

Always use bracket notation (item_models[0]) to access a list element. Writing item_models.0 makes the GRI search for a dictionary key literally named "0" instead of the first list element.

Because GET_NEXT_POSE and GET_RELATED_POSE return one object at a time, an object-relative json_path is written for a single object: use quality, not grasps[0].quality.

Choosing the returned pose: selected_return and pose_path

selected_return names the response field holding the primary objects to iterate over, e.g. grasps, matches, items or load_carriers. It can also index into a list nested deeper in the response using bracket notation, for example to iterate over the TCPs of a specific gripper:

{
   "selected_return": "grippers[0].tcps",
   "pose_path": "pose_flange"
}

pose_path tells the GRI where, inside each selected object, to find the pose (an object with position and orientation) to return to the robot. It follows the same path rules as json_path and defaults to pose, which is why it is normally omitted: all built-in pipeline return types (grasps, matches, items, load_carriers) expose their pose in a field named pose.

Set pose_path explicitly when the selected object has no pose field, or when it exposes more than one candidate pose and a specific one has to be chosen. This is the case in the gripper example above, where each TCP has separate pose_flange and pose_parent fields instead of a single pose. The same value is applied to both the primary and the related object, so it only needs to differ from the default when the relevant field is not named pose. If the resolved value is missing, or is not an object with both a position and an orientation, the job is rejected as misconfigured (MISCONFIGURED_JOB).

additional_return (module to robot)

additional_return maps extra values from the REST-API response into the response fields data_4 through data_10. Its mappings are grouped by the object they apply to:

  • primary: applied to the primary object returned by GET_NEXT_POSE (the object type named by selected_return, e.g. grasps).
  • related: applied to the corresponding related object returned by GET_RELATED_POSE (see Primary and related objects).

Each mapping is an object with the following fields:

  • target_field: the response field to write to (data_4 through data_10)
  • json_path: where to read the value in the REST-API response (see Locating values with json_path)
  • type: how to convert the value into the int32 response field:
    • int: written as an integer (the default if type is omitted); a value with a fractional part is rejected with TYPE_CONVERSION_ERROR
    • float: multiplied by 1,000,000 (analogous to the pose scaling in Pose formats)
    • bool: 1 or 0
    • map: translated to an integer via a maps lookup table (see Mapping tables (maps))

If a json_path does not resolve to a value, that field is simply skipped (MISSING_ADDITIONAL_DATA warning, see Error codes and semantics). A failed map lookup or type conversion instead aborts the whole response with an error (UNMAPPED_VALUE_ERROR / TYPE_CONVERSION_ERROR).

If a job has no selected_return, there are no primary objects to iterate over. primary mappings are then applied directly to the TRIGGER_JOB_SYNC response, and their json_path values are resolved from the root of the REST-API response. This allows returning values from global service jobs that do not return a pose.

dynamic_args (robot to module)

dynamic_args maps values from the robot request into the args of the REST-API service call, letting the robot adjust detection arguments at trigger time without reconfiguring the job. It applies to CALL_PIPELINE_SERVICE and CALL_GLOBAL_SERVICE jobs; SET_PIPELINE_PARAMETERS jobs do not use it. It is a list of entries, each with:

  • source_field: the request field to read from (data_1 through data_4, see Request body definition)
  • json_path: the target key path within the REST-API args (same path rules as Locating values with json_path)
  • type: how to convert the value before injecting it:
    • int: injected as-is (the default if type is omitted)
    • float: divided by 1,000,000
    • bool: interpreted as 1 / 0
    • map: the integer sent by the robot is looked up in a maps table to inject the corresponding value

The values are applied on top of the static args when the job is triggered, so a json_path pointing at an existing argument overwrites it. A failed map lookup or type conversion is rejected with an error (UNMAPPED_VALUE_ERROR / TYPE_CONVERSION_ERROR, see Error codes and semantics).

Mapping tables (maps)

Some arguments and return values are strings (such as IDs) rather than numbers. maps translates between the integers the robot exchanges and these string values on the GRI server. The same table is used in both directions – dynamic_args looks up robot ID to value, additional_return looks up value to robot ID – so each table must be a 1:1 (bijective) mapping. A dynamic_args or additional_return entry of type map selects the table to use via a map field:

{
   "dynamic_args": [
      { "source_field": "data_2", "json_path": "template_id", "type": "map", "map": "models" }
   ],
   "maps": {
      "models": {
         "1": "part_A_large",
         "2": "part_B_small"
      }
   }
}

If the robot sends data_2 = 2, the template ID "part_B_small" is injected into the REST-API call.

Worked examples

The following complete job definitions combine the options above. For each one, the configuration is shown first, followed by what the robot sends or receives at run time.

Example 1: pipeline service job with additional return

This ItemPick job returns grasp poses and, alongside each pose, extra information about the grasp (primary scope) and about the item the grasp was computed for (related scope).

{
   "name": "ItemPickAIJob",
   "job_type": "CALL_PIPELINE_SERVICE",
   "pipeline": "0",
   "node": "rc_itempick",
   "service": "compute_grasps",
   "selected_return": "grasps",
   "args": {
      "collision_detection": {
         "gripper_id": "MultiSuctionGripper",
         "pre_grasp_offset": { "x": 0, "y": 0, "z": -0.1 }
      },
      "item_models": [ { "type": "BAG" } ],
      "pose_frame": "external",
      "region_of_interest_id": "ROI",
      "suction_surface_length": 0.05,
      "suction_surface_width": 0.05
   },
   "additional_return": {
      "primary": [
         { "json_path": "quality", "target_field": "data_4", "type": "float" },
         { "json_path": "tcp_id",  "target_field": "data_5", "type": "map", "map": "gripper_tcps" }
      ],
      "related": [
         { "json_path": "bounding_box.x", "target_field": "data_6", "type": "float" },
         { "json_path": "bounding_box.y", "target_field": "data_7", "type": "float" },
         { "json_path": "bounding_box.z", "target_field": "data_8", "type": "float" }
      ]
   },
   "maps": {
      "gripper_tcps": { "1": "TCP1", "2": "TCP2", "3": "TCP3" }
   }
}
  • selected_return is grasps, so each GET_NEXT_POSE returns one grasp pose.
  • additional_return.primary reads two values from that grasp: its quality into data_4 (as a float) and its tcp_id into data_5 (translated to an integer through the gripper_tcps table).
  • additional_return.related reads the bounding box of the associated item into data_6 through data_8, available after GET_RELATED_POSE.

At run time, for a grasp with quality = 0.85 and tcp_id = "TCP2" on an item with bounding box (0.15, 0.10, 0.05) m:

  • GET_NEXT_POSE returns the grasp pose, data_4 = 850000 (0.85 x 1,000,000) and data_5 = 2 (the key mapped to "TCP2" in gripper_tcps).
  • GET_RELATED_POSE returns the item pose, data_6 = 150000, data_7 = 100000 and data_8 = 50000 (each bounding-box dimension x 1,000,000).

Example 2: global service job returning a pose

Global service jobs return no pose by default. This job sets selected_return and pose_path so that it returns the TCP poses stored for a gripper in the gripper database.

{
   "name": "GetMultiSuctionGripperTCPs",
   "job_type": "CALL_GLOBAL_SERVICE",
   "node": "rc_gripper_db",
   "service": "get_grippers",
   "selected_return": "grippers[0].tcps",
   "pose_path": "pose_flange",
   "args": {
      "gripper_ids": [ "MultiSuctionGripper" ]
   },
   "additional_return": {
      "primary": [
         { "json_path": "id", "target_field": "data_4", "type": "map", "map": "tcp_names" },
         { "json_path": ".grippers[0].flange_radius", "target_field": "data_5", "type": "float" }
      ]
   },
   "maps": {
      "tcp_names": { "1": "TCP1", "2": "TCP2", "3": "TCP3" }
   }
}
  • selected_return uses index addressing, grippers[0].tcps, to iterate over the TCPs of the first returned gripper as the primary objects.
  • pose_path is set to pose_flange because a TCP has no plain pose field but separate pose_flange and pose_parent poses; pose_flange is the one returned.
  • additional_return.primary mixes both path forms: the object-relative id (the current TCP’s ID, mapped to an integer via tcp_names) and the root-relative .grippers[0].flange_radius (a property of the parent gripper, the same for every TCP).

At run time, for a TCP with id = "TCP1" on a gripper with flange_radius = 0.04 m, GET_NEXT_POSE returns the TCP’s pose_flange, data_4 = 1 ("TCP1" via tcp_names) and data_5 = 40000 (0.04 x 1,000,000).

Example 3: pipeline service job with dynamic arguments

This BoxPick job lets the robot choose the rectangle dimensions to detect at trigger time, so the same job can pick different box sizes without being reconfigured. The four dimensions of the RECTANGLE item model are filled from the request fields data_1 through data_4.

{
   "name": "BoxPickDynamicRectangle",
   "job_type": "CALL_PIPELINE_SERVICE",
   "pipeline": "0",
   "node": "rc_boxpick",
   "service": "compute_grasps",
   "selected_return": "grasps",
   "args": {
      "pose_frame": "external",
      "item_models": [
         {
            "type": "RECTANGLE",
            "rectangle": {
               "min_dimensions": { "x": 0.05, "y": 0.05 },
               "max_dimensions": { "x": 0.10, "y": 0.10 }
            }
         }
      ],
      "suction_surface_length": 0.05,
      "suction_surface_width": 0.05
   },
   "dynamic_args": [
      { "source_field": "data_1", "json_path": "item_models[0].rectangle.min_dimensions.x", "type": "float" },
      { "source_field": "data_2", "json_path": "item_models[0].rectangle.min_dimensions.y", "type": "float" },
      { "source_field": "data_3", "json_path": "item_models[0].rectangle.max_dimensions.x", "type": "float" },
      { "source_field": "data_4", "json_path": "item_models[0].rectangle.max_dimensions.y", "type": "float" }
   ],
   "additional_return": {
      "primary": [
         { "json_path": "quality", "target_field": "data_4", "type": "float" }
      ]
   }
}
  • dynamic_args uses the same json_path grammar as additional_return, here indexing into item_models[0] to reach the rectangle dimensions inside args.
  • The dimensions given in args are placeholders: the values injected from the request overwrite them when the job is triggered.
  • The request fields data_1 through data_4 (filled by dynamic_args) and the response fields data_4 through data_10 (filled by additional_return) belong to separate messages, so reusing data_4 for both the sent minimum-x dimension and the returned grasp quality is not a conflict.

At run time, if the robot triggers the job with data_1 = 50000, data_2 = 50000, data_3 = 100000 and data_4 = 100000, the GRI divides each value by 1,000,000 and calls rc_boxpick/compute_grasps with min_dimensions (0.05, 0.05) m and max_dimensions (0.10, 0.10) m. Each subsequent GET_NEXT_POSE then returns a grasp pose with data_4 set to that grasp’s quality x 1,000,000.

Execution modes

The Generic Robot Interface supports two execution modes to optimize the robot’s cycle time:

  • Synchronous Execution: The robot triggers a job and waits for the first result to arrive. This mode should be chosen when results are required immediately.
  • Asynchronous Execution: The robot starts a job and can continue with other operations while the job is running in the background. The job status can be queried and results can be retrieved when ready. This mode maximizes efficiency during long detection times.

Hand-Eye Calibration

A hand-eye calibration configuration can be defined for each camera pipeline to allow for programmatic hand-eye calibration using the GRI. Each hand-eye calibration configuration consists of the following information:

  • grid_height: height of the calibration grid in meters
  • grid_width: width of the calibration grid in meters
  • robot_mounted: boolean that determines whether the camera is mounted on the robot
  • tcp_offset: 0 for 6DOF robots. For 4DOF robots: the signed offset from the TCP to the camera coordinate system (robot-mounted sensor) or the visible surface of the calibration grid (statically mounted sensor) along the TCP rotation axis in meters.
  • tcp_rotation_axis: -1 for 6DOF robots. For 4DOF robots: determines the axis of the robot frame around which the robot can rotate its TCP (0 is used for X, 1 for Y and 2 for the Z axis).

More detailed information about these settings and the hand-eye calibration in general is given in Hand-eye calibration.

The hand-eye calibration configurations can be set via the Web GUI or via the REST-API (see Job and HEC_config API).

GRI binary protocol specification

This specification defines the exact on-wire format for client-server messages. A message consists of a fixed 8-byte header and a body whose layout depends on the protocol version. Currently, there is only protocol version 1.

Note

All multi-byte integers are little-endian. Types are uint8 (8-bit unsigned), int16 (16-bit signed), int32 (32-bit signed).

Message header (8 bytes)

Table 68 Message header definition
Field Type Size Description
magic_number uint32 4 ASCII tag “GRI0”, bytes 47 52 49 00 (little-endian)
protocol_version uint8 1 Protocol version: currently 1
message_length uint8 1 Total message size (bytes), incl. header + body
pose_format uint8 1 Pose data format (see Pose formats)
action uint8 1 Command/action (see Actions)

Pose formats

The GRI always uses millimeters for representing a position. The following tables show different rotation formats that can be chosen to match to the rotation representation of the used robot. The formats are grouped by non-Euler rotation formats, Tait-Bryan-Euler rotation formats (all three axes are used) and proper Euler rotation formats (first and last rotation axis are the same).

Table 69 Non-Euler rotation formats
Name Value rot_1 rot_2 rot_3 rot_4 Units Robot Example
QUAT_WXYZ 1 w x y z – ABB
QUAT_XYZW 2 x y z w – Fruitcore HORST
AXIS_ANGLE_RAD 3 rx ry rz – rad Universal Robots

In the following notation primes indicate successive rotations in the intrinsic frame (e.g., Y’ = rotation about Y-axis after first rotation). _B and _F determine the order in which the rotation components are given. F stands for forward, meaning that the rotation components are given in the same order as the rotation is applied, and B stands for backward, meaning the rotation components are given in reverse order. _RAD and _DEG determine whether the rotation components are given in radians or degrees, respectively, if applicable. So the format EULER_ZYX_B_DEG means that the intrinsic rotation order is z-y’-x’’ (first rotate around the z axis, then rotate around the new y axis, then rotate around the new x axis), the order in which the rotation components are given is backward (so the first rotation element is the angle around the x axis), and the angels are given in degrees.

Table 70 Tait-Bryan-Euler rotation formats. Primes indicate successive rotations in the intrinsic frame (e.g., Y’ = rotation about Y-axis after first rotation). _F (Forward): [1st, 2nd, 3rd] | _B (Backward): [3rd, 2nd, 1st], _DEG: degrees | _RAD: radian.
Name Value rot_1 rot_2 rot_3 rot_4 Units Robot Example
EULER_XYZ_F_DEG 4 X Y’ Z’’ – deg  
EULER_XYZ_F_RAD 5 X Y’ Z’’ – rad  
EULER_XYZ_B_DEG 6 Z’’ Y’ X – deg  
EULER_XYZ_B_RAD 7 Z’’ Y’ X – rad  
EULER_XZY_F_DEG 8 X Z’ Y’’ – deg  
EULER_XZY_F_RAD 9 X Z’ Y’’ – rad  
EULER_XZY_B_DEG 10 Y’’ Z’ X – deg  
EULER_XZY_B_RAD 11 Y’’ Z’ X – rad  
EULER_YXZ_F_DEG 12 Y X’ Z’’ – deg  
EULER_YXZ_F_RAD 13 Y X’ Z’’ – rad  
EULER_YXZ_B_DEG 14 Z’’ X’ Y – deg  
EULER_YXZ_B_RAD 15 Z’’ X’ Y – rad  
EULER_YZX_F_DEG 16 Y Z’ X’’ – deg  
EULER_YZX_F_RAD 17 Y Z’ X’’ – rad  
EULER_YZX_B_DEG 18 X’’ Z’ Y – deg  
EULER_YZX_B_RAD 19 X’’ Z’ Y – rad  
EULER_ZXY_F_DEG 20 Z X’ Y’’ – deg  
EULER_ZXY_F_RAD 21 Z X’ Y’’ – rad  
EULER_ZXY_B_DEG 22 Y’’ X’ Z – deg  
EULER_ZXY_B_RAD 23 Y’’ X’ Z – rad  
EULER_ZYX_F_DEG 24 Z Y’ X’’ – deg KUKA
EULER_ZYX_F_RAD 25 Z Y’ X’’ – rad  
EULER_ZYX_B_DEG 26 X’’ Y’ Z – deg FANUC, Mitsubishi, Yaskawa
EULER_ZYX_B_RAD 27 X’’ Y’ Z – rad  
Table 71 Euler rotation formats. Primes indicate successive rotations in the intrinsic frame (e.g., Y’ = rotation about Y-axis after first rotation). _F (Forward): [1st, 2nd, 3rd] | _B (Backward): [3rd, 2nd, 1st], _DEG: degrees | _RAD: radian.
Name Value rot_1 rot_2 rot_3 rot_4 Units Robot Example
EULER_XYX_F_DEG 28 X Y’ X’’ – deg  
EULER_XYX_F_RAD 29 X Y’ X’’ – rad  
EULER_XYX_B_DEG 30 X’’ Y’ X – deg  
EULER_XYX_B_RAD 31 X’’ Y’ X – rad  
EULER_XZX_F_DEG 32 X Z’ X’’ – deg  
EULER_XZX_F_RAD 33 X Z’ X’’ – rad  
EULER_XZX_B_DEG 34 X’’ Z’ X – deg  
EULER_XZX_B_RAD 35 X’’ Z’ X – rad  
EULER_YXY_F_DEG 36 Y X’ Y’’ – deg  
EULER_YXY_F_RAD 37 Y X’ Y’’ – rad  
EULER_YXY_B_DEG 38 Y’’ X’ Y – deg  
EULER_YXY_B_RAD 39 Y’’ X’ Y – rad  
EULER_YZY_F_DEG 40 Y Z’ Y’’ – deg  
EULER_YZY_F_RAD 41 Y Z’ Y’’ – rad  
EULER_YZY_B_DEG 42 Y’’ Z’ Y – deg  
EULER_YZY_B_RAD 43 Y’’ Z’ Y – rad  
EULER_ZXZ_F_DEG 44 Z X’ Z’’ – deg  
EULER_ZXZ_F_RAD 45 Z X’ Z’’ – rad  
EULER_ZXZ_B_DEG 46 Z’’ X’ Z – deg  
EULER_ZXZ_B_RAD 47 Z’’ X’ Z – rad  
EULER_ZYZ_F_DEG 48 Z Y’ Z’’ – deg Kawasaki
EULER_ZYZ_F_RAD 49 Z Y’ Z’’ – rad  
EULER_ZYZ_B_DEG 50 Z’’ Y’ Z – deg  
EULER_ZYZ_B_RAD 51 Z’’ Y’ Z – rad  

All pose components (position and rotation) are int32 scaled by 1,000,000.

  • Float to Int: int = round(float * 1000000)
  • Int to Float: float = int / 1000000.0
  • Positions in millimeters before scaling
  • Angles in degrees/radians (per format) before scaling
  • Quaternions unitless, same scaling
  • rot_4 unused for Euler/axis-angle (set to 0)
  • Value range: int32 limits each scaled component to ±2147.483647, i.e. positions to ±2147.48 mm per axis. Values outside this range cannot be transmitted; the GRI then sends no response.

Actions

The following actions can be sent.

Table 72 GRI actions
Name Value Description
STATUS 1 Get system readiness; maps readiness to data_2 (1 or 0)
TRIGGER_JOB_SYNC 2 Execute job synchronously
TRIGGER_JOB_ASYNC 3 Start job asynchronously
GET_JOB_STATUS 4 Query async job status (see Job status)
GET_NEXT_POSE 5 Retrieve next available result
GET_RELATED_POSE 6 Retrieve next related pose
HEC_INIT 7 Initialize hand-eye calibration
HEC_SET_POSE 8 Provide/store calibration pose
HEC_CALIBRATE 9 Run calibration and save results

STATUS (1)

Returns system readiness information fetched from the rc_cube in data_2 (1 if ready, 0 if not).

TRIGGER_JOB_SYNC (2)

Runs the job and returns the first result immediately; additional results are stored for later retrieval. On success with results, error_code will be zero and the pose will be filled. If no results are returned, error_code will be NO_POSES_FOUND (positive warning). It also reports:

If the job does not finish within the processing timeout, or the sensor does not answer within the API timeout, error_code is PROCESSING_TIMEOUT and the job is marked FAILED.

TRIGGER_JOB_ASYNC (3)

Starts the job and returns immediately. The job’s status can be polled with GET_JOB_STATUS (4) (see Job status) and the results can be fetched with GET_NEXT_POSE (5), as soon as the job is DONE.

GET_JOB_STATUS (4)

Returns the job status. It reports:

  • data_1 = node’s return_code value
  • data_2 = job status (see table Job status values)

Error details flow through error_code. A job that timed out reports FAILED with error_code PROCESSING_TIMEOUT; for TRIGGER_JOB_ASYNC this is the case when the sensor does not answer within the API timeout.

GET_NEXT_POSE (5)

Returns the next result of the primary object. It also reports:

When no more primary objects are available, it returns NO_POSES_FOUND. The job stays DONE, so the related objects of the last primary object can still be retrieved with GET_RELATED_POSE. If the job is still running, GET_NEXT_POSE returns JOB_STILL_RUNNING; if it failed or has not been triggered yet, it returns NO_POSES_FOUND.

GET_RELATED_POSE (6)

Returns the next pose of the related object corresponding to the current primary object. It also reports:

If no related poses were found, it returns NO_RELATED_POSES.

HEC_INIT (7)

This action initializes the hand-eye calibration. It clears any existing calibration data, applies the pipeline’s configuration parameters and prepares the system for recording new poses. data_1 specifies the target pipeline.

HEC_SET_POSE (8)

This action is to be used eight times to record distinct robot poses with visible calibration pattern. The field data_2 is used to specify the image storage slot (0-7). A previous pose in a slot will be overwritten if a slot is reused. Each pose must provide a different view of the calibration pattern, as described in Hand-eye calibration. data_1 specifies the target pipeline.

HEC_CALIBRATE (9)

This action processes all recorded poses and calculates the transformation between camera and robot. It automatically saves successful calibration results. data_1 specifies the target pipeline.

Job status

The following job status values can be returned.

Table 73 Job status values
Name Value
INACTIVE 1
RUNNING 2
DONE 3
FAILED 4

Body definitions

There are different body definitions depending on whether it is a request that is sent or a response that is received. The request body consists of 54 bytes in total and its definition is given in table Request body definition.

Table 74 Request body definition
Field Type Size Description
header struct 8 Message header (see Message header (8 bytes))
job_id uint16 2 Unique job ID from job configuration
pos_x int32 4 Position X (scaled by 10^6)
pos_y int32 4 Position Y (scaled by 10^6)
pos_z int32 4 Position Z (scaled by 10^6)
rot_1 int32 4 Rotation component 1 (scaled by 10^6)
rot_2 int32 4 Rotation component 2 (scaled by 10^6)
rot_3 int32 4 Rotation component 3 (scaled by 10^6)
rot_4 int32 4 Rotation component 4 (scaled by 10^6)
data_1 int32 4 Additional parameter 1
data_2 int32 4 Additional parameter 2
data_3 int32 4 Additional parameter 3
data_4 int32 4 Additional parameter 4

The job ID is the unique identifier from the job configuration. The usage of the fields data_1...data_4 depends on the action and job. They are set to 0 if unused. For TRIGGER_JOB_SYNC/TRIGGER_JOB_ASYNC, these fields can be filled with robot-provided values via the job’s dynamic_args configuration, see Returning poses and extra data.

The response body consists of 80 bytes in total. Its definition is given in table Response body definition.

Table 75 Response body definition
Field Type Size Description
header struct 8 Protocol header
job_id uint16 2 Processed job number
error_code int16 2 GRI result status (severity by sign)
pos_x int32 4 Position X (scaled by 10^6)
pos_y int32 4 Position Y (scaled by 10^6)
pos_z int32 4 Position Z (scaled by 10^6)
rot_1 int32 4 Rotation component 1 (scaled by 10^6)
rot_2 int32 4 Rotation component 2 (scaled by 10^6)
rot_3 int32 4 Rotation component 3 (scaled by 10^6)
rot_4 int32 4 Rotation component 4 (scaled by 10^6)
data_1 int32 4 Node’s return code (0 if none)
data_2 int32 4 Additional result 2
data_3 int32 4 Additional result 3
data_4 int32 4 Additional result 4
data_5 int32 4 Additional result 5
data_6 int32 4 Additional result 6
data_7 int32 4 Additional result 7
data_8 int32 4 Additional result 8
data_9 int32 4 Additional result 9
data_10 int32 4 Additional result 10

Note

For rc_measure, mean_z is mapped to pos_x/pos_y/pos_z.

The fields data_4 through data_10 are filled according to the job’s additional_return configuration, see Returning poses and extra data.

Error codes and semantics

The error_code is int16 and encodes errors/warnings by sign:

  • Negative < 0 = error (failure)
  • Zero = 0 = success
  • Positive > 0 = warning (success with caveat)

The tables below give the different error codes and are split by sign and sorted.

Success

Name Value Description
NO_ERROR 0 Operation successful

Negative error codes

Name Value Description
UNKNOWN_ERROR -1 GRI internal, unspecified
INTERNAL_ERROR -2 GRI internal system error
API_NOT_REACHABLE -3 Cannot reach API
API_RESPONSE_ERROR -4 API call failed or returned a negative code
PIPELINE_NOT_AVAILABLE -5 Reserved, currently not used
INVALID_REQUEST_ERROR -6 Malformed request
INVALID_REQUEST_LENGTH -7 Wrong message length
INVALID_ACTION -8 Unsupported action
PROCESSING_TIMEOUT -9 Operation timed out
UNKNOWN_PROTOCOL_VERSION -10 Protocol version not supported
WRONG_PROTOCOL_FOR_JOB -11 Job configured for unsupported protocol version
JOB_DOES_NOT_EXIST -12 Invalid job ID
MISCONFIGURED_JOB -13 Invalid job configuration
HEC_CONFIG_ERROR -14 Invalid configuration parameters
HEC_INIT_ERROR -15 Calibration init failed
HEC_SET_POSE_ERROR -16 Failed to record pose in specified slot
HEC_CALIBRATE_ERROR -17 Unable to compute calibration from recorded poses
HEC_INSUFFICIENT_DETECTION -18 Calibration grid not visible or not detected
TYPE_CONVERSION_ERROR -19 Value not convertible to the configured type
UNMAPPED_VALUE_ERROR -20 Value has no entry in the referenced maps table

Positive codes

Name Value Description
NO_POSES_FOUND 1 No results available
NO_RELATED_POSES 2 No related data found
NO_RETURN_SPECIFIED 3 Job configured with no return type
JOB_STILL_RUNNING 4 Async job not complete
MISSING_ADDITIONAL_DATA 5 additional_return path not found

Node return code semantics

The modules/nodes may return a return_code. This node return code is placed in the response data_1 field (defaults to 0 if no code). The GRI’s primary status is in error_code (sign-based semantics).

API_RESPONSE_ERROR is reported when the node returns a negative return_code, when the REST-API answers with an HTTP error or without a response, and when a parameter setting job could not set all parameters. If the REST-API error carries a return_code (e.g. for a module or pipeline that is not ready), that value is reported in data_1, except for parameter setting jobs.

Malformed messages

The GRI answers a malformed message with an error and, if the byte stream can no longer be trusted, closes the connection afterwards. The robot then has to reconnect.

Message error_code Connection
wrong magic_number INVALID_REQUEST_ERROR closed
message_length does not match the protocol version INVALID_REQUEST_LENGTH closed
header received, but the body is incomplete or does not arrive in time INVALID_REQUEST_ERROR closed
header incomplete (fewer than 8 bytes arrive in time) no response closed
unsupported protocol_version, with a message_length that matches the bytes sent UNKNOWN_PROTOCOL_VERSION stays open
complete message with invalid content (e.g. HEC_SET_POSE without a pose) INVALID_REQUEST_ERROR stays open

Integration with a robot

The Generic Robot Interface offers communication on port 7100.

Different robot platforms can be supported by implementing a TCP socket client following the GRI binary protocol (see GRI binary protocol specification). This requires a robot controller with TCP/IP support and the ability to pack robot poses into binary messages and to parse binary messages into robot poses.

The implementation steps are as follows:

  1. Create TCP socket connection
  2. Compose request message:
    • Set message header (8 bytes)
    • Set job ID (2 bytes)
    • Pack position (12 bytes, 3x int32)
    • Pack rotation (16 bytes, 4x int32)
    • Pack additional data (16 bytes, 4x int32)
  3. Send request (54 bytes total)
  4. Receive response (80 bytes total)
  5. Parse response:
    • Message header (8 bytes)
    • Job ID (2 bytes)
    • Error code (2 bytes)
    • Position (12 bytes, 3x int32)
    • Rotation (16 bytes, 4x int32)
    • Additional data (40 bytes, 10x int32)

Byte interpretation in socket communication

Some robot scripting languages interpret individual socket bytes as signed values in the range [-128, 127] instead of unsigned [0, 255]. If this is the case, each byte has to be converted to unsigned before reconstructing int32 values:

# Convert signed byte to unsigned
if byte_value < 0:
    byte_value = byte_value + 256

After conversion, reconstruct the int32 using little-endian byte order, then apply signed interpretation to the most significant byte (MSB) to determine if the overall int32 value is negative.

Note

All pose components use scaling as described in Pose formats.

Job and HEC_config API

The job definitions and the definitions of HEC_configs for hand-eye calibration can be set, retrieved and deleted via the following REST-API endpoints.

GET /generic_robot_interface/hec_configs

Get defined hand-eye calibration configurations

Template request

GET /api/v2/generic_robot_interface/hec_configs HTTP/1.1

Sample response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "0": {
    "grid_height": 0.18,
    "grid_width": 0.26,
    "robot_mounted": true,
    "tcp_offset": 0,
    "tcp_rotation_axis": -1
  }
}
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
GET /generic_robot_interface/hec_configs/{pipeline}

Get hand-eye calibration configuration for the selected pipeline

Template request

GET /api/v2/generic_robot_interface/hec_configs/<pipeline> HTTP/1.1

Sample response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "grid_height": 0.18,
  "grid_width": 0.26,
  "robot_mounted": true,
  "tcp_offset": 0,
  "tcp_rotation_axis": -1
}
Parameters:
  • pipeline (string) – pipeline of the hand-eye calibration configuration (required)
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
PUT /generic_robot_interface/hec_configs/{pipeline}

Sets a hand-eye calibration configuration for the selected pipeline.

Template request

PUT /api/v2/generic_robot_interface/hec_configs/<pipeline> HTTP/1.1
Accept: application/json application/ubjson

{}

Sample response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "return_code": {
    "message": "HEC configuration saved successfully",
    "value": 0
  }
}
Parameters:
  • pipeline (string) – pipeline of the hand-eye calibration configuration (required)
Request JSON Object:
 
  • hand-eye calibration configuration (object) – example args (required)
Request Headers:
 
  • Accept – application/json application/ubjson
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
DELETE /generic_robot_interface/hec_configs/{pipeline}

Remove a hand-eye calibration configuration.

Template request

DELETE /api/v2/generic_robot_interface/hec_configs/<pipeline> HTTP/1.1
Accept: application/json application/ubjson
Parameters:
  • pipeline (string) – pipeline of the hand-eye calibration configuration (required)
Request Headers:
 
  • Accept – application/json application/ubjson
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
  • 403 Forbidden – forbidden, e.g. because there is no valid license for this module.
  • 404 Not Found – hec config for the given pipeline not found
GET /generic_robot_interface/jobs

Get defined jobs

Template request

GET /api/v2/generic_robot_interface/jobs HTTP/1.1

Sample response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "0": {
    "args": {
      "pose_frame": "external",
      "tags": []
    },
    "job_type": "CALL_PIPELINE_SERVICE",
    "name": "detect_qr_code",
    "node": "rc_qr_code_detect",
    "pipeline": "0",
    "selected_return": "tags",
    "service": "detect"
  },
  "1": {
    "job_type": "SET_PARAMETERS_SERVICE",
    "name": "set_depth_full_quality",
    "node": "rc_stereomatching",
    "parameters": {
      "double_shot": true,
      "quality": "Full"
    },
    "pipeline": "0"
  }
}
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
GET /generic_robot_interface/jobs/{job_id}

Get selected job definition

Template request

GET /api/v2/generic_robot_interface/jobs/<job_id> HTTP/1.1

Sample response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "args": {
    "pose_frame": "camera",
    "tags": []
  },
  "job_type": "CALL_PIPELINE_SERVICE",
  "name": "detect_qr_code",
  "node": "rc_qr_code_detect",
  "pipeline": "0",
  "selected_return": "tags",
  "service": "detect"
}
Parameters:
  • job_id (string) – ID of the job (required)
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
PUT /generic_robot_interface/jobs/{job_id}

Sets a job definition for the selected job ID. The required keys depend on the chosen job_type.

Template request

PUT /api/v2/generic_robot_interface/jobs/<job_id> HTTP/1.1
Accept: application/json application/ubjson

{}

Sample response

HTTP/1.1 200 OK
Content-Type: application/json

{
  "job_id": "1",
  "return_code": {
    "message": "Job configuration updated successfully",
    "value": 0
  }
}
Parameters:
  • job_id (string) – ID of the job (required)
Request JSON Object:
 
  • job definition (object) – example args (required)
Request Headers:
 
  • Accept – application/json application/ubjson
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
DELETE /generic_robot_interface/jobs/{job_id}

Remove a job definition.

Template request

DELETE /api/v2/generic_robot_interface/jobs/<job_id> HTTP/1.1
Accept: application/json application/ubjson
Parameters:
  • job_id (string) – ID of the job (required)
Request Headers:
 
  • Accept – application/json application/ubjson
Response Headers:
 
Status Codes:
  • 200 OK – successful operation
  • 403 Forbidden – forbidden, e.g. because there is no valid license for this module.
  • 404 Not Found – job with given id not found