IO and Projector Control¶
The IOControl module is a base module which is available on every rc_cube.
The IOControl module allows reading the status of the general purpose digital inputs and controlling the digital general purpose outputs (GPIOs) of the camera. The outputs can be set to LOW or HIGH, or configured to be HIGH for the exposure time of every image or every second image.
Note
This module is pipeline specific. Changes to its settings or parameters only affect the respective camera pipeline and have no influence on other pipelines running on the rc_cube.
The purpose of the IOControl module is the control of an external light source or a projector, which is connected to one of the camera’s GPIOs to be synchronized by the image acquisition trigger. In case a pattern projector is used to improve stereo matching, the intensity images also show the projected pattern, which might be a disadvantage for image processing tasks that are based on the intensity image (e.g. edge detection). For this reason, the IOControl module allows setting GPIO outputs to HIGH for the exposure time of every second image, so that intensity images without the projected pattern are also available.
Parameters¶
The IOControl module is called rc_iocontrol in the REST-API and is represented in the
Web GUI
in the desired pipeline under .
The user can change the parameters via the Web GUI, the
REST-API interface, or via GigE Vision
using the DigitalIOControl parameters LineSelector and LineSource
(Category: DigitalIOControl).
Parameter overview¶
This module offers the following run-time parameters:
| Name | Type | Min | Max | Default | Description |
|---|---|---|---|---|---|
out1_inverted |
bool | false | true | false | Inverting out1 |
out1_mode |
string | - | - | Low | Out1 mode: [Low, High, ExposureActive, ExposureAlternateActive] |
out1_ratio |
float64 | 0.0 | 1.0 | 1.0 | Ratio of exposure time that Out1 is high in ExposureActive and ExposureAlternateActive mode |
out2_inverted |
bool | false | true | false | Inverting out2 |
out2_mode |
string | - | - | Low | Out2 mode: [Low, High, ExposureActive, ExposureAlternateActive] |
out2_ratio |
float64 | 0.0 | 1.0 | 1.0 | Ratio of exposure time that Out2 is high in ExposureActive and ExposureAlternateActive mode |
Description of run-time parameters¶
out1_mode and out2_mode (Out1 / Projector and Out2)¶
The output modes for GPIO Out 1 and Out 2 can be set individually:
Lowsets the output permanently to LOW. This is the factory default.
Highsets the output permanently to HIGH.
ExposureActivesets the output to HIGH for the exposure time of every image.
ExposureAlternateActivesets the output to HIGH for the exposure time of every second image.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_iocontrol/parameters?<out1_mode|out2_mode>=<value>PUT http://<host>/api/v1/nodes/rc_iocontrol/parameters?<out1_mode|out2_mode>=<value>Fig. 42 shows which images are used for stereo matching and transmission via GigE Vision in
ExposureActivemode with a user-defined frame rate of 8 Hz.![]()
Fig. 42 Example of using the
ExposureActivemode for GPIO Out 1 with a user-defined frame rate of 8 Hz. The internal image acquisition is always 25 Hz. GPIO Out 1 is HIGH for the exposure time of every image. A disparity image is computed for camera images that are sent out via GigE Vision according to the user-defined frame rate.The mode
ExposureAlternateActiveis meant to be used when an external random dot projector is connected to the camera’s GPIO Out 1. When setting Out 1 toExposureAlternateActive, the stereo matching module only uses images with GPIO Out 1 being HIGH, i.e. projector is on. The maximum frame rate that is used for stereo matching is therefore half of the frame rate configured by the user. All modules which make use of the intensity image, like TagDetect and ItemPick, use the intensity images with GPIO Out 1 being LOW, i.e. projector is off. Fig. 43 shows an example.![]()
Fig. 43 Example of using the
ExposureAlternateActivemode for GPIO Out 1 with a user-defined frame rate of 8 Hz. The internal image acquisition is always 25 Hz. GPIO Out 1 is HIGH for the exposure time of every second image. A disparity image is computed for images where Out 1 is HIGH and that are sent out via GigE Vision according to the user-defined frame rate. InExposureAlternateActivemode, intensity images are always transmitted pairwise: one with GPIO Out 1 HIGH, for which a disparity image might be available, and one with GPIO Out 1 LOW.Note
In
ExposureAlternateActivemode, an intensity image with GPIO Out 1 being HIGH (i.e. with projection) is always 40 ms away from an intensity image with Out 1 being LOW (i.e. without projection), regardless of the user-defined frame rate. This needs to be considered when synchronizing disparity images and camera images without projection in this special mode.
The functionality can also be controlled by the DigitalIOControl parameters of the GenICam interface (Category: DigitalIOControl).
out1_ratio and out2_ratio (Out1 Ratio and Out2 Ratio)¶
The output ratios for GPIOs Out 1 and Out 2 determine how much of the image exposure time the corresponding output GPIO should be HIGH, when ExposureActive or ExposureAlternateActive are used. When the ratio is set to 1, the output will be HIGH for full amount of exposure time. In case a projector is connected to the GPIO out1, a lower out1_ratio leads to darker projections.
These parameters are only available in pipelines of type
stereo_ace.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_iocontrol/parameters?<out1_ratio|out2_ratio>=<value>PUT http://<host>/api/v1/nodes/rc_iocontrol/parameters?<out1_ratio|out2_ratio>=<value>
out1_inverted and out2_inverted (Invert Out1 and Invert Out2)¶
The
out1_invertedandout2_invertedparameters determine whether the corresponding outputs should be inverted.These parameters are only available in pipelines of type
stereo_ace.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_iocontrol/parameters?<out1_inverted|out2_inverted>=<value>PUT http://<host>/api/v1/nodes/rc_iocontrol/parameters?<out1_inverted|out2_inverted>=<value>
Services¶
Each service response contains a return_code,
which consists of a value plus an optional message.
A successful service returns with a return_code value of 0.
Negative return_code values indicate that the service failed.
Positive return_code values indicate that the service succeeded with additional information.
The IOControl module offers the following services.
get_io_values¶
Retrieves the current state of the camera’s general purpose inputs and outputs (GPIOs).
Details
This service can be called as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_iocontrol/services/get_io_valuesPUT http://<host>/api/v1/nodes/rc_iocontrol/services/get_io_valuesThis service has no arguments.The returned
timestampis the time of measurement.
input_maskandoutput_maskare bit masks defining which bits are used for input and output values, respectively.
valuesholds the values of the bits corresponding to input and output as given by theinput_maskandoutput_mask.
return_codeholds possible warnings or error codes and messages. Possiblereturn_codevalues are shown below.
Code Description 0 Success -2 Internal error -9 License for IOControl is not available The definition for the response with corresponding datatypes is:
{ "name": "get_io_values", "response": { "input_mask": "uint32", "inverter_mask": "uint32", "output_mask": "uint32", "ratio_mask": "uint32", "return_code": { "message": "string", "value": "int16" }, "timestamp": { "nsec": "int32", "sec": "int32" }, "values": "uint32" } }
reset_defaults¶
Restores and applies the default values for this module’s parameters (“factory reset”).
Details
This service can be called as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_iocontrol/services/reset_defaultsPUT http://<host>/api/v1/nodes/rc_iocontrol/services/reset_defaultsThis service has no arguments.The definition for the response with corresponding datatypes is:
{ "name": "reset_defaults", "response": { "return_code": { "message": "string", "value": "int16" } } }