Pipeline type orbbec

Note

The firmware version of the connected Orbbec camera must be at least 1.6.00, otherwise the Orbbec cannot be used.

Parameters

The camera module on a pipeline of type orbbec is called rc_camera and is represented by the Camera page in the desired pipeline in the Web GUI. The user can change the camera parameters there, or directly via the REST-API (REST-API interface).

Parameter overview

This module offers the following run-time parameters:

The rc_camera module’s run-time parameters on a pipeline of type orbbec
Name Type Min Max Default Description
exp_control string - - Auto Exposure control mode: [Manual, Auto]
exp_height int32 0 799 0 Height of auto exposure region. 0 for whole image.
exp_max float64 1.0 1999.0 665.0 Maximum exposure time in seconds in Auto exposure mode
exp_offset_x int32 0 1279 0 First column of auto exposure region
exp_offset_y int32 0 799 0 First row of auto exposure region
exp_value float64 1.0 1999.0 156.0 Exposure time in seconds in Manual exposure mode
exp_width int32 0 1279 0 Width of auto exposure region. 0 for whole image.
gain_value float64 0.0 128.0 16.0 Gain value in decibel if not in Auto exposure mode
gamma float64 100.0 500.0 300.0 Gamma factor
wb_auto bool false true true Switching white balance on and off
wb_value float64 2800.0 6500.0 4600.0 White balance value

These parameters are also available over the GenICam interface with slightly different names and partly with different units or data types (see GigE Vision 2.0/GenICam image interface).

Description of run-time parameters

Each run-time parameter is represented by a row on the Web GUI’s Camera page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI.

gamma (Gamma)

The gamma value determines the mapping of perceived light to the brightness of a pixel. Lower gamma values let dark image parts appear brighter.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?gamma=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?gamma=<value>

exp_control (Exposure Auto or Manual)

The exposure control mode can be set to Auto or Manual.

Auto: This is the default mode in which the exposure time and gain factor is chosen automatically to correctly expose the image. The last automatically determined exposure and gain values are set into exp_value and gain_value when switching auto-exposure off.

Manual: In the manual exposure mode the exposure time and gain are kept fixed independent of the resulting image brightness.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?exp_control=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?exp_control=<value>

exp_max (Max Exposure)

This value is the maximal exposure in auto-exposure mode in seconds. The actual exposure time is adjusted automatically so that the images are exposed correctly. If the maximum exposure is reached, but the images are still underexposed, the gain is stepwise increased to increase the image brightness. Limiting the exposure is useful for avoiding or reducing motion blur during fast movements. However, higher gain introduces noise into the image. The best trade-off depends on the application.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?exp_max=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?exp_max=<value>

exp_offset_x, exp_offset_y, exp_width, exp_height (Exposure Region)

These values define a rectangular region in the left rectified image for limiting the area used for computing the auto exposure. The exposure time and gain factor of both images are chosen to optimally expose the defined region. This can lead to over- or underexposure of image parts outside the defined region. If either the width or height is 0, then the whole left and right images are considered by the auto exposure function. This is the default.

The region is visualized in the Web GUI by a rectangle in the left rectified image. It can be defined using the sliders or by selecting it in the image after pressing the button Select Region in Image.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?<exp_offset_x|exp_offset_y|exp_width|exp_height>=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?<exp_offset_x|exp_offset_y|exp_width|exp_height>=<value>

exp_value (Exposure)

This value is the exposure in manual exposure mode. This exposure is kept constant even if the images are underexposed.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?exp_value=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?exp_value=<value>

gain_value (Gain)

This value is the gain factor that can be set in manual exposure mode. Higher gain factors reduce the required exposure time but introduce noise.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?gain_value=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?gain_value=<value>

wb_auto (White Balance Auto or Manual)

This value can be set to true for automatic white balancing or false for manually setting the white balance using wb_value.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?wb_auto=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?wb_auto=<value>

wb_value (White Balance Manual Value)

This value determines the white balance when wb_auto is false.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?<wb_ratio_blue|wb_ratio_red>=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?<wb_ratio_blue|wb_ratio_red>=<value>

Status values

The rc_camera module of an orbbec pipeline reports the following status values:

The rc_camera module’s status values
Name Description
baseline Internally assumed stereo baseline t in meters for disparity image computation
brightness Current brightness of the image as value between 0 and 1
color 0 for monochrome cameras, 1 for color cameras
exp Current exposure. This value is shown below the image preview in the Web GUI as Exposure.
focal Focal length factor normalized to an image width of 1
fps Current frame rate of the camera images in Hertz. This value is shown in the Web GUI below the image preview as FPS (Hz).
gain Current gain factor. This value is shown in the Web GUI below the image preview as Gain.
height Height of the camera image in pixels. This value is shown in the Web GUI below the image preview as the second part of Resolution (px).
last_capture_ok 1 if the last image capture was successful
last_timestamp_grabbed Timestamp of the last image acquired
test 0 for live images and 1 for test images
width Width of the camera image in pixels. This value is shown in the Web GUI below the image preview as the first part of Resolution (px).

Services

In a pipeline of type orbbec the rc_camera module offers the following services.

reset_defaults

Restores and applies the default values for this module’s parameters (“factory reset”).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/services/reset_defaults
PUT http://<host>/api/v1/nodes/rc_camera/services/reset_defaults
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "reset_defaults",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}