Pack

Introduction

The Pack module provides an out-of-the-box perception solution for robotic pick-and-place applications that need to place previously picked objects inside a packing volume, such as a box, bin or onto a pallet. Given the bounding box of the object to be placed and the grasp(s) that can be used to pick it up, Pack computes a pose at which the object can be placed, taking the current filling state of the packing volume into account. The place pose is chosen to be the lowest position that provides stable support for the object, thereby maximizing the residual space left after placing.

In addition, the module offers:

  • A dedicated page on the rc_cube Web GUI for easy setup, configuration, testing, and application tuning.
  • The definition of a region of interest to specify the relevant packing volume in the scene, or to restrict the search area for the load carrier (see RoiDB).
  • A load carrier detection functionality (see LoadCarrier), to place objects inside a detected load carrier only.
  • A configurable starting point to control where packing begins.
  • Support for static and robot-mounted cameras and optional integration with the Hand-eye calibration module, to provide place poses in the user-configured external reference frame.
  • 3D visualization of the packing volume and the computed place pose in the Web GUI.

Note

This module is pipeline specific. Changes to its settings or parameters only affect the respective camera pipeline and have no influence on other pipelines running on the rc_cube.

The module is an optional on-board module of the rc_cube and requires a separate Pack license to be purchased.

Computation of place poses

The Pack module offers a service for computing a place pose for an object, regardless of whether it has already been picked or is yet to be picked. The object to be placed is described by its bounding_box. Optionally, the object’s current pose and one or more grasps that can be used to pick it up can be given as well; this pose and these grasps can originate from another detection module, such as ItemPick and ItemPickAI or BoxPick. Alternatively, the grasps can be given relative to the center of the object’s bounding box.

The module discretizes the packing volume in x and y direction according to the run-time parameter resolution. Starting from the corner of the packing volume closest to the configured starting point, it searches for the lowest position at which the object, padded by the run-time parameter object_padding as a safety margin, fits without overlapping already placed objects or the load carrier. This maximizes the residual space left after placing, keeping as many packing options open as possible for the next object to be placed.

Optionally, further information can be given to the module in a place pose computation request:

  • The ID of the load carrier that defines the packing volume.
  • The ID of the 3D region of interest that defines the packing volume, if no load carrier is set, or that restricts the search area for the load carrier.

The place pose definition is complemented by the timestamp of the oldest image that was used to compute it.

Setting the starting point

The Pack module determines where to begin filling the packing volume based on the starting point. The module compares the configured starting point against the corners of the packing volume, defined by the configured load carrier or region of interest, and begins filling from whichever corner is closest to it.

The starting point can be set via the set_starting_point service or on the Pack page in the Web GUI, and is persistently stored. It can be set in the camera coordinate frame or in the external coordinate frame, in case a hand-eye calibration is available.

Setting the preferred orientation

When placing a box, each place pose has a 180° rotation ambiguity around the z axis. Among the given grasps, the Pack module selects the ones whose orientations for placing the object are closest to the preferred orientation, thus resolving the 180° placing ambiguity. The preferred orientation can be set via the set_preferred_orientation service or on the Pack page in the Web GUI. Grasps that deviate from it by more than the run-time parameter grasp_filter_orientation_threshold are discarded.

The preferred orientation can be set in the camera coordinate frame or in the external coordinate frame, in case a hand-eye calibration is available. If the preferred orientation is specified in the external coordinate frame and the sensor is robot mounted, the current robot pose has to be given to each place pose computation call.

If no preferred orientation is set, the orientation of the left camera (see Coordinate frames in the rc_visard manual) will be used as the preferred orientation.

Interaction with other modules

Internally, the Pack module depends on, and interacts with other on-board modules as listed below.

Note

All changes and configuration updates to these modules will affect the performance of the Pack module.

Camera and depth data

The Pack module makes internally use of the following data:

  • Disparity, error, and confidence images from the Stereo matching module (rc_stereomatching), in case a stereo camera is used
  • Disparity, error, and confidence images from the Blaze module (rc_blaze), in case a Basler blaze camera is used

All processed images are guaranteed to be captured after the module trigger time.

IO and Projector Control

In case the rc_cube is used in conjunction with an external random dot projector and the IO and Projector Control module (rc_iocontrol), it is recommended to connect the projector to GPIO Out 1 and set the stereo-camera module’s acquisition mode to SingleFrameOut1 (see Stereo matching parameters), so that on each image acquisition trigger an image with and without projector pattern is acquired.

Alternatively, the output mode for the GPIO output in use should be set to ExposureAlternateActive (see Description of run-time parameters).

In either case, the Auto Exposure Mode exp_auto_mode should be set to AdaptiveOut1 to optimize the exposure of both images.

Hand-eye calibration

In case the camera has been calibrated to a robot, the Pack module can automatically provide poses in the robot coordinate frame. For the Pack node’s Services, the frame of the output poses can be controlled with the pose_frame argument.

Two different pose_frame values can be chosen:

  1. Camera frame (camera). All poses provided by the module are in the camera frame, and no prior knowledge about the pose of the camera in the environment is required. This means that the configured regions of interest and load carriers move with the camera. It is the user’s responsibility to update the configured poses if the camera frame moves (e.g. with a robot-mounted camera).
  2. External frame (external). All poses provided by the module are in the external frame, configured by the user during the hand-eye calibration process. The module relies on the on-board Hand-eye calibration module to retrieve the sensor mounting (static or robot mounted) and the hand-eye transformation. If the mounting is static, no further information is needed. If the sensor is robot-mounted, the robot_pose is required to transform poses to and from the external frame.

Note

If no hand-eye calibration is available, all pose_frame values should be set to camera.

All pose_frame values that are not camera or external are rejected.

If the sensor is robot-mounted, the current robot_pose has to be provided depending on the value of pose_frame:

  • If pose_frame is set to external, providing the robot pose is obligatory.
  • In all other cases, providing the robot pose is optional.

LoadCarrier

The Pack module uses the load carrier detection functionality provided by the LoadCarrier module (rc_load_carrier), with the run-time parameters specified for this module, to determine the boundaries of the packing volume. However, only one load carrier will be used in case multiple matching load carriers could be found in the scene. In case multiple load carriers of the same type are visible, a 3D region of interest should be set to ensure that always the same load carrier is used for the Pack module.

Parameters

Pack is represented by the rc_pack node in the REST-API and are reached in the Web GUI in the desired pipeline under Modules ‣ Pack. The user can explore and configure the rc_pack module’s run-time parameters, e.g. for development and testing, using the Web GUI or the REST-API interface.

Parameter overview

This module offers the following run-time parameters:

Table 36 The rc_pack module’s run-time parameters
Name Type Min Max Default Description
drop_height float64 0.0 0.5 0.0 height above target place position (in z direction of packing volume) to release object
grasp_filter_orientation_-threshold float64 0.0 180.0 45.0 Maximum allowed orientation change between grasp and preferred orientation in degrees
object_padding float64 0.001 1.0 0.005 width in meters for padding the object dimensions in x and y direction as safety margin
resolution float64 0.001 0.1 0.005 resolution for discretizing the packing volume in x and y direction

Description of run-time parameters

Each run-time parameter is represented by a row on the Web GUI’s Pack page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI:

resolution (Resolution)

is the resolution used to discretize the packing volume in x and y direction when searching for a free placement position, in meters. The smaller this value, the finer the search grid, at the cost of additional computation time.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/parameters?resolution=<value>
PUT http://<host>/api/v1/nodes/rc_pack/parameters?resolution=<value>

object_padding (Object Padding)

is the width, in meters, used to pad the object’s bounding_box in x and y direction as a safety margin when checking whether it fits at a candidate placement position.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/parameters?object_padding=<value>
PUT http://<host>/api/v1/nodes/rc_pack/parameters?object_padding=<value>

drop_height (Drop Height)

defines the height, in meters, above the target place position, along the z axis of the packing volume, at which the gripper releases the object, e.g. to let it drop a short distance instead of being placed under full control all the way down to the surface. The place pose provided by the Pack module represents the recommended pose of the object at the moment of release.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/parameters?drop_height=<value>
PUT http://<host>/api/v1/nodes/rc_pack/parameters?drop_height=<value>

grasp_filter_orientation_threshold (Grasp Orientation Threshold)

is the maximum deviation of the TCP’s z axis at the grasp point from the z axis of the TCP’s preferred orientation (see preferred orientation) in degrees. Only grasp points which are within this threshold are returned. When set to zero, any deviations are valid.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/parameters?grasp_filter_orientation_threshold=<value>
PUT http://<host>/api/v1/nodes/rc_pack/parameters?grasp_filter_orientation_threshold=<value>

Status values

The rc_pack node reports the following status values:

Table 37 The rc_pack node’s status values
Name Description
data_acquisition_time Time in seconds required by the last active service to acquire images
last_return_code_message Return code message of the last detection
last_return_code_value Return code value of the last detection
last_timestamp_processed The timestamp of the last processed dataset
load_carrier_detection_time Processing time of the last load carrier detection in seconds
processing_time Processing time of the last detection (including load carrier detection) in seconds

Services

The user can explore and call the rc_pack node’s services, e.g. for development and testing, using the REST-API interface or the rc_cube Web GUI.

The Pack module offers the following services.

detect_place_pose

Triggers the computation of a place pose as described in Computation of place poses.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/services/detect_place_pose
PUT http://<host>/api/v1/nodes/rc_pack/services/detect_place_pose

Required arguments:

pose_frame: see Hand-eye calibration.

objects: the object to be placed, described by its bounding_box and, optionally, the pose at which it is positioned. Currently, only a single object is supported.

grasps: one or more grasps that were used, or can be used, to pick the object listed in objects, referenced via object_id. If no pose_frame is given, each grasp’s pose is interpreted relative to the center of the object’s bounding box. If a pose_frame is given, the object also requires a pose. This allows detection results from other modules, such as ItemPick and ItemPickAI or BoxPick, to be reused for Pack.

Potentially required arguments:

robot_pose: see Hand-eye calibration.

Optional arguments:

load_carrier_id: ID of the load carrier that defines the packing volume.

region_of_interest_id: ID of the 3D region of interest that defines the packing volume, if load_carrier_id is not set, or that restricts the area for detecting the load carrier.

At least one of load_carrier_id or region_of_interest_id must be provided.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "grasps": [
      {
        "gripper_id": "string",
        "id": "string",
        "object_id": "string",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "stroke_per_finger_approach_mm": "float64",
        "stroke_per_finger_grasp_mm": "float64",
        "tcp_id": "string"
      }
    ],
    "load_carrier_id": "string",
    "objects": [
      {
        "bounding_box": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "id": "string",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string"
      }
    ],
    "pose_frame": "string",
    "region_of_interest_id": "string"
  }
}

pose: the computed place pose.

grasps: the grasp(s) passed in the request that can be used to achieve the final placement.

load_carriers: the list containing the detected load carrier.

timestamp: timestamp of the image set the detection ran on.

return_code: holds possible warnings or error codes and messages.

The definition for the response with corresponding datatypes is:

{
  "name": "detect_place_pose",
  "response": {
    "grasps": [
      {
        "collision_checked": "bool",
        "gripper_id": "string",
        "id": "string",
        "object_id": "string",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "timestamp": {
          "nsec": "int32",
          "sec": "int32"
        }
      }
    ],
    "load_carriers": [
      {
        "height_open_side": "float64",
        "id": "string",
        "inner_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "outer_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "overfilled": "bool",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "rim_ledge": {
          "x": "float64",
          "y": "float64"
        },
        "rim_step_height": "float64",
        "rim_thickness": {
          "x": "float64",
          "y": "float64"
        },
        "type": "string"
      }
    ],
    "pose": {
      "orientation": {
        "w": "float64",
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "position": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    },
    "pose_frame": "string",
    "return_code": {
      "message": "string",
      "value": "int16"
    },
    "timestamp": {
      "nsec": "int32",
      "sec": "int32"
    }
  }
}

get_starting_point

Returns the starting point used to select the corner of the packing volume from which filling begins (see Setting the starting point).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/services/get_starting_point
PUT http://<host>/api/v1/nodes/rc_pack/services/get_starting_point
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "get_starting_point",
  "response": {
    "point": {
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string",
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

set_starting_point

Persistently stores the starting point used to select the corner of the packing volume from which filling begins (see Setting the starting point).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/services/set_starting_point
PUT http://<host>/api/v1/nodes/rc_pack/services/set_starting_point

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "point": {
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string"
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "set_starting_point",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

get_preferred_orientation

Returns the preferred orientation used when selecting the grasp for placing the object (see Setting the preferred orientation).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/services/get_preferred_orientation
PUT http://<host>/api/v1/nodes/rc_pack/services/get_preferred_orientation
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "get_preferred_orientation",
  "response": {
    "orientation": {
      "w": "float64",
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string",
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

set_preferred_orientation

Persistently stores the preferred orientation used when selecting the grasp for placing the object (see Setting the preferred orientation).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/services/set_preferred_orientation
PUT http://<host>/api/v1/nodes/rc_pack/services/set_preferred_orientation

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "orientation": {
      "w": "float64",
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string"
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "set_preferred_orientation",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

trigger_dump

Triggers dumping of the detection that corresponds to the given timestamp, or the latest detection, if no timestamp is given. The dumps are saved to the connected USB drive.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/services/trigger_dump
PUT http://<host>/api/v1/nodes/rc_pack/services/trigger_dump

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "comment": "string",
    "timestamp": {
      "nsec": "int32",
      "sec": "int32"
    }
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "trigger_dump",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

reset_defaults

Resets all parameters of the module to its default values, as listed in above table. Also resets the starting point and the preferred orientation.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_pack/services/reset_defaults
PUT http://<host>/api/v1/nodes/rc_pack/services/reset_defaults
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "reset_defaults",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

Return codes

Each service response contains a return_code, which consists of a value plus an optional message. A successful service returns with a return_code value of 0. Negative return_code values indicate that the service failed. Positive return_code values indicate that the service succeeded with additional information. The smaller value is selected in case a service has multiple return_code values, but all messages are appended in the return_code message.

The following table contains a list of common codes:

Table 38 Return codes of the Pack services
Code Description
0 Success
-1 An invalid argument was provided
-4 Data acquisition took longer than allowed
-11 Sensor not connected, not supported or not ready
-12 Resource busy, e.g. when trigger_dump is called too frequently
-200 Fatal internal error
100 The requested load carrier was not detected in the scene
115 No valid place pose was found within the packing volume
300 A valid robot_pose was provided as argument but it is not required
999 Additional hints for application development