Pipeline type zivid

Note

The firmware version of the connected zivid camera has to match the version required by the rc_cube, otherwise the zivid cannot be used. To update the zivid to the required firmware version, open the Web GUI, navigate to System ‣ Camera Pipelines and select the zivid pipeline. Then click on Update zivid firmware and wait for the update process to finish.

User-defined presets

The zivid camera comes with multiple pre-configured settings for capturing images, so-called presets. The 2D presets are tailored specifically for 2D image captures, focusing on settings like resolution, exposure time, brightness, and gain. They are optimized for applications requiring detailed color or monochrome images.

Users can also create own 2D presets using the Zivid Studio software (https://www.zivid.com/zivid-studio-software) and save them as .yml files. These preset files can be uploaded to the rc_cube on the Camera page of the Web GUI or using the REST-API as described in Presets API. User-defined presets can then be selected for image acquisition in the same way as the pre-defined presets via the preset_name run-time parameter. Also 3D presets including 2D settings can be uploaded and used as 2D preset. In this case, only the 2D settings will be applied.

Parameters

The camera module on a pipeline of type zivid is called rc_camera and is represented by the Camera page in the desired pipeline in the Web GUI. The user can change the camera parameters there, or directly via the REST-API (REST-API interface).

Parameter overview

This module offers the following run-time parameters:

The rc_camera module’s run-time parameters on a pipeline of type zivid
Name Type Min Max Default Description
acquisition_mode string - - Trigger Acquisition mode: [Continuous, Trigger]
fps float64 1.0 25.0 25.0 Frames per second in Hertz
preset_name string - - - Name of preset configuration

Description of run-time parameters

Each run-time parameter is represented by a row on the Web GUI’s Camera page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI.

acquisition_mode (Acquisition Mode)

This parameter determines the acquisition mode of the 2D camera images. In Continuous mode, the camera will acquire images at the specified frame rate fps. In Trigger mode, images are only acquired when the camera receives a software trigger signal, either by clicking on the Acquire button in the Web GUI, or by calling the rc_camera/acquisition_trigger service (see Services).

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_camera/services/parameters?acquisition_mode=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?acquisition_mode=<value>

fps (FPS (Hz))

This value is the camera’s frame rate (fps, frames per second), which determines the upper frequency at which camera images can be acquired.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?fps=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?fps=<value>

preset_name (Preset Name)

This parameter allows to select a preset for 2D image acquisition. The preset can be any of the zivid’s pre-configured presets which depend on the zivid model and are read from the connected device, or a user-defined preset that has been uploaded to the rc_cube (User-defined presets).

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?preset_name=<value>
PUT http://<host>/api/v1/nodes/rc_camera/parameters?preset_name=<value>

Status values

The rc_camera module of a zivid pipeline reports the following status values:

The rc_camera module’s status values
Name Description
baseline Internally assumed stereo baseline t in meters for disparity image computation
brightness Current brightness of the image as value between 0 and 1
color 0 for monochrome cameras, 1 for color cameras
exp Current exposure time in seconds. This value is shown below the image preview in the Web GUI as Exposure (ms).
focal Focal length factor normalized to an image width of 1
fps Current frame rate of the camera images in Hertz. This value is shown in the Web GUI below the image preview as FPS (Hz).
height Height of the camera image in pixels. This value is shown in the Web GUI below the image preview as the second part of Resolution (px).
last_capture_ok 1 if the last image capture was successful
last_timestamp_grabbed Timestamp of the last image acquired
test 0 for live images and 1 for test images
width Width of the camera image in pixels. This value is shown in the Web GUI below the image preview as the first part of Resolution (px).

Services

In a pipeline of type zivid the rc_camera module offers the following services.

acquisition_trigger

Triggers an image acquisition when acquisition_mode is set to Trigger.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_camera/services/acquisition_trigger
PUT http://<host>/api/v1/nodes/rc_camera/services/acquisition_trigger
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "acquisition_trigger",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

reset_defaults

Restores and applies the default values for this module’s parameters (“factory reset”).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/services/reset_defaults
PUT http://<host>/api/v1/nodes/rc_camera/services/reset_defaults
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "reset_defaults",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

Presets API

The 2D presets can be set, retrieved and deleted via the following REST-API endpoints.