Skip to content

marathon ACL#

marathon ACL is a two-channel Camera Link frame grabber supporting the Camera Link standard in version 2.0.

Two mini Camera Link connectors (SDR 26) are located directly on the slot bracket.

For connection to the computer, marathon ACL is plugged into a PCIe 2.x (Gen 2) x 4 slot of your computer.

marathon ACL

Available Documentation#

Frame Grabber Documentation#

Runtime Software and Environment#

Applet Documentation#

Tools#

Trigger Boards#

Application Notes#

SDK Documentation#

Wrappers#

Library-Specific Function References#

Log Message System#

SDK Examples#

GenTL Interface#

Third-Party Interfaces#