Skip to content

PLCamera.BslFlatFieldCorrectionModeEnum Class#

Sets the flat-field correction mode.

Applies to: boost V CoaXPress

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslFlatFieldCorrectionModeEnum

Constructors#

 NameDescription
Public methodPLCamera.BslFlatFieldCorrectionModeEnum Initializes a new instance of the PLCamera.BslFlatFieldCorrectionModeEnum class
 

Properties#

 NameDescription
Public propertyDSNUOnly

Only Dark Signal Non-Uniformity (DSNU) correction is performed.

Applies to: boost V CoaXPress

Public propertyName The full name of BslFlatFieldCorrectionMode (Overrides ParameterListEnum.Name.)
Public propertyOff

Flat-field correction is disabled.

Applies to: boost V CoaXPress

Public propertyOn

Flat-field correction is enabled. Dark signal non-uniformities (DSNU) and photo response non-uniformities (PRNU) will be corrected.

Applies to: boost V CoaXPress

 

Methods#

 NameDescription
Public methodToString The full name of BslFlatFieldCorrectionMode (Overrides Object.ToString()()()().)
 

PLCamera.BslFlatFieldCorrectionModeEnum.ToString Method#

The full name of BslFlatFieldCorrectionMode

Return Value#

Type: String
Returns the full name of BslFlatFieldCorrectionMode

PLCamera.BslFlatFieldCorrectionModeEnum Constructor#

Initializes a new instance of the PLCamera.BslFlatFieldCorrectionModeEnum class

PLCamera.BslFlatFieldCorrectionModeEnum.DSNUOnly Property#

Only Dark Signal Non-Uniformity (DSNU) correction is performed.

Applies to: boost V CoaXPress

PLCamera.BslFlatFieldCorrectionModeEnum.Name Property#

The full name of BslFlatFieldCorrectionMode

PLCamera.BslFlatFieldCorrectionModeEnum.Off Property#

Flat-field correction is disabled.

Applies to: boost V CoaXPress

PLCamera.BslFlatFieldCorrectionModeEnum.On Property#

Flat-field correction is enabled. Dark signal non-uniformities (DSNU) and photo response non-uniformities (PRNU) will be corrected.

Applies to: boost V CoaXPress