Skip to content

PLCamera.CxpLinkConfigurationEnum Class#

Sets the link configuration.

Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress and racer 2 CXP

Visibility: Beginner

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.CxpLinkConfigurationEnum

Constructors#

 NameDescription
Public methodPLCamera.CxpLinkConfigurationEnum Initializes a new instance of the PLCamera.CxpLinkConfigurationEnum class
 

Properties#

 NameDescription
Public propertyAuto

The link configuration is set to automatic discovery.

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyCXP10_X1

The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyCXP10_X2

The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

Public propertyCXP12_X1

The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps).

Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress and racer 2 CXP

Public propertyCXP12_X2

The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps).

Applies to: boost CoaXPress, boost V CoaXPress and racer 2 CXP

Public propertyCXP12_X4

The link configuration is set to 4 connections operating at CXP-12 speed (12.5 Gbps).

Applies to: boost V CoaXPress

Public propertyCXP2_X1

The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyCXP2_X2

The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

Public propertyCXP3_X1

The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyCXP3_X2

The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

Public propertyCXP5_X1

The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyCXP5_X2

The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

Public propertyCXP6_X1

The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

Public propertyCXP6_X2

The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps).

Applies to: boost CoaXPress, boost V CoaXPress and racer 2 CXP

Public propertyCXP6_X4

The link configuration is set to 4 connections operating at CXP-6 speed (6.25 Gbps).

Applies to: boost V CoaXPress

Public propertyName The full name of CxpLinkConfiguration (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of CxpLinkConfiguration (Overrides Object.ToString()()()().)
 

PLCamera.CxpLinkConfigurationEnum.ToString Method#

The full name of CxpLinkConfiguration

Return Value#

Type: String
Returns the full name of CxpLinkConfiguration

PLCamera.CxpLinkConfigurationEnum Constructor#

Initializes a new instance of the PLCamera.CxpLinkConfigurationEnum class

PLCamera.CxpLinkConfigurationEnum.Auto Property#

The link configuration is set to automatic discovery.

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP10_X1 Property#

The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP10_X2 Property#

The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP12_X1 Property#

The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps).

Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP12_X2 Property#

The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps).

Applies to: boost CoaXPress, boost V CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP12_X4 Property#

The link configuration is set to 4 connections operating at CXP-12 speed (12.5 Gbps).

Applies to: boost V CoaXPress

PLCamera.CxpLinkConfigurationEnum.CXP2_X1 Property#

The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP2_X2 Property#

The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP3_X1 Property#

The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP3_X2 Property#

The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP5_X1 Property#

The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP5_X2 Property#

The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps).

Applies to: boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP6_X1 Property#

The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps).

Applies to: ace 2 CXP, boost CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP6_X2 Property#

The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps).

Applies to: boost CoaXPress, boost V CoaXPress and racer 2 CXP

PLCamera.CxpLinkConfigurationEnum.CXP6_X4 Property#

The link configuration is set to 4 connections operating at CXP-6 speed (6.25 Gbps).

Applies to: boost V CoaXPress

PLCamera.CxpLinkConfigurationEnum.Name Property#

The full name of CxpLinkConfiguration