Generic Robot Interface¶
The Generic Robot Interface (GRI) is an integration layer that bridges the REST-API v2 and provides a standardized way to communicate with the software modules using simple TCP socket communication on port 7100. It can be activated via a separate license .
Overview¶
The GRI is used in two phases. In the configuration phase, the user creates jobs and stores them under unique numeric IDs. A job contains everything needed for one operation: the module and service to call, the arguments to use, and the data to return to the robot. Jobs, and optionally hand-eye calibration configurations, are prepared once and are defined via the Web GUI or the REST-API (see Job types).
At run time, the robot triggers these jobs by their ID over a TCP socket on port 7100, exchanging fixed-size binary messages (see GRI binary protocol specification). The GRI internally manages the REST-API communication and returns the selected pose results in a format that can be chosen specifically for the robot. A typical job trigger proceeds as follows:
- The robot sends a trigger action (
TRIGGER_JOB_SYNCorTRIGGER_JOB_ASYNC, see Actions) together with the job ID, optionally providing run-time values in the requestdatafields. - The GRI looks up the job and translates it into the corresponding REST-API call(s) to the selected module.
- The results of the module, such as grasp poses, are cached by the GRI, and the first pose is returned to the robot in the chosen pose format.
- The robot retrieves any further results one at a time with
GET_NEXT_POSEandGET_RELATED_POSE.
A job definition therefore serves as a reusable template that the robot triggers by its ID at run time. The following section describes how to define jobs; the binary protocol and the details of robot integration are described further below.
Job definition¶
Jobs are pre-configured tasks that can be triggered by the robot application. Each job has a unique ID and contains all the necessary information for a specific operation, e.g. computing grasps for bin picking or changing run-time parameters of a module. Once configured, the robot can execute these jobs using simple socket commands and, if applicable, receive the returned poses.
The jobs can be defined via the Web GUI or via the REST-API (see Job and HEC_config API).
Job types¶
The Generic Robot Interface supports three types of jobs, selected via the job_type field:
CALL_PIPELINE_SERVICE– call a service on a specific camera pipeline (e.g. to detect objects or compute grasps) and return pose data to the robot.CALL_GLOBAL_SERVICE– call a service that is not tied to a pipeline (e.g. database services for regions of interest, load carriers or grippers). Returns a pose only if explicitly configured to.SET_PIPELINE_PARAMETERS– set run-time parameters on a pipeline node. Returns no pose.
The fields selected_return, pose_path, additional_return and dynamic_args control which pose a job
returns and how the robot can influence the call. They are described in detail in
Returning poses and extra data and demonstrated on complete jobs in Worked examples.
Pipeline service job (CALL_PIPELINE_SERVICE)¶
This job calls a service on a specific camera pipeline, e.g. to detect objects or compute grasps, and returns pose data (e.g. grasp poses) to the robot.
| Field | Presence | Description |
|---|---|---|
job_type |
required | the job type CALL_PIPELINE_SERVICE |
name |
required | descriptive name to distinguish jobs |
pipeline |
required | the camera pipeline to use for the job (e.g. "0") |
node |
required | the REST-API name of the pipeline node (e.g. rc_itempick) |
service |
required | the REST-API name of the service to call (e.g. compute_grasps) |
args |
required | the REST-API JSON arguments passed to the service |
selected_return |
required | the REST-API response field holding the poses to return (e.g. grasps or matches); see Choosing the returned pose: selected_return and pose_path |
pose_path |
optional | the field inside the selected_return object that holds the pose (defaults to pose); see Choosing the returned pose: selected_return and pose_path |
additional_return |
optional | extra response fields to return in data_4 through data_10; see additional_return (module to robot) |
dynamic_args |
optional | fill args from the robot request fields data_1 through data_4; see dynamic_args (robot to module) |
A minimal pipeline service job definition is:
{
"args": {
"pose_frame": "external",
"suction_surface_length": 0.02,
"suction_surface_width": 0.02
},
"job_type": "CALL_PIPELINE_SERVICE",
"name": "Compute Grasps",
"node": "rc_itempick",
"pipeline": "0",
"selected_return": "grasps",
"service": "compute_grasps"
}
The available values for selected_return depend on the chosen node and can be e.g. grasps or matches.
Refer to the service definitions of the corresponding module for details about node, service, args and
selected_return.
Global service job (CALL_GLOBAL_SERVICE)¶
This job calls a service that is not tied to a specific pipeline, e.g. database services for setting or retrieving
regions of interest, load carriers or grippers. By default, global service jobs do not return any pose; they return a
pose only if selected_return (and, typically, pose_path) is configured.
| Field | Presence | Description |
|---|---|---|
job_type |
required | the job type CALL_GLOBAL_SERVICE |
name |
required | descriptive name to distinguish jobs |
node |
required | the REST-API name of the global node (e.g. rc_load_carrier_db) |
service |
required | the REST-API name of the service to call |
args |
required | the REST-API JSON arguments passed to the service |
selected_return |
optional | the REST-API response field holding the pose(s) to return (e.g. to retrieve gripper or TCP definitions); without it the job returns no pose; see Choosing the returned pose: selected_return and pose_path |
pose_path |
optional | the field inside the selected_return object that holds the pose (defaults to pose); see Choosing the returned pose: selected_return and pose_path |
additional_return |
optional | extra response fields to return in data_4 through data_10; see additional_return (module to robot) |
dynamic_args |
optional | fill args from the robot request fields data_1 through data_4; see dynamic_args (robot to module) |
The field pipeline must not be set for global service jobs.
A minimal global service job definition is:
{
"args": {
"region_of_interest_2d": {
"id": "2d_roi",
"width": 526,
"height": 501,
"offset_x": 558,
"offset_y": 307
}
},
"job_type": "CALL_GLOBAL_SERVICE",
"name": "Set 2D ROI",
"node": "rc_roi_db",
"service": "set_region_of_interest_2d"
}
Refer to the service definitions of the corresponding module for details about node, service and args.
Parameter setting job (SET_PIPELINE_PARAMETERS)¶
This job sets run-time parameters on a pipeline node, e.g. for adjusting camera or detection module settings. Parameter setting jobs do not return any pose.
| Field | Presence | Description |
|---|---|---|
job_type |
required | the job type SET_PIPELINE_PARAMETERS |
name |
required | descriptive name to distinguish jobs |
pipeline |
required | the camera pipeline to use for the job (e.g. "0") |
node |
required | the REST-API name of the pipeline node (e.g. rc_stereomatching) |
parameters |
required | the run-time parameters to set as key-value pairs |
A sample parameter setting job definition is:
{
"job_type": "SET_PIPELINE_PARAMETERS",
"name": "Set Stereo Parameters",
"node": "rc_stereomatching",
"parameters": {
"maxdepth": 2,
"quality": "High"
},
"pipeline": "0"
}
Refer to the run-time parameter definitions of the corresponding module for details about node and
parameters.
Returning poses and extra data¶
Each result that a job delivers carries one pose in the response’s pose fields (pos_x through rot_4). In
addition, Protocol V1 leaves several request and response fields unused, and the job configuration uses them to
exchange additional information between the robot and the REST-API:
selected_returnandpose_pathchoose which pose is returned.additional_returnreturns extra values from the REST-API response in the response fieldsdata_4throughdata_10(module to robot, see Response body definition).dynamic_argsinjects robot-provided values from the request fieldsdata_1throughdata_4into theargsof the REST-API call (robot to module, see Request body definition).mapstranslates between the integers the robot exchanges and the string values the REST-API uses.
All of these locate values inside the REST-API response or request through a json_path, which is explained
first.
Locating values with json_path¶
A json_path addresses a single value inside the REST-API response (or, for dynamic_args, inside the request
arguments). Two forms exist:
- Object-relative (no leading dot, e.g.
quality): resolved inside the primary or related object that is currently being returned byGET_NEXT_POSE/GET_RELATED_POSE. - Root-relative (leading dot, e.g.
.timestamp.sec): resolved from the root of the entire REST-API response, which is useful for global metadata or for a parent property.
To descend into a list, use bracket notation with a zero-based index, e.g. item_models[0].type.
The following annotated response shows how each form resolves, assuming the job returns grasps as primary objects
and items as related objects:
{
"timestamp": {
"sec": 1719900000
},
"grasps": [
{
"quality": 0.85,
"item_uuid": "abc-123"
}
],
"items": [
{
"uuid": "abc-123",
"bounding_box": { "x": 0.15 }
}
]
}
quality(object-relative,primaryscope) resolves to0.85.bounding_box.x(object-relative,relatedscope) resolves to0.15..timestamp.sec(root-relative) resolves to1719900000.
Note
Always use bracket notation (item_models[0]) to access a list element. Writing item_models.0 makes
the GRI search for a dictionary key literally named "0" instead of the first list element.
Because GET_NEXT_POSE and GET_RELATED_POSE return one object at a time, an object-relative json_path is
written for a single object: use quality, not grasps[0].quality.
Choosing the returned pose: selected_return and pose_path¶
selected_return names the response field holding the primary objects to iterate over, e.g. grasps,
matches, items or load_carriers. It can also index into a list nested deeper in the response using bracket
notation, for example to iterate over the TCPs of a specific gripper:
{
"selected_return": "grippers[0].tcps",
"pose_path": "pose_flange"
}
pose_path tells the GRI where, inside each selected object, to find the pose (an object with position and
orientation) to return to the robot. It follows the same path rules as json_path and defaults to pose,
which is why it is normally omitted: all built-in pipeline return types (grasps, matches, items,
load_carriers) expose their pose in a field named pose.
Set pose_path explicitly when the selected object has no pose field, or when it exposes more than one candidate
pose and a specific one has to be chosen. This is the case in the gripper example above, where each TCP has separate
pose_flange and pose_parent fields instead of a single pose. The same value is applied to both the primary
and the related object, so it only needs to differ from the default when the relevant field is not named pose. If
the resolved value is missing, or is not an object with both a position and an orientation, the job is rejected
as misconfigured (MISCONFIGURED_JOB).
additional_return (module to robot)¶
additional_return maps extra values from the REST-API response into the response fields data_4 through
data_10. Its mappings are grouped by the object they apply to:
primary: applied to the primary object returned byGET_NEXT_POSE(the object type named byselected_return, e.g.grasps).related: applied to the corresponding related object returned byGET_RELATED_POSE(see Primary and related objects).
Each mapping is an object with the following fields:
target_field: the response field to write to (data_4throughdata_10)json_path: where to read the value in the REST-API response (see Locating values with json_path)type: how to convert the value into theint32response field:int: written as-is (the default iftypeis omitted)float: multiplied by1,000,000(analogous to the pose scaling in Pose formats)bool:1or0map: translated to an integer via amapslookup table (see Mapping tables (maps))
If a json_path does not resolve to a value, that field is simply skipped (MISSING_ADDITIONAL_DATA warning, see
Error codes and semantics). A failed map lookup or type conversion instead aborts the whole response with an
error (UNMAPPED_VALUE_ERROR / TYPE_CONVERSION_ERROR).
dynamic_args (robot to module)¶
dynamic_args maps values from the robot request into the args of the REST-API service call, letting the robot
adjust detection arguments at trigger time without reconfiguring the job. It applies to CALL_PIPELINE_SERVICE and
CALL_GLOBAL_SERVICE jobs; SET_PIPELINE_PARAMETERS jobs do not use it. It is a list of entries, each with:
source_field: the request field to read from (data_1throughdata_4, see Request body definition)json_path: the target key path within the REST-APIargs(same path rules as Locating values with json_path)type: how to convert the value before injecting it:int: injected as-is (the default iftypeis omitted)float: divided by1,000,000bool: interpreted as1/0map: the integer sent by the robot is looked up in amapstable to inject the corresponding value
The values are applied on top of the static args when the job is triggered, so a json_path pointing at an
existing argument overwrites it. A failed map lookup or type conversion is rejected with an error
(UNMAPPED_VALUE_ERROR / TYPE_CONVERSION_ERROR, see Error codes and semantics).
Mapping tables (maps)¶
Some arguments and return values are strings (such as IDs) rather than numbers. maps translates between the
integers the robot exchanges and these string values on the GRI server. The same table is used in both directions –
dynamic_args looks up robot ID to value, additional_return looks up value to robot ID – so each table
must be a 1:1 (bijective) mapping. A dynamic_args or additional_return entry of type map selects the
table to use via a map field:
{
"dynamic_args": [
{ "source_field": "data_2", "json_path": "template_id", "type": "map", "map": "models" }
],
"maps": {
"models": {
"1": "part_A_large",
"2": "part_B_small"
}
}
}
If the robot sends data_2 = 2, the template ID "part_B_small" is injected into the REST-API call.
Worked examples¶
The following complete job definitions combine the options above. For each one, the configuration is shown first, followed by what the robot sends or receives at run time.
Example 1: pipeline service job with additional return¶
This ItemPick job returns grasp poses and, alongside each pose, extra information about the grasp (primary scope)
and about the item the grasp was computed for (related scope).
{
"name": "ItemPickAIJob",
"job_type": "CALL_PIPELINE_SERVICE",
"pipeline": "0",
"node": "rc_itempick",
"service": "compute_grasps",
"selected_return": "grasps",
"args": {
"collision_detection": {
"gripper_id": "MultiSuctionGripper",
"pre_grasp_offset": { "x": 0, "y": 0, "z": -0.1 }
},
"item_models": [ { "type": "BAG" } ],
"pose_frame": "external",
"region_of_interest_id": "ROI",
"suction_surface_length": 0.05,
"suction_surface_width": 0.05
},
"additional_return": {
"primary": [
{ "json_path": "quality", "target_field": "data_4", "type": "float" },
{ "json_path": "tcp_id", "target_field": "data_5", "type": "map", "map": "gripper_tcps" }
],
"related": [
{ "json_path": "bounding_box.x", "target_field": "data_6", "type": "float" },
{ "json_path": "bounding_box.y", "target_field": "data_7", "type": "float" },
{ "json_path": "bounding_box.z", "target_field": "data_8", "type": "float" }
]
},
"maps": {
"gripper_tcps": { "1": "TCP1", "2": "TCP2", "3": "TCP3" }
}
}
selected_returnisgrasps, so eachGET_NEXT_POSEreturns one grasp pose.additional_return.primaryreads two values from that grasp: itsqualityintodata_4(as a float) and itstcp_idintodata_5(translated to an integer through thegripper_tcpstable).additional_return.relatedreads the bounding box of the associated item intodata_6throughdata_8, available afterGET_RELATED_POSE.
At run time, for a grasp with quality = 0.85 and tcp_id = "TCP2" on an item with bounding box
(0.15, 0.10, 0.05) m:
GET_NEXT_POSEreturns the grasp pose,data_4 = 850000(0.85 x 1,000,000) anddata_5 = 2(the key mapped to"TCP2"ingripper_tcps).GET_RELATED_POSEreturns the item pose,data_6 = 150000,data_7 = 100000anddata_8 = 50000(each bounding-box dimension x1,000,000).
Example 2: global service job returning a pose¶
Global service jobs return no pose by default. This job sets selected_return and pose_path so that it returns
the TCP poses stored for a gripper in the gripper database.
{
"name": "GetMultiSuctionGripperTCPs",
"job_type": "CALL_GLOBAL_SERVICE",
"node": "rc_gripper_db",
"service": "get_grippers",
"selected_return": "grippers[0].tcps",
"pose_path": "pose_flange",
"args": {
"gripper_ids": [ "MultiSuctionGripper" ]
},
"additional_return": {
"primary": [
{ "json_path": "id", "target_field": "data_4", "type": "map", "map": "tcp_names" },
{ "json_path": ".grippers[0].flange_radius", "target_field": "data_5", "type": "float" }
]
},
"maps": {
"tcp_names": { "1": "TCP1", "2": "TCP2", "3": "TCP3" }
}
}
selected_returnuses index addressing,grippers[0].tcps, to iterate over the TCPs of the first returned gripper as the primary objects.pose_pathis set topose_flangebecause a TCP has no plainposefield but separatepose_flangeandpose_parentposes;pose_flangeis the one returned.additional_return.primarymixes both path forms: the object-relativeid(the current TCP’s ID, mapped to an integer viatcp_names) and the root-relative.grippers[0].flange_radius(a property of the parent gripper, the same for every TCP).
At run time, for a TCP with id = "TCP1" on a gripper with flange_radius = 0.04 m, GET_NEXT_POSE returns the
TCP’s pose_flange, data_4 = 1 ("TCP1" via tcp_names) and data_5 = 40000 (0.04 x 1,000,000).
Example 3: pipeline service job with dynamic arguments¶
This BoxPick job lets the robot choose the rectangle dimensions to detect at trigger time, so the same job can pick
different box sizes without being reconfigured. The four dimensions of the RECTANGLE item model are filled from the
request fields data_1 through data_4.
{
"name": "BoxPickDynamicRectangle",
"job_type": "CALL_PIPELINE_SERVICE",
"pipeline": "0",
"node": "rc_boxpick",
"service": "compute_grasps",
"selected_return": "grasps",
"args": {
"pose_frame": "external",
"item_models": [
{
"type": "RECTANGLE",
"rectangle": {
"min_dimensions": { "x": 0.05, "y": 0.05 },
"max_dimensions": { "x": 0.10, "y": 0.10 }
}
}
],
"suction_surface_length": 0.05,
"suction_surface_width": 0.05
},
"dynamic_args": [
{ "source_field": "data_1", "json_path": "item_models[0].rectangle.min_dimensions.x", "type": "float" },
{ "source_field": "data_2", "json_path": "item_models[0].rectangle.min_dimensions.y", "type": "float" },
{ "source_field": "data_3", "json_path": "item_models[0].rectangle.max_dimensions.x", "type": "float" },
{ "source_field": "data_4", "json_path": "item_models[0].rectangle.max_dimensions.y", "type": "float" }
],
"additional_return": {
"primary": [
{ "json_path": "quality", "target_field": "data_4", "type": "float" }
]
}
}
dynamic_argsuses the samejson_pathgrammar asadditional_return, here indexing intoitem_models[0]to reach the rectangle dimensions insideargs.- The dimensions given in
argsare placeholders: the values injected from the request overwrite them when the job is triggered. - The request fields
data_1throughdata_4(filled bydynamic_args) and the response fieldsdata_4throughdata_10(filled byadditional_return) belong to separate messages, so reusingdata_4for both the sent minimum-x dimension and the returned graspqualityis not a conflict.
At run time, if the robot triggers the job with data_1 = 50000, data_2 = 50000, data_3 = 100000 and
data_4 = 100000, the GRI divides each value by 1,000,000 and calls rc_boxpick/compute_grasps with
min_dimensions (0.05, 0.05) m and max_dimensions (0.10, 0.10) m. Each subsequent GET_NEXT_POSE then
returns a grasp pose with data_4 set to that grasp’s quality x 1,000,000.
Execution modes¶
The Generic Robot Interface supports two execution modes to optimize the robot’s cycle time:
- Synchronous Execution: The robot triggers a job and waits for the first result to arrive. This mode should be chosen when results are required immediately.
- Asynchronous Execution: The robot starts a job and can continue with other operations while the job is running in the background. The job status can be queried and results can be retrieved when ready. This mode maximizes efficiency during long detection times.
Hand-Eye Calibration¶
A hand-eye calibration configuration can be defined for each camera pipeline to allow for programmatic hand-eye calibration using the GRI. Each hand-eye calibration configuration consists of the following information:
grid_height: height of the calibration grid in metersgrid_width: width of the calibration grid in metersrobot_mounted: boolean that determines whether the camera is mounted on the robottcp_offset: 0 for 6DOF robots. For 4DOF robots: the signed offset from the TCP to the camera coordinate system (robot-mounted sensor) or the visible surface of the calibration grid (statically mounted sensor) along the TCP rotation axis in meters.tcp_rotation_axis: -1 for 6DOF robots. For 4DOF robots: determines the axis of the robot frame around which the robot can rotate its TCP (0 is used for X, 1 for Y and 2 for the Z axis).
More detailed information about these settings and the hand-eye calibration in general is given in Hand-eye calibration.
The hand-eye calibration configurations can be set via the Web GUI or via the REST-API (see Job and HEC_config API).
GRI binary protocol specification¶
This specification defines the exact on-wire format for client-server messages. A message consists of a fixed 8-byte header and a body whose layout depends on the protocol version. Currently, there is only protocol version 1.
Note
All multi-byte integers are little-endian. Types are uint8 (8-bit unsigned), int16 (16-bit signed), int32 (32-bit signed).
Message header (8 bytes)¶
| Field | Type | Size | Description |
|---|---|---|---|
| magic_number | uint32 | 4 | ASCII tag “GRI0”, bytes 47 52 49 00 (little-endian) |
| protocol_version | uint8 | 1 | Protocol version: currently 1 |
| message_length | uint8 | 1 | Total message size (bytes), incl. header + body |
| pose_format | uint8 | 1 | Pose data format (see Pose formats) |
| action | uint8 | 1 | Command/action (see Actions) |
Pose formats¶
The GRI always uses millimeters for representing a position. The following tables show different rotation formats that can be chosen to match to the rotation representation of the used robot. The formats are grouped by non-Euler rotation formats, Tait-Bryan-Euler rotation formats (all three axes are used) and proper Euler rotation formats (first and last rotation axis are the same).
| Name | Value | rot_1 | rot_2 | rot_3 | rot_4 | Units | Robot Example |
|---|---|---|---|---|---|---|---|
| QUAT_WXYZ | 1 | w | x | y | z | – | ABB |
| QUAT_XYZW | 2 | x | y | z | w | – | Fruitcore HORST |
| AXIS_ANGLE_RAD | 3 | rx | ry | rz | – | rad | Universal Robots |
In the following notation primes indicate successive rotations in the intrinsic frame (e.g., Y’ = rotation about Y-axis after first rotation).
_B and _F determine the order in which the rotation components are given. F stands for forward, meaning that the rotation components are given
in the same order as the rotation is applied, and B stands for backward, meaning the rotation components are given in reverse order. _RAD and _DEG
determine whether the rotation components are given in radians or degrees, respectively, if applicable. So the format EULER_ZYX_B_DEG means
that the intrinsic rotation order is z-y’-x’’ (first rotate around the z axis, then rotate around the new y axis, then rotate around the
new x axis), the order in which the rotation components are given is backward (so the first rotation element is the angle around the x axis), and
the angels are given in degrees.
| Name | Value | rot_1 | rot_2 | rot_3 | rot_4 | Units | Robot Example |
|---|---|---|---|---|---|---|---|
| EULER_XYZ_F_DEG | 4 | X | Y’ | Z’’ | – | deg | |
| EULER_XYZ_F_RAD | 5 | X | Y’ | Z’’ | – | rad | |
| EULER_XYZ_B_DEG | 6 | Z’’ | Y’ | X | – | deg | |
| EULER_XYZ_B_RAD | 7 | Z’’ | Y’ | X | – | rad | |
| EULER_XZY_F_DEG | 8 | X | Z’ | Y’’ | – | deg | |
| EULER_XZY_F_RAD | 9 | X | Z’ | Y’’ | – | rad | |
| EULER_XZY_B_DEG | 10 | Y’’ | Z’ | X | – | deg | |
| EULER_XZY_B_RAD | 11 | Y’’ | Z’ | X | – | rad | |
| EULER_YXZ_F_DEG | 12 | Y | X’ | Z’’ | – | deg | |
| EULER_YXZ_F_RAD | 13 | Y | X’ | Z’’ | – | rad | |
| EULER_YXZ_B_DEG | 14 | Z’’ | X’ | Y | – | deg | |
| EULER_YXZ_B_RAD | 15 | Z’’ | X’ | Y | – | rad | |
| EULER_YZX_F_DEG | 16 | Y | Z’ | X’’ | – | deg | |
| EULER_YZX_F_RAD | 17 | Y | Z’ | X’’ | – | rad | |
| EULER_YZX_B_DEG | 18 | X’’ | Z’ | Y | – | deg | |
| EULER_YZX_B_RAD | 19 | X’’ | Z’ | Y | – | rad | |
| EULER_ZXY_F_DEG | 20 | Z | X’ | Y’’ | – | deg | |
| EULER_ZXY_F_RAD | 21 | Z | X’ | Y’’ | – | rad | |
| EULER_ZXY_B_DEG | 22 | Y’’ | X’ | Z | – | deg | |
| EULER_ZXY_B_RAD | 23 | Y’’ | X’ | Z | – | rad | |
| EULER_ZYX_F_DEG | 24 | Z | Y’ | X’’ | – | deg | KUKA |
| EULER_ZYX_F_RAD | 25 | Z | Y’ | X’’ | – | rad | |
| EULER_ZYX_B_DEG | 26 | X’’ | Y’ | Z | – | deg | FANUC, Mitsubishi, Yaskawa |
| EULER_ZYX_B_RAD | 27 | X’’ | Y’ | Z | – | rad |
| Name | Value | rot_1 | rot_2 | rot_3 | rot_4 | Units | Robot Example |
|---|---|---|---|---|---|---|---|
| EULER_XYX_F_DEG | 28 | X | Y’ | X’’ | – | deg | |
| EULER_XYX_F_RAD | 29 | X | Y’ | X’’ | – | rad | |
| EULER_XYX_B_DEG | 30 | X’’ | Y’ | X | – | deg | |
| EULER_XYX_B_RAD | 31 | X’’ | Y’ | X | – | rad | |
| EULER_XZX_F_DEG | 32 | X | Z’ | X’’ | – | deg | |
| EULER_XZX_F_RAD | 33 | X | Z’ | X’’ | – | rad | |
| EULER_XZX_B_DEG | 34 | X’’ | Z’ | X | – | deg | |
| EULER_XZX_B_RAD | 35 | X’’ | Z’ | X | – | rad | |
| EULER_YXY_F_DEG | 36 | Y | X’ | Y’’ | – | deg | |
| EULER_YXY_F_RAD | 37 | Y | X’ | Y’’ | – | rad | |
| EULER_YXY_B_DEG | 38 | Y’’ | X’ | Y | – | deg | |
| EULER_YXY_B_RAD | 39 | Y’’ | X’ | Y | – | rad | |
| EULER_YZY_F_DEG | 40 | Y | Z’ | Y’’ | – | deg | |
| EULER_YZY_F_RAD | 41 | Y | Z’ | Y’’ | – | rad | |
| EULER_YZY_B_DEG | 42 | Y’’ | Z’ | Y | – | deg | |
| EULER_YZY_B_RAD | 43 | Y’’ | Z’ | Y | – | rad | |
| EULER_ZXZ_F_DEG | 44 | Z | X’ | Z’’ | – | deg | |
| EULER_ZXZ_F_RAD | 45 | Z | X’ | Z’’ | – | rad | |
| EULER_ZXZ_B_DEG | 46 | Z’’ | X’ | Z | – | deg | |
| EULER_ZXZ_B_RAD | 47 | Z’’ | X’ | Z | – | rad | |
| EULER_ZYZ_F_DEG | 48 | Z | Y’ | Z’’ | – | deg | Kawasaki |
| EULER_ZYZ_F_RAD | 49 | Z | Y’ | Z’’ | – | rad | |
| EULER_ZYZ_B_DEG | 50 | Z’’ | Y’ | Z | – | deg | |
| EULER_ZYZ_B_RAD | 51 | Z’’ | Y’ | Z | – | rad |
All pose components (position and rotation) are int32 scaled by 1,000,000.
- Float to Int:
int = round(float * 1000000) - Int to Float:
float = int / 1000000.0 - Positions in millimeters before scaling
- Angles in degrees/radians (per format) before scaling
- Quaternions unitless, same scaling
rot_4unused for Euler/axis-angle (set to 0)
Actions¶
The following actions can be sent.
| Name | Value | Description |
|---|---|---|
| STATUS | 1 | Get system readiness; maps readiness to data_2 (1 or 0) |
| TRIGGER_JOB_SYNC | 2 | Execute job synchronously |
| TRIGGER_JOB_ASYNC | 3 | Start job asynchronously |
| GET_JOB_STATUS | 4 | Query async job status (see Job status) |
| GET_NEXT_POSE | 5 | Retrieve next available result |
| GET_RELATED_POSE | 6 | Retrieve next related pose |
| HEC_INIT | 7 | Initialize hand-eye calibration |
| HEC_SET_POSE | 8 | Provide/store calibration pose |
| HEC_CALIBRATE | 9 | Run calibration and save results |
STATUS (1)
Returns system readiness information fetched from the rc_visard in data_2 (1 if ready, 0 if not).
TRIGGER_JOB_SYNC (2)
Runs the job and returns the first result immediately; additional results are stored for later retrieval.
On success with results, error_code will be zero and the pose will be filled. If no results are returned, error_code
will be NO_POSES_FOUND (positive warning). It also reports:
data_1= node’sreturn_codevaluedata_2= number of remaining primary objects (see Primary and related objects)data_3= number of remaining related objects (see Primary and related objects)
TRIGGER_JOB_ASYNC (3)
Starts the job and returns immediately. The job’s status can be polled with GET_JOB_STATUS (4) (see Job status)
and the results can be fetched with GET_NEXT_POSE (5), as soon as the job is DONE.
GET_JOB_STATUS (4)
Returns the job status. It reports:
data_1= node’sreturn_codevaluedata_2= job status (see table Job status values)
Error details flow through error_code.
GET_NEXT_POSE (5)
Returns the next result of the primary object. It also reports:
data_1= node’sreturn_codevaluedata_2= number of remaining primary objects (see Primary and related objects)data_3= number of remaining related objects (see Primary and related objects)
When no more primary objects are available, it returns NO_POSES_FOUND and resets the job.
GET_RELATED_POSE (6)
Returns the next pose of the related object corresponding to the current primary object. It also reports:
data_1= node’sreturn_codevaluedata_2= number of remaining primary objects (see Primary and related objects)data_3= number of remaining related objects (see Primary and related objects)
If no related poses were found, it returns NO_RELATED_POSES.
HEC_INIT (7)
This action initializes the hand-eye calibration. It clears any existing calibration data,
applies the pipeline’s configuration parameters and prepares the system for recording new poses.
data_1 specifies the target pipeline.
HEC_SET_POSE (8)
This action is to be used eight times to record distinct robot poses with visible calibration pattern. The field data_2 is used to specify the
image storage slot (0-7). A previous pose in a slot will be overwritten if a slot is reused. Each pose must provide a different view
of the calibration pattern, as described in Hand-eye calibration. data_1 specifies the target pipeline.
HEC_CALIBRATE (9)
This action processes all recorded poses and calculates the transformation between camera and robot. It automatically saves successful calibration
results. data_1 specifies the target pipeline.
Job status¶
The following job status values can be returned.
| Name | Value |
|---|---|
| INACTIVE | 1 |
| RUNNING | 2 |
| DONE | 3 |
| FAILED | 4 |
Body definitions¶
There are different body definitions depending on whether it is a request that is sent or a response that is received. The request body consists of 54 bytes in total and its definition is given in table Request body definition.
| Field | Type | Size | Description |
|---|---|---|---|
| header | struct | 8 | Message header (see Message header (8 bytes)) |
| job_id | uint16 | 2 | Unique job ID from job configuration |
| pos_x | int32 | 4 | Position X (scaled by 10^6) |
| pos_y | int32 | 4 | Position Y (scaled by 10^6) |
| pos_z | int32 | 4 | Position Z (scaled by 10^6) |
| rot_1 | int32 | 4 | Rotation component 1 (scaled by 10^6) |
| rot_2 | int32 | 4 | Rotation component 2 (scaled by 10^6) |
| rot_3 | int32 | 4 | Rotation component 3 (scaled by 10^6) |
| rot_4 | int32 | 4 | Rotation component 4 (scaled by 10^6) |
| data_1 | int32 | 4 | Additional parameter 1 |
| data_2 | int32 | 4 | Additional parameter 2 |
| data_3 | int32 | 4 | Additional parameter 3 |
| data_4 | int32 | 4 | Additional parameter 4 |
The job ID is the unique identifier from the job configuration.
The usage of the fields data_1...data_4 depends on the action and job. They are set to 0 if unused.
For TRIGGER_JOB_SYNC/TRIGGER_JOB_ASYNC, these fields can be filled with robot-provided values via the job’s
dynamic_args configuration, see Returning poses and extra data.
The response body consists of 80 bytes in total. Its definition is given in table Response body definition.
| Field | Type | Size | Description |
|---|---|---|---|
| header | struct | 8 | Protocol header |
| job_id | uint16 | 2 | Processed job number |
| error_code | int16 | 2 | GRI result status (severity by sign) |
| pos_x | int32 | 4 | Position X (scaled by 10^6) |
| pos_y | int32 | 4 | Position Y (scaled by 10^6) |
| pos_z | int32 | 4 | Position Z (scaled by 10^6) |
| rot_1 | int32 | 4 | Rotation component 1 (scaled by 10^6) |
| rot_2 | int32 | 4 | Rotation component 2 (scaled by 10^6) |
| rot_3 | int32 | 4 | Rotation component 3 (scaled by 10^6) |
| rot_4 | int32 | 4 | Rotation component 4 (scaled by 10^6) |
| data_1 | int32 | 4 | Node’s return code (0 if none) |
| data_2 | int32 | 4 | Additional result 2 |
| data_3 | int32 | 4 | Additional result 3 |
| data_4 | int32 | 4 | Additional result 4 |
| data_5 | int32 | 4 | Additional result 5 |
| data_6 | int32 | 4 | Additional result 6 |
| data_7 | int32 | 4 | Additional result 7 |
| data_8 | int32 | 4 | Additional result 8 |
| data_9 | int32 | 4 | Additional result 9 |
| data_10 | int32 | 4 | Additional result 10 |
Note
For rc_measure, mean_z is mapped to pos_x/pos_y/pos_z.
The fields data_4 through data_10 are filled according to the job’s additional_return configuration, see
Returning poses and extra data.
Error codes and semantics¶
The error_code is int16 and encodes errors/warnings by sign:
- Negative < 0 = error (failure)
- Zero = 0 = success
- Positive > 0 = warning (success with caveat)
The tables below give the different error codes and are split by sign and sorted.
Success
| Name | Value | Description |
|---|---|---|
| NO_ERROR | 0 | Operation successful |
Negative error codes
| Name | Value | Description |
|---|---|---|
| UNKNOWN_ERROR | -1 | GRI internal, unspecified |
| INTERNAL_ERROR | -2 | GRI internal system error |
| API_NOT_REACHABLE | -3 | Cannot reach API |
| API_RESPONSE_ERROR | -4 | API returned a negative code |
| PIPELINE_NOT_AVAILABLE | -5 | Processing pipeline unavailable |
| INVALID_REQUEST_ERROR | -6 | Malformed request |
| INVALID_REQUEST_LENGTH | -7 | Wrong message length |
| INVALID_ACTION | -8 | Unsupported action |
| PROCESSING_TIMEOUT | -9 | Operation timed out |
| UNKNOWN_PROTOCOL_VERSION | -10 | Protocol version not supported |
| WRONG_PROTOCOL_FOR_JOB | -11 | Job does not match protocol version |
| JOB_DOES_NOT_EXIST | -12 | Invalid job ID |
| MISCONFIGURED_JOB | -13 | Invalid job configuration |
| HEC_CONFIG_ERROR | -14 | Invalid configuration parameters |
| HEC_INIT_ERROR | -15 | Calibration init failed |
| HEC_SET_POSE_ERROR | -16 | Failed to record pose in specified slot |
| HEC_CALIBRATE_ERROR | -17 | Unable to compute calibration from recorded poses |
| HEC_INSUFFICIENT_DETECTION | -18 | Calibration grid not visible or not detected |
| TYPE_CONVERSION_ERROR | -19 | Value not convertible to the configured type |
| UNMAPPED_VALUE_ERROR | -20 | Value has no entry in the referenced maps table |
Positive codes
| Name | Value | Description |
|---|---|---|
| NO_POSES_FOUND | 1 | No results available |
| NO_RELATED_POSES | 2 | No related data found |
| NO_RETURN_SPECIFIED | 3 | Job configured with no return type |
| JOB_STILL_RUNNING | 4 | Async job not complete |
| MISSING_ADDITIONAL_DATA | 5 | additional_return path not found |
Node return code semantics
The modules/nodes may return a return_code. This node return code is placed in the response data_1 field (defaults to 0 if no code).
The GRI’s primary status is in error_code (sign-based semantics).
Integration with a robot¶
The Generic Robot Interface offers communication on port 7100.
Different robot platforms can be supported by implementing a TCP socket client following the GRI binary protocol (see GRI binary protocol specification). This requires a robot controller with TCP/IP support and the ability to pack robot poses into binary messages and to parse binary messages into robot poses.
The implementation steps are as follows:
- Create TCP socket connection
- Compose request message:
- Set message header (8 bytes)
- Set job ID (2 bytes)
- Pack position (12 bytes, 3x int32)
- Pack rotation (16 bytes, 4x int32)
- Pack additional data (16 bytes, 4x int32)
- Send request (54 bytes total)
- Receive response (80 bytes total)
- Parse response:
- Message header (8 bytes)
- Job ID (2 bytes)
- Error code (2 bytes)
- Position (12 bytes, 3x int32)
- Rotation (16 bytes, 4x int32)
- Additional data (40 bytes, 10x int32)
Byte interpretation in socket communication¶
Some robot scripting languages interpret individual socket bytes as signed values in the range [-128, 127]
instead of unsigned [0, 255]. If this is the case, each byte has to be converted to unsigned before
reconstructing int32 values:
# Convert signed byte to unsigned
if byte_value < 0:
byte_value = byte_value + 256
After conversion, reconstruct the int32 using little-endian byte order, then apply signed interpretation to the
most significant byte (MSB) to determine if the overall int32 value is negative.
Note
All pose components use scaling as described in Pose formats.
Job and HEC_config API¶
The job definitions and the definitions of HEC_configs for hand-eye calibration can be set, retrieved and deleted via the following REST-API endpoints.
-
GET/generic_robot_interface/hec_configs¶ Get defined hand-eye calibration configurations
Template request
GET /api/v2/generic_robot_interface/hec_configs HTTP/1.1
Sample response
HTTP/1.1 200 OK Content-Type: application/json { "0": { "grid_height": 0.18, "grid_width": 0.26, "robot_mounted": true, "tcp_offset": 0, "tcp_rotation_axis": -1 } }
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
-
GET/generic_robot_interface/hec_configs/{pipeline}¶ Get hand-eye calibration configuration for the selected pipeline
Template request
GET /api/v2/generic_robot_interface/hec_configs/<pipeline> HTTP/1.1
Sample response
HTTP/1.1 200 OK Content-Type: application/json { "grid_height": 0.18, "grid_width": 0.26, "robot_mounted": true, "tcp_offset": 0, "tcp_rotation_axis": -1 }
Parameters: - pipeline (string) – pipeline of the hand-eye calibration configuration (required)
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
-
PUT/generic_robot_interface/hec_configs/{pipeline}¶ Sets a hand-eye calibration configuration for the selected pipeline.
Template request
PUT /api/v2/generic_robot_interface/hec_configs/<pipeline> HTTP/1.1 Accept: application/json application/ubjson {}
Sample response
HTTP/1.1 200 OK Content-Type: application/json { "return_code": { "message": "HEC configuration saved successfully", "value": 0 } }
Parameters: - pipeline (string) – pipeline of the hand-eye calibration configuration (required)
Request JSON Object: - hand-eye calibration configuration (object) – example args (required)
Request Headers: - Accept – application/json application/ubjson
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
-
DELETE/generic_robot_interface/hec_configs/{pipeline}¶ Remove a hand-eye calibration configuration.
Template request
DELETE /api/v2/generic_robot_interface/hec_configs/<pipeline> HTTP/1.1 Accept: application/json application/ubjson
Parameters: - pipeline (string) – pipeline of the hand-eye calibration configuration (required)
Request Headers: - Accept – application/json application/ubjson
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
- 403 Forbidden – forbidden, e.g. because there is no valid license for this module.
- 404 Not Found – hec config for the given pipeline not found
-
GET/generic_robot_interface/jobs¶ Get defined jobs
Template request
GET /api/v2/generic_robot_interface/jobs HTTP/1.1
Sample response
HTTP/1.1 200 OK Content-Type: application/json { "0": { "args": { "pose_frame": "external", "tags": [] }, "job_type": "CALL_PIPELINE_SERVICE", "name": "detect_qr_code", "node": "rc_qr_code_detect", "pipeline": "0", "selected_return": "tags", "service": "detect" }, "1": { "job_type": "SET_PARAMETERS_SERVICE", "name": "set_depth_full_quality", "node": "rc_stereomatching", "parameters": { "double_shot": true, "quality": "Full" }, "pipeline": "0" } }
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
-
GET/generic_robot_interface/jobs/{job_id}¶ Get selected job definition
Template request
GET /api/v2/generic_robot_interface/jobs/<job_id> HTTP/1.1
Sample response
HTTP/1.1 200 OK Content-Type: application/json { "args": { "pose_frame": "camera", "tags": [] }, "job_type": "CALL_PIPELINE_SERVICE", "name": "detect_qr_code", "node": "rc_qr_code_detect", "pipeline": "0", "selected_return": "tags", "service": "detect" }
Parameters: - job_id (string) – ID of the job (required)
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
-
PUT/generic_robot_interface/jobs/{job_id}¶ Sets a job definition for the selected job ID. The required keys depend on the chosen job_type.
Template request
PUT /api/v2/generic_robot_interface/jobs/<job_id> HTTP/1.1 Accept: application/json application/ubjson {}
Sample response
HTTP/1.1 200 OK Content-Type: application/json { "job_id": "1", "return_code": { "message": "Job configuration updated successfully", "value": 0 } }
Parameters: - job_id (string) – ID of the job (required)
Request JSON Object: - job definition (object) – example args (required)
Request Headers: - Accept – application/json application/ubjson
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
-
DELETE/generic_robot_interface/jobs/{job_id}¶ Remove a job definition.
Template request
DELETE /api/v2/generic_robot_interface/jobs/<job_id> HTTP/1.1 Accept: application/json application/ubjson
Parameters: - job_id (string) – ID of the job (required)
Request Headers: - Accept – application/json application/ubjson
Response Headers: - Content-Type – application/json application/ubjson
Status Codes: - 200 OK – successful operation
- 403 Forbidden – forbidden, e.g. because there is no valid license for this module.
- 404 Not Found – job with given id not found