Installation¶
Warning
The instructions on Safety related to the rc_visard must be read and understood prior to installation.
The rc_visard is a Docker-based software stacks that can be installed on machines meeting the prerequisites given in Prerequisites. This chapter provides detailed information about installing the rc_reason_stack software.
Offline installation guide¶
This section explains the manual installation of rc_reason_stack on a host system. Unlike the automated Docker-compose workflow, the Docker images are first copied to the host machine and then loaded into Docker manually. Follow the steps below to get the stack up and running, ready for your development or production environment.
All commands must be executed on the host machine (not inside a container).
Prerequisites¶
| Component | Minimum Version |
|---|---|
| Ubuntu | 22.04 LTS |
| NVIDIA GPU | Any RTX or Jetson Orin with minimum 8GB VRAM, or better [1] |
| Docker | 20.10+ |
| NVIDIA Driver | 535+ (the guide uses nvidia-driver-575-server) |
[1] Tested with Nvidia RTX A4000, RTX 4000 Ada, RTX 3080, RTX 4070, RTX 4080, NVIDIA Jetson Orin AGX
The following files are provided by Basler and needed for installation.
| File | Description |
|---|---|
| rc_container-xx.yy.zz.tar | rc_container docker image |
| tritonserver-xx.yy.tar | triton server docker image |
| docker-compose.yml | The docker compose file |
| docker-compose.json | The docker compose file in JSON format |
Replace xx.yy.zz with the desired rc_container and tritonserver versions.
Install Ubuntu 24.04¶
This section can be skipped if a working Ubuntu 24.04 installation is present.
For installing Ubuntu, follow the official Ubuntu installation guide under https://ubuntu.com/download/desktop or https://ubuntu.com/download/server.
Install NVIDIA driver¶
The NVIDIA driver is required for the host to expose the GPU to Docker containers.
After installing the driver, the GPU and its capabilities should be visible with nvidia-smi.
If the driver is not installed or not loaded correctly, nvidia-smi will either not be found or will report “No devices were found”.
# Update package lists
sudo apt update
# run nvidia-detector to find the correct driver
sudo nvidia-detector
# Install the latest NVIDIA driver (replace 570 with the version that matches your GPU)
sudo apt install -y nvidia-driver-570-server
# Reboot to load the driver
sudo reboot
After the reboot, verify that the driver is active:
$ nvidia-smi
+-----------------------------------------------------------------------------------------+
| NVIDIA-SMI 570.195.03 Driver Version: 570.195.03 CUDA Version: 12.8 |
|-----------------------------------------+------------------------+----------------------+
| GPU Name Persistence-M | Bus-Id Disp.A | Volatile Uncorr. ECC |
| Fan Temp Perf Pwr:Usage/Cap | Memory-Usage | GPU-Util Compute M. |
| | | MIG M. |
|=========================================+========================+======================|
| 0 NVIDIA RTX A4000 Off | 00000000:06:00.0 Off | Off |
| 41% 60C P0 37W / 140W | 10719MiB / 16376MiB | 9% Default |
| | | N/A |
+-----------------------------------------+------------------------+----------------------+
+-----------------------------------------------------------------------------------------+
| Processes: |
| GPU GI CI PID Type Process name GPU Memory |
| ID ID Usage |
|=========================================================================================|
|...
+-----------------------------------------------------------------------------------------+
The table shows:
- GPU: the device ID (0, 1, …)
- Name: the GPU model (e.g., GeForce RTX 3080)
- Driver Version: the installed NVIDIA driver
- CUDA Version: the CUDA toolkit that ships with the driver
- Memory-Usage: total RAM allocated to the GPU
- GPU-Util: current GPU utilization percentage
If this output is displayed, the driver is correctly installed and the GPU is ready to be used by the NVIDIA Container Toolkit and the containers.
Install Docker¶
# Update the apt package index and install packages to allow apt to use a repository over HTTPS
sudo apt-get update
sudo apt-get install \
ca-certificates \
curl \
gnupg \
lsb-release
# Add Docker’s official GPG key
curl -fsSL https://download.docker.com/linux/ubuntu/gpg | sudo gpg --dearmor -o /usr/share/keyrings/docker-archive-keyring.gpg
# Set up the stable repository
echo \
"deb [arch=$(dpkg --print-architecture) signed-by=/usr/share/keyrings/docker-archive-keyring.gpg] https://download.docker.com/linux/ubuntu \
$(lsb_release -cs) stable" | sudo tee /etc/apt/sources.list.d/docker.list > /dev/null
# Install Docker Engine
sudo apt-get update
sudo apt-get install -y docker-ce docker-ce-cli docker-compose-plugin containerd.io
# Verify Docker installation
sudo docker --version
Install NVIDIA Container Toolkit¶
The NVIDIA Container Toolkit gives Docker the ability to see, expose, and sandbox NVIDIA GPUs inside containers. Without it CUDA workloads cannot run in the container. The toolkit is the bridge between Docker’s container runtime and the NVIDIA driver stack on the host
# Add the NVIDIA GPG key
sudo curl -fsSL https://nvidia.github.io/libnvidia-container/gpgkey | \
sudo gpg --dearmor -o /usr/share/keyrings/nvidia-container-toolkit-keyring.gpg
# Add the NVIDIA Container Toolkit repository
sudo curl -s -L https://nvidia.github.io/libnvidia-container/stable/deb/nvidia-container-toolkit.list | \
sed 's#deb https://#deb [signed-by=/usr/share/keyrings/nvidia-container-toolkit-keyring.gpg] https://#g' | \
sudo tee /etc/apt/sources.list.d/nvidia-container-toolkit.list
# Update package lists and install
sudo apt update && sudo apt install -y nvidia-container-toolkit
# Restart Docker to apply changes
sudo systemctl restart docker
# Modify /etc/docker/daemon.json. This is necessary for older docker versions
sudo nvidia-ctk runtime configure --runtime=docker
# Verify that nvidia is now available as docker runtime
docker info | grep -i runtime
For fixing an issue that lets the GPU fail after some time in the container (can be seen when nvidia-smi in the container fails),
open the file /etc/nvidia-container-runtime/config.toml and set no-cgroups = false. After changing the configuration, start
docker with:
sudo systemctl restart docker
Test that Docker can access the GPU:
sudo docker run --rm --gpus all nvidia/cuda:12.1.1-base-ubuntu22.04 nvidia-smi
Limit docker log file size¶
By default docker uses the json-file logging driver with not limit on log sizes. We recommend to switch to the local logging driver (https://docs.docker.com/engine/logging/drivers/local/) which by default limits the max log size.
In /etc/docker/daemon.json add the following:
{
"log-driver": "local",
}
Install WIBU CodeMeter runtime¶
Install the CodeMeter runtime (https://www.wibu.com/de/support/anwendersoftware/anwendersoftware.html) on the host system.
After installing, stop the runtime:
sudo service codemeter stop
Switch network licensing on by setting IsNetworkServer to 1 in the file /etc/wibu/CodeMeter/Server.ini.
Start the runtime:
sudo service codemeter start
A firewall may be used to not expose the WIBU network license server in the external network (WIBU uses the ports 22350-22352), since the license server must only be visible to the docker container.
If the CodeMeter runtime cannot be installed on the host, the environment variable CM_REMOTE_SERVER can be set to the IP
or name of a remote server. Several servers can be separated by space. The default (i.e. empty) is to broadcast to
255.255.255.255, which usually only sees the CodeMeter instance on the host.
Create network interfaces¶
This example shows a network setup using a separate ethernet port (enp9s0) for sensor0 interface via macvlan.
Adjust the name of the ethernet port accordingly, in this example port enp9s0 will be used.
For multiple cameras (e.g. rc_viscore or multiple rc_visard devices) create a separate network for each camera.
Create /etc/netplan/40-sensor0.yaml with content
network:
version: 2
renderer: networkd
ethernets:
enp9s0:
dhcp4: false
dhcp6: false
addresses:
- 172.23.42.1/28
Alternative network configuration for multiple cameras can be created as follows. In this example the interfaces enp7s0 is used for an rc_visard and interfaces ens4f0 and ens4f1 are used for an rc_viscore.
network:
version: 2
renderer: networkd
ethernets:
enp7s0:
dhcp4: false
dhcp6: false
addresses:
- 172.23.42.1/28
ens4f0:
dhcp4: false
dhcp6: false
addresses:
- 172.23.43.1/28
ens4f1:
dhcp4: false
dhcp6: false
addresses:
- 172.23.44.1/28
Change permissions and apply with:
sudo chmod 600 /etc/netplan/40-sensor0.yaml
sudo netplan apply
Create docker network with macvlan driver:
sudo docker network create -d macvlan --subnet=172.23.42.0/28 --gateway=172.23.42.1 --ip-range=172.23.42.8/29 -o parent=enp9s0 sensor0
# or for multiple interfaces
sudo docker network create -d macvlan --subnet=172.23.42.0/28 --gateway=172.23.42.1 --ip-range=172.23.42.8/29 -o parent=enp7s0 sensor0
sudo docker network create -d macvlan --subnet=172.23.43.0/28 --gateway=172.23.43.1 --ip-range=172.23.43.8/29 -o parent=ens4f0 sensor1
sudo docker network create -d macvlan --subnet=172.23.44.0/28 --gateway=172.23.44.1 --ip-range=172.23.44.8/29 -o parent=ens4f1 sensor2
Verify in docker-compose.yml (or docker-compose.json):
# docker-compose.yml with multiple sensor interfaces
#... config truncated - for readability
networks:
back-tier:
driver: bridge
sensor0:
external: true
name: sensor0
#... config truncated - for readability
services:
rc-container:
#... config truncated - for readability
networks:
back-tier:
gw_priority: 100
sensor0:
interface_name: sensor0
#... config truncated - for readability
The docker-compose.yml for multiple interfaces is as follows.
# docker-compose.yml with multiple sensor interfaces
#... config truncated - for readability
networks:
back-tier:
driver: bridge
sensor0:
external: true
name: sensor0
sensor1:
external: true
name: sensor1
sensor2:
external: true
name: sensor2
#... config truncated - for readability
services:
rc-container:
#... config truncated - for readability
networks:
back-tier:
gw_priority: 100
sensor0:
interface_name: sensor0
sensor1:
interface_name: sensor1
sensor2:
interface_name: sensor2
#... config truncated - for readability
Ensure network settings for GigE Vision¶
GigE Vision cameras stream images with high bandwidth via UDP packages. Lost packages lead to image loss that
degrades the performance of the application. To avoid that, the Ethernet read buffers should be increased on the host.
For Ubuntu, create the file /etc/sysctl.d/10-gev-perf.conf with the following content:
# Increase readbuffer size for GigE Vision
net.core.rmem_max=33554432
Apply settings with:
sudo sysctl -p /etc/sysctl.d/10-gev-perf.conf
Load container images¶
# replace xx.yy.zz with the desired rc_container and tritonserver version
gunzip -c ./rc_container-xx.yy.zz.tar.gz | docker load
gunzip -c ./tritonserver-xx.yy.tar.gz | docker load
Start the Docker stack¶
The preferred method to start the docker-compose stack is
cd /path/to/rc_container/
# use docker-compose.yml
docker compose up -d --pull never
If the host system requires a docker-compose file in JSON format, use the following command.
cd /path/to/rc_container/
# use docker-compose.json
docker compose -f docker-compose.json up -d --pull never
Wait a few minutes for all containers to start. The status can be monitored with:
docker compose ps
Access the Web GUI¶
Once the stack is running, the Web GUI can be accessed via:
http://<host-ip>:8080/
Troubleshooting¶
| Symptom | Likely Cause | Fix |
|---|---|---|
| docker: error: driver nvidia does not support the requested device | NVIDIA driver / Docker integration mismatch | Re-run the NVIDIA Container Toolkit installation and reboot |
| Containers fail to start | Wrong network name | Ensure a Docker network named sensor0 exists |
| Web GUI not reachable | Containers not up | docker compose logs to inspect errors |
| Very low depth image frame rate | GPU does not work in container | Verify by running nvidia-smi on the host and inside the container and fix problems [2] |
[2] If nvidia-smi on the host fails, ensure that packages are consistent, because an unattended upgrade under
Ubuntu may upgrade the Nvidia driver, but not the Nvidia toolkit.
This can be fixed by running sudo apt update && sudo apt upgrade manually.
Unattended upgrades may be disabled. If nvidia-smi fails inside the container,
ensure that no-cgroups = false in /etc/nvidia-container-runtime/config.toml and
restart docker if the configuration had to be changed. This configuration file may
have been overwritten by an update of the Nvidia container toolkit.
Software license¶
The rc_visard ships with a USB dongle for licensing and protection of the installed software packages. The purchased software licenses are installed on and are bound to this dongle and its ID.
The functionality of the rc_visard can be enhanced anytime by upgrading the license, e.g., for optionally available software modules.
Note
The rc_visard requires to be restarted whenever the installed licenses have changed.
Note
The dongle ID and the license status can be retrieved via the rc_visard’s various interfaces such as the page of the Web GUI.
Note
For the software components to be properly licensed, the USB dongle must be plugged to the rc_visard before power up.
Note
The rc_visard requires to be restarted, whenever the license dongle is plugged to or unplugged from the device.
Connection of cameras¶
The rc_visard offers up to four software camera pipelines for processing data from the connected sensors. The configuration of the camera pipelines is explained in Camera pipelines.