ItemPick

Introduction

The ItemPick module provides an out-of-the-box perception solution for robotic pick-and-place applications. ItemPick targets the detection of flat surfaces on unknown objects for picking with a suction gripper.

In addition, the module offers:

  • A dedicated page on the rc_visard Web GUI for easy setup, configuration, testing, and application tuning.
  • The definition of regions of interest to select relevant volumes in the scene (see RoiDB).
  • A load carrier detection functionality for bin-picking applications (see LoadCarrier), to provide grasps for items inside a bin only.
  • The definition of compartments inside a load carrier to provide grasps for specific volumes of the bin only.
  • Support for static and robot-mounted cameras and optional integration with the Hand-eye calibration module, to provide grasps in the user-configured external reference frame.
  • A quality value associated to each suggested grasp and related to the flatness of the grasping surface.
  • Selection of a sorting strategy to sort the returned grasps.
  • 3D visualization of the detection results with grasp points and gripper animations in the Web GUI.

Note

In this chapter, cluster and surface are used as synonyms and identify a set of points (or pixels) with defined geometrical properties.

The module is an optional on-board module of the rc_visard and requires a separate ItemPick license to be purchased.

Computation of grasps

The ItemPick module offers a service for computing grasps for suction grippers. The gripper is defined by its suction surface length and width.

The ItemPick module identifies flat surfaces in the scene and supports flexible and/or deformable items. The type of these item_models is called UNKNOWN since they don’t need to have a standard geometrical shape. Optionally, the user can also specify the minimum and maximum size of the item.

Optionally, further information can be given to the modules in a grasp computation request:

  • The ID of the load carrier which contains the items to be grasped.
  • A compartment inside the load carrier where to compute grasps (see Load carrier compartments).
  • The ID of the 3D region of interest where to search for the load carriers if a load carrier is set. Otherwise, the ID of the 3D region of interest where to compute grasps.
  • Collision detection information: The ID of the gripper to enable collision checking and optionally a pre-grasp offset to define a pre-grasp position. Details on collision checking are given below in CollisionCheck.

A grasp provided by the ItemPick module represents the recommended pose of the TCP (Tool Center Point) of the suction gripper. The grasp type is always set to SUCTION.

For ItemPick with an UNKNOWN item model, the computed grasp pose is the center of the biggest ellipse that can be inscribed in each surface.

The grasp orientation is a right-handed coordinate system and is defined such that its z axis is normal to the surface pointing inside the object at the grasp position and its x axis is directed along the maximum elongation of the ellipse. Since the x axis can have two possible directions, the one that better fits to the preferred TCP orientation (see Setting the preferred orientation of the TCP) is selected. If the run-time parameter allow_any_grasp_z_rotation is set to true, the x axis will not be forced to be aligned with the maximum elongation of the graspable ellipse, but can have any rotation around the z axis. In this case, the returned grasp will have the orientation that best fits to the preferred TCP orientation and is collision free, if collision checking.

_images/itempick_grasp_surface.png

Fig. 33 Illustration of a suction grasp with coordinate system and ellipse representing the maximum suction surface

Each grasp includes the dimensions of the maximum suction surface available, modelled as an ellipse of axes max_suction_surface_length and max_suction_surface_width. The user is enabled to filter grasps by specifying the minimum suction surface required by the suction device in use. If the run-time parameter allow_any_grasp_z_rotation is set to true, max_suction_surface_length and max_suction_surface_width will be equal and correspond to the shortest axis of the largest graspable ellipse.

Each grasp also includes a quality value, which gives an indication of the flatness of the grasping surface. The quality value varies between 0 and 1, where higher numbers correspond to a flatter reconstructed surface.

The grasp definition is complemented by a uuid (Universally Unique Identifier) and the timestamp of the oldest image that was used to compute the grasp.

Grasp sorting is performed based on the selected sorting strategy. The following sorting strategies are available and can be set in the Web GUI or using the set_sorting_strategies service call:

  • gravity: highest grasp points along the gravity direction are returned first,
  • surface_area: grasp points with the largest surface area are returned first,
  • direction: grasp points with the shortest distance along a defined direction vector in a given pose_frame are returned first.
  • distance_to_point: grasp points with the shortest or farthest (if farthest_first is true) distance from a point in a given pose_frame are returned first.

If no sorting strategy is set or default sorting is chosen in the Web GUI, sorting is done based on a combination of gravity and surface_area.

Setting the preferred orientation of the TCP

The ItemPick module determines the reachability of grasp points based on the preferred orientation of the TCP. The preferred orientation can be set via the set_preferred_orientation service or on the ItemPick page in the Web GUI. The resulting direction of the TCP’s z axis is used to reject grasps which cannot be reached by the gripper. Furthermore, the preferred orientation is used to select one grasp of several possible symmetries that is best reachable for the robot.

The preferred orientation can be set in the camera coordinate frame or in the external coordinate frame, in case a hand-eye calibration is available. If the preferred orientation is specified in the external coordinate frame and the sensor is robot mounted, the current robot pose has to be given to each object detection call. If no preferred orientation is set, the orientation of the left camera (see Coordinate frames ) will be used as the preferred orientation of the TCP.

Interaction with other modules

Internally, the ItemPick module depends on, and interacts with other on-board modules as listed below.

Note

All changes and configuration updates to these modules will affect the performance of the ItemPick module.

Camera and depth data

The ItemPick module makes internally use of the following data:

All processed images are guaranteed to be captured after the module trigger time.

IO and Projector Control

In case the rc_visard is used in conjunction with an external random dot projector and the IO and Projector Control module (rc_iocontrol), it is recommended to connect the projector to GPIO Out 1 and set the stereo-camera module’s acquisition mode to SingleFrameOut1 (see Stereo matching parameters), so that on each image acquisition trigger an image with and without projector pattern is acquired.

Alternatively, the output mode for the GPIO output in use should be set to ExposureAlternateActive (see Description of run-time parameters).

In either case, the Auto Exposure Mode exp_auto_mode should be set to AdaptiveOut1 to optimize the exposure of both images.

Hand-eye calibration

In case the camera has been calibrated to a robot, the ItemPick module can automatically provide poses in the robot coordinate frame. For the ItemPick node’s Services, the frame of the output poses can be controlled with the pose_frame argument.

Two different pose_frame values can be chosen:

  1. Camera frame (camera). All poses provided by the modules are in the camera frame, and no prior knowledge about the pose of the camera in the environment is required. This means that the configured regions of interest and load carriers move with the camera. It is the user’s responsibility to update the configured poses if the camera frame moves (e.g. with a robot-mounted camera).
  2. External frame (external). All poses provided by the modules are in the external frame, configured by the user during the hand-eye calibration process. The module relies on the on-board Hand-eye calibration module to retrieve the sensor mounting (static or robot mounted) and the hand-eye transformation. If the mounting is static, no further information is needed. If the sensor is robot-mounted, the robot_pose is required to transform poses to and from the external frame.

Note

If no hand-eye calibration is available, all pose_frame values should be set to camera.

All pose_frame values that are not camera or external are rejected.

If the sensor is robot-mounted, the current robot_pose has to be provided depending on the value of pose_frame and the definition of the sorting direction or sorting point:

  • If pose_frame is set to external, providing the robot pose is obligatory.
  • If the sorting direction is defined in external, providing the robot pose is obligatory.
  • If the distance-to-point sorting strategy is defined in external, providing the robot pose is obligatory.
  • In all other cases, providing the robot pose is optional.

LoadCarrier

The ItemPick module uses the load carrier detection functionality provided by the LoadCarrier module (rc_load_carrier), with the run-time parameters specified for this module. However, only one load carrier will be returned and used in case multiple matching load carriers could be found in the scene. In case multiple load carriers of the same type are visible, a 3D region of interest should be set to ensure that always the same load carrier is used for the ItemPick module.

CollisionCheck

Collision checking can be easily enabled for grasp computation of the ItemPick module by passing the ID of the used gripper and optionally a pre-grasp offset to the compute_grasps service call. The gripper has to be defined in the GripperDB module (see Setting a gripper) and details about collision checking are given in Collision checking within other modules.

If collision checking is enabled, only grasps which are collision free will be returned. However, the visualization images on the ItemPick page of the Web GUI also show colliding grasp points as black ellipses.

The CollisionCheck module’s run-time parameters affect the collision detection as described in CollisionCheck Parameters.

Parameters

ItemPick is represented by the rc_itempick node in the REST-API and are reached in the Web GUI under Modules ‣ ItemPick. The user can explore and configure the rc_itempick module’s run-time parameters, e.g. for development and testing, using the Web GUI or the REST-API interface.

The user can explore and configure the rc_itempick module’s run-time parameters, e.g. for development and testing, using the Web GUI or the REST-API interface.

Parameter overview

This module offers the following run-time parameters:

Table 34 The rc_itempick module’s run-time parameters
Name Type Min Max Default Description
allow_any_grasp_z_-rotation bool false true false Whether the grasps are allowed to have arbitrary rotation instead being aligned with the major axis of the graspable ellipse
cluster_max_curvature float64 0.005 0.5 0.11 Maximum curvature allowed within one cluster. The smaller this value, the more clusters will be split apart.
cluster_max_dimension float64 0.05 2.0 0.3 Maximum allowed diameter for a cluster in meters. Clusters with a diameter larger than this value are not used for grasp computation.
clustering_discontinuity_-factor float64 0.1 5.0 1.0 Factor used to discriminate depth discontinuities within a patch. The smaller this value, the more clusters will be split apart.
clustering_max_surface_-rmse float64 0.0005 0.01 0.004 Maximum root-mean-square error (RMSE) in meters of points belonging to a surface
clustering_patch_size int32 3 10 4 Size in pixels of the square patches the depth map is subdivided into during the first clustering step
grasp_filter_orientation_-threshold float64 0.0 180.0 45.0 Maximum allowed orientation change between grasp and preferred orientation in degrees
max_grasps int32 1 20 5 Maximum number of provided grasps

Description of run-time parameters

Each run-time parameter is represented by a row on the Web GUI’s ItemPick page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI:

max_grasps (Maximum Grasps)

sets the maximum number of provided grasps.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/parameters/parameters?max_grasps=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?max_grasps=<value>

cluster_max_dimension (Cluster Maximum Dimension)

is the maximum allowed diameter for a cluster in meters. Clusters with a diameter larger than this value are not used for grasp computation.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/parameters/parameters?cluster_max_dimension=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?cluster_max_dimension=<value>

cluster_max_curvature (Cluster Maximum Curvature)

is the maximum curvature allowed within one cluster. The smaller this value, the more clusters will be split apart.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/parameters/parameters?cluster_max_curvature=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?cluster_max_curvature=<value>

clustering_patch_size (Patch Size)

is the size of the square patches the depth map is subdivided into during the first clustering step in pixels.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/parameters/parameters?clustering_patch_size=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?clustering_patch_size=<value>

clustering_discontinuity_factor (Discontinuity Factor)

is the factor used to discriminate depth discontinuities within a patch. The smaller this value, the more clusters will be split apart.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/parameters/parameters?clustering_discontinuity_factor=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?clustering_discontinuity_factor=<value>

clustering_max_surface_rmse (Maximum Surface RMSE)

is the maximum root-mean-square error (RMSE) in meters of points belonging to a surface.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/parameters/parameters?clustering_max_surface_rmse=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?clustering_max_surface_rmse=<value>

grasp_filter_orientation_threshold (Grasp Orientation Threshold)

is the maximum deviation of the TCP’s z axis at the grasp point from the z axis of the TCP’s preferred orientation in degrees. Only grasp points which are within this threshold are returned. When set to zero, any deviations are valid.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_itempick/parameters?grasp_filter_orientation_threshold=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?grasp_filter_orientation_threshold=<value>

allow_any_grasp_z_rotation (Allow Any Grasp Z Rotation)

If set to true, the returned grasps are no longer forced to have their x axes aligned with the maximum elongation of the graspable ellipse, but can have any rotation around the z axis. The returned max_suction_surface_length and max_suction_surface_width will be equal and correspond to the shortest diameter of the largest graspable ellipse. This parameter enables the robot to get more options for grasping objects, especially in scenes where collisions can occur. However, in case of UNKNOWN item models, since the grasp is no longer aligned with the graspable ellipse, the correct orientation for placing the object must be determined by other means.

Via the REST-API, this parameter can be set as follows.

PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_itempick/parameters?allow_any_grasp_z_rotation=<value>
PUT http://<host>/api/v1/nodes/rc_itempick/parameters?allow_any_grasp_z_rotation=<value>

Status values

The rc_itempick node reports the following status values:

Table 35 The rc_itempick node’s status values
Name Description
data_acquisition_time Time in seconds required by the last active service to acquire images
grasp_computation_time Processing time of the last grasp computation in seconds
last_timestamp_processed The timestamp of the last processed dataset
load_carrier_detection_time Processing time of the last load carrier detection in seconds
processing_time Processing time of the last detection (including load carrier detection) in seconds
state The current state of the rc_itempick node

The reported state can take one of the following values.

Table 36 Possible states of the ItemPick module
State name Description
IDLE The module is idle.
RUNNING The module is running and ready for load carrier detection and grasp computation.
FATAL A fatal error has occurred.

Services

The user can explore and call the rc_itempick node’s services, e.g. for development and testing, using the REST-API interface or the rc_visard Web GUI.

The ItemPick module offers the following services.

compute_grasps

Triggers the computation of grasping poses for a suction device as described in Computation of grasps.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/compute_grasps
PUT http://<host>/api/v1/nodes/rc_itempick/services/compute_grasps

Required arguments:

pose_frame: see Hand-eye calibration.

suction_surface_length: length of the suction device grasping surface.

suction_surface_width: width of the suction device grasping surface.

Potentially required arguments:

robot_pose: see Hand-eye calibration.

Optional arguments:

load_carrier_id: ID of the load carrier which contains the items to be grasped.

load_carrier_compartment: compartment inside the load carrier where to compute grasps (see Load carrier compartments).

region_of_interest_id: if load_carrier_id is set, ID of the 3D region of interest where to search for the load carriers. Otherwise, ID of the 3D region of interest where to compute grasps.

item_models: list of items to be detected. In case of ItemPick, currently only a single item model of type UNKNOWN with minimum and maximum dimensions is supported, with the minimum dimensions strictly smaller than the maximum dimensions.

collision_detection: see Collision checking within other modules.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "collision_detection": {
      "gripper_id": "string",
      "pre_grasp_offset": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    },
    "item_models": [
      {
        "type": "string",
        "unknown": {
          "max_dimensions": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "min_dimensions": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        }
      }
    ],
    "load_carrier_compartment": {
      "box": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose": {
        "orientation": {
          "w": "float64",
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "position": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        }
      }
    },
    "load_carrier_id": "string",
    "pose_frame": "string",
    "region_of_interest_id": "string",
    "robot_pose": {
      "orientation": {
        "w": "float64",
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "position": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      }
    },
    "suction_surface_length": "float64",
    "suction_surface_width": "float64"
  }
}

load_carriers: list of detected load carriers.

grasps: sorted list of suction grasps.

items: sorted list of items corresponding to the returned grasps. In case of ItemPick, this list is always empty.

timestamp: timestamp of the image set the detection ran on.

return_code: holds possible warnings or error codes and messages.

The definition for the response with corresponding datatypes is:

{
  "name": "compute_grasps",
  "response": {
    "grasps": [
      {
        "item_uuid": "string",
        "max_suction_surface_length": "float64",
        "max_suction_surface_width": "float64",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "quality": "float64",
        "timestamp": {
          "nsec": "int32",
          "sec": "int32"
        },
        "type": "string",
        "uuid": "string"
      }
    ],
    "items": [
      {
        "bounding_box": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "grasp_uuids": [
          "string"
        ],
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "template_id": "string",
        "timestamp": {
          "nsec": "int32",
          "sec": "int32"
        },
        "type": "string",
        "uuid": "string",
        "view_name": "string",
        "view_pose_set": "bool",
        "view_uuid": "string"
      }
    ],
    "load_carriers": [
      {
        "height_open_side": "float64",
        "id": "string",
        "inner_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "outer_dimensions": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "overfilled": "bool",
        "pose": {
          "orientation": {
            "w": "float64",
            "x": "float64",
            "y": "float64",
            "z": "float64"
          },
          "position": {
            "x": "float64",
            "y": "float64",
            "z": "float64"
          }
        },
        "pose_frame": "string",
        "rim_ledge": {
          "x": "float64",
          "y": "float64"
        },
        "rim_step_height": "float64",
        "rim_thickness": {
          "x": "float64",
          "y": "float64"
        },
        "type": "string"
      }
    ],
    "return_code": {
      "message": "string",
      "value": "int16"
    },
    "timestamp": {
      "nsec": "int32",
      "sec": "int32"
    }
  }
}

set_preferred_orientation

Persistently stores the preferred orientation of the TCP to compute the reachability of the grasps, which is used for filtering and the grasps returned by the compute_grasps service (see Setting the preferred orientation of the TCP).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/set_preferred_orientation
PUT http://<host>/api/v1/nodes/rc_itempick/services/set_preferred_orientation

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "orientation": {
      "w": "float64",
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string"
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "set_preferred_orientation",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

get_preferred_orientation

Returns the preferred orientation of the TCP to compute the reachability of the grasps, which is used for filtering the grasps returned by the compute_grasps service (see Setting the preferred orientation of the TCP).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/get_preferred_orientation
PUT http://<host>/api/v1/nodes/rc_itempick/services/get_preferred_orientation
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "get_preferred_orientation",
  "response": {
    "orientation": {
      "w": "float64",
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string",
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

set_sorting_strategies

Persistently stores the sorting strategy for sorting the grasps returned by the compute_grasps service (see Computation of grasps).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/set_sorting_strategies
PUT http://<host>/api/v1/nodes/rc_itempick/services/set_sorting_strategies

Only one strategy may have a weight greater than 0. If all weight values are set to 0, the module will use the default sorting strategy.

If the weight for direction is set, the vector must contain the direction vector and pose_frame must be either camera or external.

If the weight for distance_to_point is set, point must contain the sorting point and pose_frame must be either camera or external.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "direction": {
      "pose_frame": "string",
      "vector": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "weight": "float64"
    },
    "distance_to_point": {
      "farthest_first": "bool",
      "point": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose_frame": "string",
      "weight": "float64"
    },
    "gravity": {
      "weight": "float64"
    },
    "surface_area": {
      "weight": "float64"
    }
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "set_sorting_strategies",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

get_sorting_strategies

Returns the sorting strategy for sorting the grasps returned by the compute-grasps service (see Computation of grasps).

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/get_sorting_strategies
PUT http://<host>/api/v1/nodes/rc_itempick/services/get_sorting_strategies
This service has no arguments.

All weight values are 0 when the module uses the default sorting strategy.

The definition for the response with corresponding datatypes is:

{
  "name": "get_sorting_strategies",
  "response": {
    "direction": {
      "pose_frame": "string",
      "vector": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "weight": "float64"
    },
    "distance_to_point": {
      "farthest_first": "bool",
      "point": {
        "x": "float64",
        "y": "float64",
        "z": "float64"
      },
      "pose_frame": "string",
      "weight": "float64"
    },
    "gravity": {
      "weight": "float64"
    },
    "return_code": {
      "message": "string",
      "value": "int16"
    },
    "surface_area": {
      "weight": "float64"
    }
  }
}

start

Starts the module. If the command is accepted, the module moves to state RUNNING.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/start
PUT http://<host>/api/v1/nodes/rc_itempick/services/start
This service has no arguments.

The current_state value in the service response may differ from RUNNING if the state transition is still in process when the service returns.

The definition for the response with corresponding datatypes is:

{
  "name": "start",
  "response": {
    "accepted": "bool",
    "current_state": "string"
  }
}

stop

Stops the module. If the command is accepted, the module moves to state IDLE.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/stop
PUT http://<host>/api/v1/nodes/rc_itempick/services/stop
This service has no arguments.

The current_state value in the service response may differ from IDLE if the state transition is still in process when the service returns.

The definition for the response with corresponding datatypes is:

{
  "name": "stop",
  "response": {
    "accepted": "bool",
    "current_state": "string"
  }
}

reset_defaults

Resets all parameters of the module to its default values, as listed in above table. Also resets sorting strategies.

Details

This service can be called as follows.

PUT http://<host>/api/v2/pipelines/0/nodes/rc_itempick/services/reset_defaults
PUT http://<host>/api/v1/nodes/rc_itempick/services/reset_defaults
This service has no arguments.

The definition for the response with corresponding datatypes is:

{
  "name": "reset_defaults",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

Return codes

Each service response contains a return_code, which consists of a value plus an optional message. A successful service returns with a return_code value of 0. Negative return_code values indicate that the service failed. Positive return_code values indicate that the service succeeded with additional information. The smaller value is selected in case a service has multiple return_code values, but all messages are appended in the return_code message.

The following table contains a list of common codes:

Table 37 Return codes of the ItemPick services
Code Description
0 Success
-1 An invalid argument was provided
-3 An internal timeout occurred, e.g. during box detection if the given dimension range is too large
-4 Data acquisition took longer than allowed
-8 The template has been deleted during detection.
-10 New element could not be added as the maximum storage capacity of load carriers, regions of interest or template has been exceeded
-11 Sensor not connected, not supported or not ready
-200 Fatal internal error
-301 More than one item model provided to the compute_grasps service
10 The maximum storage capacity of load carriers, regions of interest or templates has been reached
11 An existent persistent model was overwritten by the call to set_load_carrier or set_region_of_interest
100 The requested load carriers were not detected in the scene
101 No valid surfaces or grasps were found in the scene
102 The detected load carrier is empty
103 All computed grasps are in collision with the load carrier
112 Rejected detections of one or more clusters, because min_cluster_coverage was not reached.
300 A valid robot_pose was provided as argument but it is not required
999 Additional hints for application development