PrimitiveDB

Introduction

The PrimitiveDB module (geometric primitive database module) allows the global definition of geometric primitives, which can then be used in detection modules. Currently, only planes are supported.

A plane can, for example, serve as reference plane for measuring the dimensions of detected items in BoxPick.

The PrimitiveDB module is a base module which is available on every rc_visard.

Table 66 Specifications of the PrimitiveDB module
Supported primitives plane
Max. number of planes 100
Planes used for Dimensioning of detected items
Supported reference frames camera, external

Plane

A plane is defined in Hesse normal form

\mathbf{n} \cdot \mathbf{x} + d = 0,

where \mathbf{n} is the normal of the plane (normal) and d is the signed distance of the plane from the origin of the reference frame (distance) in meters. All points \mathbf{x} that fulfill this equation lie on the plane. The normal is stored as a unit vector. If a normal with a different length is given, the normal and the distance are scaled accordingly, which describes the same plane.

In the REST-API, a plane is defined by the following values:

  • id: Unique name of the plane
  • normal: normal of the plane with the components x, y and z
  • distance: signed distance of the plane from the origin of the reference frame in meters
  • pose_frame: reference frame of the plane, either camera or external

The PrimitiveDB module only stores planes and does not estimate them. A plane can be estimated from the current sensor data with the compute_plane service of the Measure module (see Estimating planes) and then stored with set_plane.

The rc_visard can persistently store up to 100 different planes. The configuration of planes is normally performed offline, during the set up of the desired application. This can be done via the REST-API interface of the PrimitiveDB module, or in the rc_visard Web GUI on the page Planes under Database.

Note

The configured planes are persistent even over firmware updates and rollbacks.

Interaction with other modules

Internally, the PrimitiveDB module depends on, and interacts with other on-board modules as listed below.

Hand-eye calibration

In case the camera has been calibrated to a robot, a plane can be provided in the robot coordinate frame by setting the corresponding pose_frame argument.

Two different pose_frame values can be chosen:

  1. Camera frame (camera). The plane is provided in the camera frame, and no prior knowledge about the pose of the camera in the environment is required. This means that the configured planes move with the camera. It is the user’s responsibility to update the configured planes if the camera frame moves (e.g. with a robot-mounted camera).
  2. External frame (external). The plane is provided in the external frame, configured by the user during the hand-eye calibration process. The module relies on the on-board Hand-eye calibration module to retrieve the sensor mounting (static or robot mounted) and the hand-eye transformation.

The plane is not transformed when it is stored, i.e. it must already be given in the desired pose_frame.

Note

If no hand-eye calibration is available, all pose_frame values should be set to camera.

All pose_frame values that are not camera or external are rejected.

Services

The PrimitiveDB module is called rc_primitive_db in the REST-API and is represented in the Web GUI under Database ‣ Planes. The user can explore and call the PrimitiveDB module’s services, e.g. for development and testing, using the REST-API interface or the Web GUI.

The PrimitiveDB module offers the following services.

set_plane

Persistently stores a plane on the rc_visard. An existing plane with the same id is overwritten. All configured planes are persistent over firmware updates and rollbacks.

Details

This service can be called as follows.

PUT http://<host>/api/v2/nodes/rc_primitive_db/services/set_plane

Details for the definition of a plane are given in Plane.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "distance": "float64",
    "id": "string",
    "normal": {
      "x": "float64",
      "y": "float64",
      "z": "float64"
    },
    "pose_frame": "string"
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "set_plane",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

get_planes

Returns the configured planes with the requested plane_ids.

Details

This service can be called as follows.

PUT http://<host>/api/v2/nodes/rc_primitive_db/services/get_planes

If no plane_ids are provided, all configured planes are returned.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "plane_ids": [
      "string"
    ]
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "get_planes",
  "response": {
    "planes": [
      {
        "distance": "float64",
        "id": "string",
        "normal": {
          "x": "float64",
          "y": "float64",
          "z": "float64"
        },
        "pose_frame": "string"
      }
    ],
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

delete_planes

Deletes the configured planes with the requested plane_ids.

Details

This service can be called as follows.

PUT http://<host>/api/v2/nodes/rc_primitive_db/services/delete_planes

All planes to be deleted must be explicitly stated in plane_ids.

The definition for the request arguments with corresponding datatypes is:

{
  "args": {
    "plane_ids": [
      "string"
    ]
  }
}

The definition for the response with corresponding datatypes is:

{
  "name": "delete_planes",
  "response": {
    "return_code": {
      "message": "string",
      "value": "int16"
    }
  }
}

Return codes

Each service response contains a return_code, which consists of a value plus an optional message. A successful service returns with a return_code value of 0. Negative return_code values indicate that the service failed. Positive return_code values indicate that the service succeeded with additional information. The smaller value is selected in case a service has multiple return_code values, but all messages are appended in the return_code message.

The following table contains a list of common codes:

Table 67 Return codes of the PrimitiveDB module’s services
Code Description
0 Success
-1 An invalid argument was provided
-10 New element could not be added as the maximum storage capacity of planes has been exceeded
10 The maximum storage capacity of planes has been reached
11 An existing plane was overwritten by the call to set_plane