Revisions
This product may be modified without notice, when necessary, due to product improvements, modifications, or changes in specifications. If such modification is made, the manual will also be revised; see revision information.
Documentation Revision 26.01.3 Jan 27, 2026
Applicable to rc_visard firmware 26.01.x
Introduction¶
Indications in the manual
To prevent damage to the equipment and ensure the user’s safety, this manual indicates each precaution related to safety with Warning. Supplementary information is provided as a Note.
Warning
Warnings in this manual indicate procedures and actions that must be observed to avoid danger of injury to the operator/user, or damage to the equipment. Software-related warnings indicate procedures that must be observed to avoid malfunctions or unexpected behavior of the software.
Note
Notes are used in this manual to indicate supplementary relevant information.