Safety¶
Warning
The operator must have read and understood all of the instructions in this manual before handling the rc_visard product.
Note
The term “operator” refers to anyone responsible for any of the following tasks performed in conjunction with rc_visard:
- Installation
- Maintenance
- Inspection
- Calibration
- Programming
- Decommissioning
This manual explains the rc_visard’s various components and general operations regarding the product’s whole life-cycle, from installation through operation to decommissioning.
The drawings and photos in this documentation are representative examples; differences may exist between them and the delivered product.
General warnings¶
Note
Any use of the rc_visard in noncompliance with these warnings is inappropriate and may cause injury or damage as well as void the warranty.
Warning
- The rc_visard needs to be properly mounted before use.
- All cable sets need to be secured to the rc_visard and the mount.
- Cords must be at most 30 m long.
- An appropriate DC power source must supply power to the rc_visard.
- Each rc_visard must be connected to a separate power supply.
- The rc_visard’s housing must be grounded.
- The rc_visard’s and any related equipment’s safety guidelines must always be satisfied.
- The rc_visard does not fall under the purview of the machinery, low voltage, or medical directives.
Risk assessment and final application:
The rc_visard may be used on a robot. Robot, rc_visard, and any other equipment used in the final application must be evaluated with a risk assessment. The system integrator’s duty is to ensure respect for all local safety measures and regulations. Depending on the application, there may be risks that need additional protection/safety measures.
Intended use¶
The rc_visard is intended for data acquisition (e.g., images, egomotion and disparity images) in stationary and mobile robotic applications. The rc_visard is intended for installation on a robot, automated machinery, mobile platform, or stationary equipment. It can also be used for data acquisition in other applications.
Warning
The rc_visard is NOT intended for safety critical applications.
The GigE Vision® industry standard used by the rc_visard does not support authentication and encryption. All data from and to the device is transmitted without authentication and encryption and could be monitored or manipulated by a third party. It is the operator’s responsibility to connect the rc_visard only to a secured internal network.
Warning
The rc_visard must be connected to secured internal networks.
The rc_visard may be used only within the scope of its technical specification. Any other use of the product is deemed unintended use. Basler will not be liable for any damages resulting from any improper or unintended use.
Warning
Always comply with local and/or national laws, regulations and directives on automation safety and general machine safety.