Computing 3D data

The following sections describe how disparity, error and confidence images can be used to compute depth data and depth errors.

Computing depth images and point clouds

The following equations show how to compute an object point’s actual 3D coordinates P_x, P_y, P_z in the camera coordinate frame from the disparity image’s pixel coordinates p_{x}, p_{y} and the disparity value d in pixels:

()P_x&=\frac{p_x \cdot t}{d}\\
P_y&=\frac{p_y \cdot t}{d}\\
P_z&=\frac{f \cdot t}{d},

where f is the focal length after rectification in pixels and t is the stereo baseline in meters, which was determined during calibration. These values are also transferred over the GenICam interface (see Custom GenICam features of the rc_visard).

Note

The rc_visard’s camera coordinate frame is defined as shown in Coordinate frames.

Note

The rc_visard reports a focal length factor via its various interfaces. It relates to the image width for supporting different image resolutions. The focal length f in pixels can be easily obtained by multiplying the focal length factor by the image width in pixels.

Please note that the equations assume that the coordinate frame is centered in the principal point that is typically in the center of the image, and p_{x}, p_{y} refer to the middle of the pixel, i.e. by adding 0.5 to the integer pixel coordinates. The following figure shows the definition of the image coordinate frame.

_images/image_coordinates.png

The image coordinate frame’s origin is defined to be at the image center – w is the image width and h is the image height.

The same equations, but with the corresponding GenICam parameters are given in Image stream conversions.

The set of all object points computed from the disparity image gives the point cloud, which can be used for 3D modeling applications. The disparity image is converted into a depth image by replacing the disparity value in each pixel with the value of P_z.

Confidence and error images

For each disparity image, additionally an error image and a confidence image are provided, which give uncertainty measures for each disparity value. These images have the same resolution and the same frame rate as the disparity image. The error image contains the disparity error d_{eps} in pixels corresponding to the disparity value at the same image coordinates in the disparity image. The confidence image contains the corresponding confidence value c between 0 and 1. The confidence is defined as the probability of the true disparity value being within the interval of three times the error around the measured disparity d, i.e., [d-3d_{eps}, d+3d_{eps}]. Thus, the disparity image with error and confidence values can be used in applications requiring probabilistic inference. The confidence and error values corresponding to an invalid disparity measurement will be 0.

The disparity error d_{eps} (in pixels) can be converted to a depth error z_{eps} (in meters) using the focal length f (in pixels), the baseline t (in meters), and the disparity value d (in pixels) of the same pixel in the disparity image:

()z_{eps}=\frac{d_{eps}\cdot f\cdot t}{d^2}.

Combining these equations allows the depth error to be related to the depth:

z_{eps}=\frac{d_{eps}\cdot{P_z}^2}{f\cdot t}.

With the focal lengths and baselines of the different camera models and the typical combined calibration and stereo matching error d_{eps} of 0.25 pixels, the depth accuracy can be visualized as shown below.

_images/reconstruction_error.png