Zivid module¶
Note
The firmware version of the connected zivid camera has to match the version required by the rc_visard, otherwise the zivid cannot be used. To update the zivid to the required firmware version, open the Web GUI, navigate to and select the zivid pipeline. Then click on Update zivid firmware and wait for the update process to finish.
The zivid module is a base module which is available on every rc_visard
and provides disparity, confidence and error images of a connected zivid structured light camera.
It only runs in camera pipelines of type zivid.
User-defined presets¶
The zivid camera comes with multiple pre-configured settings for capturing images, so-called presets.
The 3D presets that come with the zivid camera include both 2D and 3D settings, enabling simultaneous capture of color images and depth data.
However, the 2D image settings are ignored and instead the 2D image is captured with the preset chosen
in rc_camera (see User-defined presets).
The 3D presets are categorized based on application needs, such as Consumer Goods, Manufacturing etc.
Users can also create own 3D presets using the Zivid Studio software (https://www.zivid.com/zivid-studio-software)
and save them as .yml files. These preset files can be uploaded to the rc_visard on the Depth Image page of the Web GUI
or using the REST-API as described in Presets API.
User-defined presets can then be selected for depth image acquisition in the same way as the pre-defined presets via the
preset_name run-time parameter. If the 2D preset included in the user-defined 3D preset should be used, then this preset
also has to be uploaded as 2D preset and selected as the camera preset name.
Parameters¶
The zivid module is called rc_zivid in the REST-API and it is represented by the
Depth Image page in the desired pipeline in the Web GUI,
when a zivid camera is connected and running in the corresponding pipeline.
The user can change the zivid parameters there, or use the REST-API
(REST-API interface).
Parameter overview¶
This module offers the following run-time parameters:
| Name | Type | Min | Max | Default | Description |
|---|---|---|---|---|---|
acquisition_mode |
string | - | - | SingleFrame | Acquisition mode: [Continuous, SingleFrame] |
maxdepth |
float64 | 0.3 | 100.0 | 100.0 | Maximum depth in meters |
mindepth |
float64 | 0.3 | 100.0 | 0.3 | Minimum depth in meters |
preset_name |
string | - | - | - | Name of preset configuration |
Description of run-time parameters¶
Each run-time parameter is represented by a row on the Web GUI’s Depth Image page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI.
acquisition_mode (Acquisition Mode)¶
This parameter determines the acquisition mode for 3D data. The acquisition mode can be set to
ContinuousorSingleFrame. The latter is the default, which acquires a depth image upon each click of the Acquire button or when calling therc_zivid/acquisition_triggerservice (see Services of the rc_zivid module). InContinuousmode, depth images are acquired continuously, when the 2D image acquisition mode is also set toContinuous. Otherwise, depth images are only acquired when a 2D images acquisition is triggered.Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_zivid/parameters/parameters?acquisition_mode=<value>PUT http://<host>/api/v1/nodes/rc_zivid/parameters?acquisition_mode=<value>
preset_name (Preset Name)¶
This parameter allows to select a preset for 3D image acquisition. The preset can be any of the zivid’s pre-configured presets which depend on the zivid model and are read from the connected device, or a user-defined preset that has been uploaded to the rc_visard (see User-defined presets).
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_zivid/parameters?preset_name=<value>PUT http://<host>/api/v1/nodes/rc_zivid/parameters?preset_name=<value>
Status values¶
The rc_zivid module reports the following status values:
| Name | Description |
|---|---|
fps |
Actual frame rate of the disparity, error, and confidence images. This value is shown in the Web GUI below the image preview as FPS (Hz). |
height |
Current height of the disparity, error, and confidence images in pixels. This value is shown in the Web GUI below the image preview as the second number of Resolution (px). |
last_capture_ok |
1 if the last image capture was successful |
last_timestamp_grabbed |
Timestamp of the last depth data acquired |
latency |
Time in seconds between image acquisition and publishing of disparity image. This value is shown in the Web GUI below the image preview as Latency (s). |
width |
Current width of the disparity, error, and confidence images in pixels. This value is shown in the Web GUI below the image preview as the first number of Resolution (px). |
Services of the rc_zivid module¶
The rc_zivid module offers the following services.
acquisition_trigger¶
Signals the module to acquire a depth image, if the parameter
acquisition_modeis set toSingleFrame.Details
An error is returned if the
acquisition_modeis set toContinuous.This service can be called as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_zivid/services/acquisition_triggerPUT http://<host>/api/v1/nodes/rc_zivid/services/acquisition_triggerThis service has no arguments.Possible return codes are shown below.
Possible return codes of the acquisition_triggerservice call.¶Code Description 0 Success -8 Triggering is only possible in SingleFrame acquisition mode 101 Trigger is ignored, because there is a trigger call pending 102 Trigger is ignored, because there are no subscribers The definition for the response with corresponding datatypes is:
{ "name": "acquisition_trigger", "response": { "return_code": { "message": "string", "value": "int16" } } }
reset_defaults¶
Restores and applies the default values for this module’s parameters (“factory reset”).
Details
This service can be called as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_zivid/services/reset_defaultsPUT http://<host>/api/v1/nodes/rc_zivid/services/reset_defaultsThis service has no arguments.The definition for the response with corresponding datatypes is:
{ "name": "reset_defaults", "response": { "return_code": { "message": "string", "value": "int16" } } }
Presets API¶
The 3D presets can be set, retrieved and deleted via the following REST-API endpoints.