Pipeline type zivid¶
Note
The firmware version of the connected zivid camera has to match the version required by the rc_visard, otherwise the zivid cannot be used. To update the zivid to the required firmware version, open the Web GUI, navigate to and select the zivid pipeline. Then click on Update zivid firmware and wait for the update process to finish.
User-defined presets¶
The zivid camera comes with multiple pre-configured settings for capturing images, so-called presets. The 2D presets are tailored specifically for 2D image captures, focusing on settings like resolution, exposure time, brightness, and gain. They are optimized for applications requiring detailed color or monochrome images.
Users can also create own 2D presets using the Zivid Studio software (https://www.zivid.com/zivid-studio-software)
and save them as .yml files. These preset files can be uploaded to the rc_visard on the Camera page of the Web GUI
or using the REST-API as described in Presets API.
User-defined presets can then be selected for image acquisition in the same way as the pre-defined presets via the
preset_name run-time parameter. Also 3D presets including 2D settings can be uploaded and used as 2D preset. In this case,
only the 2D settings will be applied.
Parameters¶
The camera module on a pipeline of type zivid is called rc_camera and is represented by the
Camera page in the desired pipeline in the Web GUI.
The user can change the camera parameters there, or directly via the REST-API
(REST-API interface).
Parameter overview¶
This module offers the following run-time parameters:
| Name | Type | Min | Max | Default | Description |
|---|---|---|---|---|---|
acquisition_mode |
string | - | - | Trigger | Acquisition mode: [Continuous, Trigger] |
fps |
float64 | 1.0 | 25.0 | 25.0 | Frames per second in Hertz |
preset_name |
string | - | - | - | Name of preset configuration |
Description of run-time parameters¶
Each run-time parameter is represented by a row on the Web GUI’s Camera page. The name in the Web GUI is given in brackets behind the parameter name and the parameters are listed in the order they appear in the Web GUI.
acquisition_mode (Acquisition Mode)¶
This parameter determines the acquisition mode of the 2D camera images. In
Continuousmode, the camera will acquire images at the specified frame ratefps. InTriggermode, images are only acquired when the camera receives a software trigger signal, either by clicking on the Acquire button in the Web GUI, or by calling therc_camera/acquisition_triggerservice (see Services).Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_camera/services/parameters?acquisition_mode=<value>PUT http://<host>/api/v1/nodes/rc_camera/parameters?acquisition_mode=<value>
fps (FPS (Hz))¶
This value is the camera’s frame rate (fps, frames per second), which determines the upper frequency at which camera images can be acquired.
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_camera/services/parameters?fps=<value>PUT http://<host>/api/v1/nodes/rc_camera/parameters?fps=<value>
preset_name (Preset Name)¶
This parameter allows to select a preset for 2D image acquisition. The preset can be any of the zivid’s pre-configured presets which depend on the zivid model and are read from the connected device, or a user-defined preset that has been uploaded to the rc_visard (User-defined presets).
Via the REST-API, this parameter can be set as follows.
PUT http://<host>/api/v2/pipelines/<0,1,2,3>/nodes/rc_camera/parameters?preset_name=<value>PUT http://<host>/api/v1/nodes/rc_camera/parameters?preset_name=<value>
Status values¶
The rc_camera module of a zivid pipeline reports the following status values:
| Name | Description |
|---|---|
baseline |
Internally assumed stereo baseline |
brightness |
Current brightness of the image as value between 0 and 1 |
color |
0 for monochrome cameras, 1 for color cameras |
exp |
Current exposure time in seconds. This value is shown below the image preview in the Web GUI as Exposure (ms). |
focal |
Focal length factor normalized to an image width of 1 |
fps |
Current frame rate of the camera images in Hertz. This value is shown in the Web GUI below the image preview as FPS (Hz). |
height |
Height of the camera image in pixels. This value is shown in the Web GUI below the image preview as the second part of Resolution (px). |
last_capture_ok |
1 if the last image capture was successful |
last_timestamp_grabbed |
Timestamp of the last image acquired |
test |
0 for live images and 1 for test images |
width |
Width of the camera image in pixels. This value is shown in the Web GUI below the image preview as the first part of Resolution (px). |
Services¶
In a pipeline of type zivid the rc_camera module offers the following services.
acquisition_trigger¶
Triggers an image acquisition when
acquisition_modeis set toTrigger.Details
This service can be called as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_camera/services/acquisition_triggerPUT http://<host>/api/v1/nodes/rc_camera/services/acquisition_triggerThis service has no arguments.The definition for the response with corresponding datatypes is:
{ "name": "acquisition_trigger", "response": { "return_code": { "message": "string", "value": "int16" } } }
reset_defaults¶
Restores and applies the default values for this module’s parameters (“factory reset”).
Details
This service can be called as follows.
PUT http://<host>/api/v2/pipelines/0/nodes/rc_camera/services/reset_defaultsPUT http://<host>/api/v1/nodes/rc_camera/services/reset_defaultsThis service has no arguments.The definition for the response with corresponding datatypes is:
{ "name": "reset_defaults", "response": { "return_code": { "message": "string", "value": "int16" } } }
Presets API¶
The 2D presets can be set, retrieved and deleted via the following REST-API endpoints.