Basler SLP Strobe Controller#
For new Basler Lights with intelligent light control (ILC), an external SLP Strobe Controller isn't required because the control functionality is already built into the light.
Basler SLP Strobe Controller Required or Not?#
The following table shows whether a Basler SLP Strobe Controller is required for your application.
| Light Type | Basler SLP Strobe Controller Required? |
|---|---|
| Legacy Basler Lights No Integrated Controller | Yes. Required to use the Light Control feature. |
| Third-party lights No Integrated Controller | Yes. Required to use the Light Control feature. |
| New Basler Lights With Integrated Controller | No. The control functionality is built into the light. |
Light Control Modes With SLP Strobe Controller#
When a legacy light or a third-party light is operated with an external controller (for example, the Basler SLP Strobe Controller), the available legacy light control modes are Current Control Mode and Voltage Control Mode.
The active mode is selected via the BslLightDeviceControlMode parameter by setting it to one of the following values:
BslLightDeviceControlMode_CurrentBslLightDeviceControlMode_Voltage12VBslLightDeviceControlMode_Voltage24V
When the legacy current control mode is selected, the output current can be configured using the BslLightDeviceControlMode_Current parameter.
Info
If you use the Basler SLP Strobe Controller:
Every time you're switching from current to voltage control mode or vice versa, there is a short initialization phase of the controller during which the connected light lights up. This can last for up to 15 s and is normal behavior.
SLP Strobe Controller Specifications#
General Specifications#
| Basler SLP Strobe Controller | |
|---|---|
| Lighting Modes | Continuous Strobe (incl. Overdrive mode) See Use of Light Control Modes. |
| Drive Method | Current-controlled See Use of Light Control Modes. |
| Number of Channels | 1 (daisy-chaining with up to 4 devices) |
| Output Current | Continuous: 0.05 A–2 A Overdrive mode: 10 A @ 200 μs pulse width |
| Output Voltage | 1.5–40 VDC |
| Max. Output Power | Continuous: 48 W Overdrive mode: 400 W |
| Pulse Width | 50 μs–100 ms (automatic strobe mode) 100 μs–100 ms (manual strobe mode) |
| Pulse Step Size | 10 μs |
| Max. Frequency | 200 Hz |
| Size (L x W x H) | 85 x 60 x 37.5 mm |
| Weight (typical) | 200 g |
| Connectors | 6-pin Lighting 6-pin Camera 12-pin Power & I/O |
| Applicable Cameras | ace U, ace L, ace 2, boost R, dart M |
| Conformity | CE (includes RoHS), EAC, FCC, KC Certificates for the Basler SLP Strobe Controller More information is available in the Compliance section of the Basler website. |
| Software | Basler pylon Software Suite (version 4.0 or higher) Available for Windows, Linux x86, Linux ARM, macOS, and Android |
| Accessories | SLP cables Basler Lights |
Mechanical Specifications#
Requirements#
Environmental Requirements#
Temperature and Humidity#
| Housing temperature during operation | 0–50 °C (32–122 °F) |
| Humidity during operation | 20–80 %, relative, non-condensing |
| Storage temperature | -20–80 °C (-4–176 °F) |
| Storage humidity | 20–80 %, relative, non-condensing |
Electrical Requirements#
Power must be supplied to the controller via the 12-pin terminal block connector labeled Power & I/O. For information about the connector pin assignments, see the circuit diagram for the corresponding camera in the Circuit Diagram (ace L/U) or the Circuit Diagram (ace 2 and boost R) section. For dart M camera modules, see the corresponding tables in the Connecting the Controller and the Camera section.
| Voltage Requirements | Max. Power Consumption |
|---|---|
| 24 VDC (± 5 %) @ 4 A | 100 W @ 24 VDC |
Info
The actual power consumption of the Basler SLP Strobe Controller depends largely on the light you're using. Therefore, Basler recommends powering the controller via a standard power supply unit or an appropriate 24 VDC connector in a control cabinet. This allows you to adapt the components to the power consumption actually required in your application.
NOTICE – The controller produces high-energy pulses which may damage the controller if there is no protection against short circuits.
- Connect the outputs correctly.
- When switched off, energy remains stored in the controller for about 15 seconds.
Cable Requirements#
Camera-to-Controller Cable#
Info
For ace U/L, ace 2, boost R, and dart M camera modules:
If you're using your own cables, they must be shielded, and the shield must be connected to the Hirose plug and the Camera GND pin of the controller. For optimum performance and ease-of-use, Basler recommends using the following cable with ace U/L, ace 2, and boost R camera models: Basler SLP Cable HRS 6p/TBL-L, P, 3m
Controller-to-Light Cable#
The maximum cable length is 3 m.
Trigger Cable#
The maximum cable length is 3 m.
Physical Interface#
Circuit Diagrams#
Info
The 24 VDC Out pin must only be used to supply power to a camera. Don't connect another controller to it as it may get damaged. The maximum current allowed through this pin is 500 mA. If you want to connect another controller, use the daisy-chain option shown in the diagrams below.
Basler ace L/U#
Basler ace 2 and boost R#
Basler dart M#
For a Basler dart M camera module, the pin assignment depends on whether the module is used with a dart M Interface Board or with a dart M GigE Switch. For information about the pin assignments, see the corresponding table in the Connecting the Controller and the Camera section.
Connectors and Status LEDs#
The recommended cable Basler SLP Cable HRS 6p/TBL-L, P, 3m already includes a connector. If you want to build your own solution, here is an example of a compatible connector: Würth, TBL 3611.
Device Status LED#
| LED State | Meaning |
|---|---|
| Off | The controller isn't connected to power. |
| Green | Static: The controller is connected to power and fully operational. Flashing: Indicates trigger action. Flashes with a frequency of 1 Hz. |
| Yellow | Static: Indicates an error state. Possible causes are a hardware error in the light unit or the controller not being able to supply the current specified by the BslLightDeviceMaxCurrent parameter. To find out what kind of error it is, check the BslLightDeviceLastError parameter. If it's the Insufficient Current error, try lowering the maximum current until the flashing stops.Flashing: Indicates trigger action. Flashes with a frequency of 1 Hz. |
| Red | Static: The controller detected a short circuit. For more information, see Troubleshooting. Flashing: Indicates trigger action. Flashes with a frequency of 1 Hz. |
Communication Status LED#
| LED State | Meaning |
|---|---|
| Off | The controller hasn't detected a heartbeat signal from the camera yet. |
| Green | Static: The controller has detected the heartbeat signal from the camera. Flashing: This indicates data transmission. |
| Red | Indicates a communication error. The LED lights up once in that case. |
Precautions#
WARNING – Electric Shock Hazard
Unapproved power supplies may cause electric shock. Serious injury or death may occur.
You must use power supplies that meet the Safety Extra Low Voltage (SELV) and Limited Power Source (LPS) requirements.
WARNING – Fire Hazard
Unapproved power supplies may cause fire and burns.
In case of electrical malfunction, you have to ensure that the current doesn't exceed the value admissible for the cable's diameter.
To avoid this, take the following measures:
- You must use power supplies that meet the Limited Power Source (LPS) requirements.
- Power supply cabling to the controller must be rated to at least 4 A.
- The DC power supply to the controller must be externally fused to 4 A using a slow-blow fuse (T4AH, 50V).
CAUTION – Burn Injury Hazard
The controller housing can reach temperatures above 65 °C during operation at maximum ratings. This is sufficient to cause burn injuries.
- Place the controller so that staff can't accidentally touch it.
- Ensure that there is free air circulation around the controller.
Installation#
The Basler SLP Controller is supplied with a DIN rail mounting kit. If you don't want to use the DIN rail, you can also mount the controller via the mounting holes at the base of the controller using two M3 screws. Note that the mounting screws should not protrude more than 5 mm beyond the surface to which the controller is to be attached. The controller's dimensions are shown in the diagram above.
Connecting the Controller and the Camera#
NOTICE – Leaving the power source turned on while setting up the controller or connecting/disconnecting any cables may lead to the controller malfunctioning.
Always turn the power source off, when setting up the controller or connecting/disconnecting any cables.
For Basler ace U/L, ace 2, and boost R camera models, refer to the corresponding circuit diagram above when connecting the devices.
For Basler dart M camera modules, refer to the corresponding table in the dart M Interface Board or the dart M GigE Switch section when connecting the devices.
- Connect the open end of the light cable using the Light + and Light - pins of the 6-pin Lighting connector.
- Connect the camera to the controller via the green 6-pin Camera connector. The I/O connector on the camera-side depends on the camera model.
- Connect the open end of your power supply cable using the 24 VDC Power and Power GND pins of the 12-pin Power & I/O connector.
Info
Pin Assignment Differs Between ace, ace 2/boost R and dart M
The Camera I/O 2 pin of the controller's Camera connector connects to an opto-coupled line in ace camera models. This means that you have to use the Opto GND pin of the Power & I/O connector.
- In ace 2 and boost R camera models, the pin connects to a GPIO line.
This means that you have to use the standard GND pin of the Power & I/O connector. - In dart M camera modules, the connection of the pins depends on whether the camera module is used with a dart M interface board or a dart M GigE switch. For information about the pin assignments, refer to the tables below.
For detailed information about using the controller, see the Light Control topic.
dart M Interface Board#
If the dart M GigE camera module is used with a dart M Interface Board, see the pin assignment in the following table.
| Pin | Camera Connector, Strobe Controller | Pin | dart M I/O Connector, dart M Interface Board |
|---|---|---|---|
| 1 | Camera GND | 1 | Ground for camera power and general purpose I/O (GPIO) lines |
| 2 | Opto GND | 9 | Ground for opto-coupled I/O line |
| 3 | Opto In | 10 | Opto-coupled input line |
| 4 | SLP Comm | 6 | General purpose I/O (GPIO) line |
| 5 | Camera I/O 2 | 8 | General purpose out (GPO) line |
| 6 | Camera power | 2 | 12–24 VDC camera power (if Interface Board dart M GigE RJ45 AUX is used) |
dart M Switches#
If the dart M GigE camera module is used with a dart M GigE Switch, the pin assignment depends on the type of switch you use (PoE+ or AUX). See the corresponding table below.
Info
You can only connect one dart M camera module to the Basler Strobe Controller via the dart M GigE switch, not more. This is valid for all dart M GigE switches (PoE+, AUX).
If you have more than one dart M camera module connected to the dart M GigE switch, you have to decide which camera module you want to connect to the Basler SLP Controller via the switch.
Switch dart M, GigE, PoE+ (2-port and 3-port Variants)#
NOTICE – Connecting the 5 V OUT of the switch to the camera power (24 V) of the SLP strobe controller may damage the switch.
Make sure that you don't connect the 5 V OUT of the Switch dart M, GigE, PoE+ to the camera power (24 V) of the Basler SLP Strobe Controller because this may damage the switch. The connection to the camera power (24 V) of the Basler SLP Strobe Controller is only possible for Basler ace, ace 2 and boost R cameras.
| Pin | Camera Connector, Strobe Controller | Pin | dart M I/O Connector, Switch dart M, GigE, PoE+ |
|---|---|---|---|
| 1 | Camera GND | 1 | Ground for I/O lines (optionally) |
| 2 | Opto GND | 3 | Ground for I/O lines |
| 3 | Opto In | 10 or 9 | General purpose input (GPI) line for Cam 1 or General purpose input (GPI) line for Cam 2 |
| 4 | SLP Comm | 6 or 5 | General purpose I/O (GPIO) line Cam 1 or General purpose I/O (GPIO) line Cam 2 |
| 5 | Camera I/O 2 | 8 or 7 | General purpose output (GPO) line for Cam 1 or General purpose output (GPO) line for Cam 2 |
| 6 | Camera power | - | See Notice above. |
Info
- Be aware that the signals of the dart M GigE switch are not opto-coupled (optically isolated).
- Pin 1 and pin 3 of the dart M GigE PoE+ switch are connected internally.
Switch dart M, GigE, AUX (2-port and 3-port Variants)#
| Pin | Camera Connector, Strobe Controller | Pin | dart M I/O Connector, Switch dart M, GigE, AUX |
|---|---|---|---|
| 1 | Camera GND | 1 | Ground for AUX voltage and for I/O lines (optionally) |
| 2 | Opto GND | 3 | Ground for I/O lines |
| 3 | Opto In | 10 or 9 | General purpose input (GPI) line for Cam 1 or General purpose input (GPI) line for Cam 2 |
| 4 | SLP Comm | 6 or 5 | General purpose I/O (GPIO) line Cam 1 or General purpose I/O (GPIO) line Cam 2 |
| 5 | Camera I/O 2 | 8 or 7 | General purpose output (GPO) line for Cam 1 or General purpose output (GPO) line for Cam 2 |
| 6 | Camera power | 2 and/or 4 | Externally applied AUX voltage. See Notice below. |
NOTICE – A third dart M camera module connected to the dart M 2.5 GigE switch, AUX, requires an additional power supply.
If you connect three dart M camera modules to a Switch dart M, 2.5GigE, AUX, a separate power supply for the third camera module is required as the maximum current of 0.5 A for the 24 V output of the Basler Strobe Controller will be exceeded. Make sure that you use a separate power source for the third camera module. See the Power Consumption For Different Use Cases section in the Switch dart M, 2.5GigE, 3 Port, AUX topic.
Info
- Be aware that the signals of the dart M GigE switch are not opto-coupled (optically isolated).
- Pin 1 and pin 3 as well as pin 2 and pin 4 of the dart M GigE switch are connected internally.
Troubleshooting#
Short Circuit#
If the device status LED indicates a short circuit, you need to power-cycle the controller. If you're using more than one controller, the other controllers need to be power-cycled as well even if they haven't experienced any faults.
Power-Cycling the Controller#
After power-cycling the controller, it can take up to five minutes for the controller to become available again. This is normal behavior.