Library Signal

The signal library includes operators for signal data processing such as trigger signals.

The following list summarizes all Operators of Library Signal

Operator Name Short Description available since
DelayToSignal

Delays the input signal. Delay is controlled by a input link.

Version 1.2
Downscale

Reduces the input frequency by an adjustable factor.

Version 1.2
EventToSignal

Generates a signal pulse for each input pixel with value 1.

Version 1.2
FrameEndToSignal

Generates a signal pulse when the end of the input image is detected.

Version 1.2
FrameStartToSignal

Generates a signal pulse when the start of an input image is detected.

Version 1.2
Generate

Generates a periodic signal with controllable period time.

Version 1.2
GetSignalStatus

Obtain the current value of a signal link.

Version 1.2
Gnd

Provides a signal with the constant value 0 (LOW).

Version 1.2
LimitSignalWidth

Limits the maximum pulse width of the input signal using a parameterizable maximum.

Version 1.2
LineEndToSignal

Generates a signal pulse when the end of a input image line is detected.

Version 1.2
LineStartToSignal

Generates a signal pulse when the start of an input image line is detected.

Version 1.2
PeriodToSignal

Generates a periodic signal. Period time controlled by input link.

Version 1.2
PixelToSignal

Converts an image data stream into a signal stream.

Version 1.2
Polarity

Controls the polarity of the signal (invert).

Version 1.2
PulseCounter

Counts every occurrence of a one (high) at signal input link I.

Version 1.2
RsFlipFlop

Implements a set-reset flip-flop.

Version 1.2
RxSignalLink

Receives signals from a TxSignalLink operator in the design.

Version 2.0
Select

Selects a signal source from N signal sources by parameter and forward selected signal to the output.

Version 1.2
SetSignalStatus

Set a signal link status by use of a parameter.

Version 1.2
ShaftEncoder

Analyzes shaft encoder signal traces and outputs encoder pulses as well as the direction.

Version 1.2
ShaftEncoderCompensate

Compensates the rewind of a shaft encoder.

Version 1.2
SignalDebounce

Suppresses fast changing signals at the input link with adjustable minimum time.

Version 1.2
SignalDelay

Delays the input signal. Delay is controlled by a parameter.

Version 1.2
SignalEdge

Generates a pulse of one design clock cycle, if a rising-, falling- or both- edges are detected at the input.

Version 1.2
SignalGate

Gates the image stream between I and O by use of a signal input.

Version 1.2
SignalToDelay

Measures and outputs the delay between two signals.

Version 1.2
SignalToPeriod

Measures and outputs the period time of the input signal.

Version 1.2
SignalToPixel

Converts the input signal stream into a 0D pixel stream.

Version 1.2
SignalToWidth

Measures and outputs the pulse width of the input signal.

Version 1.2
SignalWidth

Generates an output pulse with controllable with for rising edges at the input.

Version 1.2
SyncSignal

Synchronizes a number of input links to a master signal.

Version 1.2
TxSignalLink

Sends signals to any RxSignalLink operator in the design.

Version 2.0
Vcc

Provides a signal with the constant value 1 (HIGH).

Version 1.2
WidthToSignal

Defines the width of a pulse. Width is controlled by a input link.

Version 1.2

Table 49. Operators of Library Signal