Franka Pose Format¶
Franka robots use a transformation matrix to define a pose.
A transformation matrix combines a rotation matrix
and a translation vector
.
The pose given by Franka’s “Measure Pose” App consists of a translation
in millimeters and a rotation
in degrees. The rotation convention is
-
-
(i.e.
-
-
) and is
computed by
Conversion from transformation matrix to quaternion¶
The conversion from a rotation matrix (with ) to a quaternion
can be done as follows:
The operator returns -1 if the argument is negative.
Otherwise, 1 is returned. It is used to recover the sign for the square root.
The
function ensures that the argument of the square root
function is not negative, which can happen in practice due to round-off errors.
Conversion from Rotation-XYZ to quaternion¶
The conversion from the angles in degrees to a quaternion
can be done by
first converting all angles to radians
and then calculating the quaternion with
Conversion from quaternion and translation to transformation¶
The conversion from a quaternion and a translation vector
to a transformation matrix
can be done as follows:
where and
if
is a unit quaternion.
Conversion from quaternion to Rotation-XYZ¶
The conversion from a quaternion with
to the
angles in degrees can
be done as follows.
Pose representation in RaceCom messages and state machines¶
In RaceCom messages and in state machines a pose is usually defined as one-dimensional array of 16 float values, representing the transformation matrix in column-major order. The indices of the matrix entries below correspond to the array indices