Skip to content

Software#

You can operate the frame grabber using the Framegrabber SDK or the pylon Software Suite.

  • If you want to operate only Basler cameras with your frame grabber, use the pylon Software Suite.
  • If you want to operate Basler and/or other cameras with your frame grabber, use the Framegrabber SDK.

Info

In some use cases you need to install pylon and the Framegrabber SDK in parallel. In that case, read the instruction in the Installing pylon and the Framegrabber SDK in Parallel topic.

However, marathon frame grabbers can't be operated with pylon, and Interface Cards can't be operated with the Framegrabber SDK. Therefore, see in the matrix below which frame grabber can be operated with which software:

Frame Grabber Only Basler Cameras Basler and/or Other Cameras
imaFlex 2 Dual 100 Framegrabber SDK Currently not supported
imaFlex CXP-12 Quad/Penta Framegrabber SDK without limitations, or
pylon Software Suite with limitationsa
Framegrabber SDK
imaWorx CXP-12 Quad pylon Software Suite Framegrabber SDK
marathon CXP-6/Camera Link Framegrabber SDK Framegrabber SDK
CXP-12 Interface Card 1C/2C/4C pylon Software Suite Framegrabber SDK

  1. The pylon Software Suite works with the imaFlex platforms only with restrictions. If you want to use the imaFlex platform with pylon, contact your Local Sales/Field Application Engineer. ↩