Skip to content

Tcl Command Reference#

Case Sensitivity and Slashes

The following commands are case sensitive. Use forward slashes to indicate paths.

Info

The notation used below for describing the parameters of individual commands is based on the Wirth Syntax Notation (WSN) :

  • Parameter names in curly brackets denote that you can specify no value, one value, or multiple values for this parameter in the command line.
  • Parameter names in square brackets denote optional parameters.

Creating, Loading, and Saving Designs#

LoadDesign#

Command Syntax
LoadDesign FileName

Command for loading the design FileName. Specify in FileName the path to the file in your file system and the file name itself. Don't forget to state the file name extension (*.va or *.tcl). Use slashes for indicating the path to the design file.

Example: LoadDesign c:/VA_TCL/BaseAreaGray8.va

If there is already a design loaded: Close the currently loaded design via command CloseDesign before using command LoadDesign.

CreateDesign#

Command Syntax
CreateDesign Name Platform

Command for creating a new design with the name Name for a hardware platform Platform. For specifying the target platform of the design, you can either use

  • the VisualApplets library name for the platform (e.g., "iF-CXP12-Q"), or
  • the full name of the platform (e.g., "imaFlex CXP-12 Quad"). Don't forget to set the full name in quotes as required by Tcl syntax for arguments that contain spaces.

Using capitals in the names has no effect.

SaveDesign#

Command Syntax
SaveDesign FileName [SaveOption]

Command for saving a design under FileName. Specify in FileName the path to the file and the file name itself. Use slashes for indicating the path to the design file.

Don't forget to add the file name extension to the file name.

  • If you specify file extension ".va", your design is saved in the standard VisualApplets design format. All contents of the file are saved. Use the *.va file format as primary data format for your VisualApplets designs.
  • If you specify file extension ".tcl" in FileName, a Tcl script is exported. Some contents of the design can't be exported.

If you want to overwrite an existing file, set the optional parameter SaveOption to overwrite.

The following information is lost during export to Tcl script:

  • The local modifications you made in a user library element instance (to adapt the instance to the surrounding design) are lost. If you re-import a Tcl script into VisualApplets, the instance is inserted as a fresh copy of the user library element. The content of the instance in your design has not been saved in Tcl.
  • The text content of info boxes is kept in Tcl format. However, the formatting of info boxes is lost.

ChangePlatform#

Command Syntax
ChangePlatform Platform FileName [SaveOption]

Command for converting the current design to another hardware platform Platform and saving the converted design as FileName.

To get an overview over all available hardware platforms, enter ChangePlatform ? - a list of the names of all available hardware platforms is returned. The currently selected hardware platform is displayed in the first entry of the list.

Specify the name of the desired hardware platform in parameter Platform. For specifying the target platform of the design, you can either use

  • the VisualApplets library name for the platform (e.g., "iF-CXP12-Q"), or
  • the full name of the platform (e.g., "imaFlex CXP-12 Quad").

Using capitals in the names has no effect. Specify in FileName the path to the file (using forward slashes), the file name itself, and the file name extension. If you want to overwrite an existing file, set the optional parameter SaveOption to overwrite.

CloseDesign#

Command Syntax
CloseDesign [Mode]

Command for closing the currently open design.

If you set the optional parameter Mode to Discard, the design will be closed even if it contains changes that you didn't save yet. The unsaved changes will be discarded.

If you use CloseDesign without using parameter Mode although the design contains changes that you didn't save yet, the command will be terminated and you receive an according error message.

SetDesignProperty#

Command Syntax
SetDesignProperty Key Value

Use this command to enter design properties for the currently loaded design.

There are four keys you can use:

  • ProjectName (the name you want the project to give)
  • Version (version of the design)
  • Description (description of the project).
  • TargetRuntime (specify here the operating system that will be used on the host PC(s) running this applet on the frame grabber.)

    The following values are allowed:

    • Win64
    • Win32
    • Linux64
    • Linux32

Example:

SetDesignProperty TargetRuntime Win64

SetDesignClock#

Command Syntax
SetDesignClock NewFrequency

Command for setting the basic clock frequency of the FPGA (in MHz).

Developing a Design#

CreateProcess#

Command Syntax
CreateProcess

Command for creating a new process. VisualApplets automatically numbers new processes.

DeleteProcess#

Command Syntax
DeleteProcess ProcName

Command for deleting a process of the name ProcName.

Example: DeleteProcess Process1

CreateModule#

Command Syntax
CreateModule OperatorType FullModuleName [InPortMultiplicity [OutPortMultiplicity {NamedPortMultiplicity}]]xPos yPos

Command for creating an instance (module) of an operator OperatorType, and for positioning the module in the design window.

In OperatorType, simply state the name of the specific operator you want to create an instance from. You do not must specify the library the operator belongs to.

With FullModuleName you define the module's hierarchical position within the design.

FullModuleName has the following syntax:

<HierLevelPath>/<ModuleName>

  • HierLevelPath you use to define the path to a specific hierarchical level in the design. Start on process level. Use forward slashes.
  • ModuleName you use for specifying the name you want the module to have. Alternatively, you can leave ModuleName empty. In this case, you must terminate FullModuleName with a slash; the module will be named automatically.

The position of the module in the design window you define via parameters xPos and yPos.

Example:

CreateModule CxpCamera Process0/cam 123 163

The return value of function CreateModule is FullModuleName (i.e., the full hierarchical path to the module including the module name).

Using the optional parameters InPortMultiplicity and OutPortMultiplicity:

Many operators are instantiated with a fix number of ports. On the other hand, there are operators with a variable number of ports. During instantiation of an operator with a variable number of ports, you can define how many ports the module will have.

For example, when instanciating operator BRANCH, you can define how many output ports the instance will have:

Command CreateModule: Enter Outputs

Thus, the number of output ports O is variable. Ports that have a variable number of ports we call multiports.

Multiports are identified via their base name. In BRANCH, for example, the base name of the output ports is O. Via an index that is added to the base name, a specific port can be identified and addressed:

Command CreateModule: Multiports

When using command CreateModule, you can use the optional value pair InPortMultiplicity and OutPortMultiplicity to specify the multiplicity of the vector inputs and the vector outputs of a module. This way, you can define the number of ports in instances (modules) of operators that have a variable number of ports, like, for example, operators BRANCH or ADD.

Example:

CreateModule BRANCH Process0/branchz 1 3 43 123

Command CreateModule: Example BRANCH with 3 Output Ports

Defaults: If you don't use InPortMultiplicity and OutPortMultiplicity, or if you set them to 0, the module is created with the default number of inports and outports (i.e., setting one or both of the two values to 0 does not result in zero inports or zero outports.). How many ports are created per default depends on the operator type.

Examples:

CreateModule BRANCH Process0/branch 43 123

Command CreateModule: Example BRANCH with 2 Output Ports

The default number of ports is created, 1 input and 2 output ports.

CreateModule BRANCH Process0/branch3 0 3 43 123

Command CreateModule: Example BRANCH with 3 Output Ports

1 input (default) and 3 output ports are created.

CreateModule BRANCH Process0/branch3 3 3 43 123

Command CreateModule: Example BRANCH with 3 Output Ports

1 input and 3 output ports are created. The definition of 3 input ports is ignored, as the operator type allows only 1 input.

CreateModule BRANCH Process0/branch4 0 4 43 123

Command CreateModule: Example BRANCH with 4 Output Ports

Optional parameter NamedPortMultiplicity: For operators that have various kinds of multiports (i.e., operators that have other multiports than input I or output O), you can use parameter NamedPortMultiplicity to specify the base name of the multiport you want to have on the module, and to specify the multiplicity (number) of this multiport. The format of NamedPortMultiplicity is MultiportBaseName:Number. You can use NamedPortMultiplicity multiple times in one command line. Using NamedPortMultiplicity overrules anything you may have stated in parameters InPortMultiplicity or OutPortMultiplicity.

Example:

CreateModule BRANCH Process0/branch 0 0 O:3 100 100

The example command translates as follows: Create an instance (module) of operator BRANCH. Place it in process 0 on top level and give it the name branch. Provide three output ports (multiport base name O for output) and position the module in the design window at position y=100 pixel and x= 100 pixel.

For MultiportBaseName, use the base name of the multiport as you find it on the VA GUI. The MultiportBaseName name is displayed in the dialog that appears when instantiating an operator that has a varying number of ports. The multiport base name is the short name of the multiport (displayed in parantheses in the GUI).

Command CreateModule: Enter Inputs

The multiport base name here is I.

You also find the multiport base name in the mouse over information to a port:

Command CreateModule: Multiport Mouseover

Multiport base name here is I (followed by the index identifying the individual instances of multiport I on the module).

InstUserLibOperator#

Command Syntax
InstUserLibOperator LibName OperatorName FullModuleName xPos yPos

Command for instantiating a user library element. Specify the user library via the parameter LibName, the name of the element (operator) in the library via the parameter OperatorName, the name you want to give the module in your design and where you want to place the module in the hierarchy via the parameter FullModuleName, as well as the position of the module in the design window via the parameters xPos, and YPos.

InstCustomLibOperator#

Command Syntax
InstCustomLibOperator LibName OperatorName FullModuleName xPos yPos

Command for instantiating a custom library element. Specify the user library via the parameter LibName, the name of the element (operator) in the library via the parameter OperatorName, the name you want to give the module in your design and where you want to place the module in the hierarchy via the parameter FullModuleName, as well as the position of the module in the design window via the parameters xPos, and YPos.

DeleteModule#

Command Syntax
DeleteModule FullModuleName

Command for deleting the module FullModuleName.

FullModuleName has the following syntax: <HierLevelPath>/<ModuleName>.

  • HierLevelPath you use to specify the path to the hierarchical level in the design where the module is located. Start on process level. Use forward slashes.
  • ModuleName you use to specify the name of the module you want to delete.

Simulation modules can't be deleted via this command. For deleting simulation modules, use the command DeleteSimModule.

ConnectModules#

Command Syntax
ConnectModules FromModule FromModuleOutputPort ToModule ToModulePort [x1 [y2 x3]]

Command for connecting module ports.

The parameters FromModule and ToModule are hierarchical names with the syntax: <HierLevelPath>/<ModuleName>.

Inner hierarchical box nodes (i.e. inner nodes for connecting hierarchical box ports) are identified via the prefixes INBOUND# or OUTBOUND#.

Example: The two inbound nodes of the hierarchical box in the figure below must be addressed by INBOUND#I000 and INBOUND#I001.

Command ConnectModules: Inbound Connections

Via the optional parameters x1, y2, and x3 you can define the geometry of the connecting polygon: horizontal line from FromModuleOutputPort to X position x1, vertical line to Y position y2, horizontal line to X position x3, vertical line to height of ToModulePort, horizontal line to ToModulePort.

Command ConnectModules: Geometry of the Connecting Polygon Example 1

Example:

ConnectModules Process0/CxpCamera O Process0/FrameBufferMultiRoi I 90 500 120

Command ConnectModules: Geometry of the Connecting Polygon Example 2

DisconnectModules#

Command Syntax
DisconnectModules FullModuleName ModulePort

Command for deleting the link that is connected to port ModulePort of module FullModuleName.

Example:

DisconnectModules Process0/Cam1 O

CreateComment#

Command Syntax
CreateComment FullBoxName Text xPos yPos

Command for creating a comment box.

The syntax of FullBoxName is <HierLevelPath>/<BoxName>.

  • HierLevelPath you use to define the path to a specific hierarchical level in the design. Start on process level. Use forward slashes.
  • BoxName you use for specifying the name you want the comment box to have. Alternatively, you can leave BoxName empty. In this case, you must terminate FullBoxName with a slash; the module will be named automatically.

Example:

CreateComment Process0/MyComment "This is my comment." 400 400

For the comment box content Text you can use Unicode characters. Don't forget to set the comment in quotes. If you use characters that are not part of ASCII, use the according TCL syntax to represent Unicode, for example:

[encoding convertfrom utf-8 "A-Umlaut: \xc3\x84"]

The position of the comment box in the design window you define via the parameters xPos and yPos.

The return value of function CreateComment is FullBoxName (the full hierarchical path to the comment box including the name of the comment box).

DeleteComment#

Command Syntax
DeleteComment FullBoxName

Command for deleting comment box FullBoxName.

The syntax of FullBoxName is <HierLevelPath>/<BoxName>.

  • HierLevelPath you use to specify the path to the hierarchical level in the design where the comment box is located. Start on process level. Use forward slashes.
  • BoxName you use to specify the name of the comment box you want to delete.

Example:

DeleteComment Process0/MyComment

Box name information: To get the name of the comment box you want to delete, you can use TCL to query which boxes are placed in a design, see TCL example QueryDesign.tcl in your VisualApplets installation folder at <VA installation directory>\Examples\AdvancedVAFunctions\Tcl Scripting\QueryDesign.tcl.

SetModuleParam#

Command Syntax
SetModuleParam FullModuleName ParameterName [FieldIndex] Value {OtherValues}

Command for setting a module parameter.

Info

Use this command only for setting an existent parameter to a specific value. You can't use this command for creating metadata parameters. (For creating new metadata parameters, use command SetParamString instead.)

Example:

SetModuleParam Process0/HierchBox1/module6 XLength 512

Field parameters: If you refer to a field parameter, you must specify parameter FieldIndex before specifying a Value. Only when referring to field parameters, you can specify further values after Value.

Example for editing field parameters:

Before entering the command:

Command SetModuleParam: Example for Editing Parameters

Entering the command

SetModuleParam Process0/module3 LUTcontent 4 12 13 14

has the following result:

Command SetModuleParam: Example for Entering Values

Command SetModuleParam has the same functionality as (depending on the parameter you use) the commands SetParamInt, SetParamFloat, SetParamEnum, SetParamString, SetParamIntField, and SetParamFloatField. However, these commands are for export only.

Use SetModuleParam when you are writing scripts manually.

Exception: If you want to add a new metadata parameter, you must use SetParamString when writing scripts manually. See definition of command SetParamString.

SetModuleParamProperty#

Command Syntax
SetModuleParamProperty FullModuleName ParameterName PropertyName PropertyValue {OtherPropertyValue}

Command for changing the properties of a module parameter. This command may replace SetModuleParamType. Single property names may have multiple values. You can change the following properties:

access: You can list several flags here as value:

  • write: If the parameter can be switched in this direction, (for instance in the operator LinkParamTranslator), it becomes a write-parameter.
  • read: If the parameter can be switched in this direction, (for instance in the operator LinkParamTranslator), it becomes a read-parameter.
  • dynamic: If the parameter can be either dynamic or static, it hereby becomes a dynamic parameter (this replaces the command SetParamDynamic).
  • static: If the parameter can be either dynamic or static, it hereby becomes a static parameter (this replaces the command SetParamStatic).

position: Definition of an integer value for the parameter PropertyValue, which defines the position of the parameter in a list of parameters in a hierarchical box.

SetParamInt#

Command Syntax
SetParamInt FullModuleName ParameterName Value

Used for TCL export only. Command for setting an integer parameter.

Info

This command is used in TCL export from VisualApplets to a *.tcl file.

Don't use this command in scripts you write manually. Use command SetModuleParam instead.

SetParamFloat#

Command Syntax
SetParamFloat FullModuleName ParameterName Value

Used for TCL export only. Command for setting a floating point parameter.

Info

This command is used in TCL export from VisualApplets to a *.tcl file.

Don't use this command in scripts you write manually. Use command SetModuleParam instead.

SetParamEnum#

Command Syntax
SetParamEnum FullModuleName ParameterName Value

Used for TCL export only. Command for setting an addressed enum parameter. Value is the string of the enum value.

Example (for an instance of operator SetSignalStatus that is placed on level Process0 and has the name SetSigSt):

SetParamEnum Process0/SetSigSt Mode High

Sets parameter Mode of operator SetSigSt that is located in Process0 to High.

Info

This command is used in TCL export from VisualApplets to a *.tcl file.

Don't use this command in scripts you write manually. Use command SetModuleParam instead.

SetParamString#

Command Syntax
SetParamString FullModuleName ParameterName Value

Use this command to define metadata parameters for a specific module.

In TCL export files, command SetParamString is used for setting any string parameter, even if it's an existent module parameter. However, this isn't practicable in scripts you write manually.

Info

When writing your own scripts, don't use this command for setting an existent module parameter to a new value, even if the module parameter is of type string.

For setting an existent module parameter to a new value, always use command SetModuleParam in your scripts.

SetParamIntField#

Command Syntax
SetParamIntField FullModuleName ParameterName Index Value {OtherValues}

Used for TCL export only. Command for setting a field parameter of type integer. Setting field Index to Value1, the following fields are populated with the following values in the given order.

Info

This command is used in TCL export from VisualApplets to a *.tcl file.

Don't use this command in scripts you write manually. Use command SetModuleParam instead.

SetParamFloatField#

Command Syntax
SetParamFloatField FullModuleName ParameterName Index Value {OtherValues}

Used for TCL export only. Command for setting a field parameter of type float. Setting field Index to Value1, the following fields are populated with the following values in the given order.

Info

This command is used in TCL export from VisualApplets to a *.tcl file.

Don't use this command in scripts you write manually. Use command SetModuleParam instead.

SetParamStatic#

Command Syntax
SetParamStatic FullModuleName ParameterName

Used for TCL export only. Command for making a parameter static. If a parameter can be static as well as dynamic, in most cases the parameter is set to dynamic per default. Use this command to set such a parameter to static.

Info

This command is used in TCL export from VisualApplets to a *.tcl file.

Don't use this command in scripts you write manually. Use command SetModuleParamType instead.

SetParamDynamic#

Command Syntax
SetParamDynamic FullModuleName ParameterName

Used for TCL export only. Command for making a parameter dynamic. Works only if the parameter can be dynamic at all.

Info

This command is used in TCL export from VisualApplets to a *.tcl file.

Don't use this command in scripts you write manually. Use command SetModuleParamType instead.

SetModuleParamType#

Command Syntax
SetModuleParamType FullModuleName ParameterName TypeFlag {OtherTypeFlags}

Command for changing the type of a parameter. The following type flags are available:

  • Dynamic: If the parameter can be dynamic or static, this flag makes the parameter a dynamic parameter (replaces command SetParamStatic).
  • Static: If the parameter can dynamic or static, this flag makes the parameter a static parameter (replaces command SetParamStatic).

Dynamic and Static mutually exclude each other.

When using type flags Dynamic or Static, this command has the same functionality as the commands SetParamStatic and SetParamDynamic. However, use SetModuleParamType when you are writing scripts manually.

SetLinkParam#

Command Syntax
SetLinkParam FullModuleName PortName ParameterName Value {OtherParameterName OtherParameterValue}

Command for configuring the format of links. The link is identified via the connection node (port) of a module. The names of the link format parameters are the same as in the VisualApplets GUI.

Info

When writing your TCL script manually, the command is only applicable for parameters that can be changed. If you try to set a link parameter that can't be changed, you will get an according error message:

Command SetLinkParam: Example

SetResourceMapping#

Command Syntax
SetResourceMapping FullModuleName ResourceName [Index] NewMapping

Command for changing the mapping of resources to a module. The resource ResourceName will be mapped to the new index NewMapping. In case the module allocates multiple resources of the same type, use the optional parameter Index for selecting the resource.

Command Syntax
SplitLink FullModuleName PortName [Number]

Command for creating a module BRANCH. The new branch module is inserted on the link that goes out of module FullModuleName on port NodeName. The new branch module has Number outgoing ports. If you don't use the optional parameter Number, the new branch module has two out ports.

The return value of function SplitLink is the FullModuleName of the new branch module (full hierarchical path to the module, including the module name).

Querying Design Structure and Design Details#

GetDesignProperty#

Command Syntax
GetDesignProperty PropertyName

This command retrieves design properties. You can use the following values for PropertyName:

  • ProjectName:name of the project
  • FileName: path to and name of the currently loaded design file *.va
  • HardwarePlatform: library name of target hardware platform, for example iF-CXP12-Q
  • Version: version of the design
  • Description: description of the project
  • Loaded: design is loaded (1 or 0)

Design property Loaded can be requested while no design is loaded at all. This doesn't cause an error message. Requesting any other design property while no design is loaded causes an error message.

GetDesignClock#

Command Syntax
GetDesignClock

This command returns the basic clock frequency of the FPGA (in MHz).

GetProcesses#

Command Syntax
GetProcesses

This command returns a list with the names of all processes of the design.

GetSubModules#

Command Syntax
GetSubModules HierarchyName

This command returns a list with the names of the modules that are located in the requested hierarchy HierarchyName.

For each sub-module, the full hierarchical name is listed.

GetParentHier#

Command Syntax
GetParentHier FullElementName

This command returns the hierarchical name (FullModuleName) of the parent of stated element FullElementName, that is, the FullModuleName of the hierarchical element in which element FullElementName is located.

FullElementName can be a module, a simulation module, or a comment box.

GetModules#

Command Syntax
GetModules Scope Specifier {ModuleList}

This command filters specific modules in the design. The command returns a list with modules that have the characteristic you specify via Scope and Specifier. The list contains the FullModuleName for all found modules (path to modules including the individual module name). If you don't want to search design-wide, but only in a specific set of modules, you can specify these modules in ModuleList (via their FullModuleName).

Scope can have the following values:

  • pattern: Use Specifier as a wildcard expression for FullModuleName. If you state "*" as specifier, all modules of the design are returned.
  • flat: Use Specifier as a wildcard expression for the FullModuleName of modules (like with pattern). Hierarchical boxes will not be returned.
  • ordered: Returns all modules of the design. Use Specifier to define a sorting pattern. You have the following options:
    • path: modules are sorted by their position in the design graph (i.e., in the order of the data stream as it runs through the modules during simulation).
    • name: modules are sorted alphabetically by their FullModuleName.
  • operatorType: Use Specifier to define the operator type of the modules you are looking for ("O", "M", "P", "O+P", "M+P", "unknown").
  • operator: For getting all instances of a specific operator. Use Specifier to name the operator name (for example, "NOP").
  • libraryType: Use Specifier to define a specific library type. All modules in the design that are instances of operators contained in libraries of this type are returned. The following values are allowed: operator, user, and custom (see also GetModuleProperty).
  • library: Use Specifier to define a specific library. All modules that are instances of operators of this library are returned.
  • version: Use Specifier to define a specific operator version. All modules that are instances of operators of this version are returned.

GetModulePorts#

Command Syntax
GetModulePorts FullModuleName [Scope]

This command returns a list with the names of all ports of the specified module. You can use the optional parameter Scope to filter for specific ports:

  • inputs: only the input ports are returned
  • outputs: only the output ports are returned
  • all: all ports of the module are returned (default)

GetModulePortProperty#

Command Syntax
GetModulePortProperty FullModuleName PortName Property

This command retrieves the properties of a module port. The following values for Property are available:

  • isConnected: Returns 1 if port is connected; otherwise 0.
  • position: Returns position of specified port in the diagram (design window) as a list (xPos, yPos). If PortName specifies an inner hierarchical box node (for example, INBOUND#I000), the position of this node within the hierarchical box design window is returned.

GetModuleProperty#

Command Syntax
GetModuleProperty FullModuleName Property

This command returns the properties of a module.

The following values for Property are available:

  • status: Returns 0 if module isn't in error status; otherwise returns error code.
  • operator: Returns name of operator the module is an instance of, for example BRANCH.
  • operatorType: Returns operator type (O, P, M, unknown). "Unknown" is returned for hierarchical boxes and user library modules.
  • libraryType: Returns the library type of the library the operator stems from. One of the following values is returned: operator, user, custom.
  • version: Returns the version of the operator the module is an instance of.
  • type: Returns the module type. One of the following values is returned: process, hierBox, operator, user, custom.
  • isHierModule: Returns 1 if the stated module is capable of containing submodules; returns 0 if the stated module can't have sub-modules.
  • isProtected: Returns 1 if the module is an instance of a protected library element.
  • library: Returns the name of the library the operator stems from.
  • position: Returns the position in a design window as a list (xPos, yPos).
  • resources: Returns a list of pairs (ResourceName,ResourceMapping)
  • name: Returns the module name.

GetModuleParams#

Command Syntax
GetModuleParams FullModuleName {ParameterNames}

Returns a list of module parameters and their current values.

If you want to get all parameters of the module together with the currently set values, use command GetModuleParams only with parameter FullModuleName.

Example:

Command GetModuleParams: Example

If you want to get only the values of specific parameters, you can optionally limit the output to the parameters {ParameterNames}. The order of the output corresponds to the order of the parameter names you state in {ParameterNames}.

Example:

Tcl Command GetModuleParams: Example with {ParameterNames}

puts [GetModuleParams Process0/FrameBufferMultiRoi RamDataWidth MaxFrameCount]

GetModuleParamProperty#

Command Syntax
GetModuleParamProperty FullModuleName ParameterName Property

Command for retrieving parameter properties.

For the parameter Property, the following values are available:

  • status: Returns 0, if the parameter isn't in error status; otherwise returns error code.
  • type: Returns the parameter type: int, intField, float, floatField, enum, or string.
  • access: Returns direction of access: write or read).
  • unit: Returns the unit of the parameter.
  • range: For integer and float data types, the command returns the value range as a list containing the three entries Min, Max, Step. For enum parameters, it returns a list of pairs of enum names and enum values.
  • size: Returns the size of the field. Only for IntField and FloatField parameters.
  • isDynamic: Returns 1 if the requested parameter is dynamic; otherwise returns 0.
  • isStatic: Returns 1 if the requested parameter is static; otherwise returns 0.
  • isEditable: Returns 1 if the requested parameter can be edited; otherwise returns 0.

GetLinkParams#

Command Syntax
GetLinkParams FullModuleName PortName {ParameterNames}

Returns a list of link parameter names and the currently set values for a specific link. The link is identified via the connection node (port) of a module. The returned list states value pairs <ParameterName><Value> that correspond to the pairs you would use to set link parameters via SetLinkParam.

If you want to get all parameters of the link together with the currently set values, use command GetLinkParams only with parameters FullModuleName and PortName.

If you want to get only the values of specific parameters, you can optionally limit the output to the parameters {ParameterNames}. The order of the output corresponds to the order of the parameter names you state in {ParameterNames}.

Example:

Tcl Command GetLinkParams: Example

GetLinkParamProperty#

Command Syntax
GetLinkParamProperty FullModuleName PortName ParameterName Property

This command retrieves the properties of a specific link parameter.

The following values for the parameter Property are possible:

  • status: Returns 0 if the parameter isn't in error condition; otherwise returns error code.
  • isEditable: Returns 1 if parameter value can be changed; otherwise returns 0.
  • range:
    • For integer data types, the command returns the value range either as a list containing three elements (Min, Max, Step), or as a list containing all allowed values. You distinguish the two kinds of lists as follows: The Min-Max-Step list contains 3 list elements; the third list element is smaller or equal to the second list element. A list stating all allowed values starts with the smalles value and ends with the highest value. If only one value is allowed, the value is returned in format {Value Value 1}, for example, { 4 4 1} for min=4, max=4, step=1.
    • For enum parameters, the command returns a list of pairs of enum names and enum values.

GetLinkProperty#

Command Syntax
GetLinkProperty FullModuleName PortName Property

This command returns a specific property of a specific link. If, with FullModuleName and PortName, you address the port of a hierarchical box, the command works as long as there is a link to or from this port within the hierarchical box.

The following options for the parameter Property are available:

  • status: Returns 0 if everything is fine (i.e., if the parameter settings of the link source and the link target match, and the DRC doesn't find an error); otherwise returns error code.
  • from: Returns the starting point of the link. The starting point can be either the out port of a foregoing module, or an inner hierarchical box node (INBOUND#...) the link is connected to. The command returns a list containing the two values FullModuleName and PortName.
  • to: Returns the end point of the link. The end point can be either the in port of a following module, or an inner hierarchical box node (OUTBOUND#...) the link is connected to. The command returns a list containing the two values FullModuleName and PortName.
  • source: Returns a list containing the value pairs FullModuleName and PortName for all foregoing links up to the source of the link. The link chain is followed up backwards through the hierarchies, from the module you state in FullModuleName back to the starting point. The order of the elements within the returned list corresponds to the backward-course of the lookup (the source module is the last entry in the list).
  • dest: Returns a list containing the value pairs FullModuleName and PortName for all following links up to the target module of the link. The link chain proceeds forwards through the hierarchies, from the module you state in FullModuleName up to the end (sink). The order of the elements within the returned list corresponds to the forward-course of the lookup – the target module (destination) is the last entry in the list.
  • hasConnectedSimModule: Returns 1 if a simulation module is connected to the link; returns 0 if no simulation module is connected.
  • connectedSimModule: Returns the hierarchical name of a connected simulation module.

GetSimModules#

Command Syntax
GetSimModules Type Scope Specifier

This command retrieves the FullModuleName of simulation sources (Type = source) or simulation probes (Type = probe) within a design. The command returns a list with simulation modules that have the characteristic you specify via the parameters Scope and Specifier. The list contains the FullModuleNames (hierarchical pathes to the indivudal simulation modules including the individual pathes).

Scope provides the following options:

  • hierarchy: Define a specific hierarchy in the parameter Specifier.
  • pattern: Use the parameter Specifier as a wildcard expression for FullModuleNames of simulation modules. If you state "*" as specifier, all source or probe simulation modules of the design are returned.

GetCommentBoxes#

Command Syntax
GetCommentBoxes Scope Specifier

This command retrieves comment boxes in a design. The command returns a list with all comment boxes that have the characteristic you specify via the parameters Scope and Specifier. The list contains the FullElementNames (hierarchical names including box name).

Scope provides the following options:

  • hierarchy: Define a specific hierarchy (via HierLevelPath) in Specifier.
  • pattern: Use Specifier as a wildcard expression for the FullElementName of comment boxes. If you state "*" as specifier, all comment boxes in the design are returned.

GetCommentProperty#

Command Syntax
GetCommentProperty FullBoxName Property

This command retrieves the properties of a comment box.

FullBoxName has the following syntax: <HierLevelPath>/<BoxName>.

  • HierLevelPath you use to specify the path to the hierarchical level in the design where the comment box is located. Start on process level. Use forward slashes.
  • BoxName you use to specify the individual name of the comment box.

Property has the following options:

  • content: The content of the comment box is returned.
  • position: the X and Y position of the left upper corner of the comment box in the design window are returned.

Box name information: To get the name of the comment box you want to get details about, you can use TCL to query which boxes are placed in a design, see TCL example QueryDesign.tcl in your VisualApplets installation folder (e.g.,<YourVisualAppletsInstallationDirectory>\Examples\AdvancedVAFunctions\Tcl Scripting\QueryDesign.tcl)

Editing the Design – Further Commands#

Move#

Command Syntax
Move FullModuleName [HierNodeName] PosX PosY

Command for re-positioning a module, a hierarchical box node, a comment box, or a simulation module to a new position within the design window.

Use the parameter [HierNodeName] only for selecting a hierarchical box node. Nodes within hierarchical boxes are identified via the prefix INBOUND# or OUTBOUND#(like you do when using command ConnectModules), for example, INBOUND#I000.

Select#

Command Syntax
Select FullModuleName [PortName]

Command for selecting a module, a simulation module, a comment box, or a link. Use parameter PortName only for selecting a link (the link is identified via the port that connects the link with the addressed module).

ClearSelection#

Command Syntax
ClearSelection [ParentHierarchy]

Command for deleting a selection of elements (modules, hierarchical box nodes, links, comment boxes, or simulation modules).

Use the optional parameter ParentHierarchy to deselect all elements on the hierarchical level ParentHierarchy.

If you don't use ParentHierarchy, element selection is deleted globally, and after carrying out the command no elements within the design are selected.

CopySelected#

Command Syntax
CopySelected [ParentHierarchy]

Command for copying the selected elements on hierarchical level ParentHierarchy. If you don't use the optional parameter ParentHierarchy, the selected elements on the hierarchical level of the currently active design window are copied.

DeleteSelected#

Command Syntax
DeleteSelected [ParentHierarchy]

Command for deleting the selected elements on hierarchical level ParentHierarchy. Only the selected modules of the hierarchical level you specify under ParentHierarchy are deleted, the selected modules on other levels remain. If you don't use the optional parameter ParentHierarchy, the selected elements on the hierarchial level of the currently active design window are deleted.

CutSelected#

Command Syntax
CutSelected [ParentHierarchy]

Command for cutting out the selected elements on hierarchical level ParentHierarchy. If you don't use the optional parameter ParentHierarchy, the selected elements on the hierarchial level of the currently active design window are cut out.

GetSelected#

Command Syntax
GetSelected Scope [ParentHierarchy]

Returns a list of selected elements on the hierarchical level ParentHierarchy. Via Scope you define if you want to get a list of selected modules (Modules), of selected links (Links), of selected simulation modules (SimModules), or of selected comment boxes (CommentBoxes).

If you don't use the optional parameter ParentHierarchy, the selected elements on the hierarchial level of the currently active design window are returned.

If you use Scope = Modules/SimModules/CommentBoxes, a list of FullModuleNames (hierarchical pathes to the respective modules including the module names) is returned.

If you use Scope = Links you get a list of link-identifying tuples consisting of FullModuleName and PortName (the port the link is connected to).

Paste#

Command Syntax
Paste [ParentHierarchy] [xPos yPos]

Command for pasting elements from the clipboard into the hierarchical level ParentHierarchy. (i.e., pasting elements that have been previously copied or cut out).

If you don't use the optional parameter ParentHierarchy, the elements are pasted to the hierarchial level of the currently active design window.

Use optional parameters xPos and yPos for defining the top left position of the inserted content in the design window.

InsertModulePort#

Command Syntax
InsertModulePort FullModuleName PortName [Where]

Command for inserting a new module port next to port PortName.

Info

You can only insert those ports that you can specify a multiplicity for in command CreateModule.

Where offers the following options:

  • before or above: new port is inserted directly before port PortName.
  • after or below: new port is inserted directly after port PortName (default).

If you don't use the optional parameter Where, the new port is inserted directly after port PortName.

RemoveModulePort#

Command Syntax
RemoveModulePort FullModuleName PortName

Command for deleting a module port.

Info

You can only delete those ports that you can specify a multiplicity for in command CreateModule. The minimum number of a given kind of port will always remain. If you try minimize further below the minimum, you will get an according error message. Example: While you can delete the third output port of operator Branch (port name: O002), the two minimum output ports (O001 and O000) can't be deleted:

Command RemoveModulePort

AppendModulePort#

Command Syntax
AppendModulePort FullHierBoxName Direction

Command for adding an input port or an output port to a hierarchical box.

FullHierBoxName has the same syntax as FullModuleName.

Direction=input: an input port is created.

Direction=output: an output port is created.

Rename#

Command Syntax
Rename FullModuleName NewName

Command for renaming a module or simulation box. In NewName you specify the new individual name of the instance without the hierarchical path.

Example:

Rename Process0/module1 DMA

SetActiveWindow#

Command Syntax
SetActiveWindow Hierarchy

Command for opening (and setting active) the design window of hierarchy Hierarchy in VisualApplets.

GetActiveWindow#

Command Syntax
GetActiveWindow

Returns information about the hierarchical level of the design window that is currently open and active in VisualApplets.

Simulating the Design#

CreateSimSource#

Command Syntax
CreateSimSource FullSimModuleName xPos yPos

Command for creating a simulation source module, and for positioning the module in the design window.

FullSimModuleName has the following syntax: <HierLevelPath>/<SimModuleName>

  • HierLevelPath you use to define the path to a specific hierarchical level in the design.
  • SimModuleName you use for specifying the individual name you want the simulation source module to have. Alternatively, you can leave SimModuleName empty. In this case, you must terminate FullSimModuleName with a slash; the module will be named automatically.

The return value of function CreateSimSource is the FullModuleName of the new simulation source module (full hierarchical path to the simulation source module including the module name).

CreateSimProbe#

Command Syntax
CreateSimProbe FullSimModuleName xPos yPos

Command for creating a simulation probe module, and for positioning the module in the design window.

FullSimModuleName has the following syntax: <HierLevelPath>/<SimModuleName>

  • HierLevelPath you use to define the path to a specific hierarchical level in the design.
  • SimModuleName you use for specifying the name you want the simulation probe module to have. Alternatively, you can leave SimModuleName empty. In this case, you must terminate FullSimModuleName with a slash; the module will be named automatically.

The return value of function CreateSimProbe is the FullModuleName of the new simulation probe module (full hierarchical path to the simulation probe module including the module name).

DeleteSimModule#

Command Syntax
DeleteSimModule FullSimModuleName

Command for deleting a simulation module (simulation source or simulation probe).

The syntax of FullSimModuleName is the same as the syntax of FullModuleName.

ConnectSimModule#

Command Syntax
ConnectSimModule FullSimModuleName TargetModuleName TargetModulePortName [xPos yPos]

Command for connecting a simulation module to a link. You identify the link via the module port the link is connected to.

The syntax of FullSimModuleName and TargetModuleName is the same as the syntax of FullModuleName. The syntax of TargetModulePortName is the same as the syntax of PortName.

Module TargetModuleName and simulation module FullSimModuleName must be located in the same hierarchy to connect them with each other.

Optionally, you can define the position of the connecting point on the link via xPos and yPos.

DisconnectSimModule#

Command Syntax
DisconnectSimModule FullSimModuleName

Command for detaching the simulation module from a link.

SetSimModuleProperty#

Command Syntax
SetSimModuleProperty FullSimModuleName Key Value {OtherValue}

Command for defining the properties of a simulation module.

Use Key to identify the property you want to set. Set the individual properties in the format stated below. Available are the following properties and according value formats:

pixelAlignmentOffset BITS

Use this parameter to specify the alignment offset as integer value BITS.

imageFileSubPixels NUMBER

Use this parameter to specify the number of file pixels that are assigned to a link pixel as integer value NUMBER.

Source: NUMBER pixels are conflated to one pixel.

Probe: One pixel is split up into NUMBER pixels in the file.

imageFilePixelBits BITS

Use this parameter to specify the bit width in the image file as integer value BITS. Allowed are the values 1, 8, and 16.

imageFileNormalize CHOICE

Use this property to configure the way simulation result images are saved.

If you want to save a 1-bit simulation result in an 8-bit file format, set imageFileNormalize to 1. "Normalizing" in this context means mapping 0 to 0 (black) and 1 to 255 (white).

The following values for CHOICE are possible: CHOICE = "1" | "0"

cropRect [imageNr] X Y WIDTH HEIGHT

This property is only available for simulation sources. Specifying the image index [imageNr] is mandatory. Use this parameter to crop an image and to specify the region of the image (ROI) you want to use for simulation. With X and Y you define the left upper corner of the ROI.

currentImage INDEX

Use this parameter to select an image within the simulation module. Specify INDEX as integer value.

AddImage#

Command Syntax
AddImage FullSimModuleName ImageFileName1 {OtherImageFileName} [ImageLibrary]

Command for adding an image to a simulation source module. If the number of kernel elements of the link the simulation source is connected to is > 1, you must specify as many images as the kernel has elements.

Optionally, you can state the image library you want to use ( ImageLibrary = "Native" | "ImageMagick").

RemoveImage#

Command Syntax
RemoveImage FullSimSourceName {ImageIndex}

Command for deleting one or all images from a simulation source module. Use the optional parameter ImageIndex to specify the image you want to delete. If you set ImageIndex to -1, or if you don't use ImageIndex at all, all images in the simulation module are deleted.

Simulate#

Command Syntax
Simulate ProcessingCycles [SaveLogfilename]

Command for simulating a design. Use parameter ProcessingCycles for defining how many processing cycles you want to carry out with with the command.

Use the optional parameter SaveLogfilename to save the log of the carried-out cycles to file. Specify in SaveLogfilename the path to the file and the file name itself. Use file name extension *.html, as the log is written in HTML format. Use forward slashes for indicating pathes.

Example:

Simulate 1 c:/temp/simlog.html

ResetSimulation#

Command Syntax
ResetSimulation

Command for resetting the simulation engine. As effect, all simulation probes in the design are cleared.

GetSimModuleProperty#

Command Syntax
GetSimModuleProperty FullSimModuleName Property [ImageIndex [LineIndex [LineCount] ] ]

Command for retrieving the properties of a simulation module. The following properties are available:

  • isConnected: returns 1 if simulation module is connected to a link; otherwise returns 0.
  • connectedLink: Returns a list containing the FullModuleName of a module the link is connected to, and the port of the module the link is connected to. The return value always describes the link by a real module port, i.e., it never states an inner H box node (like, for example, INBOUND#I000 or OUTBOUND#O000).
  • isSource: Returns 1 if the simulation module is a SimulationSource; otherwise returns 0.
  • isProbe: Returns 1 if the simulation module is a SimulationProbe; otherwise returns 0.
  • position: Returns position of the simulation module in the program window as a list (xPos, yPos).
  • imageCount: Returns the number of images in the simulation module (=value of IMAGECOUNT).
  • imageSize: Using parameter ImageIndex is mandatory. Returns the size of the image you specify in ImageIndex as a list {Width <WIDTH> Height <HEIGHT>}.
  • pixelAligmentOffset: Returns the alignment offset as integer value BITS.
  • imageFileSubPixels: Returns the number of file pixels that are assigned to a link pixel as integer value NUMBER.
  • imageFilePixelBits: Returns the setting for bit width in the image file as integer value BITS. Allowed are the values 1, 8, and 16.
  • imageFileNormalize: Returns 1 or 0 according to the settings for saving simulation result images. If set to 1, during saving a 1-bit simulation result to a file in 8-bit * format: 0 is mapped to 0 (black) and 1 is mapped to 255 (white), i.e., the simulation image's format is "normalized".
  • cropRect: This property is only available for simulation sources. Using parameter ImageIndex is mandatory. Returns a list with the following entries: {X Y WIDTH HEIGHT}.
  • currentImage: Returns the currently selected image as integer value INDEX.

SetSimImageData#

Command Syntax
SetSimImageData FullSimModuleName ImageIndex KernelRow KernelCol Component X Y Width Value {OtherValues}

Command for overwriting one pixel or several neighboring pixels in an image within a simulation module (source or probe).

You can use this command_

  • in SimSources for altering an image for simulation.
  • in SimProbes for visualizing the results within an image.

The alteration of the image is volatile. As soon as you select another image of the same simulation module or re-select the altered image, the altered image is loaded anew from hard disk and your alterations are discarded. (You select another image if you enter a command for a new image ImageIndex (of the same simulation module) in the TCL console, or if you click on another image of the same simulation module in the viewer of the VisualApplets GUI.)

However, you can make your alteration permanent by saving the altered image as long as it's active under a new file name.

You can use a volatilely altered image for simulation. However, only one image per SimSource module can be used for simulation in altered condition (because altering another image in the same SimSource resets the pixel values of the image you altered before). You can use as many volatilely altered images as you want for simulation as long as you have only one volatilely altered image per simulation module.

One value per Pixel: Command SetSimImageData allows you to write exactly one value per pixel. Thus, in gray scale pixels, you must carry out command SetSimImageData only once to write the complete color information per pixel. In color pixels, you will be able to write only one of the three color components per pixel. Thus, if you want to change all three color components of color pixel(s), you have to carry out command SetSimImageData three times.

Writing in images with kernels: When you are writing into images that have a kernel, you must specify (in addition to the exact position of the (first) pixel you want to overwrite) which kernel element of the respective pixel(s) you want to overwrite when using command SetSimImageData. If you want to overwrite all kernel elements, you must carry out command SetSimImageData exactly KernelRow * KernelCol times.

To use the command:

Before using the command, close the image viewer of the simulation module the image you want to change is located in.

Specify the image you want to alter with index ImageIndex.

ImageIndex starts with 0, whereas the numbering of the images in a simulation module in the VisualApplets GUI starts with 1. The values map as follows:

ImageIndex = 0 referes to image 1 in the viewer of the VisualApplets GUI.

ImageIndex = 1 referes to image 2 in the viewer of the VisualApplets GUI.

ImageIndex = 2 referes to image 3

and so forth.

Information: On the GUI of VisualApplets, the index of the image that is used in the next simulation cycle is displayed in square brackets and marked by a preceeding "sim" (e.g., sim[2]).

Use KernelRow and KernelCol to specify the kernel element you are going to change a pixel value for.

Which size the kernel of your simulation image has you can see in the link properties of the link the simulation module is connected to. A link that has a kernel size bigger than 1 pixel is always preceeded by an instance of an operator that allows specifying kernels (as, for example, operator FIRkernelNxM).

Counting kernel columns and kernel rows starts with 0. Thus, if you have a kernel with only one element, set both values (KernelRow and KernelCol) to 0:

Command SetSimImageData: Counting Kernel Columns and Kernel Rows

For a kernel with 4 elements, you identify an individual kernel element as follows:

Command SetSimImageData: Identifying a Kernel Element in 4 Elements

For a kernel with 9 elements, you identify an individual kernel element as follows:

Command SetSimImageData: Identifying a Kernel Element in 9 Elements

Use parameter Component to specify the color component of the pixel you want to set. In gray scale images, set Component to 0. In multi-component images (color), specify the component you want to write via its position in the color model. Example: Set Component to 0 if you want to address the red component in an RGB image, set Component to 1 if you want to address the green component in an RGB image, or set Component to 2 if you want to address the blue component in an RGB image.

Set position (X,Y) to define the starting point (first pixel) for your writing within the image.

Use Width to specify the number of neighboring pixels you want to overwrite per row. If you specify more Values than you write pixels in a row (Width), writing continues in the next row on position X. This way, you can write a region of interest (ROI) that has the width Width.

Specify the individual pixel values Value {OtherValues} in hexadecimal writing without preceding "0x". Specify negative values in two's complement notation. How many values you state in Value {OtherValues} decides how many pixels within the image are altered.

GetSimImageData#

Command Syntax
GetSimImageData FullSimModuleName ImageIndex KernelRow KernelCol Component X Y [Width [Height]]

Command for reading values of one or several neighboring pixels in an image within a simulation module (source or probe).

One value per Pixel: Command GetSimImageData returns exactly one value per pixel. Thus, in gray scale pixels, you must carry out command GetSimImageData only once to retreive the complete color information per pixel. In color pixels, you will be able to retrieve only one of the three color components per pixel. Thus, if you want to read all three color components of color pixel(s), you have to carry out command GetSimImageData three times.

Reading in images with kernels: When you are reading from images that have a kernel, you must specify (in addition to the exact position of the (first) pixel you want to read) which kernel element of the respective pixel(s) you want to read when using command GetSimImageData. If you want to read all kernel elements, you must carry out command GetSimImageData exactly KernelRow * KernelCol times.

To use the command:

Specify the image with index ImageIndex.

ImageIndex starts with 0, whereas the numbering of the images in a simulation module in the VisualApplets GUI starts with 1. The values map as follows:

ImageIndex = 0 referes to image 1 in the viewer of the VisualApplets GUI.

ImageIndex = 1 referes to image 2 in the viewer of the VisualApplets GUI.

ImageIndex = 2 referes to image 3 in the viewer of the VisualApplets GUI,

and so forth.

Information: On the GUI of VisualApplets, the index of the image that is used in the next simulation cycle is displayed in square brackets and marked by a preceeding "sim" (e.g., sim[2]).

Use KernelRow and KernelCol to specify the kernel element you want to read from.

Which size the kernel of your simulation image has you can see in the link properties of the link the simulation module is connected to. A link that has a kernel size bigger than 1 element is always preceeded by an instance of an operator that allows specifying kernels (as, for example, operator FIRkernelNxM).

Counting the columns and rows of a kernel starts with 0. Thus, if you have a kernel with only one element, set both values to 0.

Command GetSimImageData: Counting Kernel Columns and Kernel Rows

For a kernel with 4 elements, you identify an individual kernel element as follows:

Command GetSimImageData: Identifying a Kernel Element in 4 Elements

For a kernel with 9 elements, you identify an individual kernel element as follows:

Command GetSimImageData: Identifying a Kernel Element in 9 Elements

Use parameter Component to specify the color component you want to read of the pixel. In gray scale images, set Component to 0. In multi-component images (color), specify the component you want to read via its position in the color model. Example: Set Component to 0 if you want to read the red component in an RGB image, set Component to 1 if you want to read the green component in an RGB image, or set Component to 2 if you want to read the blue component in an RGB image.

Set position (X,Y) to define the starting point (first pixel) of your reading within the image.

If you don't use parameter Width, the value for exactly one pixel is returned. If you specify only Width, Width values in line Y are returned. If you specify Width and Height, Width * Height values are returned. Using Width and Height allows you to define a region of interest (ROI) you want to read the pixel values (gray)/the values of a pixel component (color) for.

The individual pixel values are returned in hexadecimal writing without preceding "0x". Negative values are returned in two's complement notation.

GetSimImageProperty#

Command Syntax
GetSimImageProperty FullSimModuleName Property ImageIndex [LineIndex [LineCount] ]

Command for retrieving the properties of a simulation image (in a source or a probe module).

The following value for Property is available:

LineWidth: Define via LineIndex for which line you want to get information about its width. If you use LineCount, you can get a number of width values (in form of a list). The first value will be the width of line LineIndex.

SaveImage#

Command Syntax
SaveImage FullSimProbeName {ImageIndex} ImageBaseName

Command for saving one or all result images from a simulation probe.

Use the optional parameter ImageIndex if you want to save a specific image out of the result images. Don't use ImageIndex or set it to -1 if you want to save all images of the probe.

Use ImageBaseName to specify the path to the directory in your file system where you want to save the image(s), and for specifying the file name of the image file(s). Make sure the directories you specify already exist in your file system. Otherwise, you can create them using command MakeDirectoryPath (see there).

Example: "c:/images/testimage". In the saving process, the file name extension (for example, *.tif) will be automatically added to the name.

If you save all images of the probe, an image index will be automatically added to the file name.

Example 1:

Enter

SaveImage Process0/mySimProbe c:/images/testimage

to get the following files:

c:/images/testimage_0001.tif

c:/images/testimage_0002.tif

c:/images/testimage_0003.tif

…

Example 2:

Enter

SaveImage Process0/mySimProbe 4 c:/images/testimage

to get the following file:

c:/images/testimage.tif

Building the Design#

Drc#

Command Syntax
Drc [SaveLogfileName]

Command for starting the first level of the Design Rule Check (DRC 1).

To get a log output, you can optionally specify the path to and the name of an html log file (*.html) in parameter [SaveLogfileName].

Drc2#

Command Syntax
Drc2 Name Platform

Command for starting the second level of the Design Rule Check (DRC 2).

To get a log output, you can optionally specify the path to and the name of an html log file (*.html) in parameter [SaveLogfileName].

SelectBuildConfiguration#

Command Syntax
SelectBuildConfiguration ConfigurationName

Command for selecting a saved build configuration as active build configuration.

Specify the name of the desired build configuration in parameter ConfigurationName.

To get an overview over all available build configurations, enter SelectBuildConfiguration ? - a list of the names of all available build configurations is returned. The currently selected build configuration is displayed in the first entry of the list.

Example:

Command SelectBuildConfiguration

The command returns the name of the currently selected build configuration. Via this return value you can check if your re-setting the build configuration was successful.

Example:

Command SelectBuildConfiguration Output

Build#

Command Syntax
Build [SaveLogfilename [MaxTime] ]

Command for starting the build flow.

To get a log output, you can optionally specify the path to and the name of an html log file (*.html) in parameter [SaveLogfileName].

To set a time limit for the build process, you can optionally specify the the maximum build time in parameter [MaxTime] (in hours). Parameter [MaxTime] is of type floating point. This way, you can specify fractions of an hour. The default setting for [MaxTime] is 24 hours.

Example for a command creating log file build_log.html and specifying the maximum Build time as ½ hour:

Build build_log.html 0.5

Handling Files, Paths, Program Instances and Messages#

Source#

Command Syntax
Source FilePath

Command for executing a TCL script out of a file. Use forward slashes for specifying the path. The command works like the TCL command source, but automatically replaces the following place holders (like command MakeDirectoryPath):

%UserDir%: User data directory for the current user (for example, c:/Users/Smith)

%AppDataDir%: Directory for application data of VisualApplets

%VaInstallDir%: Installation directory of VisualApplets

%UserLibDir%: Directory for user libraries.

%CustomLibDir%: Directory for custom libraries.

%VaVersion%: VisualApplets program version, for example, "3.1"

%CurrDateTime%: Current date and time according to ISO 8601 (basic format), for example "20170530T134522"

%DateTime%: Date and time at start of VisualApplets according to ISO 8601 (basic format), for example "20170530T134350"

%CurrDesignDir%: Directory in which the currently loaded design is stored.

MakeDirectoryPath#

Command Syntax
MakeDirectoryPath FullPath

Command for creating pathes (and their directories) of any desired depth.

The command automatically replaces the following place holders:

%UserDir%: User data directory for the current user (for example, c:/Users/Smith)

%AppDataDir%: Directory for application data of VisualApplets

%VaInstallDir%: Installation directory of VisualApplets

%UserLibDir%: Directory for user libraries.

%CustomLibDir%: Directory for custom libraries.

%VaVersion%: VisualApplets program version, for example, "3.1"

%CurrDateTime%: Current date and time according to ISO 8601 (basic format), for example "20170530T134522"

%DateTime%: Date and time at start of VisualApplets according to ISO 8601 (basic format), for example "20170530T134350"

%CurrDesignDir%: Directory in which the currently loaded design is stored.

If the command has been carried out successfully, the absolute path is returned.

GetAbsolutePath#

Command Syntax
GetAbsolutePath Path

Returns the absolute path of the path you specify in parameter Path.

The command automatically replaces the same alias names (place holders) as command MakeDirectoryPath.

You are allowed to refer in Path to a directory or a file that doesn't exist, so that the resulting path name refers to a directory or a file that doesn't exist.

Wait#

Command Syntax
Wait TimeInMilliseconds

Command for waiting the specified time TimeInMilliseconds. The VisualApplets GUI stays active during waiting time.

If you set TimeInMilliseconds to 0, at least one event loop update of the GUI is carried out by VisualApplets. You can use this for making sure that the GUI displayes the results from earlier commands.

Message#

Command Syntax
Message Type Code Text

Command for emitting

  • an error message (Type=error),
  • a warning (Type=warning), or
  • an informative message (Type=info)

In Code, define the message code for your message. Code has the value range from -999 to +999. Use only values in this range to avoid conflicts with the current and/or future versions of VisualAppets.

Use Text to enter the message. The message is completed by a dot automatically.

Exit#

Command Syntax
Exit [Mode]

Command for terminating the current VisualApplets session. You can use Exit even if you still have a design open. However, don't forget to save your changes before.

If you still have a desing open and the design contains unsaved changes:

  • If you set the optional parameter Mode to Discard, the open design will be closed even if it containes changes that you didn't save yet. The unsaved changes will be discarded.
  • If you use Exit without using parameter Mode although the open design containes unsaved changes, the command will be terminated and you receive an according error message.