Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Controller Types and Light Control Modes#

Depending on your application, a Basler Light can be operated either by the internal controller integrated into the light or by an external light controller.

The selected controller type determines the available light control modes:

Choosing the right mode depends on how you want to control the light and how much functionality your application requires. See Internal Controller and Available Light Control Types.

Legacy Lights and New Basler Lights#

Info

Legacy Basler Lights and new Basler Lights:

  • Earlier generations of Basler Lights were lights without ILC (without intelligent light control). These lights required a separate controller for light control.
    Documentation for legacy Basler lights without ILC is no longer included in the current Basler Product Documentation. If you need information about these products, refer to the offline documentation of an earlier release, that you can download by clicking here.
  • To determine which type of light is installed, check the revision number marked on the Basler Light (e.g., 2200000841-05). The last two digits following the order number indicate the light's revision. Revision 05 and later identify Basler Lights with Intelligent Light Control (ILC), i.e., with an integrated controller. Revision numbers below 05 identify legacy Basler Lights without ILC and therefore without an integrated controller.

Changes to the Pin Assignment#

Info

The pin assignment has changed from legacy Basler Lights without intelligent light control (ILC) to current Basler Lights with ILC.

When You Need to Adapt the Wiring

  • If a legacy Basler Light is replaced with a new Basler Light with ILC (Intelligent Light Control) and an external controller is used (Basler SLP Controller or a third-party controller), the pin assignment must be adjusted accordingly. This is necessary because the pin assignment of Basler Lights with ILC differs from that of legacy Basler Lights.
    If the legacy pin assignment is used, the new light will not turn on.
  • Verify that you are using the correct pin assignment when connecting the light.

For information about the pin assignment for different uses cases, refer to the topics Operating Basler Lights with Internal Controller or Operating Basler Lights with External Controller.

Internal Controller and Available Light Control Types#

If you use the controller integrated into a Basler Light, no external light controller is required. Depending on your application, you can operate the light in one of the following light control modes:

Trigger Control Mode#

Use the trigger control mode when you want a simple and direct lighting setup.
In this mode, the light is controlled through a dedicated trigger input, the peripheral control protocol isn't used. The light follows the state of the trigger signal:

  • Trigger HIGH (> 2.8 V on the signal pin/pin 3): Light ON
  • Trigger LOW (< 1.4 V on the signal pin/pin 3): Light OFF

The trigger signal can be provided by a camera output (for example, Exposure Active or User Output) or by another external trigger source. Because the light reacts directly to the electrical trigger signal with no further communication, a fine pulse resolution and high strobe frequencys can be achieved. <!–_SK: Beide Modes (ILC und Trigger) reagieren nahezu gleich schnell, die Auflösung des ILC-Strobes beträgt aber 10µs und die FPS ist auf ~200Hz begrenzt >

Key Charcteristics

  • No external controller required
  • No compatible camera required
  • Direct hardware-based triggering
  • Very short trigger pulses possible
  • No status feedback from the light
  • No built-in synchronization between multiple lights
  • No advanced light management features

Typical Use Case

Applications where a camera or PLC directly triggers the illumination and a simple, deterministic setup is required.

Requirements

For further information, e.g., pin assignment and circuit diagram examples, see the Trigger Control Mode section in the Operating Basler Lights with Internal Controller topic.

Intelligent Light Control Mode#

Use the intelligent light control mode (ILC) when you want the camera to control and configure the lighting system. In this mode, a compatible camera communicates with the light through the SLP (Standard Light Protocol). The light is configured and controlled through the camera's GenICam interface. In the intelligent light control mode, pin 3 serves as a dedicated communication line. SLP commands are transmitted over the same line, allowing communication between the connected devices without requiring an additional signal connection.

Unlike the trigger control mode, the camera actively manages the light and can access advanced lighting features.

Key Charcteristics

  • No external controller required
  • Compatible camera required
  • Camera-controlled operation through GenICam
  • Independent control of up to four lights
  • Status feedback and device monitoring
  • Heartbeat supervision
  • Built-in overdrive functionality
  • Software-configurable pulse generation

Typical Use Case

Integrated vision systems where lighting should be configured, monitored, and controlled directly from the camera.

Requirements

For further information, e.g., pin assignment and circuit diagram examples, see the Intelligent Light Control Mode section in the Operating Basler Lights with Internal Controller topic.

External Controller and Available Light Control Type#

Use an external controller when integrating a Basler Light with intelligent light control (ILC) into an existing system that relies on a light controller without SLP functionality. In this case, the light can only be operated in External Control Mode.

External Control Mode#

In this mode, the light is connected to a dedicated external controller without SLP functionality. The controller determines all operating parameters, including timing, current levels, protection mechanisms, and optional overdrive functions. The capabilities of the system depend entirely on the selected controller.

Key Characteristics

  • External controller required
  • Timing and current regulation handled externally
  • Controller-specific features and performance
    The available features for External Control Mode (e.g., built‑in overdrive or time resolution) depend entirely on the controller you choose.
  • Suitable for demanding strobe applications
  • User must ensure compliance with the electrical limits of the light.

Typical Use Case

High-performance machine vision applications requiring specialized strobe control, custom timing, or advanced illumination management.

Requirements

The External Control Mode section in the Operating Basler Lights with External Controller topic provides a sample circuit diagram and connection information for using an external LED controller with a Basler Light in external control mode.

Choosing the Right Light Control Mode#

If you want to Recommended Light Control Mode
Directly switch the light with a hardware trigger signal Trigger Control Mode
Configure and control the light from a compatible camera Intelligent Light Control Mode
Use a separate external LED controller External Control Mode

Pin Assignment Changes in Light Revision 05#

Info

For information about pin assignment changes introduced with Basler Light Revision 05, see the Basler Lights topic.

Further Information#

Installation (Basler Lights).