clsersis#
clsersis.dll is this library for Basler frame grabbers. CLAllSerial loads clsersis.dll from the directory in CLSERIALPATH. For more information about how the serial connection is made, see the GenTL Interface documentation.
clsersis.dll provides the serial connection. BaslerClProtocol.dll is the CLProtocol library, and it is a different file from clsersis.dll.
ProducerCL doesn't use clsersis.dll. If pylon and a GenTL consumer use the same frame grabber, see Installing pylon and the Framegrabber SDK in Parallel.
To use the library, the include file clser.h should be added to the source code.
#include <clser.h>
Additionally, clsersis.lib should be added to your Microsoft Visual Studio Project, or libclsersis.so to your Linux project. If you use CMake, the package name is ClSerSis, the libraries are stored in the variable ${clsersis_LIBRARIES} and the include directory is stored in the variable ${clsersis_INCLUDE_DIR}. See Prerequisites for more details on projects and how to use CMake.
For further information about the API, see the Camera Link standard.
Refer to the Camera Link Specifications document for further information about how to use Camera Link Serial. In addition, the documentation of your camera contains details about how to implement the vendor specific protocol to access camera features.